High-Quality Small Batch Guitar Effect Pedal PCBs with JLCPCB Manufacturing
3 min
- Design challenge
- Support for JLCPCB
- Conclusion
Fuzz Fields is an innovative guitar effect pedal that combines three modulated sounds to offer dynamically controlled fuzzy sound effects. Unlike traditional static pedals, Fuzz Fields can adjust the timbre in real time based on the dynamic input of the performer, achieving various effects such as "screaming", "swelling", "saturation" and "trembling". Its core feature is an inbuilt oscillator that can be modulated through external control, making it suitable for scenarios such as guitar tone exploration, synthesizer music, and live performances.
Fuzz Fields with JLCPCB high-quality 4-layer PCB placed inside
Design challenge
In order to achieve the audio effect function with the maximum quality within the limited space, the design of Fuzz Fields faces the following challenges:
1.Compact PCB design: All electronic components need to be integrated within a limited space to ensure that the size of the circuit board fits the standard effect pedal housing.
2.High-density assembly: Due to its complex functions, multiple components need to be arranged on the PCB, requiring high-density soldering and precise component positioning.
3.Multi-layer circuit board: To achieve complex circuit functions, a four-layer PCB design is adopted to ensure signal integrity and power supply stability.
The core PCB polished smoothly with the electronic components neatly arranged
Support for JLCPCB
In the Fuzz Fields project, JLCPCB provided comprehensive PCB manufacturing and assembly services. The specific support includes:
1. Rapid PCB manufacturing and efficient assembly services: JLCPCB offers ultra-fast PCB manufacturing and efficient PCBA assembly services, with 48-hour ultra-fast delivery. On average, it reaches consumers 2 to 4 days faster than local overseas suppliers, shortening the project cycle and ensuring on-time project delivery.
2. High-quality PCB delivery: Fuzz Fields' complex circuit designs require high-quality 4-layer PCBS to stably achieve functionality. To ensure quality, JLCPCB's products undergo multiple tests before shipment, including AOI, flying probe testing, and pre-shipment inspection. At present, it has been trusted by over six million engineers from more than 180 countries around the world and has obtained multiple international certifications such as ISO, UL, and RoHS.
3. Low cost and high efficiency: The low-cost manufacturing solution provided by JLCPCB helps the project team complete high-quality production within the budget, ensuring the economic viability of the project. Low-board PCBS (1 to 4 layers) are widely praised for their ultra-low prices starting from 2 US dollars.
4. Reliable supply chain support: JLCPCB 's electronic component inventory comprises over 600,000 SKUs provides a stable supply of components and has efficient production scheduling, ensuring the smooth progress of the project.
No irregular lines or welding defects even with a close-up shot
Conclusion
JLCPCB provided all-round support for the success of the Fuzz Fields project. As a globally leading PCB manufacturer, JLCPCB is always committed to providing reliable solutions for innovative projects and helping to develop high-performance and scalable technological breakthroughs. Whether it is complex multi-layer circuit design or high-density component assembly, JLCPCB can provide professional technical support and high-quality manufacturing services.
Popular Articles
• PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
• ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
• From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
• Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
• Premium Portable Speaker Built with 8-Layer PCBs, DSP & Smart Amps
Keep Learning
PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
Key Takeaways The piBrick Pocket-CM5 is a fully functional, smartphone-sized Raspberry Pi CM5 handheld PC with a physical QWERTY keyboard, AMOLED display, and M.2 NVMe SSD The project utilizes JLCPCB's 4-layer PCB fabrication with controlled impedance (90-ohm for USB, 100-ohm for PCIe/MIPI DSI) to maintain signal integrity Designed using EasyEDA and fabricated by JLCPCB, the project was submitted to the EasyEDA Spark program, successfully securing parts and materials sponsorship for its development. J......
From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
Note Motivation: Replaced a dust-prone membrane keyboard with a durable, custom DIY alternative. Specs: 87-key TKL layout powered by Raspberry Pi Pico (RP2040), featuring hot-swap support, QMK, OLED, and an encoder. Design: A unique 3-layer PCB stack featuring symmetrical routing, an exposed controller, and visible "diode art". Support: Designed using EasyEDA and fabricated by JLCPcB, the project was submitted to the EasyEDA Spark program successfully securing parts and materials sponsorship for its d......
Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
In the world of FPGA development, having a reliable, low-cost JTAG programmer used to mean either buying expensive vendor cables or adding high-cost FTDI chips to every board. Maker Khaled Magdy changed that by turning a $4 Raspberry Pi Pico into a fully functional JTAG adapter using DirtyJTAG firmware and OpenFPGALoader — then had his custom FPGA boards professionally assembled by JLCPCB. The entire solution is 100% open-source. You can download the firmware, follow the Windows installation steps, an......
ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
Key Takeaways Accessible Design: ANGELO is an open-source €10 listening aid created to assist everyday voice amplification. Analog Audio Architecture: Uses a TL072 op-amp to boost speech frequencies (1–4 kHz) with low latency and low power. EasyEDA & JLCPCB Workflow: Designed in EasyEDA and produced via JLCPCB SMT assembly for fast, reliable hardware execution. The ANGELO Project Overview ANGELO is an open-source audio hardware project designed to amplify voices and improve everyday communication expe......
Athena: Building a High-Performance 6-Layer PCB for Rocket Avionics
Key Takeaways Athena is an open-source flight computer with a triple-MCU architecture, redundant sensors, and multiple communication interfaces on a compact 6-layer PCB. The 80 × 140 mm board integrates three STM32 MCUs, three IMUs, barometers, GNSS, LoRa, Bluetooth, CAN, USB, flash storage, SD card, and power management. The 6-layer PCB provides routing capacity, organized power distribution, signal organization, and compact functional integration for this complex design. The project demonstrates how......
Designing a Precision 72-LED Wearable Watch: Building a 40mm Round PCB with JLCPCB SMT Assembly
Key Takeaways This case study explores the design and fabrication of a 72-LED wearable watch built on a precision 40mm round PCB. Learn how JLCPCB SMT assembly eliminated hand-soldering 70+ 0603 LEDs, how ENIG surface finish ensures reliability in wearable applications, and how a clever panelization strategy with mouse-bite breakaway tabs enabled automated assembly of a circular board. The project demonstrates a complete workflow from EasyEDA schematic capture to firmware optimization and commercial-g......