Quality Control and Testing in Bare Board Manufacturing
5 min
Bare printed circuit boards, or PCBs, are the foundation of almost all electronic devices made today, from computers and cellphones to industrial control systems and aeronautical electronics. Quality control and testing in bare board manufacturing have grown more important since these applications require more dependability. Defects at the PCB level might cause even the most sophisticated circuit designs to fail in the absence of adequate quality assurance. In order to guarantee long-term performance and dependability, this article examines the essential quality control procedures and testing techniques utilized in bare board production.
What is a Bare Board?
An unpopulated PCB, often referred to as a bare board. So what exactly does it exactly contain? What type of PCB is it? These are the normal questions that came into mind. It has copper traces, vias, pads, and dielectric layers. They are the things required to support and link electronic components. So we can say at all, It is a printed circuit board that has no soldered components on it but a fully fabricated PCB. Every electronic assembly is built on bare boards. Any flaws that are introduced during their manufacturing might result in mechanical weaknesses, electrical failures or functional faults in the finished product.
Why Quality Control Matters in Bare Board Manufacturing
Applying a solder mask, and surface finishing are all part of the PCB manufacturing process. Every PCB goes through the complex procedures including laminating, drilling, plating, imaging and etching. And these are basically very common yet precise steps followed in fabrication of PCBs. Every stage raises the possibility of flaws like openings, shorts or surface irregularities. So inspections should be performed so that bare boards guarantee all the design specifications. Industry standards (such as IPC-6012 for rigid PCBs) and customer expectations through quality control.
6 Main Quality Control Processes in Bare Board:
1) Incoming Material Inspection
Finding premium raw materials is the first step in ensuring the quality of incoming material inspection. Solder masks, prepregs, copper-clad laminates, and surface finish chemicals must all adhere to certain material specifications and certifications (such as UL and RoHS compliance). Visual inspection, copper weight, bare board damage, and supplier certificates are among the inspections that will be carried out under this heading.
2) In-Process Inspection
Every step of PCB manufacture is monitored for quality via in-process inspections. By ensuring early defect discovery, these intermediate inspections lower scrap rates and rework expenses. Here, we'll examine drill pad layouts, solder mask coverage, and etching issues.
3) Electrical Testing (Continuity and Isolation Tests)
Each bare board is electrically tested after production to ensure that the circuit designs are intact. This testing guarantees that there are no unexpected connections (isolation) and that all connections are accurate (continuity). This is an open/short circuit test.
We have two tests under electrical testing: the bed of nail test and the flying probe test. The flying probe test, which is best suited for prototypes and small quantities, tests nets using moving probes instead of a physical fixture. For testing big production runs, we have a fixture in the bed of nails with spring-loaded pins.
4) Automated Optical Inspection (AOI)
To find flaws in the PCB's tiny characteristics, such trace width, pad widths, missing features, or shorts between closely spaced traces, AOI systems employ cameras and image processing. AOI is usually carried out following the solder mask, etching, and imaging phases. It is employed to identify copper-related problems such as solder mask misregistration, surface contamination, trace breakage, and missing copper.
5) Microsection (Cross-Section) Analysis
To assess internal quality, a cross-sectional slice of the PCB is sliced, embedded in resin and examined under a microscope. This technique is used to identify voids or delamination. Microsection analysis is used for critical applications or multilayer PCBs. It can also be used to examine the thickness of copper plating in vias and through-holes.
6) Surface Finish Quality Inspection
Bare boards can be finished with:
● ENIG (Electroless Nickel Immersion Gold)
● HASL (Hot Air Solder Leveling)
● OSP (Organic Solderability Preservative)
Which depends on the application. Before assembly the quality control makes sure that these finishes are free of contamination and oxidation.
Common Defects Detected During Testing
Industry Standards for PCB Quality
IPC-600 (Acceptability of Printed Boards) and IPC-6012 (Qualification and Performance Specification for Rigid PCBs) are often followed by bare board manufacturers. These guidelines provide acceptability requirements for flaws and craftsmanship, which are divided into:
● Class 1: General electronic products (consumer goods)
● Class 2: Dedicated service electronic products (industrial equipment)
● Class 3: High-reliability electronics (medical, aerospace and telecommunications)
Further reading: PCBA Testing Guide: Methods, Processes, and Quality Standards
Conclusion
Strict quality control procedures are necessary to ensure that the finished product satisfies the necessary standards. PCB engineering hardware is a complicated process. To ensure that the boards are free of flaws and fulfill the required performance standards. Quality control techniques such automated optical inspection, X-ray inspection and visual inspection. Improved dependability and fewer errors are just a few advantages of effective quality control in PCB manufacturing services. PCB makers must place a high priority on quality control. At JLCPCB, we implement rigorous testing protocols to ensure every bare board we produce is dependable and ready for assembly. Improved reliability, lower failure rates, and consistent quality make strong quality control not just important—but essential.
Keep Learning
PCB Testing Methods: A Comprehensive Guide to Testing and Characterizing PCBs
Key Takeaways PCB testing helps identify manufacturing defects, verify electrical connections, and ensure product quality. Different testing methods serve different purposes: AOI and X-ray detect visual and hidden defects, while Flying Probe and ICT identify electrical issues. Functional and reliability testing help evaluate circuit performance under specific operating conditions. Combining appropriate inspection and testing methods improves quality control across PCB fabrication and PCBA assembly. JL......
How PCB Thermal Cycling Tests Reveal Manufacturing Reliability
Key Takeaways Exposes Hidden Faults: Thermal expansion opens tiny cracks, catching via failures that room tests miss. Expansion Mismatch Stress: Heat differences weaken vias and solder joints over time. Standardized Testing: Follows IPC and JESD rules, failing when resistance increases. Process Prevention: High Tg materials, thick copper, and filled vias boost board life. Destructive Test: Consumes board life, so tested samples must be scrapped. A PCB thermal cycling test can detect faults that a room......
Why PCB Inspection Microscopes Matter in Electronics Manufacturing
Key Takeaways Precise Faults: ICT tests individual components to report exact pin-level failures. Layout-Driven: Coverage relies on test pad size, pitch, and component clearance. Speed vs. Tooling: Bed-of-nails tests in seconds; flying probe requires no custom fixture. Guarded Isolation: Isolates components from parallel paths to catch early defects. Layered QA: Pairs with AOI and AXI for full quality coverage. A PCB inspection microscope earns its place on a production line because the costliest defe......
How Sustainable Materials and Expert Manufacturing Ensure RoHS Compliant PCBs
Have you ever experienced that a finished shipment of products was detained at the EU customs due to a single component on the board not passing the RoHS screening? It is higher than most engineers think, and the financial blow is far bigger than the impounded goods. Wasted time, remodeling expenses, and a compliance audit that is capable of halting your whole product introduction, that is the actual cost of doing RoHS wrong. The point is as follows: RoHS-compliant PCBs cease to be a checkbox exercise......
Ensuring Superior Solderability: The Critical Role of Testing in Reliable PCB Production
Key Takeaways Core Purpose: Verifies solder wetting before assembly to prevent yield drops and joint failures. Destructive Test: Per J-STD-002, tested components and coupons cannot be reused in production. Pass Standards: Requires 95 percent solder coverage on leads and 80 percent on exposed thermal pads. Key Defects: Catches non-wetting (exposed metal), dewetting (solder pulling back), and black pad on ENIG. DFM Prevention: Use thermal relief, keep silkscreen off pads, and select the right surface fi......
Solder Joint Inspection in PCB Manufacturing : A Complete Guide to Catching Defects Early
Key Takeaways Solder Joint Inspection is critical in modern PCB manufacturing to catch defects early and ensure product reliability. By combining Solder Paste Inspection (SPI), 3D AOI for visible joints, and X-ray for hidden BGA/QFN issues, manufacturers can effectively detect common defects such as bridging, cold joints, tombstoning, and head-in-pillow. Following IPC-A-610 standards with a layered inspection strategy significantly reduces field failures while improving first-pass yield. JLCPCB’s prof......