PCB Design Tips: How to Prevent Breakage of Traces during Board Bending
1 min
- PCB Design Tips:
- How to avoid breaking the board when the thin and narrow connection is broken?
PCB Design Tips:
How to avoid breaking the board when the thin and narrow connection is broken?
In actual production, sometimes there are narrow and long connections, some of which may be wired. After the PCB is processed by V-cutting, the customer's force is uneven when dividing the board, and the force on the narrow place is weak. It is easy to break when breaking the board (at A in the figure below). At this time, we can change the way of jigsaw puzzles, and open a gap of 1.6-2MM between the boards, so that these narrow and long connection positions can be made out of the edge (as shown in B in the figure below), so that there is no need to break them. Open this place to avoid breaking the board.
Special attention: If the depaneling method is adopted, the width of the narrow and long connection position needs to be more than 1MM, and the length should be within 30MM. If the length exceeds this length, the connection position needs to be appropriately widened!
Keep Learning
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......
The Role of PCB Test Fixtures in High-Volume Manufacturing
In high-volume manufacturing of Printed Circuit Boards (PCBs), quality, efficiency, and reliability are paramount. One of the most crucial tools in achieving these goals is the PCB test fixture. These fixtures play a vital role in ensuring that PCBs meet the required performance standards before they are integrated into electronic devices. This article delves into the importance of PCB test fixtures, their types, and how they contribute to the efficiency of high-volume manufacturing. Specialized and c......