PCB temperature: Tips regarding improving the thermal management of PCBs
7 min
Thermal management is of utmost importance while designing PCBs. This is because the temperature of PCBs can guarantee the reliability, performance, and longevity of PCBs and the electronic equipment of which they are an integral component. Thus, enhanced Printed Circuit Board heat management is a necessity for reliable operation and to protect against damage to electronic components.
In the upcoming chapter, we will discuss several approaches to strengthen PCB temperature management.
Reasons of heat generation
There are various reasons why heat is produced on a printed circuit board (PCB). For example, power dissipation, joule heating, inefficient power conversion, high-frequency operation, and insufficient thermal management. The functionality, dependability, and durability of electronic components on a PCB can all be adversely impacted by excessive temperatures. To effectively control temperature and guarantee the PCB operates at its optimum level, proper thermal design is also mandatory.
Tips for enhancing thermal management in Printed Circuit Board
· Tips 1: Component Placement
One strategy for significantly reducing heat concentration is to arrange components on the PCB with a proper design and location. To be specific, the heat-generating components should be positioned near fans or heat sinks, or other cooling gadgets, and in regions with adequate ventilation. Moreover, we should also make sure that parts with various heat requirements are not positioned too near to one another. To be specific, it is not possible to put components that have a high power or thermal burden next to one another. They have to be separated by at least 20 mm. It can prevent excessive local heat load on the PCB in this way. And placing the components too close will not only cause thermal burden, but may also cause interfere problems. This can lead to noise, signal integrity and other issues. Furthermore, we may arrange high-power parts in a group and make sure there's enough space between them to allow for sufficient heat dissipation.
In other words, elevated temperatures have the potential to hasten ageing, deteriorate functionality, and possibly cause untimely failures. Longevity and dependable operation of components are ensured by maintaining them within their safe operating temperature range through effective thermal management.
· Tips 2: Heat Sink Selection - Passive cooling method
A heat sink is a passive thermal management device that employs thermal conduction to absorb and dissipate heat produced by electronic elements on PCBs. Heat sinks are typically made from a thermally conductive material, such as aluminum or copper, and have fins or other extended surfaces. These fins significantly increase the surface area available for heat transfer. Therefore, designers can increase the effective cooling surface area by attaching a heat sink to the component, which can transfer heat to the surrounding air more efficiently.
Also, by expanding the surface area of the heat sink, convection cooling is encouraged. The surrounding air comes into contact with the fins or expanded surface as heat is transmitted to the heat sink. This promotes improved convection, which aids airflow and heat dissipation. In other words, heat is removed by the flowing air, which lowers the radiators and their connected components' temperature. Moreover, we can choose to use a high-quality thermal interface material such as thermal paste or thermal pad between the component and the heat sink. It is because the TIM fills microscopic air gaps and enhances thermal conductivity, which improves heat transmission between components and heat sinks. In addition, to satisfy particular cooling needs, we could occasionally need a heat sink that is specially constructed. To develop and optimize heat sinks for particular applications, we can collaborate with thermal engineers or heat sink manufacturers.
· Tips 3: PCB Material Selection
First of all, it is possible to use materials with high thermal conductivity, which efficiently moves heat away from high-power components. Since copper has such good heat conductivity, it is employed extensively in this situation. Also, copper or aluminum core metal core printed circuit boards (MCPCBs) can improve thermal performance. We can also choose materials with a similar coefficient of thermal expansion to the component, thus minimizing thermal stress and preventing mechanical failure due to temperature changes. Because when the coefficients do not match, there may be a risk of solder joint failure or component damage. Moreover, while designing PCBs, designers could opt for materials with lower dielectric constants to minimize heat retention. This is because of the fact that materials with a lower dielectric constant facilitate greater heat dispersion and lessen the possibility of hot spots forming.
In Addition, we may also experiment with employing several layers, such as copper planes or power planes, in our PCB design. This is because the heat is dispersed across the PCB by these flat surfaces, which function as effective heat pipes. Furthermore, we can take the material's heat resistance into account while choosing materials. As it gauges how well a substance dissipates heat. In this case, we could go with materials that allow for more effective heat transfer and dissipation by having lower thermal resistance. Also, it is worth noting that if using a heat sink, consider the PCB material and heat sink connection method. Like thermal adhesive or mechanical mounting compatibility. To guarantee a secure and reliable radiator connection, some materials might need to be prepared specifically or have adhesives that work with them.
Overall, when it comes to thermal management, material selection should be consistent with the specific requirements and constraints of the PCB application. Therefore, balancing thermal performance, electrical performance, cost considerations, and other design requirements is incredibly important.
· Tips 4: Keep Traces Short
It's imperative to remember that short traces can aid in temperature control. Why can maintaining a short transmission distance enable the thermal management of PCBs? This is because keeping the transmission distance short reduces resistance, reduces voltage drop, speeds up signal propagation, improves signal integrity, and reduces thermal coupling. To be specific, take reduced resistance as an example, as shorter traces have lower resistance, which reduces power dissipation due to resistive losses. When current flows through a trace, it encounters resistance, which converts some of the electrical energy into heat. So when you keep traces short, you can minimize resistive losses and reduce the amount of heat generated, thereby achieving thermal management. At the same time, if we use longer traces we may be more susceptible to signal distortion, such as signal reflections and crosstalk. These signal integrity issues can lead to increased switching noise and signal degradation. So these issues can be alleviated by keeping traces short, resulting in clearer signals, lower noise, and lower power consumption.
· Tips 5 Copper Pour and Traces
One of the most effective ways to manage PCB thermal management is by increasing the copper and trace width in areas where components generate a lot of heat. The wider copper traces and pours have less resistance. Because the resistance of a trace is directly proportional to its length and inversely proportional to its cross-sectional area. So by increasing the width of a trace, you lower its resistance and minimize resistive losses. This reduces power consumption and subsequently, the heat generated.
Conclusion
In conclusion, by using component placement, heat sink selection, PCB material selection, maintaining traces short, and widening traces, we can control and manage the temperature while designing PCBs. Of course, it is not limited to these above methods, we can also enhance the thermal management of PCBs by placing Vias near heat-generating components, using thermal Vias to connect the thermal pad of a component to inner or outer copper layers, etc... However, thermal management is a complex and multifaceted challenge because PCB design is complex and demanding. Therefore, different technologies and strategies must be implemented according to different situations. In summary, when implementing thermal management techniques, we must consider the thermal characteristics of the component, the operating environment, and the overall system design.
Keep Learning
Common Design Issues and Recommendations for PCB Optimized Design
To help customers avoid common issues that may arise during the PCB production process due to design problems, we' ve summarized the most frequent cases below. These issues have been detailed on our website to assist customers in identifying and addressing them more effectively. The following points include important design considerations and suggested modifications: 1. Missing Slots, Cutouts, Millings and V-Cut Issue: Missing Slots, Cutouts, Millings and V-Cut due to improper design. Recommendation: ......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Thermal Vias in PCB Design for Heat Management
Thermal vias are specialized vias designed to transfer heat from one layer of a PCB to another. These vias are placed near heat-generating components to create a thermal pathway, helping to dissipate heat and reduce the risk of overheating. They are often used with heat sinks, thermal pads, or copper planes to enhance their effectiveness. They are simply plated through holes (PTHs) that are located under a surface-mounted heat source component in a printed circuit board (PCB) that allow heat transfer.......
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......