Addressing Panelization Issues with Irregular Shapes and Structures
2 min
- Case One:
- Case Two:
In production, JLCPCB has frequently had to process panel designs which have insufficient consideration for V-cutting. Simply tiling multiple boards together is suitable for uniformly sized and regularly shaped rectangular boards. However, for irregularly shaped boards with varying sizes, such a naive panel design is not feasible. Instead, it requires a consideration of the capabilities and requirements of the machines involved in production. Below, we will provide specific analyses using real-world examples to illustrate the shortcomings of these improper panel designs:
Case One:
In the example below, although fill-in have been added to surround the irregularly shaped board, there is no mechanical support at locations such as the upper left and lower left corners. Milling these areas leaves them suspended from one end, and when they pass through the V-cut machine, they deform. As a result, during the forming process, the uneven force distribution leads to a non-straight V-cut, causing scrap.
The correct panelization method, as shown below, eliminates this issue:
This image follows the same principle: the support points have a small load-bearing area, thus although the shape is different, as before, it is not suitable for V-cut.
Case Two:
In the image below, you might not immediately spot the issue, but this panelization is problematic. The details can be combined with the findings from Case One to identify the problem.
The correct panelization eventually involves adding tabs on the left and right sides to provide horizontal tension for the leftmost edge.
Let's take a look at another type of panelization, where the lack of horizontal balance leads to V-cut misalignment.
The image below represents the correct panelization, with the addition of extra process borders for support.
This image depicts the correct panelization approach, where V-cutting is avoided on the left and right sides, and instead, a routing (CNC) method is used for shaping.
Keep Learning
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
Why Tolerance Analysis Is Key to Reliable and Cost-Effective PCB Production
Key Takeaways Tolerance analysis bridges CAD perfection and manufacturing variations to ensure reliable PCB assembly. Focus on critical areas: annular rings, hole tolerances, trace/space, layer registration, and solder mask alignment. Apply Worst-Case, RSS, or Monte Carlo methods for effective tolerance stack-up. Proper analysis boosts yield, cuts respins and costs — start with JLCPCB’s DFM review. Have you ever sent a board to fabrication, which appeared flawless on the computer screen, but then foun......
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
Copper Balancing in PCBs: Achieving Optimal Performance and High Yields with JLCPCB
Key Takeaways Copper balancing strategically distributes copper across PCB layers to create uniform density, preventing warpage, uneven plating, inconsistent etching, and signal integrity issues. The ideal copper density target sits within the 40%–60% golden ratio, with mirrored layers maintaining density variation within 15%–20% per IPC-6012 standards. Copper thieving (dot patterns or crosshatch meshes) equalizes current density during electroplating without introducing parasitic capacitance on spars......
PCB Design : How to Resolve Short Circuit Defects Caused by HASL
Key Takeaways In high-density PCB designs, HASL frequently causes solder bridging and short circuits due to its uneven surface and molten solder flow, especially on fine-pitch and dense traces. The most effective solution is to switch to ENIG (Electroless Nickel Immersion Gold), which provides superior planarity, significantly reduces bridging risks, and improves assembly yield. By selecting ENIG for dense layouts, optimizing solder mask design, and running DFM checks, designers can effectively elimin......