Common Design Issues and Recommendations for PCB Optimized Design
7 min
- 1. Missing Slots, Cutouts, Millings and V-Cut
- 2. Gold Finger Chamfering Issues
- 3. Mirrored Single Sided PCB Designs
- 4. Gerber Viewer Accuracy
- 5. Mismatch Between Gerber Files and Hole Attributes
- 6. Incorrect Barcode or Serial Number Placement
- 7. Via Covering Issues
- 8. Short Circuit Detection
- 9. NPTH Not Properly Designed
- 10. Discrepancies Between Gerber Files and Order Options
- 11. Important Ordering Notes
- 12. Overlapping Drills and Slots
- 13. Breaks in Process Edges or Connection Points
- 14. Layer Naming Standards
- 15. Stencil Opening Mismatch
- Important Reminders:
To help customers avoid common issues that may arise during the PCB production process due to design problems, we' ve summarized the most frequent cases below. These issues have been detailed on our website to assist customers in identifying and addressing them more effectively. The following points include important design considerations and suggested modifications:
1. Missing Slots, Cutouts, Millings and V-Cut
Issue: Missing Slots, Cutouts, Millings and V-Cut due to improper design.
Recommendation: Ensure Slots, Cutouts, Millings and V-Cut are designed on the same outline layer. If there are multiple outline layers, prioritize the mechanical layer with the smallest number.
For more details, refer to our [ordering instructions]
Note: The mechanical layer should take precedence over the keepout layer.
2. Gold Finger Chamfering Issues
Issue: Gold fingers do not have the required chamfered edges.
Recommendation: Ensure that the gold fingers are designed at the board edge and that there is adequate clearance from traces to prevent damage during chamfering. The chamfering principle is illustrated below.
For further details, refer to Instructions for Chamfering Gold Fingers .
3. Mirrored Single Sided PCB Designs
Issue: Mirror image processing on single sided boards.
Recommendation: For single layer of Aluminum and Copper Core boards, ensure that the copper, solder mask, and silkscreen are all correctly designed on the top layer. In production, to avoid burrs and spikes, mirrored designs may be used, but this won' t affect the final design structure. Please note that our FR4 single sided boards are limited to one copper layer, one solder mask layer, and two silkscreen layers (depending on the customer's design).
4. Gerber Viewer Accuracy
Issue: Discrepancies between Gerber Viewer and the actual production file.
Recommendation: The Gerber Viewer is for reference only and may not guarantee accurate representation. It is crucial to choose the "confirm production file" option before submitting your order. For details on confirming production files, please refer to How to confirm the production file.
5. Mismatch Between Gerber Files and Hole Attributes
Issue: Holes not matching Gerber file attributes, such as plated versus nonplated.
Recommendation: Ensure that hole attributes are consistent with the Gerber file to avoid issues during production.
Please refer to the example below. The holes is designed as plated in Gerber file, but the properties are defined as non-plated.
6. Incorrect Barcode or Serial Number Placement
Issue: QR codes and serial numbers placed randomly or incorrectly on the board.
Recommendation: QR codes should be designed in the silkscreen layer as solid blocks (5x5, 8x8, or 10x10 mm). If both QR codes and serial numbers are selected, only the QR code needs to be designed, and the serial number will automatically be placed beneath it. Ensure the design aligns with order options to prevent discrepancies. For detailed instructions, see How to mark on PCB .
7. Via Covering Issues
Issue: Failure to cover vias in certain conditions.
Recommendation: Vias will be not plugged if they have single or double-sided pad openings; ≤0.35mmdistance from pads cannot be plugged. For more information on via covering, refer to this article.
8. Short Circuit Detection
Issue: Short circuits due to improper DRC (Design Rule Check) settings.
Recommendation: Use DRC during design to automatically detect potential design errors when designing. However, be aware that different design rules may have varying results.
9. NPTH Not Properly Designed
Issue: NPTH not properly isolated from copper traces, causing short circuits.
Recommendation: Leave at least 2mm clearance between npth and copper traces to prevent short circuits. Review this incorrect design example for reference.
10. Discrepancies Between Gerber Files and Order Options
Issue: Tented vias produced despite selecting untented options (or vice versa).
Recommendation: Ensure that order options align with the Gerber files to avoid mismatches during production. In case of any conflict between the options and the files, we will follow the Gerber files you provided.
11. Important Ordering Notes
- If you do not want the order number printed on your PCB, select the "remove mark" option.
- When choosing "panel by customer," please upload the panelized file instead of the single board file.
- Special stencil thickness requests can be noted in the remark section.
- Aluminum PCB is single sided only.
- Ensure that the layers in your Gerber files match the selected options.
- Castellated holes: If your design includes castellated holes, please select this option in the order. If not selected, we assume you accept the potential risks, such as copper traces being incomplete. Additionally, the minimum size for castellated holes is 10*10mm.
12. Overlapping Drills and Slots
Issue: Overlapping drills and slots can cause production issues.
Recommendation: Ensure that drills do not overlap with slots or use the remark section to specify which layer should take precedence. If there is any overlap in the outline layer, we will prioritize the smaller dimension for processing; If both of them are in the drill layer, we will use the bigger one; While if one of them is in the outline layer, the other is in the drill layer, we will make the size according to the one in the outline layer, and make the attribute according to the one in the drill layer.
13. Breaks in Process Edges or Connection Points
Issue: Process edges or connection points breaking during production due to insufficient mechanical strength.
Recommendation: Increase the width of the process edges or add more connection points. For SMT assembly, we recommend a process edge of 5 mm, 2 mm tooling holes, and 1 mm fiducials placed 3.85 mm from the panel edge.
For more information, refer to Specifications for Adding Process Edges and Positioning Holes.
14. Layer Naming Standards
Issue: Inconsistent or incorrect layer names leading to misinterpretation during manufacturing.
Recommendation: Follow standardized naming patterns for layers to improve recognition accuracy.
A guide to suggested naming patterns is available.
15. Stencil Opening Mismatch
Issue: The stencil openings do not match the pads for soldering.
Recommendation: Stencils are created based on the solder paste layer and not the solder mask or other layers. Double check your design to ensure proper alignment.
Important Reminders:
1. Testing: Always test your PCB before soldering components to prevent further damage.
2. Order Confirmation: Please carefully check your Gerber file and confirm the production files before proceeding your order.
3. Return Process: Save your boards and packages until the customer service issue is resolved.
4. Logistics Claims: If your PCB arrives damaged due to shipping, initiate a claim and provide photos of the packages and damaged boards.
5. Please note that we only accept complaints based on the original order. Therefore, we strongly recommend inspecting the first batch of PCBs upon arrival to ensure there are no issues before placing a re-order. This will ensure a safer and smoother process.
6. IPC 2 Class Standard: Our production quality follows the IPC 2 Class standard, and products within this standard are acceptable. Complaints based on this standard will not be accepted.
7. Design Validation: We do not verify design errors in Gerber files. Please ensure thorough checks before submitting.
8. Updates: Customer feedback may result in updates to our website. Please stay tuned for any changes.
By following these guidelines and reviewing the provided resources, you can significantly reduce the occurrence of production issues and ensure a smoother PCB manufacturing process.

Keep Learning
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......