Comparison of BGA vs LGA in High-Power Applications
9 min
- Understanding BGA and LGA Packages:
- Thermal Considerations for BGA Packages:
- Thermal Considerations for LGA Packages:
- Industry Applications and Case Studies:
- Case Studies:
- FAQ about Comparison of BGA vs LGA
- Conclusion:
Key Takeaways
In high-power PCB designs, BGA and LGA packages offer strong high I/O performance but require effective thermal management. BGA excels with solder balls and thermal vias, while LGA relies on direct pad contact with TIMs and thermal pads. Key to success are thermal vias, thicker copper layers, ground planes, and simulations to reduce thermal resistance and maintain reliable junction temperatures.
As electronic devices continue to shrink in size while increasing in performance, managing heat dissipation has become a critical consideration in PCB design. Two popular package styles used in high-power applications are ball grid array (BGA) and land grid array (LGA). While both BGA and LGA offer unique advantages, they possess distinct structural features that result in different thermal characteristics. This article will provide an overview of BGA and LGA packages, explore the thermal challenges at high power levels, and discuss design considerations and solutions for effective thermal management.
Understanding BGA and LGA Packages:
A ball grid array (BGA) package utilizes a grid of solder balls underneath the IC chip to connect with the PCB. The balls provide an electrical connection, while also facilitating heat transfer from the die to the board through the solder balls. BGAs are widely used for their high I/O density, electrical performance, and ability to scale to large die sizes.

In contrast, a land grid array (LGA) utilizes metal pads rather than solder balls to make contact with the PCB. An LGA requires an interposer or retention mechanism to ensure adequate contact pressure between the IC pads and PCB lands. While LGAs do not solder to the board, they facilitate heat transfer through the pad contacts. LGAs offer advantages such as reworkability and reduced stresses compared to BGAs.
For high-power applications, both packages support complex ICs with high I/O counts. However, the heat fluxes generated—often exceeding 100-500 W in demanding scenarios—require optimized PCB layouts to prevent thermal throttling and ensure long-term reliability.
Thermal Considerations for BGA Packages:
For BGA packages, the solder balls provide the main conduit for heat transfer from the die to the PCB. To maximize the BGA’s thermal performance, the PCB must be designed to effectively spread heat laterally and transfer it to the board edge or to a heat sink.

One technique is to place thermal vias underneath the BGA pads on the PCB. The thermal vias provide a direct thermal conduction path to inner board layers or bottom ground planes. This minimizes the heat spreading distance to extract heat from the package. High thermally conductive materials, such as copper paste or conductive epoxy, should be used to fill vias where possible, as air-filled or standard plated vias have significantly higher thermal resistance.
Increasing the number of thermal vias reduces the package’s junction-to-board thermal resistance. For example, a dense array of 0.3 mm diameter vias on a 1 mm pitch can reduce thermal resistance by 40-70% depending on board stackup and copper thickness, though exact gains require simulation. However, too many vias can compromise solder joint reliability due to reduced solder volume and potential CTE mismatch stresses. Tradeoffs must be evaluated to optimize heat transfer while minimizing mechanical stresses on solder balls. Designers often use via-in-pad techniques for fine-pitch BGAs (0.5 mm or below) to maintain routing density without sacrificing thermal paths.
Larger copper pads on the PCB will also improve heat spreading from BGA solder balls.Thicker copper layers (1 oz or 2 oz) enhance in-plane thermal conductivity.Thermal simulations help predict temperature gradients and identify hot spots underneath BGAs. Copper heat sinks or thermal slugs embedded in the PCB can further augment heat dissipation. In practice, combining thermal vias with dedicated ground planes and external heatsinks or liquid cooling interfaces is common in high-power designs exceeding 100 W.
Thermal Considerations for LGA Packages:
LGAs rely on conduction through the interface between the package pads and PCB lands to transfer heat. As such, the thermal interface is critical for minimizing thermal resistance. LGAs intended for high-power use will incorporate thermal pads rather than electrical pads on some array locations to maximize heat transfer.
The application of thermal interface materials (TIMs) between LGA pads and lands is essential to fill surface voids and improve heat conduction. Typically, a thermally conductive paste or film TIM is applied to the LGA or PCB lands before assembly. The TIM should exhibit high thermal conductivity (e.g., 5-15 W/m·K or higher) and be sufficiently compliant to accommodate surface roughness, flatness tolerances, and minor warpage under pressure.
Thermal vias in the PCB underneath LGA thermal pads further enhance heat extraction. Similar to BGA designs, dense via arrays connected to thick copper planes provide vertical heat paths, while larger thermal pad areas improve contact efficiency. As with BGAs, thermal simulations of the LGA and PCB assembly are important when evaluating thermal performance. Factors such as LGA land dimensions, via quantity, TIM thickness, and contact pressure must be modeled to achieve the required heat dissipation. Proper clamping force from the retention mechanism is also vital to maintain consistent low thermal resistance over time and temperature cycles.
Table: Key Thermal Design Comparison Between BGA and LGA
| Aspect | BGA | LGA | Common Best Practice |
|---|---|---|---|
| Primary Heat Path | Solder balls + thermal vias | Direct pad contact + TIM | Dense thermal vias + copper planes |
| Thermal Resistance Impact | Good with via arrays (40-70% reduction possible) | Excellent with optimized TIM & pressure | Thermal simulation mandatory |
| Rework / Reliability | Solder joints more stress-prone | Higher reworkability, lower stress | Evaluate CTE and via density |
| High Power Suitability | Strong for soldered high I/O | Strong for large thermal pads | Combine with 1-2 oz copper & heatsinks |
Industry Applications and Case Studies:
BGA and LGA packages find extensive applications across various industries, including telecommunications, automotive, aerospace, and consumer electronics. Let's explore some notable industry applications and case studies:

Telecommunications:
BGA and LGA packages are widely used in high-performance networking equipment, such as routers, switches, and base stations. These applications demand efficient thermal management due to the high-power components involved. By implementing optimized thermal design strategies, manufacturers have achieved reliable operation and extended product lifespans.
Automotive:
In the automotive industry, BGA and LGA packages are employed in electronic control units (ECUs), sensors, and infotainment systems. The stringent temperature requirements and harsh operating conditions in vehicles necessitate robust thermal management solutions. Through careful PCB design and thermal simulations, automotive electronics have been able to maintain optimal performance under extreme temperature environments.
Aerospace:
BGA and LGA packages are utilized in avionics systems, satellite communication equipment, and flight control systems. Aerospace applications demand exceptional reliability and thermal performance due to the critical nature of these systems. By incorporating advanced cooling techniques, such as heat pipes and liquid cooling, engineers have successfully managed heat dissipation and ensured thesafe operation of aerospace electronics.
Consumer Electronics:
BGA and LGA packages are prevalent in consumer electronic devices, including smartphones, tablets, gaming consoles, and high-end audio equipment. These devices often require compact form factors while delivering high computing power, making thermal management crucial. Through innovative thermal solutions such as vapor chambers, heat spreaders, and advanced cooling techniques, manufacturers have enhanced device performance and prevented overheating issues.
Case Studies:
In 5G base station radios, BGAs efficiently dissipate heat from high-power mmWave beamforming ICs. Thermal vias, copper pads, and heat sinks maintain junction temperatures safely below 125°C despite 200W+ heat fluxes, enabling continuous high-throughput operation.
LGA processors in high-performance computing clusters use large thermal pads to conduct heat to liquid cold plates. The direct contact cooling maintains 45°C chip temperatures under 500W.
In radar and electronic warfare systems, stacked BGA memory devices with thermal vias handle 300W per module. The vias connect to thick center ground layers in multilayer boards to spread heat.
FAQ about Comparison of BGA vs LGA
Q: What is the main difference between BGA and LGA packages?
BGA packages use an array of solder balls for electrical and thermal connection to the PCB, while LGA packages use flat metal pads that require a retention mechanism for contact pressure. BGA offers easier soldering but higher mechanical stress, whereas LGA provides better reworkability and lower stress on the board.
Q: Which package is better for high-power applications — BGA or LGA?
Both are suitable for high-power use, but the choice depends on specific needs. BGA excels in high I/O density and soldering reliability, while LGA is often preferred when large dedicated thermal pads and easier rework are required. Effective thermal management (vias, TIMs, copper planes) is more critical than the package type itself.
Q: How do thermal vias improve heat dissipation in BGA packages?
Thermal vias placed underneath BGA pads create direct vertical heat conduction paths from the solder balls to inner copper layers or ground planes. A dense array of vias can significantly reduce junction-to-board thermal resistance (θjb), often by 40-70%, helping maintain safe operating temperatures in high-power designs.
Q: Why are Thermal Interface Materials (TIMs) important for LGA packages?
TIMs fill microscopic air gaps between LGA pads and PCB lands, dramatically reducing thermal resistance at the critical interface. Using high-conductivity TIMs (5–15 W/m·K or higher) combined with proper contact pressure ensures efficient heat transfer, especially when paired with thermal pads and vias.
Q: Should I use thermal simulations when designing with BGA or LGA packages?
Yes. Thermal simulations are highly recommended to predict temperature gradients, identify hotspots, and optimize via placement, copper thickness, and stackup before manufacturing. They help balance thermal performance with mechanical reliability and prevent costly design iterations.
Q: What PCB design techniques best support high-power BGA and LGA applications?
Key techniques include using dense thermal vias (possibly via-in-pad), thicker copper layers (1oz or 2oz), dedicated ground/power planes for heat spreading, larger thermal pads, and Metal Core PCBs for extreme heat dissipation. Proper via filling and strategic heatsink integration further enhance performance.
Conclusion:
In conclusion, both BGA and LGA packages offer unique advantages and challenges in terms of thermal characteristics. By understanding the specific thermal considerations for each package style and implementing appropriate design solutions, you can effectively manage heat dissipation and enhance the performance and longevity of high-power electronic systems.
When it comes to manufacturing electronic systems, JLCPCB is your reputable and reliable provider of PCB fabrication and assembly services. Click the botton below to empower your next electronic project!
Keep Learning
QFN Package: Structure, PCB Design, and Assembly
Key Takeaways Choose the correct PCB footprint: Follow the QFN manufacturer’s recommended land pattern and package datasheet. Optimize thermal management: Use appropriate thermal pads and thermal vias to improve heat transfer. Control solder paste application: Design stencil apertures to achieve suitable solder volume and reduce assembly defects. Inspect hidden solder joints: Use X-ray inspection when required by the product’s reliability needs and inspection plan. Design for manufacturability (DFM): ......
Navigating Automotive PCB Manufacturing Standards and High-Reliability Fabrication
Key Takeaways Harsh Operating Environments: Engineered to survive 15 years under thermal cycling (-40 °C to 150 °C) and severe vibration. Strict Compliance: Guided by IATF 16949, AEC-Q200 components, and IPC Class 3 standards. Targeted Materials: Leverages high-Tg/heavy copper for power and Rogers substrates for 77 GHz radar. Zero-Defect Inspection: Employs 3D AOI and X-ray testing to eliminate hidden solder joints failures. An automotive PCB has to keep working for fifteen years in the same place. Bo......
Battery PCB Board: What You Need to Know
Key Takeaways Battery PCB boards support power distribution, protection, monitoring, and cell balancing. PCB types include single-layer, multilayer, flexible, and HDI designs. Current capacity, thermal management, and routing density are key design considerations. Reliable manufacturing depends on proper materials, fabrication, assembly, and testing. Battery PCB boards are used in a wide range of battery-powered electronics, from smartphones and laptops to electric vehicles and energy storage systems.......
Medical PCB Manufacturing: Key Standards, Types, and High-Reliability Fabrication
Key Takeaways Strict Compliance: Demands ISO 13485 QMS certification, IPC Class 3 specs (25 µm copper barrels), and IEC 60601-1 safety rules. Targeted Substrates: High-Tg FR-4 handles autoclave heat, polyimide flex serves wearables, and metal/ceramic cores manage high power. Quality & Traceability: Layered AOI, X-ray inspection, and full IPC-1782 lot tracking prevent critical field failures. A medical PCB carries a level of responsibility that consumer electronics rarely face, because a patient’s diag......
A Complete Guide to Package Substrates: Materials, Structure, Types, and PCB Differences
Key Takeaways Definition: A package substrate is the fine-pitch organic carrier connecting a bare die to the system board. Not a PCB: Substrates are routed several times finer than advanced HDI and use entirely different dielectrics. Materials: BT resin cores carry wire-bond and CSP work, while glass-free ABF build-up film carries flip chip. Process: Semi-additive plating, not etching, is what makes single-digit micrometer lines possible. Constraint: Substrate capacity, not wafer supply, now limits hi......
Comprehensive Guide to QFN Packages: Advantages, Types, and Applications in Electronics
Key Takeaways Thermal Vias: Place 0.3mm vias in the exposed pad to draw heat away from the IC. Voiding Control: Apply a window-pane stencil (50–75% coverage) to prevent solder voids. Prevent Wicking: Use tented vias or Via-in-Pad to stop solder from leaking. Hidden Joints: Require X-ray inspection (AXI) since QFN leads are under the package. JLCPCB SMT: Fully supports 0.4mm pitch QFNs, Via-in-Pad, and AXI quality checks. Quad flat no-lead (QFN) packages are a type of IC package that are small, lightwe......