How to Create Your Own PCB Trace Width Calculator with Python
6 min
- Parameters to Consider
- Features of the Python Trace Width Calculator
- How to Run the Trace Calculator in an Online Python Compiler
- Python Code:
- Final Thoughts:
PCB traces are critical for current carrying, signal integrity, and thermal performance in any design. While IPC-2152 provides the standard formulas, manual calculations are time-consuming. In this tutorial, we’ll create a lightweight Python trace width calculator based on IPC-2152. You can run it in any online compiler and cross-verify results with JLCPCB’s free online impedance calculator for real-world manufacturing accuracy.
Let's start with an example: if I am designing a power PCB and my trace is 10mm long and consists of a current of 5 A, then what will be the thickness? So we have to calculate by going into IPC, but in the era of computers, hand calculations are not done! Oh yes, you can use any online calculator, but why rely on them? We will design our independent code.
Coming back to the main question - How wide should my copper trace be? The answer depends on several factors, like the current it must carry, the acceptable temperature rise, the copper thickness, and whether the trace is on an internal or external layer. To streamline this process, I developed a Trace Width Calculator in Python based on IPC-2152 guidelines. In this post, I’ll walk you through the design process, the parameters considered, and the features of the tool. And finally, how you can run it in any online Python compiler.
Parameters to Consider
When designing the calculator, the following key parameters (based on IPC-2152 and JLCPCB capabilities) were included:
1. Current Capacity (A) – The amount of current the trace must safely carry.
2. Temperature Rise (°C) – How much the trace temperature is allowed to increase above ambient.
3. Layer Type – External traces dissipate heat better than internal traces, so their formulas differ.
4. Copper Weight (oz/ft²) – Commonly 1 oz or 2 oz copper; affects thickness and resistance.
5. Trace Length (mm) – Important for calculating resistance and voltage drop.
6. Trace Width (mm) – Used when calculating maximum current from a given size.
JLCPCB minimum trace width/spacing is 0.10 mm (4 mil) for standard 1 oz copper.
Features of the Python Trace Width Calculator
The code is very lightweight, hence it does not have any UI. So it can be run online using any Python compiler. Here’s what my calculator can do:
Two Modes:
1) Width from Current – Enter current, get the required trace width.
2) Current from Width – Enter width, get the maximum supported current.
Additional Calculations:
- Trace resistance (Ω)
- Voltage drop (V) for a given load
- Power loss in the trace (W)
After calculation, always cross-check results with JLCPCB’s free online impedance calculator and select “Controlled Impedance” during quoting for ±10% tolerance verification.
How to Run the Trace Calculator in an Online Python Compiler
You don't need a local Python setup to use this tool. Just copy the code below given code and here is how to run the guide:
1. Visit any online Python compiler and paste the code into it. I am using Programiz just for example, you can choose any local one.
2. Click Run.
3. Follow the prompts in the terminal window to input your parameters.
First, it will ask the user to select between the two given modes: Width from Current or Current from Width. The respective output and prompts are given below:
Width from Current:
Current from Width:
This makes it possible to run the calculator from any device, even without installing Python.
Python Code:
import math
def calculate_trace_width(current, temp_rise=10, is_external=True):
# IPC-2152 constants
if is_external:
k = 0.048
b = 0.44
c = 0.725
else:
k = 0.024
b = 0.44
c = 0.725
width_mils = (current / (k * (temp_rise ** b))) ** (1 / c)
width_mm = width_mils * 0.0254
return width_mm
def calculate_trace_properties(width_mm, length_mm, copper_oz):
# Constants
copper_thickness_mm = {1: 0.035, 2: 0.07} # in mm
resistivity = 1.68e-8 # Ohm-meter for copper
# Get thickness
thickness_mm = copper_thickness_mm.get(copper_oz, 0.035)
cross_section_mm2 = width_mm * thickness_mm
# Convert to meters
length_m = length_mm / 1000
area_m2 = cross_section_mm2 * 1e-6
# Resistance
resistance = resistivity * length_m / area_m2
return resistance
# --- Main Program ---
mode = input("Choose mode (1 = Width from Current, 2 = Current from Width): ")
if mode == '1':
current = float(input("Enter current (A): "))
temp_rise = float(input("Enter temperature rise (°C, default 10): ") or 10)
layer = input("Is it external layer? (y/n): ").lower() == 'y'
length_mm = float(input("Enter trace length (mm): "))
copper_oz = int(input("Copper weight (1 or 2 oz): "))
width_mm = calculate_trace_width(current, temp_rise, layer)
resistance = calculate_trace_properties(width_mm, length_mm, copper_oz)
voltage_drop = current * resistance
power_loss = current ** 2 * resistance
print(f"\n--- Results ---")
print(f"Required trace width: {width_mm:.3f} mm")
print(f"Trace resistance: {resistance:.4f} Ω")
print(f"Voltage drop: {voltage_drop:.4f} V")
print(f"Power loss: {power_loss*1000:.2f} mW")
elif mode == '2':
width_mm = float(input("Enter trace width (mm): "))
temp_rise = float(input("Enter temperature rise (°C, default 10): ") or 10)
layer = input("Is it external layer? (y/n): ").lower() == 'y'
length_mm = float(input("Enter trace length (mm): "))
copper_oz = int(input("Copper weight (1 or 2 oz): "))
width_mils = width_mm / 0.0254
if layer:
k = 0.048
else:
k = 0.024
b = 0.44
c = 0.725
current = k * (temp_rise ** b) * (width_mils ** c)
resistance = calculate_trace_properties(width_mm, length_mm, copper_oz)
voltage_drop = current * resistance
power_loss = current ** 2 * resistance
print(f"\n--- Results ---")
print(f"Maximum supported current: {current:.2f} A")
print(f"Trace resistance: {resistance:.4f} Ω")
print(f"Voltage drop: {voltage_drop:.4f} V")
print(f"Power loss: {power_loss*1000:.2f} mW")
else:
print("Invalid option.")Final Thoughts:
This is a simple yet powerful Python project based on IPC-2152. To make it work, a designer needs to have proper parameter information and needs to go through the IPC guidelines for the trace calculator. The results may differ from the online calculators because some of them are running a previous version of the code.
For real manufacturing on JLCPCB:
- Use the calculator for quick prototyping.
- Verify final values with JLCPCB’s free impedance calculator.
- Select “Controlled Impedance” when ordering for ±10% tolerance (or ±5% optional) and TDR testing.
You can easily extend the code with a GUI using Tkinter or Streamlit. Feel free to share your version and tag JLCPCB — we love seeing community tools!
Popular Articles
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
• AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
• GPT-6 Astra PCB Design in KiCad: From Brief to Verified Native Project
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• How to Design Your Own Keyboard PCB: From Layout to Firmware
Keep Learning
AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
AI tools can now assist with PCB architecture, schematic generation, component selection, placement, routing, and design verification. However, different tools target different stages of the PCB workflow. This guide compares AI tools for PCB design based on what they actually do, what inputs they require, and where they fit within a real engineering workflow. In this guide, you will learn: The 6 types of AI PCB tools and the input each one needs What AI PCB design tools do, compared stage by stage How......
Free Online Circuit Simulator for Electronics Engineers
Key Takeaways Simulate First: Free circuit simulators prevent fried components and cut PCB re-spins. Fix AC Sweep: Enter pure numbers for points per decade, not time units. Use SMD Parts: Swap ideal models for standard SMD resistors and SOT-23 transistors. Control Parasitics: Board trace capacitance and via inductance alter high-frequency signals. Verify Before Order: Pair SPICE simulation with DFM checks to ensure board success. If all electronic engineers had a dollar for each burnt-out resistor or ......
Mastering PCB Design Rules: A Comprehensive Guide for Optimal Results
Key Takeaways Follow core PCB design rules for reliable electrical and mechanical performance. Optimize trace width, spacing, impedance, and vias for signal integrity and manufacturability. Apply DFM and DRC early to identify potential manufacturing and layout issues. Consider thermal management, grounding, and testing during the PCB design stage. Align design rules with your PCB manufacturer’s capabilities to improve production reliability and reduce redesigns. PCB design rules are essential guidelin......
KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
Key Takeaways Claude can design PCBs in KiCad: By connecting Claude to KiCad through an MCP server, you can use AI to create and modify PCB designs. In this project, Claude helped turn a 5 A XL4015 buck converter netlist into a two-layer, 63 × 33 mm PCB layout with zero ERC violations and zero DRC errors after minor initial fixes. Set up Claude securely: Use a KiCad MCP server that starts in read-only mode. Review the server code before installing it, connect through stdio, and allow editing only in a......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
How to Design a PCB with Flux.ai (Step-by-Step Guide)
Key Takeaways This step-by-step Flux PCB design tutorial demonstrates the complete workflow by creating a compact 15 × 15 mm USB 2.0 hub, refining the layout, routing high-speed differential traces, and preparing manufacturing files for JLCPCB PCB fabrication and assembly. We are all hearing news; new AI models are being released every month. And it has finally reached the schematic editor. Flux.ai is a browser-based AI PCB design tool with a built-in AI agent that behaves like a junior hardware engin......