How Aluminum PCBs Improve Thermal Conductivity
5 min
- What Is an Aluminum PCB?
- Why Thermal Conductivity Matters in Electronics
- Thermal Conductivity in Aluminum PCBs
- Thermal Dissipation and Expansion in Aluminum PCBs:
- Aluminum PCBs vs Traditional FR-4 PCBs
- Applications of Aluminum PCBs
- Conclusion
Thermal management has become one of the most important issues in electronic design as contemporary electronics get smaller and more potent. PCBs have a variety of cores and materials. In the past, we have covered a wide range of materials. Today, however, metal core PCBs are the primary emphasis. Poor heat dissipation in basic PCBs causes electrical devices to perform worse, last less time, or possibly fail catastrophically.
Compared to conventional FR-4 boards, aluminum PCBs have better heat conductivity, making them an efficient alternative. The qualities that vary are listed in this article below. Additionally, we will examine the construction, benefits, and uses of aluminum PCBs, as well as how they improve heat conductivity.
What Is an Aluminum PCB?
An aluminum printed circuit board (PCB) is a metal-based printed circuit board. It is designed to control the heat produced by power electronics in a circuit board. It substitutes aluminum for conventional fiberglass (FR-4) as the foundation substrate. The basic Structure of Aluminum PCB is:
1. Copper Circuit Layer: The main function of this layer is to give all components electrical connectivity to all components on the PCB. Compared to standard CCLs (one to ten ounces), the copper layer utilized is comparatively thicker. When pricing for a PCB, you have the option to select the copper weight. A higher current carrying capacity is associated with a thicker coating of copper.
2. Dielectric Layer (Insulating Layer): The dielectric layer is known as the insulating layer which is around 50 to 200 μm thick. Now because it acts as a layer of electrical isolation and thermal conduction it should have lower resistance to heat and higher to electrical signals.
3. Metal Base Layer (Aluminum): The aluminum base is composed of aluminum substrate. It provides mechanical strength to the PCB. But the main use is to dissipate heat by acting as a thermal conductor.
4. Aluminum Base Membrane Layer: This type of membrane is selective. It serves a protective purpose by preventing undesired etching and scratching of the metal surface.
Why Thermal Conductivity Matters in Electronics
Heat is produced during the operation of electronic parts such as power converters, LEDs, and vehicle electronics. The surrounding components will get heated if this heat doesn't swiftly disperse to the surroundings. Excessive heat accumulation can shorten component lifespans and lead to solder joint fatigue. Overheating the component might cause it to burn and ignite the PCB and entire circuit.
Thermal Conductivity in Aluminum PCBs
1. Superior Thermal Conductivity of Aluminum
It can be seen from the characteristics by comparing the two substrates side by side. FR-4 has thermal conductivity of 0.3 to 0.4 W/mK. On the other hand aluminum has a thermal conductivity of about 205 W/mK. According to the comparison the conventional FR-4 PCBs have a thermal resistance of 5.50 × 10⁻⁴ °C/W. Which is almost 30% greater than that of aluminum PCBs. As a result their heat dissipation efficiency is greatly decreased.
2. Role of the Dielectric Layer
Even though aluminum has a high thermal conductivity. The thermal transmission is greatly aided by the dielectric layer that sits between the copper traces and aluminum. In some designs the insulating layer's thermal conductivity lies between 1 W/mK and 10 W/mK.
Thermal Resistance Equation:
Better heat conduction is indicated by a lower Rth value. Manufacturers greatly enhance aluminum PCBs' heat performance by maximizing dielectric materials and reducing thickness.
Thermal Dissipation and Expansion in Aluminum PCBs:
In heat removal the aluminum PCBs outperforms standard FR4 PCBs. For an example: An aluminum PCB with a thickness of 1.6 mm will have a thermal resistance (TR) of 2-3 degrees per watt. While on the other hand a FR4 PCB of the same thickness has TR between 22–25 degrees per watt. The coefficient of thermal expansion also varies from material to material. Aluminum PCBs do not have thermal expansion/contraction problems due to its good thermal dissipation capabilities.
Aluminum PCBs vs Traditional FR-4 PCBs
Applications of Aluminum PCBs
1. LED Lighting: Aluminum PCBs are frequently used in LED fixtures and bulbs to control the heat produced by high-brightness LEDs. Since the base of the PCB may be connected straight to the closest heatsink, they are present in all LED bulbs.
2. Power Electronics: It is used when there is a greater need for power or when a voltage/current conversion is being performed. Power supply, voltage regulators, and converters are a few examples.
3. Consumer Electronics: Small heatsinks may not be the best choice these days due to the shrinking electronics items. There, a metal core PCB will be the preferable choice. Applications in consumer electronics include computers, mobile devices, and LCD backlights.
4. Medical Equipment: MRI scanners, surgical lights, and diagnostic instruments are a few examples of the most precise electrical equipment that should always be kept on the cold side.
Conclusion
In cases where component heating is a major problem, we have seen several reasons why aluminum PCBs are superior. Aluminum PCBs are now the go-to option for thermal management due to the growing need for high-power and small devices. They outperform FR4 in terms of mechanical toughness and strong thermal conductivity. However, there are further techniques to prevent heat from entering circuits while they are operating, and there are always cooling solutions available. Active cooling techniques, heatsinks, heatpipes, and basic CPU fans. Engineers may create durable, effective electrical devices by comprehending heat transfer principles.
Keep Learning
Understanding PCB Laminates Materials, Types, and Why They Matter
A PCB is a flat board made of a non-conductive substrate material with conductive pathways and components attached to it. One of the critical components of a PCB is the PCB laminate. A typical laminate PCB consists of a core material, such as fiberglass or composite epoxy. So what it actually do is ● Provides structural support ● Improves Signal Integrity ● Bond the layers to the core material The fiberglass layers are stacked on top of each other and pressed together with heat and pressure to create ......
Why UL94 V0 Matters for Safe and Reliable PCB Manufacturing
Key Takeaways UL94 V0 is the highest flame rating for PCB materials, requiring self-extinguishing within 10 seconds with no flaming drips. It greatly reduces fire risk and has become the de facto standard for safe, reliable PCBs in consumer, industrial, automotive, and medical applications. JLCPCB offers UL94 V0 compliant FR4 and high-Tg materials by default, ensuring regulatory compliance (UL, CE, CCC) and long-term reliability without compromising performance or budget. Never sacrifice V0 rating for......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
PCB Material Guide : Types, Selection, and Impact on Performance
If PCB materials could talk, FR-4 would probably say, "I run 80% of the electronics industry, and still nobody appreciates me." Rogers would boast, "I'm expensive because I'm special," while Polyimide would flex literally and say, "I bend, but I don't break." The purpose of this blog is to introduce you to the types of PCB substrates available to you and how those materials affect your PCB's performance, thermal stability, signal integrity, and overall longevity. The choice of PCB material will be bas......
The Critical Role of Copper Peel Strength in Durable PCB Performance
Key Takeaways Standard Test: Measured via the IPC-TM-650 90° pull test in N/mm. Core Function: Prevents pad lifting and delamination under thermal stress and CTE mismatch. Foil Types: ED foil provides higher adhesion; RA foil yields lower signal loss. Material Benchmarks: Standard FR4 averages 1.0–1.4 N/mm, while High-Tg FR4 achieves 1.2–1.6 N/mm. Design Tips: Add teardrops, eliminate unsupported copper slivers, and perform DFM checks. Ever wonder what's making the copper stay put on your circuit boar......
Navigating Standard PCB Thickness: A Step-by-Step Guide to Selecting the Ideal Thickness for Your PCB Prototype
The thickness of a printed circuit board (PCB) may seem like a small detail, but it plays a crucial role in the performance and reliability of your electronic devices. Standard PCB thickness has become an industry norm, offering a range of benefits that impact mechanical stability, electrical performance, thermal management, and component compatibility.In this article, we will be taking a deep look at why the varying thickness of your PCB matters and provide you with a guide to choosing the right thic......