High Voltage PCB Layout Tips: From Material Selection to Safe Design Practices
5 min
- What Is a High-Voltage PCB?
- Materials for High-Voltage PCBs:
- PCB Design Considerations for High Voltage:
- High-Voltage PCB Layout Techniques:
We have seen PCBs for high speeds and high power, and MCPCBs for thermal management; now it's time to see the HV PCBs. These are not some special PCBs, but rather the simple ones tamed to handle high voltages. At these high voltages, currents are in mA, which is why power is not a concern. However, the HV lines are not easy to handle because, in HVs, electrons leap across gaps, arc over surfaces, and create catastrophic failures.
That’s why high-voltage PCB layout isn’t just about making traces wider; it’s about applying careful design rules, proper material selection, and layout strategies that keep power where it belongs. If done poorly, you don’t just get a design bug; you get smoke, sparks, and possibly a fried lab bench. It becomes difficult when HV and LV traces are running on the same PCB. For example, if an MCU is working at 3.3V, and somehow it gets a spike of 1kV, everything is destroyed. Let’s explore high voltage design in this article.
What Is a High-Voltage PCB?
A high-voltage PCB (HV PCB) is any printed circuit board designed to operate above standard voltage limits. At this voltage, insulation, creepage, and clearance become critical factors. In general terms, HV is mentioned as follows:
- >30 VAC
- >60 VDC
which fall under high-voltage design considerations per IPC standards.
Applications include:
- Power supplies and inverters.
- Electric vehicles (EV power electronics).
- Medical equipment (X-ray, MRI).
Materials for High-Voltage PCBs:
The substrate material is crucial in determining how much voltage your PCB can handle safely. From the materials listed below, you can get a general idea of which one to select according to the voltage range.
Standard FR-4: Being the most common PCB material, it is suitable for low to medium voltages (~200–250 V). It has higher moisture absorption and lower Comparative Tracking Index (CTI).
High-CTI FR-4: It is known as enhanced FR-4 laminates with higher tracking resistance. It performs better in polluted or humid environments than standard FR-4.
Polyimide / PTFE / Ceramic Substrates:These are made to work in very high-voltage (>1 kV) or high-frequency designs. It has a pretty high dielectric strength and excellent thermal stability.
PCB Design Considerations for High Voltage:
1. Creepage Distance:
The shortest distance along the surface of the PCB between two conductors. It is critical because contaminants like dust, moisture, or flux residue can reduce surface insulation. Use the standards defined in IPC-2221 and IEC-60664. The higher the voltage range, the longer the creepage distance should be.
2. Clearance Distance:
The shortest air gap between two conductors. At HV, the flow of charges can occur if there is a small air gap, known as dielectric breakdown. Especially critical in high-altitude applications where thinner air reduces dielectric strength.
3. Isolation Requirements
For safety and EMI reasons, HV circuits often need isolation slots, cut-outs, or wider gaps in the board. Physical barriers like milling slots can increase creepage effectively. These guidelines can be used to route the HV and LV traces on the same board.
4. Dielectric Breakdown
The PCB laminate has a dielectric strength (measured in kV/mm). Designers must ensure the dielectric thickness between layers is sufficient to withstand the applied voltage. The dielectric strength of different materials can be seen in the datasheets provided by manufacturers.
High-Voltage PCB Layout Techniques:
Now, let’s get into practical layout rules:
Wider Traces: IPC-2152 gives the accurate sizing; HV traces should be wider than those for standard signals.
Rounded Corners: Avoid sharp 90° trace corners, as they create electric field concentration points that increase the risk of corona discharge. You can use two 45° bends or curved traces instead of a 90° turn.
Keep-Out Zones: Define proper no-go zones around HV nets to prevent accidental routing of sensitive signals nearby. In these areas, any signal or LV traces are prohibited from entering.
Multi-Layer Considerations: Keep HV nets isolated on dedicated layers. Separate them from low-voltage planes with sufficient dielectric spacing.
Conclusion:
As we have seen, the guidelines of design and routing for a high-voltage PCB require more than just wider traces. It’s about creating a safe, reliable environment where high voltage behaves predictably by routing all the other signals away from it. We have covered the material selection and design considerations to understand the HV better. Some of the best practices include:
- A dedicated separate ground plane for HV and LV circuits is used, and both grounds are connected through the star grounding method.
- Optocouplers and transformers are used to keep the HV isolated from the LV.
- Mark the safety zones on the silkscreen itself.
When integrating HV with LV circuits, remember to segregate, isolate, and shield. And never forget the compliance with IPC and IEC standards. A better way is to apply the conformal coating or potting the PCB to improve the creepage resistance and add an additional insulation layer over the PCB.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
• Design Guidelines for PCB Using FR4 Substrates
Keep Learning
Understanding Multilayer PCB Stackup
Key Takeaways Layer Arrangement: Optimize signal, ground, and power layer placement for better performance. Material Selection: Choose suitable core, prepreg, and copper materials. Signal Integrity: Control impedance and minimize crosstalk and EMI. Stackup Design: Use symmetrical structures to reduce warpage risks. Manufacturability: Consider layer count, via structures, and manufacturing limits early in design. Performance & Cost: Balance electrical requirements, reliability, and production costs. In......
EMC Design for PCB: EMI, EMS, Testing Standards & Compliance Guide
Key Takeaways EMC design means controlling both EMI (unwanted emissions) and EMS (immunity to external disturbances); a board that meets emission limits but resets during an ESD test has not achieved EMC. Every interference problem can be analyzed with the source–path–victim model, and solved by reducing the source, interrupting the path, or hardening the victim. Core PCB techniques include minimizing current-loop area, maintaining continuous reference planes, controlling impedance, decoupling power p......
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Antennas on PCB: A Beginner to Advance Guide
In today’s world of widespread wireless connectivity, the demand for small, affordable, and reliable antennas is higher than ever. Antennas act as real-world implementations of electromagnetic wave principles. They enable the sending and receiving of signals for a variety of wireless uses. While there is a lot of theoretical and experimental research in this area, only a few designs become widely used in actual products. Among the different options, Printed Circuit Board (PCB) antennas have become a p......
PCB Antenna Design: Types, Principles, and Best Practices
In the world surrounded with wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. Antennas are the application of electromagnetic waves. There are many theories and practicals available on antennas, but only few of them get recognised. For wireless data transfer the one solution can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating t......
How to Choose and Place Decoupling Capacitors for PCB Design
Every digital PCB depends on decoupling capacitors, yet a surprising number of boards still suffer from voltage dips, glitches, and electromagnetic interference (EMI) issues caused by one simple mistake: incorrect placement or selection. This guide walks through what decoupling capacitors do, how to choose the right value, where to place them, and which layout mistakes to avoid, so your next board runs clean on the first try. Key Takeaways Place one decoupling capacitor near each IC's power pin. Use 1......