The Benefits of High Speed PCBs : Advanced Design and Manufacturing for Reliable Data Rates
12 min
- Advanced Materials Essential for High Speed Performance
- Proven Design Approaches for Reliable High Speed PCBs
- Precision Manufacturing for Flawless High Speed PCBs
- JLCPCB’s Specialized Capabilities in High-Speed PCB Production
- Frequently Asked Questions (FAQ)
What is high-speed PCB design, then? It is not just the frequency cut-in, High-speed. When the characteristics of the traces become unfriendly to the signal, trace impedance, via parasitic, material losses, signal coupling, etc., really begin to affect the signal quality, and you can no longer simply plug it in and hope for the best, it must be designed.
Practically, that typically implies rise times in the range of nanoseconds, data rates in the range of gigabit per lane, or clock speeds in the range of several hundred megahertz. However, modern interfaces are far beyond those limits: PCIe Gen5 can run at 32GT/s, USB4 at 40GB/s, DDR5 at 6.4GB/s, and 100G/400G Ethernet at 25-56GB/s per lane. With such speeds per mil of trace, every via transition, every material selection is a design choice that has an impact on the performance of the system.

Electronics engineers have made high-speed PCB design a professional skill and not a niche capability. Almost all modern SoCs, FPGAs, or processors have at least one high-speed interface, which requires the use of appropriate PCB design methods.
Common Signal Integrity Challenges at High Frequencies
High-speed digital signals face the same physical challenges as RF signals, but the context is different. Where an RF engineer worries about insertion loss and return loss, a digital signal integrity engineer thinks about eye diagram margins and bit error rates. The underlying physics, however, is identical.
The primary challenges include frequency-dependent loss (higher harmonics of fast digital edges are attenuated more than lower harmonics, rounding the signal edges and closing the eye), impedance discontinuities at vias, connectors, and routing changes that create reflections appearing as ringing and overshoot, crosstalk from adjacent aggressor signals coupling noise into victim traces, and power delivery network noise injecting jitter through supply-induced timing variations.
As data rates increase, these effects compound. A signal that looked clean at 5 Gbps may be completely unusable at 25 Gbps on the same PCB because the higher-frequency content experiences disproportionately more loss, and the timing margin shrinks from nanoseconds to picoseconds.
Advanced Materials Essential for High Speed Performance
Low-Loss Dielectrics and High-Performance Laminates
Standard FR-4 has served the industry well for decades, but high-speed PCB materials requirements have outpaced its capabilities. At 10 GHz (the relevant frequency for 25 Gbps NRZ signals), standard FR-4 introduces approximately 1 dB/inch of dielectric loss alone, which can consume most of a link’s loss budget over a typical trace length.

The high-speed PCB material industry has a couple of layers. Mid-loss options like Isola FR408HR and Panasonic Megtron 4 provide a decent increase over regular FR -4, but the price increase is moderate, and they are fine in projects up to about 10-16 Gbps. When you are pushing to 25-56Gbps, consider low-loss mates, such as Megtron 6, Isola I-Tera MT40, or Tachyon 100G - they tend to reach Df values of 0.003-0.005 at 10GHz. To have the very best, highest-end 100+ Gbps stuff, you will also require ultra-low-loss boards that are near PTFE performance.
Material selection should be driven by channel loss budget analysis, not by blanket specifications. Some traces are short enough that even standard FR-4 provides adequate margin; others need premium materials. Analyze each critical net individually.
Copper Roughness Control and Thermal Properties
Copper roughness contributes significantly to conductor loss at high frequencies — the same skin effect phenomenon that concerns RF designers. For high-speed digital at 25+ Gbps, the difference between standard and reverse-treated (low-roughness) copper foil can be 0.2-0.4 dB/inch, which adds up quickly on 10+ inch trace lengths.
Thermal properties of high-speed laminates matter for reliability, especially in systems with high power dissipation. Glass transition temperature (Tg), decomposition temperature (Td), and CTE (coefficient of thermal expansion) must be adequate for the assembly reflow profile and the product’s operating temperature range. Most premium high-speed materials offer improved thermal properties alongside their electrical benefits.
Material Trade-Offs for Cost, Reliability, and Speed
Material selection for high-speed PCB manufacturing involves balancing multiple factors. Premium materials reduce signal loss but increase board cost by 2-5x. They may also affect fabrication yield if the manufacturer is not experienced with the specific material. Some ultra-low-loss materials have lower Tg or more challenging processing requirements than standard FR-4.
The most cost-effective approach is to analyze your specific link budgets and select the minimum material performance that provides adequate margin. Use a hybrid stackup if only certain layers require premium materials. And always verify that your fabricator has production experience with your chosen material — an unfamiliar material can introduce yield issues that negate the cost savings of choosing a less expensive option.
Pro-Tip: Run a channel loss simulation (using tools like Keysight ADS, Ansys HFSS, or even free tools like Saturn PCB Toolkit) before selecting materials. The simulation will tell you exactly how much loss budget you have and what material performance level you need — no guessing required.
Proven Design Approaches for Reliable High Speed PCBs
Impedance Control, Differential Pair Routing, and Layer Stackup
So all high-speed signals must be implemented as a controlled-impedance transmission line. Single-ended signals are typically driven to 50 ohms; differential pairs are driven to 85 ohms, 90 ohms, or 100 ohms, depending on the interface standard. The geometries of the traces that reach those targets are determined by the stack-up design layer thicknesses, dielectric constants, and copper weights.

In routing pairs of differential traces, you must maintain the distance between the + and the – traces uniform throughout. The length overlap among pairs (intra-pair skew) must be comparable to a few mils in such multi-gigabit signals. Inter-pair skew, or the difference between various pairs of differentials in a bus, is a little looser, but you still need to consider it in parallel interfaces such as DDR5.
An excellent high-speed stack-up lays all the signal layers immediately adjacent to a solid reference plane and the most important signals are on the layers nearest to the board center to ensure the maximum amount of shielding. The use of signal and ground/power planes alternating in the stack-up ensures that the return path remains solid.
Via Back-Drilling and Crosstalk Mitigation Techniques
Via stubs are the unused portion of a through-hole via extending past the target layer — create quarter-wave resonances that cause deep notches in the frequency response. For a standard 62-mil thick board, the via stub resonance falls around 12 GHz, right in the middle of the frequency band needed for 25 Gbps signals.
Back-drilling removes the stub by mechanically drilling away the unused via barrel from one or both sides of the board. The process requires precise depth control (±4 mils typical) to ensure complete stub removal without damaging the target signal layer. For designs above 10 Gbps, back-drilling is nearly always worthwhile.
Crosstalk mitigation combines several techniques: maintaining adequate trace spacing (at least 3x the dielectric height between the trace and its reference plane), using ground-referenced vias between signal via pairs, inserting ground traces or copper pours between adjacent high-speed channels, and avoiding parallel routing of aggressor and victim traces over long distances.
Simulation and DFM Integration Early in Design
Pre-layout simulation is not optional for high-speed designs; it is the foundation of a successful board. Channel simulation validates that the combination of material, stackup, trace geometry, via transitions, and connectors delivers adequate signal quality for the target data rate. This analysis should happen before routing begins, not after.
DFM integration during the design phase ensures that your simulated design is actually manufacturable. Trace widths and spacings must fall within the fabricator’s capability range for the chosen material and copper weight. Via geometries must be compatible with the drill aspect ratios that the fabricator can reliably produce. Back-drill depths must have an adequate margin for the fabricator’s process capability. Early DFM review avoids the painful cycle of discovering manufacturing constraints after the design is complete.
Precision Manufacturing for Flawless High Speed PCBs
Tight Tolerance Etching, Drilling, and Registration Processes
High-speed PCB manufacturing demands fabrication precision that standard boards do not require. Trace width tolerance of ±0.5 mil or better ensures impedance stays within the specified window. Layer-to-layer registration of ±2 mils or better maintains consistent impedance by keeping signal traces properly aligned with their reference planes.
Drill positional accuracy is determined via-to-pad alignment and affects the quality of back-drilled vias. For back-drilling, the drill must stop within ±4 mils of the target depth, which is close enough to remove the stub without penetrating the signal layer. This requires Z-axis controlled drilling equipment with real-time depth monitoring.
Etching profile controls the cross-sectional shape of the finished trace and affects the impedance accuracy beyond what trace width alone determines. Advanced etching processes that minimize undercutting produce more rectangular profiles that better match the impedance calculated by design tools.
Surface Finish and Lamination for Minimal Signal Degradation
Surface finish selection impacts high-speed signal performance at the component interface. ENIG provides a flat, reliable surface for fine-pitch BGAs but introduces magnetic loss from the nickel layer that can be measured at frequencies above 5 GHz. Immersion silver offers lower loss and excellent flatness but has a shorter shelf life. OSP is the lowest-cost, lowest-loss option for boards assembled shortly after fabrication.
Lamination quality directly affects impedance control and dielectric loss. Precise resin flow control maintains consistent dielectric thickness between signal layers and reference planes. Inadequate resin flow leaves voids that change the effective dielectric constant; excessive flow thins the dielectric and shifts impedance.
Comprehensive Testing Including TDR and Eye Diagram Analysis
TDR (Time Domain Reflectometry) testing on impedance coupons verifies that the fabricated impedance matches the design target. For high-speed boards, ±7% or ±5% impedance tolerance may be specified depending on the link budget analysis.

Eye diagram measurements on dedicated test channels provide the most comprehensive validation of high-speed PCB quality. By driving a PRBS pattern through a fabricated test structure and measuring the received eye diagram, you can directly assess the combined impact of all loss, reflection, and coupling mechanisms on signal quality. This measurement is the ultimate proof that the board will support the target data rate. Leading-edge high-speed PCB design services providers include TDR and insertion loss data as standard quality documentation, giving designers confidence that their boards will perform as simulated.
JLCPCB’s Specialized Capabilities in High-Speed PCB Production

Premium Material Partnerships and Cutting-Edge Fabrication Lines
JLCPCB maintains partnerships with leading laminate manufacturers to offer a comprehensive range of high-speed materials, from enhanced FR-4 through ultra-low-loss options. Combined with precision fabrication equipment capable of the tight tolerances demanded by multi-gigabit signal integrity, JLCPCB provides end-to-end high-speed PCB manufacturing capability.
Expert DFM Reviews Tailored for High Speed Designs
High-speed designs require DFM attention beyond standard board checks. JLCPCB’s DFM process evaluates stackup feasibility, impedance achievability with available materials, back-drill depth requirements, and other high-speed-specific factors. This specialized review catches issues that generic DFM tools miss, preventing production delays and performance surprises.
Scalable Manufacturing with Proven High-Yield Results

From prototype validation to high volume production, JLCPCB maintains the PCB performance solid. The same material specifications, process control, and quality check will work at each scale, and thus your prototype-tested design will run the same when you spin it up to thousands of boards.

Frequently Asked Questions (FAQ)
What qualifies as a high-speed PCB?
Any PCB where signal interconnect behavior significantly affects signal quality qualifies as high-speed. In practice, this includes boards with data rates above 1 Gbps, rise times below 1 ns, or interfaces like PCIe Gen 3+, USB 3.0+, DDR4/5, or multi-gigabit Ethernet.
When should I switch from FR-4 to a premium laminate?
When channel simulation shows that FR-4 loss consumes too much of your link budget to maintain adequate eye opening, as a rough guideline, interfaces above 10 Gbps typically benefit from enhanced or low-loss materials, and interfaces above 25 Gbps almost always require them.
How important is back-drilling for high-speed designs?
Very important for through-hole vias carrying signals above approximately 8-10 Gbps. The via stub resonance can create deep notches in the channel frequency response that dramatically degrade signal quality. Back-drilling removes this resonance and is standard practice for 25+ Gbps designs.
What impedance tolerance should I specify?
Standard ±10% is adequate for most high-speed digital applications up to about 10 Gbps. For 25+ Gbps, specify ±7% or ±5% based on your link budget analysis. Tighter tolerance increases fabrication cost, so match the spec to your actual performance requirement.
Can high-speed and standard designs coexist on the same board?
Absolutely. Most modern boards combine high-speed interfaces (PCIe, DDR, Ethernet) with standard-speed control signals and power management. The key is applying high-speed design techniques only where needed, using controlled impedance and premium materials for the fast signals while routing standard signals conventionally.
Keep Learning
Signal Integrity and Jitter Analysis Using Eye Diagrams
The way a signal travels across a wire varies depending on the transmitter and receiver. This is where methods for error identification and correction are useful. However, how can we tell if a signal is different? It goes without saying that we need to use a device to track at both TX-RX ends and view the data bit by bit. And why is the signal shifting, and is it possible to stop the cause? Yes, it is somewhat feasible, but there is little we can do to protect a wireless channel from noise. Due to EMI......
The Benefits of Coplanar Waveguide in High-Frequency PCB Design
Key Takeaways Coplanar waveguide (especially GCPW) improves high-frequency PCB performance by keeping the return path close and confining fields, which boosts signal integrity and reduces EMI/radiation. It also gives more impedance/layout flexibility (tuning both trace width and gap), but demands tighter manufacturing control of gap tolerances, copper roughness, and material Dk/Df—so field-solver impedance design and DFM checks are essential, with low-loss laminates preferred at higher GHz. Have you e......
6-Layer PCB Stackup and Buildup Guidelines
Printed Circuit Boards (PCBs) are the backbone of modern electronics, providing the necessary infrastructure for connecting and supporting various electronic components. As electronic devices become more complex and compact, the demand for multi-layer PCBs has increased. Among these, the 6-layer PCB is a popular choice for many applications. This article will delve into the specifics of 6-layer PCB stackup, its applications, optimal configurations, and guidelines for selecting the best manufacturer. W......
Designing Antennas on PCB: A Beginner to Advance Guide
In today’s world of widespread wireless connectivity, the demand for small, affordable, and reliable antennas is higher than ever. Antennas act as real-world implementations of electromagnetic wave principles. They enable the sending and receiving of signals for a variety of wireless uses. While there is a lot of theoretical and experimental research in this area, only a few designs become widely used in actual products. Among the different options, Printed Circuit Board (PCB) antennas have become a p......
Understanding Multilayer PCB Stackup
Key Takeaways Layer Arrangement: Optimize signal, ground, and power layer placement for better performance. Material Selection: Choose suitable core, prepreg, and copper materials. Signal Integrity: Control impedance and minimize crosstalk and EMI. Stackup Design: Use symmetrical structures to reduce warpage risks. Manufacturability: Consider layer count, via structures, and manufacturing limits early in design. Performance & Cost: Balance electrical requirements, reliability, and production costs. In......
PCB Antenna Design: Types, Principles, and Best Practices
In the world surrounded with wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. Antennas are the application of electromagnetic waves. There are many theories and practicals available on antennas, but only few of them get recognised. For wireless data transfer the one solution can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating t......