This website requires JavaScript.
Coupons
Ship to
Blog

PCB Routers: Essential Tools for Modern Circuit Design

Published Dec 19, 2024, updated Oct 29, 2026

7 min

Table of Contents
  • Introduction
  • How JLCPCB Handles Routing (2026 Capabilities)
  • Conclusion
  • Frequently Asked Questions (FAQ)

Introduction

In modern PCB production, routing machines (commonly called PCB routers or CNC routers) play a critical role. They are used to cut the board outline, create V-grooves for depanelization, mill slots, and finish edges with high precision. As electronic devices become smaller and more complex, PCB routers ensure clean, accurate, and repeatable results. This article explains what PCB routers are, their types, key applications, best practices, and how JLCPCB integrates advanced routing in its manufacturing process.

What is PCB Router

In modern PCB manufacturing, a PCB router (also called a PCB milling machine or CNC router) is a precision CNC machine used primarily for board outline routing, V-CUT scoring, slot milling, and edge finishing after the inner layers and solder mask are complete.

Unlike the etching process that removes unwanted copper to form traces, the PCB router physically cuts the board perimeter, creates V-grooves for depanelization, mills slots for connectors, and removes tabs or mouse bites. It ensures clean edges, tight dimensional tolerance (±0.1 mm typical), and safe panel separation without damaging sensitive traces or components.

Types of PCB Routers

PCB routers come in many varieties, each appropriate for a different use and need:

⦁ Manual PCB Routers:

Hand-operated or semi-automatic machines, suitable for prototyping, repair, or very low-volume custom work. They offer flexibility but require skilled operators and are less consistent for production.

⦁ Automated PCB Routers:

Computer-controlled with high repeatability (±0.01 mm positioning accuracy). Ideal for medium to high-volume manufacturing. JLCPCB uses automated CNC routers with automatic tool changers and vision alignment for precise panel routing.

⦁ High-Speed PCB Routers:

Equipped with high spindle speeds (up to 60,000 RPM), automatic tool changers, and large working areas. Designed for mass production with minimal downtime. JLCPCB’s production lines employ this type for fast, clean depanelization of panelized boards.

Importance of PCB Routers in PCB Design

For many reasons, PCB routers are essential components of the PCB production process:

⦁ Precision and Accuracy:

PCB routers guarantee extremely accurate cutting of the complex traces and pads on a circuit board. Especially in high-frequency applications, this accuracy is crucial for preserving the integrity and performance of electronic circuits.

⦁ Complex Design Handling:

PCB routers help to produce complex designs that would be difficult or impossible to accomplish with hand techniques as current electronic gadgets became more complicated. Essential for modern technologies, they can manage minute pad sizes and precise traces.

⦁ Efficiency and Productivity:

By reducing manual labor and processing time, automated PCB routers greatly increase manufacturing efficiency. By doing several cutting operations in combination, they can accelerate manufacturing and lower general production costs.

Best Practices for Using PCB Routers

The following best practices help to optimize the advantages of a PCB router:

⦁ Proper Tool Selection:

Choose router bits according to task: 0.8–2.0 mm end mills for outline routing, 30°/45° V-cutters for scoring, smaller bits (0.4–0.6 mm) for fine slots. JLCPCB recommends carbide bits for FR-4 to minimize chipping.

⦁ Optimize Router Settings:

Typical parameters on JLCPCB production lines:

- Spindle speed: 40,000–60,000 RPM

- Feed rate: 0.5–2.0 m/min (depending on material thickness)

- Depth per pass: ≤0.5 mm for clean cuts

- Proper vacuum hold-down and dust collection are essential to prevent board movement and dust contamination.

⦁ Maintain Router Maintenance:

Design mouse bites, V-CUT or tab routing in EasyEDA or your layout tool. JLCPCB standard:

- V-CUT residual thickness: 0.2–0.3 mm

- V-CUT angle: 30° or 45°

- Tab width: 2–3 mm recommended

Always follow JLCPCB panelization guidelines to avoid stress on components during depanelization.

Applications of PCB Routers

PCB routers find use in several sectors and for different purposes:

⦁ Consumer Electronics:

PCB routers are used in consumer electronics to build circuit boards for household appliances, tablets, and cellphones. PCB routers' accuracy and efficiency help to explain the dependability and performance of many common devices.

⦁ Automotive Electronics:

PCB routers are used in automotive electronics to generate circuit boards for engines control units, safety systems, and entertainment systems. PCB routers' strong precision and durability guarantee that car electronics run consistently in difficult environments.

⦁ Industrial Machines:

Manufactured PCBs for industrial machines and automation systems are PCB routers. They guarantee operational efficiency and dependability by helping to create circuit boards monitoring and controlling different industrial operations.

⦁ Industrial Equipment:

PCB routers are absolutely essential in the medical sector for producing PCBs used in pacemakers, diagnostic tools, and other medical devices. The accuracy and safety of medical technologies depend on PCB routers' exacting performance.

Choosing the Right PCB Router

Selecting a PCB router calls for many important factors:

⦁ Routing Capabilities:

Review the router's features including speed, accuracy, and adaptability for several PCB materials. Choose a router that satisfies your production-related particular needs.

⦁ Size and Capacity:

Think on the PCB sizes you will be working with and the router's capacity to manage those measurements. Verify the router's capacity for your board size and production volume.

⦁ Cost vs. Performance:

Balance the PCB router's features and pricing to its performance. Although more expensive models could have advanced features and more accuracy, make sure the investment fits your budget and manufacturing requirements.

How JLCPCB Handles Routing (2026 Capabilities)

JLCPCB uses high-precision CNC routers with:

- Positioning accuracy ±0.01 mm

- Repeatability ±0.005 mm

- Automatic tool changers and vision alignment

- Support for panelized boards up to 460×610 mm

- V-CUT + routing combination, mouse bite, and tab removal all in one automated proces

Designers do not need to own routers — simply follow JLCPCB’s panelization rules in EasyEDA, and the factory handles precise, clean depanelization at scale.

Accelerate Your PCB Projects with JLCPCB

Conclusion

Made of printed circuit boards, PCB routers are essential for the fabrication of complex and exact designs since they help to enable them. PCB routers guarantee that circuit boards satisfy required levels of accuracy and dependability whether for consumer electronics, automotive systems, industrial machinery, or medical devices. Manufacturers may maximize their PCB production techniques and help to improve electronic technology by knowing the several kinds of PCB routers, their uses, and best practices for operation.

PCB routers will become ever more important as technology develops in guaranteeing effective and high-quality PCB manufacture. Following top standards and choosing the correct PCB router will enable outstanding performance in the always demanding electronics sector.

To get started, upload your design to JLCPCB via EasyEDA or Gerber files. Use the panelization tool to set V-CUT or mouse bites, and receive instant DFM feedback and accurate routing quotation — fast turnaround and high-quality edges guaranteed.

Frequently Asked Questions (FAQ)

1. What is a PCB router used for?  

  A PCB router (CNC routing machine) cuts board outlines, creates V-grooves for depanelization, mills slots and finishes edges with high precision after inner layers and solder mask are complete.

2. What are the main types of PCB routers?  

  Manual (for prototypes), automated/CNC (high repeatability for production), and high-speed/production routers (fast processing with automatic tool changers).

3. Why are PCB routers important in manufacturing?  

  They ensure clean edges (±0.1 mm tolerance), reliable depanelization without damaging components, high throughput, and support for complex shapes in consumer, automotive, and medical PCBs.

4. How does JLCPCB handle PCB routing?  

  JLCPCB uses high-precision CNC routers (±0.01 mm accuracy, 40,000–60,000 RPM) with V-CUT + routing combo, mouse bites/tabs, and automated vision alignment for clean, fast depanelization.

Keep Learning