Lead-Free vs Lead Solder: What’s the Real Difference?
6 min
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties of solder are used in the electronics industry:
● Lead-based solder
● Lead-free solder
The classic ingredients for solder are tin and lead. The electronics industry has relied on this combination for a long time. There has been a dramatic transition away from lead-based solders. Which were formerly the norm, due to increased health and environmental concerns. In this article we will learn why lead-free solder has surpassed lead ones. We'll go over the composition differences, melting points and regulatory standards.
What is Lead Solder?
Lead solder is an alloy of solder that contains lead with tin. Lead solder is usually named as 63/37 which is the ratio of tin and lead. Means it will contain 63% tin and 37% lead. But why do we use LEAD based solders? And why are they so popular? The answer is because of their low melting point of about 185°C. There were a number of reasons why this solder was formerly the standard:
Cooling and Curing: Lead solder cools down more slowly than other metal options. This reduces the possibility of the joint cracking also there will be no issues like dry soldering.
Wetting the joints: Wetting the joints means making the two wires which are going to solder more effective. Means giving them an extra adhesiveness. Using this type of solder is effective in wetting joints.
We can not rely on lead based products, its poisonous. Lead has negative impacts on ecosystems and human health. It comes under the health issues linked to lead exposure according to the CDC in the US.
What is Lead-Free Solder?
The amount of metals in lead-free solder compositions might vary. Metals such as tin, copper, silver, nickel, and zinc can be used as components. For better performance and environmental safety lead-free solder substitutes are also available.Lead with alternative metals include bismuth (Bi) or antimony (Sb). Among lead-free mixes, tin-copper is the most popular due to its melting point of 217°C. When compared to conventional lead-tin solders the lead-free solders have unique characteristics. Because of these quirks the manufacturers have to make adjustments to their product designs and processes.
Common Lead-Free Solder Compositions:
● SAC305: 96.5% Tin, 3% Silver, 0.5% Copper and has a melting point: 217-221°C
● SnCu0.7: 99.3% Tin, 0.7% Copper and has a melting point: 227°C
Tin and copper make up the lead-free combination that sees the most action. A greater melting point is associated with lead-free solder than lead-based alternatives. When compared to lead soldering this technique also produces tougher and stronger junctions.
Key Differences Between Lead and Lead-Free Solder:
Comparing Costs of Lead-Free vs Leaded Solder:
Lead is not very expensive, this is the second reason it is used. On the other hand if we use other alternatives or if we use more tin it will be an expensive option. Manufacturers can save up to 10 times if they are using lead. Other alternatives like silver makes the deal more expensive but due to the conductivity can be used in high end systems.
Using lead-free solder could add to the overall cost, not to mention the initial investment. Because more resources and processing to make the lead-free solder is usually more expensive than leaded solder. Equipment wear and tear and energy expenses might both rise due to greater melting points.
Melting Point Equations:
To put a number on this impact, we may utilize a linear equation that describes the connection between alloy composition, melting point, and temperature (Tm):
The equation T=Tm −kC
Where:
The alloy has a melting point denoted by T.
C is the element's concentration in the alloy.
Tm is the temperature at which a pure metal, like lead or tin, melts.
k remains constant.
Global Regulatory Requirements:
Lead is toxic and can accumulate in the body as a result of chronic exposure. Contaminating land and groundwater, it is a hazardous waste product. The EU Restriction of Hazardous Substances regulation came into effect in 2006. Lead solder is now restricted in EU devices thanks to this rule.
European Union (EU):
European Union (EU) restricts the incorporation of lead and other toxic materials into electrical devices . In homogenous materials, the content cannot be more than 0.1% by weight according to the new limitations regulation.
United States:
While there is no federal RoHS rule, several states have imposed their own regulations. The proven dependability of lead solder leads to its exemption.
Conclusion:
The controversy over lead-free vs lead solder goes beyond a simple technicality. Progress towards a cleaner electronics sector, compliance and sustainability are the key issues. Due to the pervasiveness of electronics in our daily lives it is crucial to steer clear of items containing lead. Electronics assembly is one area where lead-free solder excels. But it isn't a good fit for aeronautical or medical applications. There may not be enough surface tension in lead-free soldered junctions to withstand impact.
This is not a big problem for PCB uses because the majority of electronics are not subject to harsh conditions. Use of lead-free solder has several advantages. It is crucial for manufacturers, engineers and enthusiasts to understand the important distinctions in composition. In order to educate them to make a decision. Understanding the key differences between lead and lead-free solder helps manufacturers, engineers, and hobbyists make informed decisions.
Keep Learning
Breaking Down PCB Pricing: How is the Cost Determined
PCB quote packaging involves gathering and organizing all the necessary details to estimate the cost of manufacturing a PCB. This process includes not only design specifications but also material selection, manufacturing methods, and engineering considerations. It goes beyond a simple financial estimate and provides a thorough engineering analysis to ensure the quote is accurate, feasible, and optimized for production. Every aspect affecting production such as material type, size, complexity, and prod......
Flex PCB Manufacturers for Compact Electronics: Sourcing Guide
When choosing a flex PCB manufacturer for your compact electronics application, be sure to consider not only their maximum trace density, maximum stackup thickness, maximum bend radius, and stiffener thickness, but also whether they routinely build such parts. Since a design based on the manufacturer's best-case fabrication limits may be very tight in terms of production yield and/or dimensional tolerances, and long-term reliability, particularly in compact devices where space may be limited and repea......
Quick Turn PCB: How to Get High-Quality Prototypes Fast
Printed Circuit Boards (PCBs) are a vital part of modern electronics, and the demand for faster and more efficient development made a quick turn PCB services extremly important. In this article, we will discuss what quick turn PCB is, its importance, the lead time for JLCPCB's quickturn PCB fabrication, how quick turn PCB can help businesses, and how to choose a good quick turn PCB manufacturer. What is Quick Turn PCB? Quick turn PCB refers to the process of manufacturing and delivering PCBs within a ......
How to Build a Bulletproof Bill of Materials for Flawless PCB Production
Have you ever sent a PCB design to be assembled only to receive an email requesting why you have not provided a part number or the package has not been matched? In that case, you are already aware that a single slip in your bill of materials will bring a flawless board down. Take a small CH32V003-based dev board consisting of 29 components distributed on 11 different footprints on a 2-layer copper PCB. It has an MCU, USB-C input, 24MHz crystal, USB-to-TTL bridge, indicator LEDs, and programming/GPIO h......
The True Cost of Custom PCBs: Understanding the Factors that Affect the Bottom Line
Key Takeaways Optimize Layout & Size: Simplify circuit design and keep board size within 100mm x 100mm for basic promo rates. Stick to Standard Specs: Use 1.6mm board thickness and 1 oz copper weight to avoid material surcharges. Respect DFM Limits: Maintain trace width/spacing ≥ 5/5 mil and via drills ≥ 0.3mm to prevent fine-feature fees. Select Low-Cost Finishes: Choose HASL over ENIG for prototypes unless fine-pitch BGAs are required. Printed circuit boards (PCBs) are integral to modern technology,......
Crafting Success: Choosing the Right PCB Manufacturer for Hobbyist
As a PCB hobbyist or engineer, finding a reliable and professional PCB manufacturer is crucial to ensure the success of your projects. The right PCB manufacturer can provide you with valuable guidance, access to advanced manufacturing technologies, and the support needed to excel in the dynamic world of PCB design and manufacturing. In this article, we will explore key characteristics to consider when selecting a PCB manufacturer, with a focus on professional instruction, customization options, qualit......