How AI is Revolutionizing PCB Design: A Comprehensive Guide
16 min
- Where AI is Being Applied in PCB Design
- Looking to the Future: Generating CAD Data
- How each layer is used
- Should I Use AI in My Board Design Process?
- Advantages of AI for PCB Design:
- Disadvantages of AI for PCB Design:
- How to Effectively Use AI for PCB Design
- How AI Optimizes PCB Design
- Challenges in PCB Layout
- How AI Helps With PCB Layout
- Challenges of PCB Manufacturing
- How AI Is Changing Circuit Board Technology
- AI Can Automate PCB Manufacturing
- Challenges in PCB Design
Your favorite machine learning, optimization, and generative AI algorithms may soon be used in your favorite PCB design program. Now that ChatGPT has become a household name and competitor companies are developing their own GPT equivalents (Claude, LLaMa, etc.), EDA startups are looking at how to leverage these tools to help PCB designers and engineers be more productive. With so many industries touched by automation and AI, it was only a matter of time before PCB designers would get their own tools.
Artificial intelligence (AI) is revolutionizing many industries, including printed circuit board (PCB) technology. From optimizing PCB layout and design to improving the surface mount manufacturing process, AI adds a game-changing element, more specifically, in terms of efficiency and precision.
Using artificial intelligence in manufacturing processes may provide higher quality and faster production times, reduce costs, and minimize errors. If you're interested in exactly how AI is changing circuit board technology in significant ways, learn more below.
Where AI is Being Applied in PCB Design
PCB design involves a multitude of tasks, ranging from circuit design to PCB layout and preparation for production. As of 2023, there is no single system that will handle all of your engineering and PCB design tasks. But the range of options available today is impressive, both in the design and manufacturing space.
Component selection or descriptions - Accuracy here varies wildly, but plugins are helpful for providing specific information or datasheets (see here). There are millions of components, and an AI-driven supply chain with tagged data could help with part selection.
Basic calculations - If you don't have formulas memorized, you can always query ChatGPT for the formulas or for an example calculation.
Datasheet questions using plugins - Internet search features allow users to pass datasheet URLs to a chatbot, so you can now use information from datasheets in other prompts.
For electronics designers and PCB designers, the biggest use case is the last point I mention above: analyzing datasheets. This hugely expands the scope of what you can do in a generative platform.
Looking to the Future: Generating CAD Data
I still think the future of AI in PCB design is direct generation of CAD data, including in the PCB layout. This could include generative placement of components, such as in groups (e.g., using the Rooms feature) as well as in critical spots for mechanical, thermal, or UX reasons. Once placed (both generatively and manually), your AI-based autorouter comes into play to route specific parts of the design. Finally, having a human-in-the-loop approach to qualify the outputs enables reinforcement learning so that only the best results remain part of the training set.
In my opinion, and in the opinion of other startups, a reinforcement learning approach is the best option for building AI-driven PCB design models. Any portion of a design that has some data associated with it (which is everything in a PCB layout) or that can be categorized can be used to build an AI model for PCB design.
AI-driven PCB design takes two components: building models and design optimization. Model building is all about creating a numerical model relating features in a PCB layout (component placement, routing, etc.) with design performance metrics, such as:
Power integrity specifications
Signal integrity specifications
Power output/consumption
Types of interfaces present in the design
How each layer is used
The more tagging applied to the design, the better. The biggest front-end task is categorizing and tagging your designs so that the training data is consistent to certain design domains. For example, if you want to generate a switching power supply layout, you shouldn't use a single-board computer as training data!
Once you have a generative model for a PCB domain, the system can generate CAD data and this can be examined by the PCB designer to verify placement, routing, constraints, and mechanical form factor. After tweaking the design manually, the design can be put back into the training set. One way to integrate modeling with optimization within a reinforcement learning method is outlined below.
Training: Data is input into a training dataset and is used to build a prediction model for a specific aspect of the PCB layout. This aspect could be the arrangement of circuit blocks, layer stackups, routing decisions, or other features.
Generated PCB data: The model can then be used to generate CAD data that attempts to conform to the constraints (PCB design rules) specified by the PCB designer. This could be placement or routing.
Human evaluation: A human designer would need to go back and check the results to ensure constraint conformance and manufacturability. This could involve manual inspection, simulation, etc.
Once a design is generated, evaluated, modified, and accepted, it can be added back into the training set as a new input. This reinforcement learning process allows the generative model to be continuously updated and tuned with acceptable designs.
As these design tools and workflows develop, rest assured that we'll be there to guide you through the brave new world of AI-driven PCB design. No matter what kind of product you need to design and build, make sure you use the complete set of PCB design features in Altium Designer®. To implement collaboration in today's cross-disciplinary environment, innovative companies are using Altium 365™ to easily share design data and put projects into manufacturing.
We have only scratched the surface of what's possible with Altium Designer on Altium 365. Start your free trial of Altium Designer + Altium 365 today.
Should I Use AI in My Board Design Process?
As with all technologies or innovations, when and if you should adopt them into your workflow is an important decision. This decision is further complicated by the sometimes inflated claims of the benefits that will be realized. Therefore, it is important to understand clearly the advantages and disadvantages of incorporating AI for PCB design into your process.
Yes, incorporating AI into your PCB design process can enhance efficiency, accuracy, and innovation. AI-powered tools can assist in component placement, routing optimization, and design rule checking, significantly reducing design time and human errors. Machine learning algorithms can analyze vast amounts of historical design data to suggest optimal layouts and improve signal integrity.
AI also helps with thermal management, power distribution, and manufacturing optimization by predicting potential issues early in the design phase. Automated design tools powered by AI can generate multiple layout options, allowing engineers to select the most efficient and cost-effective solution.
However, AI is not a complete replacement for human expertise. Complex designs still require engineering judgment, creativity, and domain knowledge. Additionally, AI-driven tools may have limitations in understanding unique design constraints and industry-specific requirements.
Integrating AI into your workflow can streamline processes, but it is best used as an augmentation tool rather than a full replacement for traditional methods. Engineers should leverage AI to handle repetitive tasks and analyze complex datasets while retaining control over critical design decisions.
Ultimately, using AI in board design depends on your project complexity, budget, and willingness to adopt new technologies.
Advantages of AI for PCB Design:
- Faster research
- Automating manual processes
- Better informed design decisions
Speed of research and results compilation is a major reason to employ AI. The amount of development time saved can be hours or days. For P & R tasks, automation can save weeks from a complex project. Another usage of AI is data aggregation and statistical analysis, which can translate into helpful suggestions for your design. However, AI for PCB design also can have disadvantages.
Disadvantages of AI for PCB Design:
- Inaccurate component information
- Limited design complexity
- Limited EDA Tool integration
The greatest concerns with using AI technology are not related to its mathematical principles and techniques. Machine learning algorithms; such as reinforcement learning, neural networking, and others, have been proven to be scientifically sound and effective at solving engineering problems. Issues arise when unreliable or unverified data is used, which leads to inaccurate results. Problem size and ease of integration can also be significant drawbacks.
Today, understanding the pros and cons is essential for making an informed decision about using AI for PCB design. With the pace at which development of AI software tools for circuit design is advancing, finding PCB design software without an AI engine may be the challenge in the near future.
How to Effectively Use AI for PCB Design
- Clearly understand what AI can and cannot do for your design process.
- Choose an AI program or application that easily integrates with your EDA tool(s).
- Ensure that any data sourced, for example component datasheet information, is from a reliable source.
If you're looking for CAD models for common components and accurate and implementable information, like how to effectively use AI for PCB design, Ultra Librarian helps by compiling all your sourcing and CAD information in one place.
How AI Optimizes PCB Design
AI is revolutionizing PCB layout and design by addressing many of the challenges associated with traditional methods. AI-powered solutions bring automation, efficiency and precision to the design process. This efficiency level helps increase productivity and the quality of the final PCB.
1. Automated Design Optimization
AI algorithms excel at analyzing vast amounts of data and performing complex calculations quickly. In PCB design, AI can optimize component placement and routing based on predefined design rules and objectives. They use historical design data and machine learning (ML) models, helping them suggest layouts that minimize signal interference. Engineers can use AI to improve thermal management and enhance performance with these insights.
2. Streamlined Workflow
AI tools can streamline the workflow by automating repetitive tasks that traditionally require manual intervention. For instance, AI algorithms can generate multiple design iterations in a fraction of the time it would take a human designer. This acceleration allows engineers to explore more design possibilities and select the most optimal layout sooner in the development cycle.
3. Predictive Analysis and Simulation
AI enables predictive analysis and simulation of PCB designs before physical prototypes are built. Engineers can use AI models to simulate electrical performance, thermal behavior and mechanical stress under various operating conditions. This capability reduces the need for extensive physical testing. As such, AI can also help lower development costs and speed up time-to-market (TTM). There are various ways of reducing PCB costs and turnaround times — AI is one of the many avenues.
4. Enhanced Accuracy and Reliability
Unlike human designers, AI algorithms do not suffer from fatigue or subjectivity. They consistently apply design rules and constraints with precision. AI's precision helps minimize the risk of errors and ensure PCB layouts meet stringent performance criteria. Their reliability translates into higher-quality PCBs with improved reliability and manufacturability.
5. Real-Time Collaboration and Feedback
AI can facilitate real-time collaboration between engineers by providing immediate feedback on design changes. Design teams can interact with AI systems in many ways. They can use AI to explore alternative design scenarios, evaluate trade-offs and make informed decisions based on data-driven insights.
Challenges in PCB Layout
Designing a PCB involves many difficult tasks, which determine the board's functionality and reliability. Here are the critical challenges faced in PCB layout design:
1. Component Placement
Proper component placement is crucial to ensure efficient routing, signal integrity and thermal management. Engineers must strategically position components to minimize signal interference, reduce noise and optimize the use of available board space.
2. Routing Complexity
Routing involves creating pathways, or traces, on the PCB to connect components electrically. Routing becomes increasingly challenging as PCBs become more densely packed with components and intricate circuitry. Engineers must navigate obstacles such as avoiding signal cross-talk, achieving impedance control, and maintaining signal integrity across different layers of the PCB.
3. Power Integrity
Ensuring power integrity involves managing power distribution networks (PDNs) to minimize voltage drops, noise and electromagnetic interference. Improper PDN design can lead to performance issues, reliability problems and even functional failures in the final product.
4. Design Rule Checks (DRC)
DRC involves verifying that the PCB design meets specific manufacturing and functional requirements. These checks include minimum trace widths, clearance between traces and components, solder mask clearances, and adherence to electrical constraints. Failing to comply with DRCs can result in manufacturability issues, costly rework or even non-functional PCBs.
How AI Helps With PCB Layout
The use of technology in PCB layout design brings many benefits and opportunities. Here's how AI and ML algorithms address the complexities and challenges inherent in traditional design processes:
1. Automated Design Optimization
AI algorithms can automate and optimize component placement and routing. By examining various aspects of PCB layout design — like design restrictions, electrical performance needs and thermal factors — AI can produce layouts that minimize signal interference. AI may even help lower power consumption and enhance board performance.
2. Predictive Analysis and Simulation
AI enables predictive analysis and simulation of PCB designs. Engineers can use AI-powered tools to simulate different characteristics and behaviors under various operating conditions. This capability helps identify potential design flaws early in the development cycle, reducing the need for costly physical prototypes and accelerating TTM.
3. Real-Time Design Assistance
AI tools can provide real-time assistance to engineers during the design process. For example, AI-powered design assistants can suggest optimal component placements, routing paths and layer configurations. Their recommendations are based on historical data and ML models. It's a collaborative approach that enhances design creativity and efficiency while ensuring designs meet performance targets.
4. Enhanced Design Verification
AI may enhance DRC capabilities by automating the verification process against design rules and specifications. AI algorithms can quickly identify potential violations — like spacing violations or incorrect trace widths — and provide actionable insights to engineers. This proactive approach minimizes design errors and can improve design quality.
5. Iterative Improvement
AI continuously learns from previous design iterations and user feedback, improving its design recommendations over time. Engineers can benefit from AI's ability to iterate quickly through design options, explore alternatives and refine layouts to achieve optimal performance and manufacturability.
6. Integration With CAD Tools
AI can also integrate with computer-aided design (CAD) tools commonly used in PCB design. This integration may improve the functionality of existing design software by adding AI-driven features. Examples of these features include layout optimization, design validation and automated documentation generation.
Challenges of PCB Manufacturing
PCB manufacturing involves intricate processes critical to producing functional and reliable circuit boards. Let's discuss the challenges faced in PCB manufacturing:
How AI Is Changing Circuit Board Technology
1. Inspection Bottlenecks
Traditional visual inspection methods can be time-consuming and run the risk of human error. Manufacturers must inspect PCBs for defects, such as soldering issues or component misalignment, which require meticulous attention to detail and can create bottlenecks in production throughput.
2. Quality Control
Ensuring consistent quality across PCB batches is essential but challenging. Variations in manufacturing processes, materials and environmental conditions may lead to defects that impact the performance and reliability of the final product.
3. Cost Management
PCB manufacturing costs can escalate due to factors like material wastage, rework required for defects and inefficient production processes. Effective cost management strategies are crucial to maintaining market competitiveness.
4. Lead Time Management
Meeting deadlines for PCB delivery is crucial in fast-paced industries. Effectively managing lead times requires a few responsibilities. These tasks can include coordinating with suppliers, optimizing production schedules and minimizing delays that can impact project timelines.
AI Can Automate PCB Manufacturing
AI can introduce advanced technologies that enhance PCB manufacturing efficiency, quality and cost-effectiveness:
1. Automated Visual Inspection
AI-powered visual inspection systems may significantly improve inspection accuracy and speed. Using ML algorithms, these systems can analyze images of PCBs to detect defects such as soldering defects, component misplacements or hairline cracks that human inspectors may miss. This automation reduces inspection time and boosts product quality.
2. Predictive Maintenance
AI can help with predictive maintenance in PCB manufacturing equipment. By analyzing real-time sensor data from machines involved in the surface mount manufacturing process, AI algorithms can predict equipment failures before they occur. This proactive approach minimizes unplanned downtime and maintenance costs and ensures continuous production flow.
3. Quality Assurance Enhancement
AI can continuously monitor manufacturing processes. ML models can analyze data from various production stages to identify trends, anomalies or potential issues early on. This capability allows manufacturers to implement corrective actions quickly, improving product consistency and reliability.
4. Cost Optimization
AI-driven analytics can help optimize manufacturing costs by identifying process inefficiencies. AI algorithms can analyze production data to optimize material usage, reduce scrap rates and improve yield rates. This data-driven approach helps manufacturers save costs without compromising product quality or performance.
5. Real-Time Decision Support
AI provides manufacturing personnel with real-time decision support. AI systems can analyze and interpret vast amounts of data, providing valuable insights into areas such as production scheduling, supplier selection and process optimization. This capability helps with agile decision-making that aligns with business objectives and market demands.
6. Enhanced Supply Chain Management
AI can help predict demand fluctuations and optimize inventory levels. Algorithms analyze historical data, market trends and other external factors to recommend optimal procurement strategies and mitigate supply chain risks. This proactive management reduces lead times and ensures timely delivery of PCBs to customers.
Challenges in PCB Design
Traditional PCB design processes have long relied on manual processes. These methods are effective, but they come with several challenges that can slow the design process, introducing errors that affect the final circuit board’s function and reliability.
1. Complexity and Time Consumption
Designing a PCB involves placing components and routing connections so they function correctly. This process becomes increasingly complex as circuits become more intricate and compact. Engineers must calculate trace widths, component placements and signal paths manually. This process is slow and prone to human error.
2. Trial and Error Iterations
Getting an optimal PCB layout often requires many iterations of trial and error. Engineers may need to repeatedly adjust component placements and routing to meet design specifications, ensure signal integrity and manage thermal considerations. Each iteration cycle can prolong the design phase and increase development costs.
3. Risk of Signal Interference and Heat Dissipation Issues
Incorrect placement of components or inefficient routing can lead to signal interference, noise or heat dissipation problems. These issues can degrade the PCB’s performance, reliability and even its longevity. If these problems arise, redesigns must be made, thus potentially delaying product launches.
4. Skill and Experience Dependency
Effective PCB layout and design require specialized knowledge and experience. As experienced engineers retire, there’s a growing concern about transferring this expertise to younger engineers with different practical knowledge.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......