This website requires JavaScript.
Coupons APP Download
Ship to
Blog

Solder Paste vs Flux: Key Differences, Uses, and How to Choose for Perfect Soldering

Published Feb 19, 2024, updated Mar 05, 2026

11 min

The manufacturing process that turns electronic circuits into working devices depends heavily on PCB assembly. Flux and solder paste are essential parts of this procedure. You need to be aware of their roles and how they help with successful PCB assembly as an electronics enthusiast, engineer, student, or professional.



What is Solder Paste?


Solder paste is a crucial material used in PCB assembly that facilitates the attachment of electronic components to the circuit board. It is a mixture of finely powdered solder alloy and flux. The solder alloy typically consists of a combination of tin and lead or other lead-free alternatives. The flux component in solder paste is responsible for removing oxidation from the metal surfaces and promoting the formation of strong and reliable solder joints.


Solder paste plays a vital role in the assembly process as it provides the medium for component attachment. It acts as a temporary adhesive, holding the components in place during the reflow soldering process. Additionally, solder paste ensures the proper wetting and bonding of the solder joints, contributing to the overall reliability of the PCB.



Solder Paste used in PCB assembly



What is Solder Flux?


Solder flux is a chemical compound used in soldering to remove oxide layers from the metal surfaces being joined. It prepares the surfaces for soldering by promoting the flow and adhesion of molten solder. Flux also helps to prevent the formation of new oxides during the soldering process.


There are different types of flux available, including rosin-based flux, water-soluble flux, and no-clean flux. Each type has its own characteristics and is chosen based on the specific assembly requirements and processes. Flux plays a critical role in ensuring the proper wetting and bonding of solder joints, improving the overall quality and reliability of the assembly.



A Container of Solder Flux


Solder Paste vs Flux: Comprehensive Comparison


AspectSolder PasteFlux
DefinitionA mixture of powdered solder alloy and flux in paste form.A chemical compound that removes oxides and promotes solder flow.
CompositionContains metal solder particles (Sn-Pb or lead-free alloys) + flux.Made of activators, resins, solvents (rosin-based, water-soluble, or no-clean).
Primary
Function
Supplies solder alloy and acts as a temporary adhesive for components.Cleans metal surfaces, removes oxides, and ensures proper wetting of solder.
Role in PCB
Assembly
Holds components in place before reflow; melts to form solder joints.Prepares pads and leads for bonding, preventing weak joints and voids.
Form/StateThick paste (mixture of flux + solder alloy).Available in liquid, gel, or paste forms.
Application
Method
Applied using stencil printing, dispensing, or syringe methods.Applied by brushing, spraying, dipping, or included in solder paste itself.
When UsedEssential in SMT (Surface Mount Technology) and reflow soldering.Used in both SMT and through-hole soldering (wave soldering, hand soldering, rework).
Key TypesLead-based solder paste, lead-free solder paste (SAC alloys).Rosin-based flux, water-soluble flux, no-clean flux.
Impact on
Reliability
Provides the alloy to form strong solder joints, ensuring electrical and mechanical connection.Improves solder joint reliability by cleaning surfaces and preventing oxidation during soldering.
LimitationsShelf life is limited; requires refrigeration; printing process sensitive to environment.Can leave residues (rosin or water-soluble need cleaning); improper choice may affect assembly quality.
Used Alone?Rarely used without flux
(flux is already part of solder paste).
Can be used independently in hand soldering or as additional support in reflow processes.
Thermal
Behavior
Melts during reflow to form solder joints, with controlled melting point depending on alloy composition. Does not melt; instead, it activates chemically at elevated temperatures to clean oxides and improve wetting.



Solder Paste and Flux: How They Work Together in PCB Assembly


Solder paste and flux work together in a complementary manner to achieve successful PCB assembly. Solder paste provides the necessary solder alloy and acts as an adhesive, holding the components in place during assembly. Flux, on the other hand, prepares the surfaces for soldering by removing oxides and promoting proper wetting.


During the reflow soldering process, the solder paste melts, creating a liquid phase that enables the formation of solder joints. The flux within the solder paste activates, removing contaminants and promoting the flow of molten solder. This combination of solder paste and flux ensures reliable and robust solder joints, leading to high-quality PCB assemblies.



Solder Paste Application Techniques


The accurate and consistent application of solder paste is crucial for achieving reliable solder joints. There are two primary techniques for applying solder paste: stencil printing and dispensing.


Stencil printing involves using a stencil with apertures that correspond to the solder paste deposition areas on the PCB. The solder paste is applied through the stencil onto the PCB, ensuring precise placement and controlled amounts of solder paste. Dispensing, on the other hand, involves using a dispenser to apply solder paste directly onto the PCB.


The selection of the appropriate application technique depends on factors such as board complexity, component density, and assembly requirements. Proper application techniques contribute to the uniform distribution of solder paste and minimize the risk of defects in the solder joints.


Further reading: Solder Paste Inspection (SPI): A Complete Guide to Process Control in SMT Assembly


Technician operating solder paste stencil printer for PCB assembly



Solder Flux Considerations


Flux is applied during various soldering processes, including wave soldering, hand soldering, and reflow soldering. The selection of the appropriate flux depends on the assembly process and requirements.


Wave soldering involves immersing the PCB into a molten solder wave, and flux is applied before the wave to prepare the surfaces for soldering. Hand soldering typically requires the use of flux-cored solder wire, where the flux is integrated into the wire. Reflow soldering relies on solder paste, which contains flux.


When selecting flux, considerations such as compatibility with the solder alloy, residue characteristics, and cleaning requirements should be taken into account. A reliable solder joint can be formed and the likelihood of flaws like solder bridges or inadequate wetting can be decreased by using the right flux and applying it correctly.

Further read: How to Apply Solder Flux When Hand Soldering Components


Engineer soldering electronic components on a PCB using flux and solder paste



How Solder Paste and Flux Affect Solder Joint Reliability


The quality and reliability of solder joints are crucial for the overall performance and longevity of electronic devices. Solder paste and flux play significant roles in ensuring the integrity of the solder joints.


To achieve mechanical strength and electrical conductivity, the solder joints must be properly bonded and wet. Solder paste and flux work together to facilitate the creation of robust intermetallic bonds, encourage flux activation, and eliminate oxides.


By using high-quality solder paste and flux, manufacturers can minimize the occurrence of defects such as voids, tombstones, and solder bridging. Robust solder joints contribute to the long-term reliability of the PCB assembly, reducing the chances of premature failures or intermittent connections.



Green circuit board with holes.



PCB Assembly Quality Control: Solder Joint Testing Methods


To ensure the reliability of PCB assemblies, quality control and testing are crucial steps. Inspection and testing methods are employed toevaluate the quality of solder joints and overall assembly. These methods include visual inspection, X-ray inspection, and electrical testing.


Visual inspection allows for the detection of visible defects such as solder voids, insufficient wetting, or solder bridges. Through the use of X-ray inspection, concealed flaws like voids or inadequate solder coverage can be found by obtaining a more thorough view of the solder joints.


Electrical testing, such as continuity testing and functional testing, assesses the performance of the assembled PCB. These tests verify the electrical connections and ensure the proper functionality of the circuit.


Solder paste and flux are integral to meeting industry standards and specifications for solder joint quality. By implementing stringent quality control measures and testing protocols, manufacturers can guarantee the reliability and performance of their PCB assemblies.




Circuit board shows labeled solder joints.


FAQs about Solder Paste vs Flux


Q1: How can I tell if a product labeled “solder paste” is actually just flux?

Mislabeling is a common issue, especially on some online marketplaces. A key distinction is that solder paste always contains finely powdered solder alloy mixed with flux, whereas flux alone is just a chemical cleaning agent. Solder paste typically appears gray or metallic because of the solder alloy, while flux tends to be amber, brown, or clear. To be sure, check the product specifications: solder paste will list an alloy composition (such as Sn63/Pb37 or SAC305), while flux products do not.


Q2: Can I use flux alone instead of solder paste for reflow soldering?

No. Flux and solder paste serve different purposes. Flux by itself only cleans oxides and improves wetting, but it does not contain the metal alloy needed to create solder joints. For reflow soldering in PCB assembly, you must use solder paste, since it provides both the solder alloy and flux in the right ratio. Using flux alone will result in cleaned pads, but no electrical or mechanical connections between the components and the board.


Q3: What form factors of flux are available and when should each be used?

Flux is available in several different forms, each suited for specific applications:

  • Liquid flux – typically used for wave soldering or large-area applications.
  • Flux pens – provide precise application for rework or touch-ups on small areas.
  • Gel or paste flux – thicker, stays in place, ideal for manual soldering of SMD components or reballing BGAs.
  • No-clean flux – leaves minimal residue and is preferred when post-solder cleaning is difficult.

Choosing the right flux form depends on your assembly method, level of precision required, and whether post-cleaning is possible.


Q4: Why does solder paste have limited shelf life and how can I extend it?

Solder paste has a relatively short shelf life—usually 3 to 6 months—because the metal particles can separate from the flux medium and the paste can dry out over time. Temperature and humidity also accelerate degradation. To extend shelf life, solder paste should be stored in sealed containers, kept refrigerated (usually 0–10 °C), and allowed to reach room temperature before use. Stirring or kneading the paste before printing helps restore uniform consistency. Using expired paste may cause printing defects, poor wetting, or unreliable solder joints.


Q5: Are there safety or board damage risks if using plumbing or industrial flux on electronics?

Yes, using the wrong type of flux can seriously damage a PCB. Plumbing or industrial fluxes are usually highly acidic and designed for copper pipes or mechanical joints, not delicate electronics. They can corrode PCB pads, leave conductive residues, and cause long-term reliability failures. For PCB assembly, always use fluxes or solder pastes specifically labeled for electronics. These are formulated to be non-corrosive, electrically safe, and compliant with industry standards such as IPC.


Q6: Is flux inside solder paste?

Yes. Solder paste is a mixture of finely powdered solder alloy and flux. The flux is included inside the paste to remove oxides and promote wetting during the soldering process. This combination allows solder paste to both hold components in place before reflow and create reliable solder joints during heating. Without flux, solder paste would not bond properly to the PCB pads or component leads.


Q7: What can I use if I don't have flux?

Ideally, always use flux designed for electronics to ensure reliable solder joints. If you don’t have flux available, the solder may still melt and bond, but the risk of poor wetting, oxidation, and weak connections increases significantly. Some people attempt to use substitutes like rosin from electronics-grade solder wire, but these are not as effective as dedicated flux. For PCB assembly and rework, using the correct no-clean flux, rosin flux, or water-soluble flux is strongly recommended for best results.


Q8: Why is my solder not sticking? Could it be a flux issue?

Yes, insufficient or degraded flux is a common reason why solder does not stick to pads or component leads. Without active flux, oxides remain on the metal surfaces, preventing the molten solder from wetting properly. Other possible reasons include dirty or oxidized pads, expired solder paste, or incorrect heating profiles during reflow. To troubleshoot, make sure you are using fresh solder paste or flux, clean PCB pads thoroughly, and apply the proper reflow temperature curve.



Conclusion: Solder Paste vs Flux: How to Choose the Right One for PCB Assembly


Solder paste and flux are both essential materials in modern PCB assembly, but they serve different roles in the soldering process. Solder paste provides both the solder alloy and flux needed to form reliable electrical and mechanical connections, while flux primarily improves solderability by removing oxidation and promoting proper wetting.


Understanding the difference between solder paste vs flux helps engineers select the right material for different manufacturing processes, whether in automated SMT assembly or manual soldering applications.


At JLCPCB, advanced SMT production lines and strict process control ensure accurate solder paste deposition and optimized flux activity for consistent, high-quality solder joints. This helps reduce assembly defects and improves overall PCB reliability.




Keep Learning