How to Avoid Shorts and Open Circuits in Dry Film Etching Process
5 min
- Maintaining Adequate Trace Width and Spacing
- Guidelines for Hatched Copper Pours
- Copper Pour Clearances and Design Verification
- Conclusion
- FAQ
When utilizing the dry film etching process, it is crucial to take precautions to prevent short circuits and open circuits in printed circuit boards (PCBs). JLCPCB emphasizes specific considerations to ensure the integrity and functionality of PCB designs. This article provides guidelines for maintaining adequate trace width and spacing as well as utilizing hatched copper pours effectively to avoid defects during the dry film etching process.
Maintaining Adequate Trace Width and Spacing
JLCPCB employs a dry film etching process, which requires careful attention to trace width and spacing. In the case of boards with 2 oz copper, a minimum trace width and spacing of 0.16/0.16 mm must be maintained, as specified in JLCPCB's official PCB manufacturing capabilities. This is essential to avoid the occurrence of shorts and open circuits caused by dry film fragments getting stuck between traces or being washed off thin traces during the etching process. Thicker copper layers (such as 2 oz) are more challenging to etch uniformly than 1 oz copper (which allows 0.10 mm minimum), making these minimum dimensions critical for high-yield production. To ensure reliable connections and prevent circuit discontinuities, any traces in a design that fall short of the specified width and spacing must be adjusted before fabrication.
Guidelines for Hatched Copper Pours
In the dry film etching process, specific focus must be given to hatched copper pours to prevent defects such as open circuits and shorts caused by dry film fragments. When utilizing hatched copper pours, it is crucial to consider the grid line width and spacing. JLCPCB recommends that both the grid line width and spacing should be equal to or greater than 0.254 mm to ensure the desired etching results. This minimum prevents dry film cracking and fragment adhesion, which can also affect subsequent solder mask adhesion.
If hatched copper pours are designed with insufficient width or spacing, it is advisable to either scale up the dimensions or consider making the copper pour solid. These guidelines are vital to mitigate the risk of dry film fragments causing disruptions or unwanted electrical connections during the etching process. For most modern designs, solid copper pours are preferred for superior reliability with dry film technology.
Copper Pour Clearances and Design Verification
Maintaining Proper Clearance in Copper Pours
Moreover, when implementing copper pours—whether hatched or solid—maintaining proper clearance from adjacent traces, pads, and vias is critical to prevent etching residues that could cause shorts. JLCPCB recommends a minimum clearance of 0.2 mm from standard traces and pads, or 0.5 mm for high-speed signal traces, when using solid copper pours. This extra spacing compensates for potential under-etching variations inherent in the dry film process, ensuring clean electrical isolation and reducing the risk of unwanted connections or open circuits in the final PCB.
Utilizing JLCPCB’s Free DFM Checker
To proactively identify and eliminate any violations of these dry film etching rules before submitting files for production, JLCPCB offers a free online DFM (Design for Manufacturability) checker at jlcdfm.com. By uploading your Gerber files, the tool automatically analyzes trace width, spacing, copper pour grid dimensions, and clearances against JLCPCB’s dry film capabilities—such as the 0.16 mm minimum for 2 oz copper and the 0.254 mm recommendation for hatched pours. This instant feedback allows designers to catch potential shorts or open circuits early, significantly improving first-pass yield and avoiding unnecessary fabrication revisions.
Conclusion
By adhering to JLCPCB's instructions and manufacturing capabilities, designers and manufacturers can significantly reduce the likelihood of short circuits and open circuits in PCBs during the dry film etching process. Maintaining adequate trace width and spacing, as well as properly configuring hatched copper pours (or opting for solid pours where possible), ensures the integrity and functionality of the PCB design. These precautions, combined with JLCPCB's advanced dry film technology, contribute to the production of reliable and high-quality PCBs, promoting efficient circuit performance and reducing the need for rework or troubleshooting.
FAQ
Q: What is the minimum trace width and spacing for 2 oz copper boards using JLCPCB’s dry film etching process?
The minimum is 0.16/0.16 mm. Thinner traces risk dry film fragments causing shorts or open circuits.
Q: Why does JLCPCB require a minimum grid line width and spacing of 0.254 mm for hatched copper pours?
Smaller grids can cause dry film cracking and fragments, leading to etching defects and reliability issues.
Q:Should I use solid copper pours instead of hatched ones?
Should I use solid copper pours instead of hatched ones?
Q: What clearance is required between copper pours and adjacent traces, pads, or vias?
Maintain at least 0.2 mm for standard traces/pads or 0.5 mm for high-speed signals to prevent etching residues and shorts.
Q: How can I check my design for dry film etching violations before ordering?
Upload your Gerber files to JLCPCB’s free DFM checker at jlcdfm.com for instant analysis of trace width, spacing, pours, and clearances.
Q: Does the dry film etching process apply the same rules to all copper weights?
No. 1 oz copper allows 0.10 mm minimum, while 2 oz requires 0.16 mm due to thicker copper being harder to etch uniformly.
Keep Learning
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......
The Role of PCB Test Fixtures in High-Volume Manufacturing
In high-volume manufacturing of Printed Circuit Boards (PCBs), quality, efficiency, and reliability are paramount. One of the most crucial tools in achieving these goals is the PCB test fixture. These fixtures play a vital role in ensuring that PCBs meet the required performance standards before they are integrated into electronic devices. This article delves into the importance of PCB test fixtures, their types, and how they contribute to the efficiency of high-volume manufacturing. Specialized and c......
SMT or Through Hole Technology?Which is Better for Your Project?
When designing and manufacturing electronics, one of the most important steps is selecting the appropriate assembly method. Nowadays we have through-hole technology and surface mount technology, which become the industry standards and are the two main approaches. The surface-mount technology (SMT) uses components that are perfectly aligned with the PCB surface. On the other hand through-hole technology (THT) uses leads that are placed into pre-drilled holes in the PCB and thereafter soldered. Consider......