4 Layer vs 6 Layer vs 8 Layer PCB: How to Choose the Right Stackup
6 min
- What is a Multilayer PCB?
- PCB Stackup Basics: Terms and Design Goals
- Typical 4-Layer PCB: Stackup, Advantages, and When to Use
- Typical 6-Layer PCB: Stackup, Advantages, and When to Use
- Typical 8-Layer PCB: Stackup, Advantages, and When to Use
- Side-by-Side Technical Comparison
- Cost and Manufacturing Notes
Random selection of layers in electronics may lead to serious signal integrity issues. That's why we always design our stackup before designing the PCB. Stackup decides the type of PCB and how it gonna perform under high-frequency conditions. There are a lot of things that directly affect the stackup of the PCB, related to impedance matching, routing density, signal and power integrity, electromagnetic compatibility (EMC), and cost. Knowing the requirements before design and the most critical components in the PCB also becomes equally important. Optimal layer count depends on functional needs and manufacturability constraints. This article explains the principles behind stackups, compares 4-, 6-, and 8-layer boards, and provides a practical decision guide on how to choose the layers.
What is a Multilayer PCB?
A multilayer PCB stacks alternating copper layers (signal and plane layers) separated by dielectric (cores and prepregs). Talking about only 2 layers, we usually route signal and power traces as mixed ones, but as we increase the number of layers, signals are not possible to route at each plane. In the internal layers, typically continuous power and ground planes for low-impedance distribution and EMI shielding are routed. The outer layers are usually used for component placement and routing. For professional guidance on stackup planning and layer usage, manufacturers and EDA resources provide typical examples and recommendations.
PCB Stackup Basics: Terms and Design Goals
Key terms and goals to keep in mind:
⦁ Signal Layer: The layer that carries routed traces. Surface layers are usually for parts and dense routing.
⦁ Ground Plane: These are the continuous copper planes used as a reference, return path, and EMI shield.
⦁ Power Plane: Dedicated copper plane for power distribution; when adjacent to ground, it forms a plane pair with excellent decoupling.
⦁ Impedance Control: Maintaining a target differential or single-ended impedance by controlling trace geometry and dielectric thickness.
⦁ Coupled Planes: Adjacent power/ground planes reduce loop inductance and improve PDN (power distribution network) performance. Best practices recommend putting power and ground planes next to each other.
Typical 4-Layer PCB: Stackup, Advantages, and When to Use
Typical 4-layer stackup (common):
⦁ Layer 1 (Top): Signal + components
⦁ Layer 2: Ground plane
⦁ Layer 3: Power plane/Ground plane
⦁ Layer 4 (Bottom): Signal + components
Why choose a 4-layer board?
A 4-layer board is used most of the time in embedded systems and antenna-related applications, where, due to some microcontroller and BLE, the routing becomes denser. At the same time, we also have to consider the impedance matching. It is quite Straightforward to fabricate, and the technology is well-matured for controlled impedance design. Some more applications can be consumer electronics, power supplies where separate planes help decoupling, and many IoT/microcontroller products.
Although 4 layers can not accommodate more signals, when it comes to routing of high-pin-count BGAs or dense QFNs. For very high-speed (>1–2 GHz) or highly noise-sensitive designs, a 4-layer board may lack the plane pairs and isolation.
Typical 6-Layer PCB: Stackup, Advantages, and When to Use
Common 6-layer stackup examples:
⦁ Top (Signal) — GND — Signal — Signal — PWR — Bottom (Signal)
⦁ Top (Signal) — GND — Signal — PWR — GND — Bottom (Signal)
The first one is good for power integrity, but the 2nd one gives better noise immunity.
Why choose a 6-layer board?
A 6-layer board has extra internal signal layer(s) and additional plane(s), which let you route more layers adjacent to a plane for controlled impedance and short return paths. You can add shielding planes and split routing to reduce emissions. It becomes more convenient when the design has multiple high-pin ICs (BGAs), mixed-speed busses, or requires many differential pairs. This type of stackup is used for high-end FPGA prototyping and DSP controllers.
It will increase the cost relative to 4-layer boards (material and process steps increase). Fabrication complexity also rises with layer registration, sequential lamination, and via processing (e.g., blind/buried vias if used), which can add lead time. Choose a good manufacturer that has better capabilities. JLCPCB has been producing 6-layer PCBs for 5-6 years, and over this time, it has gained expertise in the region.
Typical 8-Layer PCB: Stackup, Advantages, and When to Use
Example 8-layer stackup:
⦁ L1 (Top): Signal/Components
⦁ L2: Ground
⦁ L3: Signal (routing)
⦁ L4: Power
⦁ L5: Power (or split plane)
⦁ L6: Signal (routing)
⦁ L7: Ground
⦁ L8 (Bottom): Signal
Why choose an 8-layer board?
It is Best for high-speed/high-density designs because multiple plane pairs let you place controlled impedance pairs adjacent to reference planes. It has superior EMI performance and PDN stability, and multiple return planes and plane pairing reduce loop area and radiated emissions. 8-layer PCBs find application in servers, telecom/5G radio units, high-speed data converters, and aerospace/defense systems.
Higher number of layers and processing costs are usually higher because they take potentially longer lead times. Careful symmetry and material selection are needed to prevent warpage. If not designed well, the 8-layer one gives the performance of 2 2-layer PCB.
Side-by-Side Technical Comparison
Key Design Considerations (Signal, Power, EMI, Thermal)
Signal Speed & Return Path: when the signal is travelling as DC, the return path can be the nearest ground, but as the frequency increases, the signal travels in the dielectric, and the PCB becomes a waveguide structure, and the return path should trace back the actual path; otherwise, the signal integrity degrades.
Plane Pairing: Pair power and ground planes closely to form a capacitance that damps PDN impedance. Adjacent plane pairs reduce EMI and improve decoupling.
Impedance Control: For differential pairs, control dielectric thickness, trace width, and spacing according to fabricator stackup tables. Use your CAD tool’s stackup manager to target impedances.
Thermal Management: More layers help distribute heat (internal copper planes act as spreaders), but thicker copper and thermal vias are often necessary for power dissipation.
Cost and Manufacturing Notes
Layer count is a major cost driver, but not the only one; board area, copper weight, and number of routed layers matter too. Many fabs quote that moving from 4→6 or 6→8 layers increases cost roughly 30–40% per step, but actual numbers depend on volume and the fab’s process flow. Small-volume prototype runs magnify layer-cost effects: prototyping an uncommon layer count (e.g., small-run 6-layer) can be disproportionately expensive versus larger production runs. Community experience and industry Q&A highlight that 6-layer mid-volume pricing can be unexpectedly high due to lower fab throughput for that class.
Conclusion
⦁ Budget + simple routing: 4-layer.
⦁ For balanced performance and cost: 6-layer.
⦁ For the highest performance, high-density, strict EMI/PDN needs: 8-layer.
Layer count directly depends on the type of project; we always design for the best possible number of layers. If not possible, then we have to move to bigger stackups. If cost is not taken into account and we need the best performance, then it is better to go with a higher layer design, which also reduces the crosstalk of signals.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Design Guidelines for PCB Using FR4 Substrates
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
Via Stitching Guide : Core Functions, Pitch Rules & Placement
key takeaway Core Purpose: Ties ground layers together to cut EMI, reduce impedance, and shorten return paths. Pitch Rules: Space vias at λ/10 for ground grids and λ/20 for edge rings and shielding fences. Layer Transitions: Place stitching vias adjacent to signal vias to minimize return current loop area. Avoid Over-Stitching: Overuse perforates power planes, alters trace impedance, and increases drilling costs. DFM Control: Follow hole spacing rules, tent non-test vias, and maintain proper edge copp......
Relay Pinout Explained: Diagrams, Pin Functions & Multimeter Testing
Key Takeaways Pin functions: A standard electromechanical relay has two coil pins, and each pole adds a common (COM), normally open (NO), and normally closed (NC) pin. Viewing side: Relay footprints are often drawn in bottom view, with the pins facing you. When a drawing does not state its view, confirm NC and NO with a continuity check. Relay Pin Count: A 5-pin relay is typically SPDT, a 4-pin relay is usually SPST, and an 8-pin relay is commonly DPDT. However, pin arrangements can vary between PCB, ......
How to Connect and Choose a Flyback Diode for a Relay
Key Takeaways Diode Placement: Connect the flyback diode across the relay coil, with its cathode connected to the positive side and its anode to the negative side. Why It Matters: When the relay switches off, the diode provides a safe path for the remaining coil current, preventing a high-voltage spike that could damage the transistor. Choosing the Right Diode: Select a diode with a reverse-voltage rating above the coil supply voltage and a forward-current rating suitable for the coil current. Common ......
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Reliable BMS Boards Start With Quality PCB Manufacturing
Key Takeaways Dual Duty: BMS PCBs handle heavy currents and millivolt sensing simultaneously, requiring strict layout isolation. Power & Heat: Currents over 10A need 2 oz+ copper pours with via stitching to drop resistance and heat. Clean Sensing: Kelvin differential routing and split grounds prevent load noise from corrupting cell voltage readings. Materials & Finish: High-Tg FR-4 and ENIG surface finishes ensure heat tolerance and flat mounting pads. DFM & Testing: Design for heavy-copper etch toler......
What is Solder Mask and How Does it Impact Your PCB Designs?
Solder mask may not be the most exciting topic in PCB manufacturing, but it's definitely one of the most crucial. Without proper solder mask, your Printed Circuit Boards (PCB's) could suffer from shorts, bridges, corrosion, and other costly and time-consuming issues. So, if you want to ensure the quality, reliability, and longevity of your electronic products, you need to know everything about solder mask - from it's purpose and types to it's application and design implementations. In this ultimate gu......