Rogers vs PTFE vs Teflon: Choosing the Best PCB Laminate for High-Frequency Design
5 min
- Why Material Choice Matters in PCB Design
- Understanding the Materials
- Practical Impact: Transmission Line Example
- Choosing the Right Material
- Conclusion:
FR4, being the most popular one, is not always used in high-frequency PCBs because this PCB laminate can degrade the signal performance at high frequencies. Not because they consist of any wrong conduction material, but the reality lies in the substrate dielectric properties. The dielectric itself attenuates the signal at high frequency. So, after a lot of research in this area, we got some really good materials. The three alternatives for high-performance PCBs are Rogers, PTFE, and Teflon laminates. They offer better dielectric control, lower signal loss, and superior thermal stability. But they differ a lot from the cost perspective from standard FR4. In this guide, we will get through:
- Basics of Rogers, PTFE, and Teflon laminates.
- Compare their dielectric constants, losses, and thermal performance
- Provide a detailed design example showing how material choice impacts a PCB trace for RF use.
Why Material Choice Matters in PCB Design
Two key electrical properties of a laminate define how it will behave in high-frequency circuits:
1. Dielectric Constant (Dk or εr):
It determines the speed of signal propagation. Lower the value of Dk means faster signal speed, longer wavelength. The dielectric constant of a material also affects impedance calculation for traces. Rogers typically offers Dk = 2.2–6.5, PTFE/Teflon often ~2.1.
2. Loss Tangent (Df or tan δ):
It represents dielectric losses (how much RF energy is lost as heat). Lower loss tangent means higher efficiency. A table below is given for all FR4, Roger, and PTFE for comparison:
● FR-4: ~0.015–0.02 at 1 GHz
● Rogers RO4350B: ~0.0037
● PTFE/Teflon: ~0.0002–0.0009
Understanding the Materials
1. Rogers Laminates:
Rogers Corporation produces a wide range of high-frequency PCB laminates (e.g., RO4000, RO3000 series). The composition includes hydrocarbon-ceramic or PTFE composites.
Because of the laminate properties, it is excellent from hundreds of MHz into tens of GHz due to low losses. Rogers has better stability to heat than any other high-frequency material. They are particularly used in radar, satellite, and precision RF technologies.
2. PTFE (Polytetrafluoroethylene) Laminates
It is a type of polymer with an extremely low dielectric constant variation over frequency. It has the lowest losses among all but is more affected by heat. It has very good electrical signal handling properties, but is mechanically very soft in nature, because of which the copper layer may expand or contract as per temperature. It is commonly used in medical and radar applications.
3. Teflon Laminates
Teflon is a brand name for PTFE (registered by DuPont/Chemours). In PCB terminology, "Teflon boards" are usually PTFE-based PCBs. Same low-loss, low-Dk characteristics as PTFE, but “Teflon” often refers to pure PTFE or PTFE composites. They need special manufacturing processes due to their softness. And commonly used in very high-frequency microwave boards (>10 GHz), aerospace communication.
Practical Impact: Transmission Line Example
Let’s take a real-world example: Designing a 50 Ω microstrip trace at 10 GHz. Let the thickness of the PCB be 0.8mm and the copper thickness if 35 μm. We’ll calculate the trace width required for 50 Ω impedance.
1. Case A: Rogers RO4350B
Dk = 3.48, Df = 0.0037, Using microstrip impedance formulas:
● Required width ≈ 1.6 mm
● Attenuation ≈ 0.26 dB/inch
2. Case B: PTFE/Teflon
Dk = 2.1, Df = 0.0005, Using microstrip impedance formulas:
● Required width ≈ 2.45 mm
● Attenuation ≈ 0.04 dB/inch
3. Case C: FR-4 (for comparison)
Dk ≈ 4.4, Df ≈ 0.017, Using microstrip impedance formulas:
● Required width ≈ 1.35 mm
● Attenuation ≈ 0.82 dB/inch (significant signal loss at 10 GHz)
Lower Dk means wider traces for the same impedance. This can impact board real estate. PTFE/Teflon drastically outperforms FR-4 and even Rogers for ultra-high frequency due to extremely low loss tangent. Rogers is easier to process than pure PTFE/Teflon.
Choosing the Right Material
When to Choose Rogers:
● Mid- to high-frequency designs up to ~20 GHz.
● Need a balance of performance and manufacturability.
● Mixed-signal boards with both RF and digital sections.
When to Choose PTFE/Teflon:
● Ultra-low loss needed (radar, satellite comms).
● Frequencies >20 GHz.
● High reliability in extreme conditions (space).
Conclusion:
The decision between Rogers, PTFE, and Teflon comes down to:
● Frequency and loss budget
● Manufacturing capability
● Budget
● Mechanical constraints
All these are discussed in a very detailed format in this blog. For many RF designers, Rogers RO4350B is the “sweet spot” for up to 20 GHz. For bleeding-edge, ultra-low-loss systems, PTFE/Teflon remains unmatched. With high-frequency material, we will always encounter some fabrication challenges.
Keep Learning
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......