How to Select the Best Materials for Your Flexible PCB Designs
5 min
- 1. Substrate Materials: The Foundation of Flexibility
- 2. Adhesive Systems: Bonding the Layers
- 3. Protective Coatings: Coverlays & Overlays
- Conclusion:
Flexible printed circuit boards (Flex PCBs) have revolutionized the electronics industry. Now we can pack the circuit in a small housing space with highly compact, lightweight, and flexible form factors. FPCs are everywhere from wearable devices to medical implants and aerospace systems. These circuits rely on special materials that offer the right balance of mechanical flexibility and electrical performance.
When designing a Flex PCB, choosing the right combination of substrates, adhesives, and coatings is crucial. We have mastered the rigid PCBs and there is a lot of information, but FPC design still lacks the sector. The materials form the backbone of the circuit and directly influence its reliability. In this article, we explore the most commonly used materials and offer guidelines to help you make material choices based on your application needs.
1. Substrate Materials: The Foundation of Flexibility
The substrate is the base layer of a Flex PCB, the “flex” in flex circuits. It supports the copper traces and plays a key role in determining the mechanical and thermal properties of the board. There are 3 major types of materials used in FPCs:
1) Polyimide (PI): The Industry Standard
2) Polyester (PET): A Cost-Effective Alternative
3) PTFE (Teflon) and LCP (Liquid Crystal Polymer)
1) Polyimide (PI):
As FR4 in rigid PCB dominates the 70% and becomes an industry standard for low cost and hobby PCB manufacturing, the same role polyamide plays in FPC. Polyimide is the most widely used substrate material in Flex PCBs due to its excellent flexibility, thermal resistance, and dielectric properties. It is mostly used in low frequency consumer electronics. Some of the key benefits are listed below:
⦁ High temperature tolerance (up to 260°C short-term)
⦁ Excellent dimensional stability
⦁ Good chemical and solvent resistance
2) Polyester (PET):
Polyester is more cost-effective than PI and suitable for less demanding applications. This is mostly used in fully optimized circuits to lower down the production cost. It has lower thermal resistance (melting point ~260°C), limited use in high-temp soldering processes. Some use cases include: Wearables, disposable electronics, low-power sensors
Key Benefits:
⦁ Good dielectric properties
⦁ Lower moisture absorption
⦁ Cost-efficient for high-volume, low-stress applications
3) PTFE (Teflon) and LCP (Liquid Crystal Polymer):
PTFE comes with the best dielectric properties, it is the most expensive material. It is used in niche applications where high-frequency signal integrity or extreme chemical resistance is required. Mostly in research applications, aerospace and medical implants. The table of comparison of all the properties with other two materials is given in the first section.
2. Adhesive Systems: Bonding the Layers
Adhesives are used to bond the copper foil to the substrate and also to attach coverlays and stiffeners. The choice of adhesive affects not just adhesion strength but also flexibility and thermal stability. Here are 3 type of adhesives/methods which are widely used for bonding:
⦁ Acrylic Adhesives
⦁ Epoxy Adhesives
⦁ Adhesiveless Constructions
1) Acrylic Adhesives:
Acrylic adhesives are thermoplastic or thermosetting polymer adhesives based on acrylic resins. In flexible PCB manufacturing, they are commonly used to bond copper foil to polyimide or polyester substrates. These are used in general-purpose Flex PCBs in industrial and consumer products. But Prone to outgassing and may absorb moisture over time. Some key benefits are:
⦁ Excellent adhesion and flexibility
⦁ Good thermal endurance up to ~150°C
2) Epoxy Adhesives:
They are used in high thermal resistance and chemical durability critical situations. They offer excellent bonding strength. Can withstand temperatures up to 180°C or higher, making them ideal for demanding environments. Some key benefits are:
⦁ Higher thermal stability than acrylic
⦁ Good resistance to chemicals and solvents
3) Adhesiveless Constructions:
In some high-reliability applications, manufacturers use adhesiveless base films. In this process the copper is laminated directly onto the substrate through casting or sputtering. These are highly accurate but costly methods, used in high density PCBs and with low pitch component pads. Some benefits include:
⦁ Thinner construction
⦁ Improved dimensional stability
⦁ Better signal integrity for high-speed circuits
3. Protective Coatings: Coverlays & Overlays
Coverlays serve as protective layers that insulate and shield copper circuitry from environmental damage. Flex PCBs often use coverlays instead of traditional solder masks. There are 2 types of coverlay coatings available:
⦁ Polyimide Coverlay + Adhesive
⦁ Liquid Photoimageable Solder Mask (LPI)
1) Polyimide Coverlay + Adhesive
It comes with a layer of polyimide film pre-coated with adhesive which provides excellent mechanical strength and insulation. It can withstand repeated flexing without cracking.
2) Liquid Photoimageable Solder Mask (LPI)
LPI is similar to solder masks on rigid PCBs but adapted for Flex PCBs. It is compatible with automated PCB manufacturing and easy to apply for pine pitch components.
4. Other Considerations in Material Selection
Thermal Requirements:
Choose the material that can withstand thermal cycling, and prolonged exposure to elevated temperatures. Polyimide and epoxy systems generally perform well under these conditions.
Mechanical Flexing:
The flex cycle and time of FPC matters; dynamic-flex applications require thin and highly flexible substrates. Thicker constructions are better suited for static-flex designs.
Electrical Performance:
For signal integrity and high speed applications choose a material with low dielectric losses. High-frequency and impedance-controlled designs benefit from low-dielectric constant materials like PTFE.
Conclusion:
Material selection in Flex PCB design isn’t one-size-fits-all. Each application from wearables to aerospace systems has unique requirements in terms of flexibility, thermal issues and signal integrity. Choosing the right substrate, adhesive, and protective layer is one of the main tasks of an electronics engineer. By understanding the strengths and limitations of different materials, engineers can design Flex PCBs that not only meet but exceed expectations in their intended use cases.
If you’re ready to bring your Flex PCB designs to life, JLCPCB offers state-of-the-art manufacturing, competitive pricing, and fast turnaround — from single prototypes to large-scale production.
Keep Learning
Understanding PCB Laminates Materials, Types, and Why They Matter
A PCB is a flat board made of a non-conductive substrate material with conductive pathways and components attached to it. One of the critical components of a PCB is the PCB laminate. A typical laminate PCB consists of a core material, such as fiberglass or composite epoxy. So what it actually do is ● Provides structural support ● Improves Signal Integrity ● Bond the layers to the core material The fiberglass layers are stacked on top of each other and pressed together with heat and pressure to create ......
Why UL94 V0 Matters for Safe and Reliable PCB Manufacturing
Key Takeaways UL94 V0 is the highest flame rating for PCB materials, requiring self-extinguishing within 10 seconds with no flaming drips. It greatly reduces fire risk and has become the de facto standard for safe, reliable PCBs in consumer, industrial, automotive, and medical applications. JLCPCB offers UL94 V0 compliant FR4 and high-Tg materials by default, ensuring regulatory compliance (UL, CE, CCC) and long-term reliability without compromising performance or budget. Never sacrifice V0 rating for......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
PCB Material Guide : Types, Selection, and Impact on Performance
If PCB materials could talk, FR-4 would probably say, "I run 80% of the electronics industry, and still nobody appreciates me." Rogers would boast, "I'm expensive because I'm special," while Polyimide would flex literally and say, "I bend, but I don't break." The purpose of this blog is to introduce you to the types of PCB substrates available to you and how those materials affect your PCB's performance, thermal stability, signal integrity, and overall longevity. The choice of PCB material will be bas......
The Critical Role of Copper Peel Strength in Durable PCB Performance
Key Takeaways Standard Test: Measured via the IPC-TM-650 90° pull test in N/mm. Core Function: Prevents pad lifting and delamination under thermal stress and CTE mismatch. Foil Types: ED foil provides higher adhesion; RA foil yields lower signal loss. Material Benchmarks: Standard FR4 averages 1.0–1.4 N/mm, while High-Tg FR4 achieves 1.2–1.6 N/mm. Design Tips: Add teardrops, eliminate unsupported copper slivers, and perform DFM checks. Ever wonder what's making the copper stay put on your circuit boar......
Navigating Standard PCB Thickness: A Step-by-Step Guide to Selecting the Ideal Thickness for Your PCB Prototype
The thickness of a printed circuit board (PCB) may seem like a small detail, but it plays a crucial role in the performance and reliability of your electronic devices. Standard PCB thickness has become an industry norm, offering a range of benefits that impact mechanical stability, electrical performance, thermal management, and component compatibility.In this article, we will be taking a deep look at why the varying thickness of your PCB matters and provide you with a guide to choosing the right thic......