Rogers PCB & PTFE PCB: High Frequency PCB is available on JLCPCB
Product Update
Mar 09, 2023- The following specifications are currently supported by high frequency PCBs on JLCPCB
- Specifications for Rogers PCB on JLCPCB
- Specifications for PTFE Teflon PCB on JLCPCB
- High Frequency PCB, What Is It?
- How to Choose a High-quality High Frequency PCB
- Advantages of Rogers PCB
- Advantages of PTFE Teflon PCB
Recently, we have received lots of valuable feedback from our beloved customers, who are very eager to order high frequency PCBs from us. After unremitting efforts, we can finally bring you good news: Right now, Rogers PCB and PTFE Teflon PCB are both available on JLCPCB, and you can easily order high-quality high frequency PCBs by choosing the right base material on the website. Due to large-scale production capabilities, we can offer a special price for both HF base materials within 10cm*10cm 5pcs, that is Rogers PCBs start from $99.5, and PTFE PCBs from $50.5. Save you more than $100 compared to other HF PCBs on the market.
The following specifications are currently supported by high frequency PCBs on JLCPCB
- Base material: Rogers, PTFE Teflon
- Layer: 2 layers
- Soldermask: Green
- Silkscreen: White
- Outer Copper Weight: 1 oz
Specifications for Rogers PCB on JLCPCB
- PCB Thickness:0.51/0.76/1.52
- PCB Laminates: RO4350B (Dk=3.48, Df=0.0037)
Specifications for PTFE Teflon PCB on JLCPCB
- PCB Thickness:0.76/1.52
- PCB Laminates: ZYF255DA(Dk=2.55, Df=0.0018)/ ZYF265D(Dk=2.65, Df=0.0019)/ ZYF300CA-C(Dk=2.94, Df=0.0016)/ ZYF300CA-P(Dk=3.00, Df=0.0018)
High Frequency PCB, What Is It?
High frequency PCBs, also known as HF PCBs, are special circuit boards with high electromagnetic frequencies that provide faster signal flow rates and up to 100 GHz frequency ranges, typically applicate to high-speed designs, high reliability and complex design, radio frequency (RF), microwave, wireless communication devices, and telecommunications. Generally, high frequency PCB has a lower dielectric constant and lower dissipation factor. It is a good choice for highly complex electronic devices.
How to Choose a High-quality High Frequency PCB
1.Choose the base material with appropriate Dk/Df. PCBs with lower Dk have faster phase velocities than boards with higher Dk. For circuits that are sensitive to delay accuracy, such as high-speed digital circuits, which may be affected by transmission lines with different phase speeds or transmission delays, in this situation, more attention should be paid to the Dk value of the PCB base material.
Also, a PCB base material with a higher Dk produces a smaller wavelength at a certain frequency, which results in a smaller circuit size on PCB.
2.The coefficient of thermal expansion of the substrate is preferably consistent with that of the copper foil. The inconsistency might cause the copper foil to separate when the temperature changes greatly.
3.Try to choose PCBs with better heat resistance, chemical resistance, and deformation resistance.
Advantages of Rogers PCB
Rogers-RO4350B: This material is a strengthened glass hydrocarbon/ceramic material with a dielectric constant of 3.48 at 10GHz, which makes it commonly used in high-frequency power amplifier designs. The RO4350B laminate has a low Z-axis coefficient of thermal expansion (CTE), which ensures high stability of multilayer circuits interconnected by plated through holes (PTH). (The thickness of the finished product is 0.6/0.9/1.65mm in three specifications).
Features of Rogers PCB:
- Glass-reinforced Hydrocarbon and ceramic dielectric
- Volume manufacturing process
- Excellent high-frequency performance
- Low Z-Axis expansion, excellent dimensional stability
- Integrated thin film resistor benefit
- CAF resistant
Typical Applications:
- Global communication system
- High reliability and complex multi-layer circuits
- Wireless communication devices
Advantages of PTFE Teflon PCB
PTFE Teflon PCB has outstanding comprehensive performance in practical use and is an ideal material choice for high-complexity and high-reliability designs. It has good temperature resistance, strong heat dissipation, excellent dielectric properties, and good mechanical stability. Very durable in use and can withstand a certain amount of oxidation and UV rays, so it is also a cost-effective option.
How to order Rogers PCB & PTFE Teflon PCB on JLCPCB
1.Upload the Gerber file to the website.
2.Select 'Rogers' or 'PTFE' according to your needs.
3.Select 'PCB Thickness' and 'PCB Laminates'
4.Select other specs you prefer.
5.Save to the cart and checkout
JLCPCB always aims at making innovation easier for every engineer & maker. Due to large-scale capabilities, JLCPCB is able to offer high-quality PCBs at a very favorable price, saving your budget for more innovative possibilities.
Get your high-quality High Frequency PCBs on our quote page.
Recent News
• JLCPCB Enhances Lead-Free OSP PCB Surface Finish with New Chemistry
Oct 26, 2026
• JLCPCB Officially Launches HDI PCB Manufacturing Services
Nov 09, 2026
• JLCPCB High Multilayer PCB Lead Time Update
Aug 26, 2026
• JLCPCB Launches Compliant Overseas Component Consignment Service
Aug 13, 2026
• JLCPCB Launches OSP Starting from 2-Layer PCBs: High Quality at No Extra Charge
Jul 31, 2026