The Importance of Drill Drawings in PCB Production
6 min
- Types of Drill Holes:
- How Drill Files Are Arranged in a Gerber Package:
- Drill Data Given to Machine:
- What a Drill Table Consists of?
- NC Drill Chart File:
- How Drill Drawings Help Engineers During Fabrication:
- Conclusion:
In the realm of printed circuit board (PCB) manufacturing, drill drawings are often overlooked yet critically essential components of the design process. They act as a roadmap for accurate hole placement and dimensions. These drawings guide the drilling process, ensuring precise alignment and compatibility with components, mechanical fixtures, and electrical connections. From enhancing communication between designers and manufacturers to reducing production errors, drill drawings are integral to the fabrication of reliable, high-quality PCBs. To know, how PCBs are assembled in JLCPCB factory, see our detailed post from here.
- Enhanced Communication: Drill drawings bridge the gap between designers and manufacturers by providing clear specifications for hole placement, sizes, and types.
- Prevention of Errors: By detailing every hole’s purpose (e.g., vias, mounting holes), drill drawings prevent costly fabrication errors.
- Simplified Production: They streamline the production process by organizing drill data, making it easier for manufacturers to meet design requirements.
This blog delves into the importance of drill drawings, their types, file formats, and how they contribute to the PCB production process.
Types of Drill Holes:
Plated Through Holes (PTH): Used to connect layers in multi-layer PCBs. These are lined with conductive material to allow signal transmission.
Non-Plated Through Holes (NPTH): Typically used for mechanical purposes, such as mounting or aligning PCBs, and lack electrical connectivity.
Blind Vias: Connect outer layers to one or more inner layers but do not pass through the entire board.
Buried Vias: Connect only inner layers, remaining invisible from the board's exterior.
Micro Vias: Tiny vias used in high-density interconnect (HDI) designs, typically placed between adjacent layers.
How Drill Files Are Arranged in a Gerber Package:
Drill files, commonly in Excellon or NC Drill formats, are an essential component of the Gerber file package sent to manufacturers. They include:
Hole Coordinates: X and Y positions for each hole.
Tool List: List the drill bit sizes required for the various hole diameters.
Layer Information: Identifies where the holes begin and end, such as through-hole or layer-specific vias.
Drill Type Identification: Identify whether holes are plated or non-plated.
Drill files are often arranged alongside the Gerber files, including copper layers, solder masks, and silkscreens. Proper organization ensures efficient processing by the manufacturer, reducing turnaround times.
Drill Data Given to Machine:
Position: The Drill Table position can be selected from "Top", "Bottom", "Right", or "Left". The position is shown from the edge of the PCB document object.
Offset X: Use this field to specify the distance by which the table should be moved along the X axis.
Offset Y: Use this field to specify the distance by which the table should be moved along the Y axis.
Unit: The unit can be selected from "mm, "mil", or "inch".
Frame Line Width: The Frame Line Width of the Drill Table can be set.
Frame Margins: The Margin width of the Drill Table and Setting Values can be set.
Mark Size: The size of the symbol displayed on the drill position can be set.
The board origin is the location where all dimensional and positional measurements are relative to. Usually the lower left corner of the PCB is set as the origin or 0,0. Ironically, the example I chose for this example has the origin set at the lower left corner.
What a Drill Table Consists of?
Drill drawings are the visual representation of data, on the other hand drill tables consist of information in tabular format. A drill table lists the size and number of holes for each drill used on the board. Each drill size can be represented by a symbol, a letter or the actual hole size. When a drill drawing is generated for the board, each actual drill site is marked by a symbol as shown in the image below. But this type of tables are not required in Gerber format, hence can not be seen there. A typical drill table consists of:
Size - The size the hole or slot should be after copper plating and final finish are applied.
Quantity - The total number of drill hits made at this size.
Plated - The attribute of the hole. Either PLATED (PTH) or NON-PLATED (NPTH).
Tolerance - The accepted tolerance range for the finished hole size. IPC Class 2 standard is ±3 mil (0.076mm) for PTH and ±2 mil (0.05mm) for NPTH. Upon request we can accommodate a ±2 mil PTH tolerance for press fit connectors for a small additional charge.
NC Drill Chart File:
NC drill chart files are created for each combination of the start layer and end layer of drills. You can also generate separate NC drill files for plated and unplated holes. For example:
- Top-Bottom: A NC drill chart from a Top layer to a Bottom layer
- Top-2: A NC drill chart from a Top layer to a second layer
- 2-3: A NC drill chart from a second layer to a third layer
- 3-Bottom: A NC drill chart from a third layer to a Bottom layer
How Drill Drawings Help Engineers During Fabrication:
Hole Alignment: Drill drawings ensure precise alignment between components and PCB layers, crucial for multi-layer designs.
Component Placement: For example, connectors or pin headers require accurately placed holes for proper mounting and electrical contact.
Thermal Management: Vias outlined in drill drawings play a significant role in dissipating heat from high-power components.
Improved Signal Integrity: Properly placed vias and plated through-holes minimize signal loss and electromagnetic interference (EMI).
For example:
In an HDI design for a wearable device, micro vias are essential for connecting dense circuitry. Drill drawings provide the exact specifications for these tiny holes, ensuring that signal integrity and design functionality are maintained.
Conclusion:
Drill drawings are the backbone of PCB fabrication, merging precision with functionality. By outlining every hole’s specification, they ensure seamless integration of electrical and mechanical elements. For engineers and designers, understanding the importance of drill drawings and their integration into the PCB manufacturing process is vital. By paying attention to drill data, you can ensure a smoother transition from design to fabrication, reducing costs and improving final product reliability.
For top-tier PCB manufacturing, companies like JLCPCB ensure that drill data is optimized and accurately translated into flawless boards, turning designs into reality. Let your next project succeed by trusting experts who prioritize precision and quality.
Keep Learning
How to Choose the Right Prepreg Material for Reliable Multilayer PCB
Have you ever wondered what makes all those copper layers stick to a cross-section of a multilayer PCB? Prepreg material is the answer, and it is of much more importance than most engineers think it is. Choose the prepreg selection wrong, and you are predetermined to delamination, impedance drift, and long-term reliability problems. Prepreg is not only glue. It is a designed composite that determines your dielectric separation, dictates your impedance, affects signal loss, and determines your board be......
How to Detect PCB Short Circuits by Inspecting Gerber Files
Key Takeaways PCB short circuits can originate from design issues, manufacturing defects, soldering defects, or component failures; design-related shorts can be spotted before fabrication by inspecting Gerber files. Load copper layers, drill files, and solder mask layers in a Gerber viewer like JLCDFM, then look for plated holes that connect copper features belonging to different nets across layers. Three practical examples show how to trace shorts: a 12V-to-GND via short, a 3.3V-to-GND short across a......
PCB Depaneling for Cleaner Edges and Reliable Production
Key Takeaways Timing: Depaneling happens post-soldering, putting stress directly on finished parts. Methods: Choose V-cut for straight high-volume boards, mouse-bites for irregular shapes, and lasers for stress-free precision. MLCC Safety: Keep parts $\ge$ 1.0 mm from V-cuts, align MLCCs parallel to break lines, or add relief slots. Panel Limits: Cap assembly panels at 250 × 250 mm with 5 mm rails, 2 mm tooling holes, and 1 mm fiducials. File Prep: Mark "V-CUT"/"CNC" on the outline layer, keep copper ......
Step-by-Step Guide to the Printed Circuit Board Manufacturing Process
Key Takeaways Core Role: PCBs provide the physical foundation and electrical connections for modern electronics. Multi-Step Process: Manufacturing spans design imaging, substrate creation, inner/outer layer etching, lamination, and surface finishing. Precision and Quality Control: Features micro-drilling (down to 100 μm) for layer connectivity, Automated Optical Inspection (AOI), and final electrical testing. Protection and Finish: Solder masks and surface finishes (e.g., ENIG, HASL) protect copper tr......
How to Achieve Reliable Through-Hole Soldering on PCBs
key Takeaways Wetting & Fill: Heat the lead, barrel, and planes past melting point with active flux to achieve ≥75% vertical fill. Process & Prep: Bake damp boards to prevent blowholes, and match wave, selective, or hand soldering to board volume. Defect Prevention: Use thermal reliefs to stop heat-sink cold joints, and limit dwell time to avoid pad lifting. DFM & Materials: Size holes to max lead dimensions, keep full annular rings, and choose high-Tg FR-4 for multi-pass durability. Through-hole sold......
Technical Guidance: Character Design Specifications
To facilitate component assembly, future maintenance, and traceability of PCB manufacturing information (such as manufacturer, production date, batch number, etc.), various character markings are typically silk-screened onto the PCB. These include component designators, polarity marks, test point labels, company logos, and production traceability information. Traditional PCB character silk-screening uses the screen printing process, hence the term “silk-screen characters.” High-definition characters a......