How to confirm the production file?
Last updated on Nov 10, 2026

Why do we Suggest "Confirm the Production File"?
The production file is the file generated by JLCPCB engineer from customer's original Gerber file according to the capacity and production rules of JLCPCB.
Confirming production file provides a chance for our customers to double check everything before the production file being adopted for production. It often happens that customers find unexpected file issues by checking production file which they didn't notice when ordering. So we highly recommend you choose this service, especially if the project is urgent or of high value.
It is also a good opportunity to compare the design file and production file.
How to Choose "Confirm Production File" Option?
If customers choose the "confirm production file" option when placing orders as shown below, we will send an email to the registered email address later to remind customers to confirm the production file after payment.
How to Confirm Production File?
But how to confirm the production file?
First, please log in to your account on the website of JLCPCB, and go to "order history".
There will be a button for "confirm production file" as shown below.
First, please click the button, and see the page below.
But please don't click the button "Yes, please proceed to production" directly, because the pictures of the PCB can only be for reference.
Second, click the button "download production file" as shown above to check the file first before proceeding.
Third, after downloading the production file, you may need to extract the zip/rar file. There will be three folders inside, which are info, yg and ok.
In the yg folder, the file is the original file you uploaded when placing an order.
And the ok folder is the one engineer makes, but please ignore the ddw file/tgz file inside, just use gerber viewer to check other layers in Gerber format.
The info folder can be ignored.
Please use any tool that can open the Gerber file to open the ok folder to check the production file~
Finally, if the production file in the ok folder is correct, you may click the first button "Yes, please proceed to production" and submit so that we can start production soon.
If there is something that needs to be modified, please click the second button "not good, modification needed" and leave a remark as shown below to let us know where needs to be modified and submit it.
Then there will be an email from support@jlcpcb.com to inform you of checking the new production file later after the engineer modifies it.
Please reply to the email whether the new production file is OK or not. We will proceed with production once you confirm it is OK or ask the engineer to modify the file again if it is not OK.
Only if the latest production file is confirmed OK finally by email/livechat, can it continue to proceed with the order.
Once it is confirmed, the status will be shown as "confirmed production file" as shown below:
The Meanings of Layer Names in the Production File
The meanings of layer names in the production file can be checked here.
If there are any other questions, please contact us (support@jlcpcb.com) when you are free.
The meaning of the layers in the production file of FR-4/Aluminum/Copper Core/Rogers/PTFE Teflon
| Layer name in the production file | Corresponding layer meaning |
|---|---|
| to | Top Silkscreen |
| ts | Top Soldermask |
| tl | Top Layer |
| l2, l3, l4, l5... | Inner layers |
| bl | Bottom Layer |
| bs | Bottom Soldermask |
| bo | Bottom Silkscreen |
| drl | Drills |
| ko | Board Outline |
| sk | The vias which will be filled with resin/copper/solder mask ink |
| vcut | V-cut layer if it is needed |
| ko_pp | Direct heatsink pad layer if needed (copper core board only) |
| baobian | If edge plating option is chosen, there will be such layer in the production file. |
The meaning of the layers in the production file of the Flex board
| Layer name in the production file | Corresponding layer meaning |
|---|---|
| csa | Top EMI Shielding Film |
| to | Top Silkscreen |
| ct/ts | Top Soldermask |
| tl | Top Layer |
| bl | Bottom Layer |
| cb/bs | Bottom Soldermask |
| bo | Bottom Silkscreen |
| ssa | Bottom EMI Shielding Film |
| drl | Drills |
| ko | Board Outline (the outline of the finished boards) |
| ko_jg | Outline used for production (including the connections between boards ) |
| ko_h | File for making stainless steel stiffener |
| bqt | Top stiffener layer |
| bqb | Bottom stiffener layer |
| pit_0.1 | Top PI stiffener with 0.1mm thickness |
| pib_0.1 | Bottom PI stiffener with 0.1mm thickness |
| gpt_0.1 | Top stainless steel stiffener with 0.1mm thickness |
| gpb_0.1 | Bottom stainless steel stiffener with 0.1mm thickness |
| fr4t_0.2 | Top FR4 stiffener with 0.2mm thickness |
| fr4b_0.2 | Bottom FR4 stiffener with 0.2mm thickness |
| pst_3m468 | Top 3m468 Tape stiffener |
| psb_3m9077 | Bottom 3m9077 Tape stiffener |
Warm reminder:
Please confirm the production file as soon as possible to avoid any delay.