How to Choose the Right UL94 Rating for Safe and Reliable PCBs
10 min
- Understanding UL94 Ratings and Their Importance
- Why UL94 Rating Matters for PCB Safety and Performance
- Matching UL94 Rating to Your PCB Application
- Manufacturing Considerations for UL94 Compliant PCBs
- JLCPCB's Expertise in UL94 Rated PCB Manufacturing
- FAQ about UL94 Rating
Key Takeaways
This article explains how to choose the right UL94 rating to ensure PCB fire safety and compliance: V-0 is the common baseline for most electronics, V-1/HB are typically for lower-risk or non-regulated uses. It also stresses that rating performance depends on material selection, thickness, and process control, so use UL-certified laminates and a traceable, UL-capable manufacturer.
Have you heard that just one PCB that catches fire can produce poisonous fumes, annihilate an entire product, and put your company at grave risk of legal action? This is precisely the reason why the UL94 rating is available. It is the best-known flammability classification system of plastic and polymer materials, and it is a key factor in making your printed circuit board as safe as it can be. The flammability behavior of your PCB substrate is not something that you can ignore, whether you are creating a simple LED driver or a complicated automotive control module. The regulatory authorities in North America, Europe, and Asia demand certain UL94 flame ratings before your product can make it to the shelves of stores.
Neglecting this stipulation not only puts your safety at risk, but also your whole market access. As we are going to see today, we will dissect the UL94 rating system step by step. You will find out what each of the classifications entails, the way the tests operate, and what the correct rating would be in your particular application. Let's get into it.
Understanding UL94 Ratings and Their Importance
Underwriters Laboratories published the UL94 standard, which classifies materials by their behavior under the influence of a controlled flame source. It gives a definite rating which informs you of how fast a material will self-extinguish and whether it will also leave drips of flaming material that may start up other materials. To PCB designers, this rating is a direct indication of the fire safety profile of the base laminate of the board. Because PCBs conduct electricity and produce heat when used, the substrate should be resistant to ignition and contain the spread of fire in case of an accident.
What UL94 Rating Means and How It Is Tested
The UL94 test is a test method that exposes a specimen to a calibrated Bunsen burner flame. In vertical burn tests (V-0, V-1, V-2), there are five specimens with a size of 125 mm x 13 mm. The flame is applied twice, 10 seconds each, and the key measurements taken are:
- After flame time after first flame application (t1)
- After flame time after second flame application (t2)
- Afterglow time after second application (t3)
- Burns to the holding clamp or not.
- The ignition of a cotton indicator at 300 mm below by drips of flaming.
To perform the tests in horizontal burn (HB rating), the specimen is placed in a horizontal position, the flame is imposed on the specimen for a period of 30 seconds, and the rate at which the specimen burns is measured over a width of 75 mm.
Common Ratings (V-0, V-1, HB) and What They Represent
The UL94 system defines several classification levels. Here is a comparison of the most relevant ratings for PCB applications:
| Rating | Orientation | Max Afterflame (per specimen) | Total Afterflame (5 specimens) | Flaming Drips | Burn to Clamp |
|---|---|---|---|---|---|
| V-0 | Vertical | 10 seconds | 50 seconds | Not allowed | No |
| V-1 | Vertical | 30 seconds | 250 seconds | Not allowed | No |
| V-2 | Vertical | 30 seconds | 250 seconds | Allowed | No |
| HB | Horizontal | No limit | No limit | Not tested | Rate < 76 mm/min |
The maximum vertical burn rating is V-0, which is the default for most PCB applications. The material should extinguish itself in 10 seconds per specimen without dripping or flaming. This is the rating that you will find on all FR4 laminates in professional manufacturing.
V-1 permits as much as 30 seconds of afterflame per specimen, yet does not permit drips of flaming. V-2 also allows dripping flames and is not suitable for most electronics. The lowest classification is HB (Horizontal Burn), which is not usually adequate when it comes to controlled markets.
Why UL94 Rating Matters for PCB Safety and Performance
Electronics fire safety is not an imaginary issue. A large proportion of product recalls is due to poor material flammability ratings. The PCB substrate is the backbone of the assembly, and how it behaves in fire directly influences the safety of the end product.
Fire Risk in Electronics and Regulatory Requirements
Local temperatures may exceed the glass transition temperature of the laminate due to component failures, short circuits, and overcurrent conditions. When the substrate burns and cannot put out the flame on its own, the consequences may be disastrous. The world has regulatory frameworks that require certain UL94 ratings:
- UL/cUL (North America): UL listing of most electronics needs V-0 rated substrates.
- IEC 62368-1: International safety standard of IT and AV equipment cites UL94 classifications.
- EN 45545: The performance of flammability required in railway applications in Europe is strict.
- Automotive: The highest levels of flammability are required in critical ECUs by functional safety requirements.
- IPC-4101: This base material specification uses the laminate classification sheets of UL94.
Your product cannot obtain the regulated market certifications without the right UL94 rating. It is not a recommendation, but a gatekeeper.
Impact on Long-Term Reliability and Market Compliance
UL94 rating is also an indicator of material quality and consistency. A V-0 rated laminate has been developed using flame-retardant additives carefully controlled and has successfully undergone extensive third-party testing. The same material characteristics, which inhibit flame spread, also help provide thermal stability during reflow, delamination resistance, and uniform dielectric performance throughout the product life. UL94 V-0 is a common requirement in the list of approved vendors of many OEMs. In case your PCB fails to meet this specification, you will not be regarded as a supplier, irrespective of design quality.
Matching UL94 Rating to Your PCB Application
Selecting Ratings for Consumer, Industrial, and Automotive Use
| Application Sector | Minimum Rating | Typical Material | Key Driver |
|---|---|---|---|
| Consumer electronics | V-0 | Standard FR4 (Tg 130-150C) | UL/IEC certification |
| LED lighting | V-0 | FR4 or aluminum MCPCB | UL 8750 / EN 62031 |
| Industrial controls | V-0 | Mid-Tg FR4 (Tg 150-170C) | IEC 61010 |
| Automotive ECUs | V-0 | High-Tg FR4 (Tg 170C+) | ISO 26262 |
| Medical devices | V-0 | High-Tg or specialty laminates | IEC 60601 |
| Aerospace / Military | V-0 or 5VA/5VB | Polyimide laminates | MIL-STD, DO-160 |
In the case of consumer electronics, V-0 is universal. The automotive industry requires V-0 plus materials that can resist -40C to +125C temperatures, vibration, and humidity. In such conditions, high-Tg FR4 or polyimide substrates are required.
Balancing Flammability, Cost, and Mechanical Properties
This is the real world. UL94 V-0 is already achieved by standard FR4 of renowned manufacturers such as Shengyi, Kingboard, or Nanya. It is not a premium on fire safety. When you require better properties than V-0, there are some cost considerations.
- High-Tg FR4 (170 °C+): 10-20% premium, needed for lead-free reflow and high-temperature environments
- Low-Dk/Df laminates: Materials such as Megtron 6 or Rogers have V-0 but with better signal integrity.
- Polyimide flex: Flame resistant by nature, but 3-5 times more expensive than rigid FR4.
- Halogen-free FR4: Uses phosphorus-based retardants instead of bromine, meets IEC 61249-2-21 while maintaining V-0.
Manufacturing Considerations for UL94 Compliant PCBs
The most important thing is that you can have a UL94 V-0 rating on your completed PCB, not only by choosing the correct laminate. The flame-retardant properties should be maintained during the entire fabrication process.
Material Selection and Process Controls
The journey starts with copper-clad laminate (CCL) selection. The parameters that determine the UL94 performance are:
- Flame retardant system: Conventional FR4 employs brominated epoxy; halogen-free versions employ phosphorus or nitrogen additives.
- Resin content: The higher the resin in prepreg layers, the greater the flammability and dielectric properties.
- Thickness: UL94 ratings depend on thickness. A material with a V-0 of 1.6 mm can only be V-1 at 0.4 mm.
- Glass weave style: Styles such as 1080, 2116, and 7628 affect mechanical strength and flame resistance.
- Copper weight: Copper is a heat sink, and it has an effect on local flame behavior.
Over thermal stressing of the lamination process, improperly cured solder mask, and contamination of wet processing may all reduce flame-retardant characteristics of the completed board.
Testing and Certification in Professional Production
The laminate manufacturer is UL certified for the particular construction. The PCB manufacturer then operates under certified parameters, such as approved ranges of thickness and processing conditions. Manufacturers that are UL recognized have their own UL E-number, which assures that their facility has been audited by Underwriters Laboratories. This includes a system of periodic inspections, material traceability, and sample testing. Always ensure that your PCB supplier has the capability of giving the UL certifications and material traceability of the laminate used in your order.
JLCPCB's Expertise in UL94 Rated PCB Manufacturing
Access to Certified High-Performance Materials
JLCPCB has a variety of UL94 V-0 certified materials that span the entire spectrum of applications. No matter what type of design you require: standard FR4, high-Tg FR4, or specialty laminates, the choices are there with complete certification documentation and traceability.
Rigorous Quality Assurance and Compliance Support
JLCPCB has incoming material verification, in-process controls, and final quality checks that are based on IPC-A-600 Class 2. Each batch of new laminate is checked with its UL certification, and processing parameters are regulated to maintain flame-retardant properties. AOI and electrical testing of boards is the norm, making it easier to certify your products to UL or CE.
Reliable Production from Prototype to Volume
One of the practical benefits of using JLCPCB is that it is possible to prototype using the identical UL94 V-0 materials as those used in production. The flammability properties of your prototype boards are the same; you are certifying on the real material on the first day. Pricing as low as 2 and production times as short as 1-2 days allow you to iterate very fast without sacrificing material quality. The SMT assembly service also simplifies the design-to-manufactured product process on a single roof.
FAQ about UL94 Rating
Q: What is the most common UL94 rating used in PCB manufacturing?
UL94 V-0 is the industry standard. Standard FR4 from major laminate manufacturers is V-0 rated by default.
Q: Can a PCB lose its UL94 rating during manufacturing?
Yes. If fabrication conditions exceed certified parameters, such as excessive thermal stress or improper curing, flame-retardant properties can degrade. This is why choosing a manufacturer with proper process controls matters.
Q: Is UL94 HB acceptable for any PCB application?
Only for non-regulated applications like hobbyist projects or internal prototypes. For any commercial product, V-0 is the minimum.
Q: What is the difference between UL94 V-0 and 5VA?
V-0 uses a 50W test flame, while 5VA uses a 500W flame. 5VA-rated materials resist ignition from a much larger flame source and show no burn-through. This rating is typically for enclosures rather than PCB substrates.
Keep Learning
How to Select Tg of PCB ?
What is the Tg of PCB? In PCB manufacturing, "Tg" stands for Glass Transition Temperature. It is the temperature at which the PCB substrate material transitions from a rigid, glassy state to a soft, rubbery state. PCBs are flame-retardant (UL94 V-0) and do not burn easily; instead, they soften above Tg. The Critical Correlation Between Tg and Z-Axis CTE (Coefficient of Thermal Expansion) When the temperature exceeds the Tg point, the PCB substrate material (such as standard FR-4) undergoes a physical ......
Choosing the Right CTI Value for Safer High-Voltage PCBs
Key Takeaways Higher CTI (≥600V, Group I) allows shorter creepage distances while preventing surface tracking in high-voltage designs. Standard FR4 (CTI ~175V) is often inadequate for mains voltage — upgrade to high-CTI materials for safety and compactness. Always match CTI material group to your working voltage and pollution degree for IEC/UL compliance. Clean assembly and good layout practices are essential to realize the full benefits of high-CTI laminates. Choose certified high-CTI materials and e......
Maximize Efficiency with PCB Panelization in High-Volume Manufacturing
Whenever a new PCB designer begins to spin the wheels, they are soon enough faced with the transition of creating a few prototypes into a volume production venture. As well as that, change brings a new idea that prototype-based engineers tend to forget: PCB panelization. In essence, panelization refers to loading a number of copies of your board design (or even a variety of designs) onto a single standardized production panel such that all of the fabrication and assembly processes treat them as a sing......
Inside the PCB Structure : How Layers, Stackup, and Buildup Define Modern Circuit Board Performance
Printed circuit boards may look like flat green rectangles, but beneath the surface, they are sophisticated multi-layer structures. As devices get more compact and complex, engineers turn to multilayer boards with carefully chosen materials and stackups to meet electrical and mechanical demands. This article peels back those layers to explore how substrate choice, layer stackup, and buildup methods shape PCB performance. Here we’ll cover PCB design fundamentals from the base materials up to high-densi......
The Benefits of Bed of Nails Testing in Professional PCB Manufacturing
Have you ever wondered how manufacturers can test thousands of PCBs daily and not make the production line crawl? The answer, as frequently as not, is a deceitful-appearing device called a bed of nails test set-up. The platform contains hundreds of little spring-loaded pins on it, and each of those pins is aligned very precisely to touch a specific test point on your circuit board. It can check the electrical integrity of a whole PCB, shorts, opens, and component defects in a few seconds, before the b......
Understanding PCB Dielectric Constant : Choosing Materials for Optimal Signal Performance
Key Takeaways The PCB dielectric constant (Dk) is a critical factor that directly determines signal propagation speed, characteristic impedance, and transmission loss in high-frequency designs. Selecting the right material — from standard FR4 for general use to low-Dk Rogers, PTFE, and LCP for multi-gigahertz applications — enables better performance, tighter impedance control, and reduced signal degradation. Success ultimately comes from matching Dk to your frequency needs, optimizing layer stackup, ......