Protective Measures for PCBs: Safeguarding Electronics from Environmental Factors and Electrical Hazards
7 min
- Environmental Protection:
- Electrical Protection:
- Thermal Management:
- Mechanical Protection:
- PCB Layout Design:
- Conclusion
Printed Circuit Boards (PCB’s) serve as crucial parts of electronic devices providing the framework for connecting various electrical components. Put in place strong protection measures to guarantee the dependable and durable operation of PCBs. PCB protection means preventing external influences, electrical problems, mechanical stress, and excessive temperatures from harming the board and it’s components.
In the subsequent sections, we will delve into nine methods, which are summarized into five major areas. Let's explore the world of PCB protection and discover how to safeguard your PCB’s against the challenges they may face in their operational environment.
Environmental Protection:
One crucial component of PCB protection is environmental protection. We often subject PCBs to a variety of environmental conditions, including moisture, dust, chemicals, and temperature fluctuations. These behaviors might lead to corrosion, short circuits, component failure, and degraded performance.
Conformal Coating: Conformal coating is a thin protective layer put on the surface of the PCB. It blocks fluctuations in temperature, chemicals, dust, and moisture. Acrylics, silicone, urethane, and epoxy are some examples of common conformal coating materials. Using techniques like spray coating, dip coating, or brush coating, we apply the coating to the PCB, following its curves to cover the solder connections, components, and traces.
Encapsulation: Encapsulation refers to entirely covering the PCB with a protective layer, or to simply a few selected components having a protective layer. To form a robust and long-lasting barrier, protective material is poured or injected around the PCB or component. Encapsulation improves mechanical strength, electrical insulation, and shock and vibration resistance. As a result, the PCB receives protection from physical harm, chemicals, moisture, and dust.
Varnish/Dipping: Protection against moisture, corrosion and a certain degree of mechanical stress is achieved by dipping or coating the PCB with a varnish or protective solution to provide a protective layer. Because the PCB is immersed or coated in a varnish or protective solution, we form a thin layer on the surface of the circuit board. This technology is more typically employed in applications where a more cost-effective way of protection is required.
Environmental Sealing: Sealing methods such as gaskets, O-rings, or watertight housings can provide a barrier against external pollutants when we need to protect a PCB from water, dust, or other environmental variables. In addition, we will put the seals around ports, connectors, and other holes in order to keep moisture and dust out of PCBs and enclosures.
Electrical Protection:
Over-current and Over-voltage Protection: We might use circuit breakers, varistors, and transient voltage suppressors (TVS diodes) to protect of PCBs from over-current and over-voltage situations. These gadgets aid in preventing harm from spikes in voltage or high current.
Grounding: Grounding entails creating a reference point or common ground potential for all components and circuitry on the PCB. It lessens the chance of EMI and minimizes voltage variations. In practice, we can connect all ground terminals of components and subsystems to a single common ground point on the PCB. This behavior reduces ground loops and ensures a consistent reference potential. Or, in mixed-signal PCBs, separate analog and digital ground planes to prevent noise coupling between sensitive analog components and noisy digital circuitry. We can use separate Vias for connection.
Shielding: Shielding is using conductive materials to form barriers around sensitive components or circuits. The purpose of that is aiming to block external EMI. To achieve this, we could use metal cans or boxes to confine electromagnetic radiation around sensitive components like oscillators or high-frequency circuits. For efficient shielding, connect the shield container to the ground plane.
ESD Protection: Electrostatic discharge (ESD) protection measures such as ESD diodes, grounding, and proper handling procedures are implemented to safeguard the PCB from ESD events. By applying appropriate grounding and shielding procedures, we may reduce radio frequency interference (RFI) and electromagnetic interference (EMI). When using this method, we need to pay attention to the proper placement and routing of ground traces, the use of ground planes, and the use of shielding techniques (such as conductive enclosures or shielding materials) to prevent unwanted electrical noise and interference.
There are 15 types of ESD gadgets in JLCPCB to help you protect device:
At JLCPCB, we offer a range of circuit protection devices
Thermal Management:
Excessive heat can adversely affect PCB components and their performance. Overheating can lead to component failure, thermal runaway, and reduced service life. Adequate thermal management, including the use of heat sinks, fans, and proper ventilation. Additionally, incorporate thermal Vias into the PCB design. Vias provide a path for heat to flow from a component to a larger ground plane or heat sink. Use copper pours or large-area copper connections to thermal Vias to enhance heat dissipation. The copper area acts as a heat sink, helping to distribute heat to the PCB surface and improve thermal conductivity. Not only that, choose PCB materials with high thermal conductivity, such as metal-core PCBs or PCBs with thermally conductive dielectric layers. These materials facilitate efficient heat transfer and help dissipate heat from Vias and components more effectively.
Mechanical Protection:
Mechanical stress on PCBs can arise from bending, vibration, and shock. This stress can cause solder joint failures or disconnected components. Stiffeners and support structures are examples of mechanical reinforcement techniques that help reduce the effects of mechanical stress and improve the PCB's overall longevity.
Specifically, when installing the PCB, we can use the proper mounting approaches, such as screws, standoffs, or snap-fit connections. By providing a robust and secure mounting, these strategies lessen the chance of PCB bending and the strain on the Vias. Additionally, we may strengthen PCB key spots such as those close to Vias or vulnerable to mechanical stress. To improve the mechanical strength and stability of the PCB, we would add more copper traces, strengthen with epoxy or glue, or employ methods like layers of carbon fiber or fiberglass. Besides that, we can use shock-absorbing materials like foam or rubber gaskets between the PCB and the mounting surface. Because these materials absorb and attenuate shock and vibration, they reduce stress on Vias and other components.
PCB Layout Design:
The design of the PCB layout is of the utmost importance to provide the PCB with efficient protection.
As we previously discussed, proper PCB layout design practices may help lower electromagnetic interference (EMI) and increase overall PCB reliability and protection. These practices include trace routing, ground planes, signal integrity concerns, and the separation of high- and low-power components. By avoiding routing sensitive traces or components close to high-voltage networks, we reduce the chance of damage from high-voltage spikes. In the early PCB design process, you must decide on the pads' and holes' sizes. Finding the ideal ratio of pad to hole size becomes more crucial as both pad and hole sizes shrink. In particular, while utilizing through holes. One further crucial factor to consider is the PCB pads' form. Depending on the manufacturing process, the PCB footprint may change. For instance, we usually need a greater floor area for wave soldering than for infrared re-flow soldering.
Conclusion
Through comprehension and application of these PCB protection techniques, you may reduce the possibility of malfunctions, lengthen the lifespan of your PCBs, and augment the general dependability of your electronic apparatuses. To guarantee outstanding performance and safeguard your investment, you must be knowledgeable about and apply PCB protection techniques.
Keep Learning
Avoid PCB Assembly Failures: Mastering Solder Mask Expansion Rules and Best Practices
Solder mask protects copper traces and pads from oxidation, bridges, and contamination during assembly. Incorrect solder mask expansion—the clearance around features where mask is pulled back—leads to defects like shorts or exposed copper. Engineers must set expansion values precisely to ensure reliable soldering and long-term performance. Introduction: Why Solder Mask Expansion is Critical for PCB Reliability Understanding Solder Mask and Expansion Basics Solder mask is a polymer layer applied over t......
Why Copper Oxidation Matters in PCB Design & How to Prevent It
Key Takeaways Copper oxidation is a critical concern in PCB design that directly impacts solderability, contact resistance, and long-term reliability. By understanding how oxidation forms and damages copper surfaces, designers can effectively prevent it through appropriate surface finishes (such as HASL, ENIG, and OSP), strategic solder mask application, and strict adherence to proper storage and handling practices per IPC-1601 guidelines. Protecting copper from oxidation ensures better assembly yield......
Choosing the Right Surface Finish for Your PCB: An Overview of HASL, ENIG, OSP, Immersion Tin and Immersion Silver
Key Takeaways Lead-Free HASL: Best low-cost, RoHS-compliant finish for general PCB builds. ENIG: Superior flatness and 12+ month shelf life for fine-pitch BGAs. OSP: Ultra-flat, lowest-cost option for high-volume SMT (3–6 month shelf life). Immersion Silver: Ideal for high-frequency RF by eliminating nickel signal loss. Immersion Tin: Best for press-fit connectors and fine-pitch assembly. Printed Circuit Boards (PCBs) are essential components in the manufacturing of electronic devices ranging from sma......
Conformal Coating in PCB Technology: Benefits, Challenges, and Future Developments
If you're searching for conformal coating, you're likely looking for a reliable way to protect your PCB from moisture, dust, chemicals, or harsh environments. Choosing the right coating directly affects product reliability, performance, and lifespan. In this guide, you'll learn what conformal coating is, the main types available, and how to select the best option for your application. We'll also cover key benefits, application methods (manual, automated, and selective), as well as inspection, rework, ......
PCB Gold Fingers: Why They Matter and How to Design Them
Key Takeaways PCB gold fingers provide reliable electrical and mechanical contact for PCBs that connect to external connectors or card slots. ENIG is suitable for general contact applications, while electroplated hard gold offers higher wear resistance for repeated insertion and removal. Gold fingers should remain fully exposed, with solder mask and silkscreen kept away from the contact area. Proper chamfering and gold finger orientation are essential to ensure smooth insertion and prevent damage duri......
Comparing HASL and ENIG Surface Finishes for PCBs
Selecting the right surface finish for a printed circuit board (PCB) is crucial to ensuring its performance, reliability, and longevity. Two of the most commonly used finishes are Hot Air Solder Leveling (HASL) and Electroless Nickel Immersion Gold (ENIG). Each of these surface finishes offers distinct advantages and disadvantages, making them suitable for different applications. In this article, we will compare HASL and ENIG to help you determine which finish is best suited for your PCB project. What......