How to Waterproof a PCB: A Step-by-Step Potting Guide
5 min
- What is Potting?
- What Potting Helps to Achieve?
- Materials Used in PCB Potting:
- Tools and Supplies Needed for Potting
- Step-by-Step Guide to Potting a PCB
- Potting vs Conformal Coating:
- Best Practices and Tips
- Conclusion:
PCBs are everywhere, they are an integral part of nowadays essential things. We can not imagine a world without them. Almost all the things which have power or that can take power have at least a PCB. Because they are used so often the circuit needs to operate in challenging environments. Mostly we are talking about outdoors, under the hood or in humid industrial settings. The term potting becomes a crucial solution for all this. Potting a printed circuit board (PCB) helps protect it from moisture, dust and electrical shock. It extends the life of electronics and enhances reliability. We’ll walk you through the entire process of potting a PCB. From preparation to curing, and explore tips for selecting the right potting compound for your specific use case.
What is Potting?
Potting is the process of enclosing a PCB or electronic assembly in a protective compound. It is basically a kind of epoxy, polyurethane or silicone. The liquid material is poured into a casing or mold that houses the PCB. Then allowed to cure into a solid, protective shell. Now because the PCB has this protective coating the circuit housing becomes waterproof. This is the similar method used in underwater pool lighting electronics products.
Potting is not always done because of environmental reasons, there are some manufacturers who want to keep their product OEM and do not want others to copy so they also use the same strategy.
What Potting Helps to Achieve?
Potting offers several advantages:
- Waterproofing: Prevents moisture ingress and makes the electronics suitable for outdoor or marine electronics.
- Dust and dirt protection: Blocks contaminant particles from reaching circuit elements, this helps in archiving an IP rating to a product.
- Vibration damping: Absorbs shocks in automotive or aerospace environments.
- Electrical insulation: Prevents arcing and leakage in high-voltage circuits.
Materials Used in PCB Potting:
Always check compatibility with your PCB components because some resins can attack plastic housings or corrode metal parts.
Tools and Supplies Needed for Potting
- PCB to be potted
- Potting compound (resin and hardener)
- Mixing container and stir sticks
- Protective gloves and eye protection
- Vacuum chamber (optional, for degassing)
- Mold or enclosure (plastic or metal casing)
- Masking tape or silicone plugs
- Heat gun (optional, for bubble removal)
- Curing oven or ambient cure space
Step-by-Step Guide to Potting a PCB
Step 1: Choose the Right Potting Compound
Select a material based on your application requirements. Here are some examples:
- If you need Waterproofing & rigidity choose Epoxy
- If flexible & vibration resistant are main concern then choose Polyurethane
- If you need high temperature tolerance then choose Silicone
The datasheet comes with each material which states its dielectric strength, thermal conductivity and cure time.
Step 2: Prepare the PCB and Enclosure
First of all, clean the PCB and remove any remaining dust particles or flux residue, dry it well at 60–80°C for 30 minutes. Secure the PCB in a potting box or its final product casing. Use tape or silicone plugs to cover connectors and test points.
Step 3: Mix the Potting Compound
Read the mix ratio on the manufacturer's label the common ratios are 1:1 or 2:1. Which is basically resin : hardener. Mix slowly and thoroughly to avoid air entrapment. If available, degass in a vacuum chamber for 2–5 minutes to eliminate bubbles.
Step 4: Pour the Potting Material
Pour the potting material slowly and steadily into one corner of the enclosure. Allow the material to flow naturally over and around components. Tap gently the assembly to help bubbles escape. Additionally you can use a heat gun briefly to pop surface bubbles (careful not to overheat). This process is similar to the epoxy filling in a pot.
Step 5: Let It Cure
Cure time depends on the compound and temperature, if curing at room temperature it will take 6–24 hours, and at 60–120°C for 1–3 hours. Avoid any movement of the assembly during the curing process. Ensure proper ventilation and urethanes that may emit fumes.
Step 6: Post-Cure Finishing
Trim excess material with a craft knife if necessary. Remove masking materials and inspect for coverage gaps. Conduct basic electrical tests to confirm proper functionality.
Potting vs Conformal Coating:
Choose conformal coating for lightweight protection and potting for robust, long-term durability.
Best Practices and Tips
- Only choose the components that can survive encapsulation or be sealed off. There are several connectors, LEDs, or switches available for this purpose.
- Use thermally conductive potting compounds if heat dissipation is needed. Because in electronics heat management is a necessity, under the excessive heat system may fail.
- Either potting is done in a box, by placing all the electronics inside and filling the rest with the solution OR we can use the mold.
- Avoid potting batteries unless approved. Some chemistries can become hazardous when encapsulated.
Conclusion:
Potting is one effective way to safeguard your PCB from environmental threats. It is important but not essential to do always, there are only certain conditions in which a PCB housing needs potting. Although this method offers long-lasting protection, moisture resistance, and enhanced reliability.
There are a lot of potting materials available in the market, you can choose one as per your requirements. The above given table in this article will help you. By following this step-by-step potting guide you can manually do it at home. By following this step-by-step potting guide you can manually do it at home. And if you’re looking to start your next project right away, JLCPCB makes it easy to order affordable, high-quality PCBs online — with $70 new user coupons to help you get started.
Keep Learning
Why Copper Oxidation Matters in PCB Design & How to Prevent It
Key Takeaways Copper oxidation is a critical concern in PCB design that directly impacts solderability, contact resistance, and long-term reliability. By understanding how oxidation forms and damages copper surfaces, designers can effectively prevent it through appropriate surface finishes (such as HASL, ENIG, and OSP), strategic solder mask application, and strict adherence to proper storage and handling practices per IPC-1601 guidelines. Protecting copper from oxidation ensures better assembly yield......
Choosing the Right Surface Finish for Your PCB: An Overview of HASL, ENIG, OSP, Immersion Tin and Immersion Silver
Key Takeaways Lead-Free HASL: Best low-cost, RoHS-compliant finish for general PCB builds. ENIG: Superior flatness and 12+ month shelf life for fine-pitch BGAs. OSP: Ultra-flat, lowest-cost option for high-volume SMT (3–6 month shelf life). Immersion Silver: Ideal for high-frequency RF by eliminating nickel signal loss. Immersion Tin: Best for press-fit connectors and fine-pitch assembly. Printed Circuit Boards (PCBs) are essential components in the manufacturing of electronic devices ranging from sma......
Conformal Coating in PCB Technology: Benefits, Challenges, and Future Developments
If you're searching for conformal coating, you're likely looking for a reliable way to protect your PCB from moisture, dust, chemicals, or harsh environments. Choosing the right coating directly affects product reliability, performance, and lifespan. In this guide, you'll learn what conformal coating is, the main types available, and how to select the best option for your application. We'll also cover key benefits, application methods (manual, automated, and selective), as well as inspection, rework, ......
PCB Gold Fingers: Why They Matter and How to Design Them
Key Takeaways PCB gold fingers provide reliable electrical and mechanical contact for PCBs that connect to external connectors or card slots. ENIG is suitable for general contact applications, while electroplated hard gold offers higher wear resistance for repeated insertion and removal. Gold fingers should remain fully exposed, with solder mask and silkscreen kept away from the contact area. Proper chamfering and gold finger orientation are essential to ensure smooth insertion and prevent damage duri......
Comparing HASL and ENIG Surface Finishes for PCBs
Selecting the right surface finish for a printed circuit board (PCB) is crucial to ensuring its performance, reliability, and longevity. Two of the most commonly used finishes are Hot Air Solder Leveling (HASL) and Electroless Nickel Immersion Gold (ENIG). Each of these surface finishes offers distinct advantages and disadvantages, making them suitable for different applications. In this article, we will compare HASL and ENIG to help you determine which finish is best suited for your PCB project. What......
Avoid PCB Assembly Failures: Mastering Solder Mask Expansion Rules and Best Practices
Solder mask protects copper traces and pads from oxidation, bridges, and contamination during assembly. Incorrect solder mask expansion—the clearance around features where mask is pulled back—leads to defects like shorts or exposed copper. Engineers must set expansion values precisely to ensure reliable soldering and long-term performance. Introduction: Why Solder Mask Expansion is Critical for PCB Reliability Understanding Solder Mask and Expansion Basics Solder mask is a polymer layer applied over t......