How to Solve Common Wave Soldering Defects
5 min
- Wave Soldering Defects
Wave Soldering Defects
The wave soldering process is the primary process that causes defects in PCBA components. It causes a defect rate of up to 50% in the entire PCBA assembly process. Wave soldering is best suited for through-hole components (components with leads inserted into drilled holes in the circuit board).
The following are some common problems and their solutions during the wave soldering process:
Incomplete Solder
Incomplete soldering occurs when the solder fails to adhere properly to the soldering points during the soldering process of electronic components. This can lead to weak solder joints or intermittent contact issues. Soldering defects may be caused by various factors, such as inadequate soldering temperature, insufficient flux, inadequate soldering time, dirty soldering surfaces, etc. To prevent the issue of poor soldering, you can implement the following measures:
- Ensure that the soldering temperature is appropriate to allow the solder to fully melt and effectively wet the soldering surface.
- Use an appropriate amount of flux to enhance the adhesion of the solder to the soldering surface.
- Control the soldering time to ensure that the soldering is fully completed but not too short.
- Clean the soldering surface before soldering to ensure that the soldering point is clean and free of contamination.
- Regularly check the soldering quality, detect, and promptly repair issues such as weak welds.
Void
Outgassing issues are a common challenge in wave and hand soldering. Porosity refers to the gas holes that appear in welded joints. The formation of pores may be related to the presence of oxides, grease, or impurities on the solder surface, or it may be caused by gas release during the soldering process. These pores may appear as tiny holes or larger cavities on the surface of the joint.
In through-holes, the correct copper plating thickness is critical, with a minimum of 25µm of copper thickness on the surface of the hole wall. At the same time, ensure that the soldering surface is clean and free of any oxides, grease, or impurities. Adjust soldering parameters, such as increasing soldering temperature and solder flow, to reduce gas generation and accumulation. Through these measures, porosity problems can be effectively reduced, and soldering quality and reliability can be improved.
Excess Solder
Common soldering beginners often believe that more solder is better, but excessive solder can lead to the component terminals and pins being engulfed in solder or the formation of bubbles in the middle of the solder joints, which are typically round and convex in shape.. Possible causes include excessive protruding lead length, insufficient flux, excessive solder drag, and improper nozzle stripping motion.
Excess solder can usually be removed using the tip of a hot iron. In extreme cases, a solder extractor or solder wick can also be helpful.
Solder Flag
The solder joint tip refers to the abnormal shape of the solder joint that appears during the soldering process, exhibiting a sharp or protruding form. After trimming, the solder joint tip needs to conform to the overall component foot and extend beyond the PCB by no more than 2mm.
The main causes of solder tip tinning issues include the soldering iron tip leaving the solder joint in the wrong direction, the soldering iron moving too slowly from the solder joint, poor solder quality, excessive impurities in the solder, and soldering at a temperature that is too low. The consequences of tipping include poor appearance and the potential to cause bridging. In high-voltage circuits, tip discharge may also occur.
To prevent the issue of solder joint sharpening, it is essential to focus on controlling the angle, speed, and temperature during the soldering process, choosing high-quality solder, and ensuring the proper functioning of the soldering equipment. Through proper soldering operations and quality control, the occurrence of solder joint sharpening can be effectively minimized, leading to improved soldering quality and reliability.
Cold Solder
It is called solder disorder. The surface of the solder joints exhibits irregular marks and unevenness. Cold soldering is the same as virtual soldering. It is difficult to fully disclose during the production process. Users often need to use it for a period of time, which could range from days to months or even years. This will not only have extremely negative effects but also lead to extremely serious consequences. Due to the low strength of cold soldering, the conductivity is not good.
● The chain vibrates and is affected by external forces during cooling, causing the solder to become disordered.
● If the soldering temperature is too low or the chain speed is too fast, the viscosity of the molten solder will be too high, resulting in a wrinkled surface of the solder joint.
● To repair a cold solder joint, simply reheat the joint with a hot soldering iron until the solder flows.
Solder Joints Bridged or Shorted
Solder joint bridging is a common defect in wave soldering. The component pins are too close together, or the wave is unstable. The possible reasons are as follows: the soldering temperature is set too low, the soldering time is too short, and the soldering temperature drops after the soldering is completed. The time passes too quickly, and the amount of flux sprayed is too minimal.
In this case, it is necessary to check the waveform and confirm whether the soldering coordinates are correct. This can be improved by increasing the soldering temperature or preheating temperature, extending the soldering time, prolonging the cooling time, and increasing the amount of flux sprayed.

Popular Articles
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Wire Bonding vs Flip Chip: Key Differences in Semiconductor Packaging
In the rapidly evolving world of semiconductor packaging, the choice between Wire Bonding and Flip Chip technology is more than just a mechanical decision—it is a strategic pivot that dictates your product’s performance, thermal limits, and bottom line. Are you looking for the cost-effective reliability of traditional interconnects, or does your application demand the high I/O density and superior signal integrity of modern flip-chip architectures? In this comprehensive guide, we draw on years of high......
Chip Scale Package (CSP) Explained: Types, Benefits & More
Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action. By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds t......
How to Solder Wires to a Circuit Board Properly: Step-by-Step Guide
Learning how to solder wires to a circuit board is a fundamental skill for electronics repair, prototyping, and PCB assembly. Whether you are attaching power leads, signal wires, or test connections, a weak solder joint can cause intermittent failures, lifted pads, or long-term reliability issues. In this step-by-step guide, you'll learn the correct tools, preparation methods, and soldering techniques needed to create strong, clean, and reliable wire-to-PCB connections. From preparing the wire and PCB......
BGA Reballing Explained: Complete Process, Tools, Risks, and Best Practices
In modern electronics design, the Ball Grid Array (BGA) is the standard for high-performance silicon, enabling thousands of I/O connections in a tiny footprint. However, this density creates a "black box" scenario: connections are hidden, and defects like cold joints or thermal fatigue cracks are invisible to the naked eye. Unlike a QFP that can be fixed with a soldering iron, a failed BGA threatens the viability of the entire board. BGA reballing is the critical solution to this problem. It is the pr......
SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
Surface Mount Devices (SMDs) are essential components in modern electronic devices, including smartphones, tablets, and IoT systems. Unlike older through-hole methods, where components were inserted through drilled PCB holes, soldering SMD components manually can be challenging, especially for beginners. The extremely small sizes and tight spacing on modern PCBs require high precision, and achieving reliable solder joints often depends on using the best SMD soldering tools. Common issues arising from ......
IC Package Types Explained: A Practical Guide for PCB Designers
Walk into any electronics lab, and you'll hear the same debate: "Which IC package should I use here?" It sounds like a simple question until you realise the answer determines your PCB footprint, thermal headroom, assembly process, rework feasibility, and field reliability - all at once. This guide breaks down every major IC package type used in modern PCB design, helping you understand the differences between common IC package types in plain engineering language so you can make the right call from the......