SMT vs Through Hole: Which PCB Assembly is Most Cost-Effective?
7 min
- 1. Standard Soldering Technologies:
- 2. SMT PCB Assembly:
- 3. Through-Hole Assembly:
- 4. Comparing SMT and Through-Hole Assembly Costs
- Conclusion
Performance and cost in the realm of electronics production depend on choosing the correct assembly method. Of the several approaches accessible, Surface Mount Technology (SMT) and Through-Hole Technology (THT) are the two most often used ones for PCB assembly. These two assemblies can be combined to create some products or used as individual technologies. Though seemingly little, this variance affects several aspects including board design, materials and techniques employed, heat dissipation, and related labor and setup expenses.
⦁ Complete SMD: The PCB can have the components attached on one side or both sides.
⦁ MIXED: It's frequently utilized when some components aren't SMD accessible. With so many process stages, this assembly type is the most complicated one to produce. SMDs and through-hole components are combined here.
⦁ Fully TH: Prototyping or testing significantly rely on this. In this the components either on both sides (double-sided) or one side (single-sided) of the PCB.
Both have certain benefits and are applied in various situations. This article offers a thorough comparison of SMT and Through Hole so that procurement experts and design engineers could decide with knowledge. Economically, nevertheless the decision will rely on various technological and financial considerations.
1. Standard Soldering Technologies:
Surface Mount Technology (SMT): Surface Mount Devices (SMDs) typically have smaller footprints, allowing for smaller designs and high-density layouts. Using automated pick-and-place devices, components are put directly onto the surface of the printed circuit board.
Through-Hole Technology (THT): The leads of the components are soldered into place after being put into pre-drilled holes in the printed circuit board (PCB) using through-hole technology (THT). On the flip side either we can do wave soldering or manual handling. Commonly used for mechanically stressed components, large capacitors, or connections.
2. SMT PCB Assembly:
Direct component mounting onto printed circuit boards is accomplished by surface mount technology (SMT) PCB assembly, which is employed in batch solder reflow. Solder paste is put to the PCB to begin the procedure. Careful placement of the components on the board will be done in a safe manner. The next step is to carefully heat the assembly in a reflow oven. A connection is formed between the PCB and the components when the solder paste melts, also known as "reflow," beneath the heat. After cooling, the solder cures, creating a solid bond between the PCB and the components. SMT assembly makes extensive use of robotics. This might result in significant labor cost savings for large manufacturing runs.
Small metal or ceramic contacts on their bottom allow them to be connected straight into pads on the PCB rather than wire leads. Lighter components and high density assembly are guaranteed by this special packaging. SMDs have unique packaging unlike that of conventional components.
3. Through-Hole Assembly:
THT assembly begins with exact hole drilling into the PCB. These holes fit the requirements for the components to be fastened. These holes are filled with leads from the THT components thus ready for the soldering operation. Two techniques of soldering are selective soldering and wave soldering.
A solid electrical and physical connection between the lead and the PCB assembly can be achieved by filling the hole with hot solder. A molten pool of solder is passed across the PCBA during wave soldering. A "wave" of solder is created by a pump and adheres to the printed circuit board assembly (PCBA), securing the components. Conversely, PCVA locations that require soldering are specifically targeted by selective soldering. This method eliminates the need for solder masks by precisely dropping solder on the board where it is required.
4. Comparing SMT and Through-Hole Assembly Costs
| Cost Factor | SMT Assembly | Through-Hole Assembly | Notes |
|---|---|---|---|
| Labor Cost | Lower | Higher | SMT is largely automated with pick‑and‑place and reflow; through‑hole often requires manual insertion or selective soldering. |
| Setup & Tooling | Lower for volume runs | Higher | SMT stencils are low‑cost at scale; through‑hole fixtures and wave solder setups increase costs, especially for low quantities. |
| Component Cost | Depends | Depends | SMDs and THT parts may cost similarly; differences often depend on package availability and sourcing efficiency. |
| Board Complexity Cost | Efficient | More Expensive | SMT supports high density without extra PCB machining; complex through‑hole layouts (e.g., plated holes) increase fabrication steps. |
| Production Speed | Faster | Slower | Automated SMT lines produce faster cycle times, reducing per‑unit cost. Through‑hole requires slower manual/ selective processes. |
| Yield & Rework Cost | High | Variable | SMT yields high consistency with AOI/X‑ray; through‑hole rework can be more labor‑intensive. |
| Inspection & Test Cost | Moderate | Moderate | Both require inspection; SMT often uses AOI/X‑ray, through‑hole uses AOI + manual checks. |
| Prototype Cost | Moderate | Higher | SMT prototypes benefit from stencil reuse; through‑hole prototypes cost more per unit. |
| Small Batch Cost | Favorable | Less Favorable | SMT scales better for small batches; through‑hole’s manual costs are amplified at low volumes. |
| High‑Volume Cost | Most Cost‑Effective | Less Efficient | SMT has significant volume economy due to automation and speed. |
| Total Cost of Ownership | Lower in most cases | Higher in niche cases | Unless design constraints force through‑hole (mechanical strength), SMT tends to deliver lower overall costs. |
1) Material and Component Costs
Because of their standardized containers and broad availability, SMT components—which are usually smaller and less expensive to manufacture in great numbers—are Their less weight lowers shipping costs and resource use. Conversely, especially when manufacturers move manufacturing toward SMT for mainstream electronics, THT components often be bigger, heavier, and more costly.
2) PCB Manufacturing Costs
Particularly for multilayer boards the through-hole assembly calls for drilling holes in the PCB. Which adds an additional fabrication process step and raises manufacturing costs. Because they need less plated-through holes therefore lowering manufacturing complexity and material utilization is there. SMT PCBs are simpler and less expensive to construct.
3) Equipment and Setup Costs
Establishing an SMT assembly line calls for large upfront equipment purchases including automated placement systems and reflow furnaces. But since reduced per-unit assembly costs allow this arrangement to become more affordable over time for big manufacturing runs. Although through-hole assembly initially has less setup costs, human labor and lengthier manufacturing cycles cause it to become more costly on scale.
4) Testing and Quality Control
With the use of automated inspection systems like AOI and SPI. SMT processes assist in fault detection rates and rework cost reduction. Conversely, for more complicated assemblies through-hole assembly often calls for human inspection that raises both time and personnel expenses in quality control.
5) Repair and Rework Costs
Because of their greater size, through-hole components are usually easier to replace during rework; yet, rework SMT boards calls for specific tools and qualified experts, hence raising repair costs. Higher assembly precision in automated SMT lines, however, sometimes results in a lesser demand for rework.
Conclusion
Because of automation, reduced component sizes, and lower per-unit costs at volume, SMT is obviously the more cost-effective assembly technique for most modern electronic products especially in consumer electronics, telecommunications and computers. Still, through-hole assembly is important in specialized uses where mechanical strength, durability, or particular component availability take front stage. SMT is the recommended solution for small and high-density designs, usually where mass production is taken into account.
Through-hole may offer the greatest value for goods but depends on conditions like limited batch runs and high labour. Production volume, application type, and functional requirements ultimately define the most affordable strategy.
To support these diverse needs, JLCPCB offers both SMT and through-hole assembly services with professional quality, fast turnaround, and competitive pricing. Whether you’re prototyping or moving into large-scale production, you can rely on JLCPCB to bring your designs to life
Popular Articles
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Everything You Need to Know About Solder Wire
The Latin word solidare means "to make solid," this is where the term solder gets its start. For joining two metal parts, this alloy is used because of its low melting point. Solder is a substance that is used to attach items, basically we can say wires and leads components together. Soldering is considered a skill in electronics for assembly of components onto a bare board PCB. The solder wire used has a significant impact on how well a soldering project turns out. It consists of alloys, mostly based......
SMT vs Through Hole: Which PCB Assembly is Most Cost-Effective?
Performance and cost in the realm of electronics production depend on choosing the correct assembly method. Of the several approaches accessible, Surface Mount Technology (SMT) and Through-Hole Technology (THT) are the two most often used ones for PCB assembly. These two assemblies can be combined to create some products or used as individual technologies. Though seemingly little, this variance affects several aspects including board design, materials and techniques employed, heat dissipation, and rel......
PCB Soldering Basic Techniques and Overview
Soldering means joining metal components with a melted metal called solder, which has a low melting point compared to other metals. Soldering is crucial in the electronics industry and is the primary method of joining electrical components. There are different types of soldering materials based on quality and their melting points. The most common combination is a tin or lead metal alloy mixed with silver or brass. The soldering iron melts the metal so it can be used like glue to connect two pieces. On......
Lead-Free Solder vs Lead Solder : What is the Difference?
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties ......
How to Repair a Burnt Circuit Board (and When to Replace It)
Key Takeaways Find out why the board burnt before you repair anything. The part that charred is often a victim of a fault somewhere else. Charred FR-4 conducts. A repair only lasts if every trace of carbon is cut out and the area measures as an insulator again. Heat that went through the board, blistering, or a burn among vias or under a BGA usually means replacing the board. Rebuild a burnt trace heavier than the original, and keep conductive epoxy off power paths. Power the repaired board from a cur......
How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?
Wave soldering is a process used for soldering electronic components by inserting them into the holes on a Printed Circuit Board (PCB) and securing the components to the board using a molten solder wave generated by a wave soldering machine. Temperature is a crucial parameter during the wave soldering process, as it directly affects the quality and efficiency of soldering. Therefore, setting the temperature correctly for wave soldering is essential. Temperature for Wave Soldering Wave soldering machin......