How Photodiode Differs from Phototransistor
7 min
- What is a Photodiode?
- What is a Phototransistor?
- Key differences between a Photodiode and a Phototransistor
- When to Choose Between a Photodiode and a Phototransistor
- Conclusion
- FAQ
For two centuries, light-sensitive devices have been widely employed, primarily for wireless applications. From the automatic street lamps to your television remote. Photodiodes and phototransistors are two of the most popular elements to make this happen. The main principle here is to convert light energy into electrical signals, and then these electrical signals are processed to take further action. However, the operational processes, signal types, and applications of photodiodes and transistors are significantly distinct. Understanding these differences can help you select the right one for your electronic design.
What is a Photodiode?
A photodiode is a semiconductor electronic component that produces an electrical charge (based on electron and hole pairs). The phenomenon happens when light falls on the backside or front side of a prepackaged silicon, GaAs, InGaAs, SiC, or other semiconductor wafer. A photodiode is essentially a PN junction diode, but biased in reverse bias. When a reverse bias is applied, a depletion region forms. When light falls upon the junction, the generation of an electron-hole pair is referred to as photocurrent.
Circuit Symbol of Photodiode
(Arrows pointing toward the diode indicate incoming light.)
Structure
A photodiode is a single PN junction. It is composed of semiconductor materials such as Silicon (Si) for visible and near-infrared applications, or Gallium Arsenide (GaAs) for infrared.
Working Principle:
A photodiode mainly works in reverse bias. In reverse bias, the depletion region expands, and more of the light-induced carriers have the opportunity to support current. The operation has two modes:
Photovoltaic Mode (No external supply)
- It generates a voltage when the photodiode is illuminated.
- It is used in solar cells, energy harvesters, and low-power sensors.
Photoconductive Mode (Reverse-biased)
- Size and speed are improved under reverse bias.
- Enables fast response to changing light intensity.
The output current is directly proportional to the intensity of the incident light. This thing makes photodiodes extremely useful for accurate linear measurement of light levels.
Where It Is Used
Photodiodes are ideal for applications requiring high speed, high accuracy, and linear response, such as:
- Optical fiber communication receivers
- Barcode scanners
- Medical instruments (pulse oximeters, spectrometers)
- Light meters and scientific measuring equipment
- Smoke and flame detection systems
JLCPCB's ultra-precision PCB fabrication for custom sensor PCBs encloses photodiodes, guarantees low-noise routing and signal integrity (signal quality is critical for sensitive analog light-measurement circuits).
What is a Phototransistor?
A phototransistor is a transistor that responds to light. One can think of it as having a photodiode integrated as a BJT. The base here accepts the light as excitation, but the overall signal is amplified due to its operation as a BJT. A light-induced base current flows; this current can be amplified by the transistor's current gain. This leads to an output current quite a bit larger than what you could get from a photodiode.
Circuit Symbol of Phototransistor
(Arrows indicate incoming light on a transistor structure.)
Structure:
A phototransistor is made in the form of a standard BJT with three semiconductor layers, including collector, base , and emitter. It's an NPN or a PNP configuration, possible. Some phototransistors have only two leads (collector and emitter) and use the base lead connected to the case.
Working Principle:
The phototransistor is a forward-active device, so that light operates its base current. Light hits the base region, then a respective current as a function of light is produced. The transistor amplifies this current by its current gain (β), and a much larger collector current is obtained at the output. This internal amplification makes phototransistors sensitive to even small levels of light. However, due to the internal capacitance and carrier storage, it has a slower response than a photodiode.
Where It Is Used:
Phototransistors are good for high sensitivity and switching applications, such as:
- Infrared receiving and remote control systems
- Light-activated switches and alarms
- Optocouplers for isolation
- Security and object detection systems
- Automatic brightness control and light-triggered relays
When building phototransistor-based sensing circuits, JLCPCB’s PCB Assembly (PCBA) service can automatically place these fragile parts with precision for reliable sensor performance.
Key differences between a Photodiode and a Phototransistor
| Basis of Difference | Photodiode | Phototransistor |
| Definition | A photodiode is a semiconductor element including a PN junction therein, which converts incoming light into electric signals. | A phototransistor is a photosensitive transistor that generates and amplifies current when exposed to light. |
| Circuit Symbol | ||
| Terminals | It has two contacts known as the anode and the cathode. | It has two or sometimes three terminals — emitter, collector, and perhaps base. |
| Semiconductor Regions | Comprised of a P-type region and an N-type region. | It consists of a collector as well, a base, and an emitter. |
| Number of PN Junctions | Contains a single PN junction. | Contains two PN junctions. |
| Types | Photodiodes generally have a single basic structure without classification. | Phototransistors are classified as NPN or PNP types. |
| Biasing | Operates in reverse bias to detect light effectively. | Works in forward bias to allow current flow and amplification. |
| Main Function | It is a light-activated device to directly converts the solar energy into electricity. | Converts light energy into electrical energy and further amplifies the resulting signal. |
| Sensitivity | Offers lower sensitivity since it lacks internal amplification. | Translates light into electricity and amplifies the resultant signal. |
| Response Time | Responds very quickly to light changes, offering fast switching. | Responds relatively slowly because of its internal amplification process. |
| External Power Requirement | It can function without an external power supply. | Requires an external power source for proper operation. |
| Cost | Simple design makes it inexpensive. | A more complex design makes it costlier. |
| Output Type | Produces both voltage and current output, depending on the configuration. | Primarily produces a current output. |
| Applications | Used in solar cells, optical communication, smoke detectors, object counters, and safety systems. | It is widely used in light sensors, infrared receiving, remote control, and security devices. |
When to Choose Between a Photodiode and a Phototransistor
Use a Photodiode when:
- You need a fast response and precision.
- The system involves light measurement or data communication.
- Accuracy and linearity matter more than signal strength.
Use a Phototransistor when:
- You need a simple, sensitive light sensor.
- You want a strong output without extra amplifiers.
- Response speed is not the top priority.
In authetic designs, one typically combines a photodiode’s speed with its sensitivity by adding amplifiers to amplify the signals from the photosensors. Phototransistors, in contrast, may generally be driven with no other element, so that circuitry is simplified. But being a PCB engineer, why not just prototype both of them and see which one works better in the field? The cheap PCB prototyping by JLCPCB makes this process straightforward and budget-friendly.
Conclusion
In this article, the first devices have been presented and classified according to sensitivity as diodes or transistors. Both photodiodes and phototransistors are important in modern electronics. Their applications differ due to the structural and operating differences. Photodiodes have a fast response time, excellent linearity, and a high level of precision. These are widely used where the transients occur more often. On the other hand, phototransistors provide higher sensitivity to light and are well-suited for applications requiring switching or precise duty cycles. Such differences facilitate good choices for engineers and designers, which is very helpful to achieve the best performance in optical sensing systems. Knowing these differences means you will select the correct component for your circuit. And now JLCPCB is making your sensor ideas a reality with high-quality PCBs, making it easier for innovation, testing, or the end product.
FAQ
Q: Can a photodiode work without external power?
Yes. In photovoltaic mode it generates voltage directly from light with no external supply needed.
Q: Why is a phototransistor more sensitive?
It has internal current amplification (β gain), producing a much larger output from the same light level.
Q: Which device is better for high-speed applications?
Photodiode. It offers faster response time without the carrier storage delay of a phototransistor.
Q: Are phototransistors suitable for precise light measurement?
No. They are better for switching or detection; photodiodes provide superior linearity and accuracy.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
• Design Guidelines for PCB Using FR4 Substrates
Keep Learning
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......
A Practical Guide to Circuit Design from Concept to PCB
Key Takeaways Define clear circuit requirements and select suitable components based on electrical ratings, performance, and availability. Follow a structured design workflow from schematic capture and simulation to PCB layout and validation. Optimize component placement, routing, power distribution, and signal integrity to improve circuit performance. Apply DFM guidelines and complete ERC/DRC checks to prevent design errors and ensure smooth PCB manufacturing. Choose appropriate PCB materials, layer ......
PCB Silkscreen: All You Need to Know
Key Takeaways The PCB Silkscreen Guide demonstrates that a properly designed legend layer is essential to prevent assembly failures and ensure long-term hardware reliability. By mastering modern manufacturing methodologies like Direct Legend Printing (DLP) and aligning layouts with JLCPCB's strict DFM design rules—including the absolute 0.8 mm character height limit and the automated 0.15 mm silkscreen clipping protocol driven by solder mask precedence—engineers can seamlessly eliminate cold joints an......
The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
Note Need a quick reference while reading schematics? Download our free, printable Circuit Symbols Cheat Sheet (PDF), featuring the most common IEC and ANSI symbols organized by category. Keep it on your desktop or print it for easy reference at your workbench. ⬇ Download the Free Circuit Symbols Cheat Sheet (PDF) Every electronic diagram is written in a visual language, and circuit symbols are its alphabet. From your first electrical schematic to a multi-layer board, knowing circuit symbols can make ......
Understanding Electrical Schematics: A Comprehensive Guide
Key Takeaways Schematics vs. Block Diagrams: Schematics detail exact components and connections; block diagrams only show high-level functions. Mark Polarity: Essential to prevent circuit failure and automated SMT placement errors at JLCPCB. Clean Layout: Use modular blocks and net labels (VIN, GND) to eliminate visual clutter. Manufacturing Ready: Follow DFM trace rules and export standard Gerber, BOM (LCSC C-IDs), and CPL files. Fast Troubleshooting: Isolate schematic blocks to test expected voltage......
PCB Board Design: A Step-by-Step Guide for Beginners
Key Takeaways This PCB Design Guide offers beginners a practical step-by-step approach to designing a compact 3A IP2312 lithium battery charger PCB — an upgraded alternative to the popular TP4056 module. It focuses on key techniques like schematic creation, optimized layout, proper trace routing for 3A current, and ground planes to build efficient and reliable boards. Printed Circuit Boards (PCBs) form the backbone of most modern electronic devices, providing a platform to connect electronic component......