Blank PCB and Parts : Building on Empty Boards
7 min
- Blank PCB Material Breakdown & Selection
- Top Blank PCB Formats for DIY & Prototyping
- Essential Parts to Pair with Blank PCBs
- Turning a Blank PCB into a Working Project
- Conclusion
A blank PCB refers to an unpopulated circuit board with no components assembled. A blank PCB is an empty circuit board, manufactured from a copper-clad substrate, drilled, masked, and finished. It’s the canvas engineers use for prototypes, experiments and hobby builds. Blank boards are simple PCBs without components. Let’s dig deeper into the article to find out some standards and technologies used in the industry.
Universal Blank Boards vs Pre-routed Prototyping Boards
Universal blank boards are copper-clad sheets and generic protoboards. These are sheets or panels of copper on an insulating substrate. You can etch or manually wire them. Great for custom shapes and one-off experiments. Ideal for labs, low-volume custom etching, or when you want to do your own trace design by hand.
Pre-routed prototyping boards are perfboard and SMD grids. These come with ready-made hole grids or SMD footprint arrays. They’re convenient for breadboard-to-PCB transitions and blank PCBs for diy projects where you want speed over custom routing. Both have their place: universal blanks for custom and pre-routed prototyping boards for speed.
Copper Clad Types: Single vs Double-Sided vs Multi-layer
- Single-sided (1-layer): Copper is applied only to one side of the circuit board. They are cheaper than double-sided boards and have a good degree of mechanical stability. Single-Sided Layouts are suitable for a project that does not require a complex wiring scheme and may include some jumper wires.
- Double-sided (2-layer): Copper is applied to both faces of the printed circuit board with plated through holes and vias. Most double-sided circuit boards allow routing of traces on both faces, which makes them the most common type of printed circuit board. They typically include a ground plane on one face and signal traces on the opposite face. Double-sided circuit boards are typically an economical solution for lower complexity PCB designs.
- Multi-layer (4+ layers): For dense and more complex designs, we require multiple layers with a proper stackup. Through which we can control impedance, or noisy/fast circuits. For high-speed design, it is recommended to keep signal and power integrity rules in mind.
Blank PCB Material Breakdown & Selection
FR-4, CEM-1, Aluminium, Flexible – When to Use Each
FR-4 (glass-epoxy) is the most commonly used one. FR-4 is low-cost and has good mechanical stability. FR-4 can be used for fast blank PCB prototyping.
CEM-1 / CEM-3: CEM-1 is a paper-based laminate with a single fibreglass layer. It is typically single-sided and has lower mechanical strength. These substrates do not perform well under high frequency. CEM-3, on the other hand, uses woven fibreglass similar to FR-4. It offers better strength and double-sided support.
Aluminium (MCPCB): Metal-core PCBs are suitable for thermal dissipation. They are ideal for LED arrays and power-dissipating modules. Prototype aluminium boards commonly start at a higher price than FR-4.
Flexible (polyimide): Use when you need bendability in wearables. Flex adds design complexity and cost but enables unique form factors.
Match material to thermal, mechanical, and routing needs.
Thickness, Copper Weight & Temperature Rating Quick Table
| Property | Typical values |
| Board thickness | 0.8 mm / 1.0 mm / 1.6 mm (standard) / 2.0 mm |
| Copper weight | 1 oz (35 µm), 2 oz (70 µm), heavier |
| Tg (glass transition) | Standard FR-4 = 130–140 °C; High-Tg = 170–230 °C |
| Thermal conductivity | 1–3 W/mK (depends on core) |
Top Blank PCB Formats for DIY & Prototyping
Standard Eurocard Sizes & Stripboard Alternatives
Standard eurocard sizes are100 × 160 mm and 100 × 100 mm. Stripboard is a continuous copper strip for through-hole prototyping. They are fast for discrete circuits but messy for dense routing. Stripboard alternatives include perfboard, pad-per-hole protoboards, and SMD grid boards. If you plan on repeating iterations, choose a standard size that matches your fab’s most cost-effective panelization.
SMD-Friendly Blank Boards (0603/0402 Footprint Grids)
Many blank SMD protoboards ship with grid footprints for 0603/0805 packages. Fewer support ultra-tiny 0402 without careful layout. If you plan to hand-place SMDs, verify pad sizes and spacing. For tiny SMD work, we can design a custom SMD grid with generous pad fillets and thermal relief.
Through-Hole Perfboard Evolution (2.54 mm vs 2.0 mm)
2.54 mm (0.1") is the standard perfboard and is compatible with DIP ICs and most hobby connectors. Similarly, the 2.0 mm one is used for compactness but reduces interchangeability. Hence, choose a pitch based on the components you expect to mount.
Essential Parts to Pair with Blank PCBs
Must-Have Connector Strips, Pin Headers & Terminal Blocks
Pin headers with a 2.54 mm pitch are lifesavers for modular testing. They allow easy mating with breadboards and jumpers. Terminal blocks are essential for speaker outputs, power inputs or field wiring on a blank PCB for diy projects. Similarly, the edge connectors or card edge pads are used for designing Eurocard-like modules. Invest in a handful of vertical and right-angle headers, as well as a few types of terminal blocks.
Prototyping Jumper Wires, Sockets & Breakout Helpers
Female and male jumper wires are required for rapid wiring. IC sockets DIP or SMD adaptors are used for hot-swapping and burn-in. Breakout boards for tiny QFN/BGA parts reduce soldering risk. These parts are worth their weight in gold for saving time and frustration.
Turning a Blank PCB into a Working Project
How you populate a blank board matters, so choose a method that fits volume:
Dead-Bug vs Manhattan vs Proper Etching Routes
- Dead-bug: Flip ICs upside down and solder wires to their pins. It is a fast method for RF due to its lower lead inductance.
- Manhattan style: Use small copper islands glued to a copper pad and wire components between them.
- Proper etching / routed PCB: Design traces by using plated through-hole vias and a professional route with repeatable reliability.
For quick experiments or RF tweaks, Manhattan is a lifesaver.
5-Minute SMD Soldering Tricks on Blank Boards
Tack one corner, align, then flow the remaining pins with hot air or reflow. Apply liquid flux liberally because it reduces heat time and eases bridging. Use a solder paste stencil or syringe for arrays of pads of the same size; this speeds up assembly. Pre-tinning pads can help with larger parts to prevent tombstoning. If your project involves blank PCB prototyping with numerous SMDs, consider using a cost-effective stencil from your fabrication facility.
Conclusion
This is all about blank boards; we have covered the types and standards of blank boards. Standard FR-4 can be used in electronics for general applications; Aluminium is used for power/ heat dissipation for this type of use; Flex PCBs may be employed for wearable or curved product designs. Most prototyping types require 1 Oz copper and 1.6mm thickness, while upgrading the copper thickness will be necessary for any use case that requires substantial current to flow through the PCB.
- For cheap prototyping, small two-layer runs from online fabs can be highly affordable. Consider the tradeoff between unit price, turn time and shipping.
- For thermal-heavy designs (MCPCB), expect higher prototype costs; small aluminium boards typically cost more than FR-4, ranging from $10–$100, depending on size.
Popular Articles
• AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
• GPT-6 Astra PCB Design in KiCad: From Brief to Verified Native Project
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• How to Design Your Own Keyboard PCB: From Layout to Firmware
Keep Learning
AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
Note This article is intended to provide an independent technical overview of AI-powered PCB design tools based on publicly available product information. Product features and capabilities may change over time. AI tools can now assist with PCB architecture, schematic generation, component selection, placement, routing, and design verification. However, different tools target different stages of the PCB workflow. This guide compares AI tools for PCB design based on what they actually do, what inputs th......
KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
Key Takeaways Claude can design PCBs in KiCad: By connecting Claude to KiCad through an MCP server, you can use AI to create and modify PCB designs. In this project, Claude helped turn a 5 A XL4015 buck converter netlist into a two-layer, 63 × 33 mm PCB layout with zero ERC violations and zero DRC errors after minor initial fixes. Set up Claude securely: Use a KiCad MCP server that starts in read-only mode. Review the server code before installing it, connect through stdio, and allow editing only in a......
From Concept to Production: PCB DFM Guidelines and Analysis
Key Takeaways PCB DFM (Design for Manufacturing) is the bridge between design intent and manufacturing reality, ensuring a board can actually be fabricated and assembled with high yield. Essential DFM guidelines cover trace width and spacing, annular rings, via placement and drill sizes, soldermask and silkscreen, surface finish, and panelization. Modern DFM analysis is data-driven and automated, and many manufacturers now offer free DFM tools that check Gerber and drill files against fabrication and ......
Understanding PCB Resistance: Key Factors, Testing Methods, and Design Best Practices
How easily current flows through a circuit board is determined by its resistance. Although some resistance is provided by each trace and component on the board, the objective is to reduce it. When the material that electrons pass through blocks or slows down their flow, resistance results. Energy is lost as a result of this obstruction, frequently as heat. Trace resistance is a crucial factor in determining the circuit's operational current in power-related circuits, such as amplifier units. To guaran......
PCB Routers: Essential Tools for Modern Circuit Design
Introduction In modern PCB production, routing machines (commonly called PCB routers or CNC routers) play a critical role. They are used to cut the board outline, create V-grooves for depanelization, mill slots, and finish edges with high precision. As electronic devices become smaller and more complex, PCB routers ensure clean, accurate, and repeatable results. This article explains what PCB routers are, their types, key applications, best practices, and how JLCPCB integrates advanced routing in its ......
Creating Clear and Professional Reference Designators for Better PCB Assembly
Key Takeaways Reference designators are essential for accurate PCB assembly, debugging, and maintenance. Use minimum 0.8 mm text height and 0.15 mm line width for clear silkscreen printing. Keep designators on solder mask with proper clearance from pads and vias. Maintain consistent font, size, and orientation across the board. For high-density designs, use an assembly drawing instead of crowded silkscreen. Always run DFM checks to avoid overlapping or missing labels. Ever wonder about the little labe......