Diving Deep in PCB Etching
6 min
- Understanding PCB Etching
- Traditional Etching Techniques
- Innovations in PCB Etching
- Examples of Each Type of PCB Etching:
- Best Practices in PCB Etching
- Conclusion
Hi there! Creating printed circuit boards (PCB's) requires a complex process called PCB etching, which we will examine in this article along with the methods and innovations that have driven this field. Regardless of your background—engineering, hobbyist, student, professional, or enthusiast—JLCPCB provides insightful information about PCB etching.
Understanding PCB Etching
PCB etching is a fundamental step in the production of printed circuit boards. It involves selectively removing copper from the board's surface to create conductive pathways or traces that connect electronic components. The etching process ensures precision and accuracy in creating intricate circuit patterns.
Traditional Etching Techniques
Traditionally, PCB etching has been achieved using chemical methods. Chemical etching is the most widely used method in PCB manufacturing. It involves applying a chemical solution, typically an acid, to selectively remove the copper or unwanted copper from the substrate. The patterned areas are protected by a resist material, which prevents the etching solution from attacking the copper. The most commonly used technique is the Ferric Chloride etching process. Ferric Chloride is a corrosive chemical that reacts with copper, dissolving it and leaving the desired circuit traces intact. This technique has been widely adopted due to its effectiveness and cost-efficiency.
Another popular method is the Ammonium Persulfate etching process, which offers a safer alternative to Ferric Chloride. Ammonium Persulfate is a non-toxic chemical that provides a reliable etching solution, ensuring high-quality results.
Innovations in PCB Etching
With advancements in technology, new techniques and innovations have emerged, revolutionizing the PCB etching process. Here are some notable developments:
Laser Etching:
Laser etching has gained popularity in recent years, is a non-contact etching method that uses a high-power laser to selectively remove the copper from the board. It offers precise control and is suitable for producing intricate patterns on PCBs. Laser etching is commonly used for rapid prototyping or low-volume production. It involves using a laser beam to selectively remove the copper layer, eliminating the need for chemicals. Laser etching provides greater flexibility and accuracy, making it suitable for complex PCB designs.
Electroless Copper Deposition:
This innovative technique involves depositing a thin layer of copper on the entire surface of the PCB, including the etched areas. The deposited copper enhances conductivity and protects the circuit traces from oxidation. Electroless copper deposition improves the overall performance and reliability of the PCB.
Plasma Etching:
Plasma etching is a dry etching process that uses ionized gases to remove the unwanted copper from the board. It offers precise control over the etching depth and allows for etching on different materials, including ceramics and polymers. Plasma etching is commonly used for high-density interconnect (HDI) PCBs and microelectronics. Plasma etching is especially useful for etching very fine features that traditional chemical etching may not be able to achieve.
Photochemical Etching:
Photochemical etching utilizes a photographic process to create a pattern on the PCB. A photosensitive resist is applied to the substrate, exposed to UV light through a mask, and then developed to remove the uncured resist. The exposed areas are subsequently etched using a chemical solution. This method allows for high precision and is often used in the production of complex circuitry.
Examples of Each Type of PCB Etching:
1. Chemical Etching:
Ferric chloride solution: It is commonly used in hobbyist and low-volume PCB production due to its effectiveness and affordability.
Ammonium Persulfate: This etchant is often favored for its faster etching speed and reduced environmental impact compared to traditional acids.
Cupric chloride: It offers a high level of control and is frequently used for fine pitch and high-density circuit boards.
2. Plasma Etching:
Reactive Ion Etching (RIE): It uses a combination of gases such as oxygen and fluorine to create reactive species that selectively remove the copper. RIE provides precise control for advanced PCBs with intricate features.
Ion Beam Etching (IBE): This technique uses a focused beam of ions to etch the copper, allowing for even higher precision and control.
3. Laser Etching:
CO2 laser etching: This method uses a high-powered CO2 laser to vaporize or ablate the unwanted copper, leaving behind the desired circuit pattern. It is commonly used for rapid prototyping or small-scale production.
Nd:YAG laser etching: This laser etching technique offers higher precision and is suitable for more complex PCB designs. It can accurately etch fine features, making it popular for high-density circuit boards.
4. Photochemical Etching:
Dry film resist etching: It involves applying a photosensitive dry film resist to the copper surface, exposing it to UV light through a patterned mask, and developing to remove the uncured resist. The exposed areas can then be etched using a chemical solution.
Liquid photoresist etching: This method uses a liquid photoresist that is applied to the substrate and cured under UV light. The cured resist is then selectively removed using a solvent, allowing for precise control during etching.
*The choice of etching technique depends on factors such as the complexity of the design, production volume, and desired level of precision.
Best Practices in PCB Etching
To ensure optimal results and maintain the integrity of the circuit design during the etching process, it is essential to follow best practices. Here are some recommendations:
Etchant Agitation:
Proper agitation of the etchant solution helps maintain a consistent etching rate and prevents the formation of uneven traces. Stir or agitate the etchant regularly during the etching process.
Temperature Control:
Monitor and control the temperature of the etchant solution. Higher temperatures can accelerate the etching process, but excessive heat may lead to overetching or poor quality traces.
Masking and Alignment:
Accurate alignment and proper masking techniques are crucial to ensure precise etching. Use high-quality masks and align the PCB carefully to avoid any misalignment or errors in the circuit pattern.
Conclusion
PCB etching is a vital process in the production of printed circuit boards, enabling the creation of intricate circuit patterns that drive modern electronics. In this article, we explored traditional etching techniques as well as innovative methods. By following best practices and embracing new advancements, you can achieve high-quality PCBs with enhanced performance.
Here at JLCPCB, our goal is to give you the most recent information on industry developments, PCB design, manufacturing, and assembly knowledge. We hope our blog has deepened your understanding of PCB etching and inspired you to explore new possibilities in your electronic projects.Watch this space for additional educational content as we immerse our readers in the world of PCB technology through inspiration, education, and engagement!
Keep Learning
Technical Guidance: Mouse Bite Panelization Guide
The conventional method of panelization uses V-grooves. However, for irregularly-shaped boards or special requirements (such as JLCPCB's economic SMT assembly), mouse bite panelization, which resembles postage stamps on an envelope, is required. PCBs panelized using this method are called "mouse bite panels" or "mouse bite connections". Mouse bite panelization can be referred to as "universal panelization." As long as there is a position to add mouse bites, boards of various shapes can be interconnect......
Technical Guidance: V-Cut Panelization Standards
For boards with regular rectangular shapes, V-cut (V-scoring) panelization is an efficient method. This process involves cutting V-shaped grooves of a specific depth on both sides of the panel along the board boundaries, leaving a thin web of material (typically about 1/3 of the board thickness) that allows easy manual separation after SMT assembly. After separation, minor thread-like fibers or rough edges may remain and can be lightly scraped off. Due to material expansion and cracking during depanel......
How Laser-Made PCBs Are Used in Rapid Prototyping
Key Takeaways Speed & Precision: Digital lasers enable 24-hour quick-turn HDI and FPC prototyping without mechanical tooling. LDI Patterning: Replaces physical photo-films to deliver precise circuit traces down to 2/2 mil. HDI Microvias: UV/CO2 lasers drill 0.075–0.15 mm blind vias (1:1 aspect ratio) for 1+N+1 to 3+N+3 stackups. Laser Profiling & Stencils: Achieves ±0.05 mm FPC cut accuracy and ±0.003 mm LPKF stencil aperture precision. Laser DFM: Maintain ≥ 0.30 mm copper clearance on FPCs and ≥ 0.07......
A Beginners Guide to Tented vs Untented Vias
Via’s are important, If working at high speed design and HDI boards then they become super important. Choosing a type of via during PCB manufacturing matters. Via’s are basically joining two or more layer traces together. Shape, size and track length guidelines became more interesting at high frequency and high speed signals. Today in this article we will explore a fabrication side, the decision to use tented or untented vias. This beginner-friendly guide explains what tented vias are, the differences......
Flex PCB Fabrication: Process, Materials, Design Rules & Cost
Many of the basic steps in rigid PCB fabrication also apply to flexible PCB fabrication. However, it is made with thin polyimide or PET films that can swell or shrink during processing due to moisture and temperature changes. These material attributes bring further complexities to considerations of layer alignment, coverlay openings, and bend-zone design. For instance, if there's not enough room for adhesive flow in a coverlay opening, or if a via falls in a bend zone, manufacturing defects or assembl......
Smart PCB Array Design for Higher Yield and Lower Production Costs
Key Takeaways Smart PCB array design is a critical strategy for achieving higher manufacturing yield and significantly lower production costs. By optimizing panelization with proper board spacing, V-scoring, tab routing, and mouse bites, designers can dramatically improve material utilization by 20-30%, enhance production throughput, and simplify handling and depaneling while minimizing mechanical stress and defects. Effective use of fiducials and careful component clearance further ensures high-quali......