PCB Basic 3: Understanding PCB Manufacturing Processes
9 min
- Substrate Selection: Laying the Foundation
- Layer Imaging and Etching: Giving Shape to Your Design
- Finishing: Protecting and Enhancing Your PCB
- Advanced Manufacturing Techniques: Pushing the Boundaries
- Quality Control Measures and Inspection Methods
- Conclusion:
Welcome to the third installment of our PCB Basics series. In this article, we will unravel the step-by-step process of PCB manufacturing, guiding you through each stage with clarity and precision.
Join us as we embark on this educational journey and discover how JLCPCB's advanced manufacturing capabilities and technology together with unparalleled commitment to quality assurance can elevate your PCB designs to the next level.
Substrate Selection: Laying the Foundation
One of the critical steps in PCB manufacturing is selecting the right substrate material. The substrate serves as the foundation upon which the circuitry is built. It is essential to choose a substrate material that meets the electrical, thermal, mechanical, and cost requirements of your design. The choice of substrate material can impact the performance, reliability, and manufacturability of the PCB.
FR-4 is the most commonly used substrate material in the industry due to its excellent electrical insulation properties and cost-effectiveness. It is composed of woven fiberglass impregnated with an epoxy resin. The combination of fiberglass and epoxy provides a robust and rigid base for the PCB. JLCPCB uses Grade A FR-4 laminates from suppliers including Nan Ya, KB, and Shengyi, with Tg options of 130°C (standard) or 155°C (high Tg) for enhanced thermal performance. Additionally, FR-4 offers good thermal stability and dimensional stability, making it suitable for a wide range of applications.
Flexible materials, such as polyimide (PI), are ideal for applications that require flexibility or bending. These materials offer excellent resistance to heat and chemicals, making them suitable for aerospace, automotive, and wearable electronics.
Specialized substrates, such as Rogers materials (including Rogers and PTFE/Teflon variants), are designed for high-frequency applications where signal integrity is crucial. These materials have low dielectric loss and can provide consistent performance at high frequencies.
By carefully considering the electrical, thermal, mechanical, and cost requirements of your design, you can select the most suitable substrate material that ensures optimal performance and reliability.
Layer Imaging and Etching: Giving Shape to Your Design
Once the substrate is selected, the next step is layer imaging and etching. Layer imaging involves transferring the PCB design onto the substrate surface. The process begins by applying a thin layer of photosensitive material, called photoresist, onto the substrate. The photoresist is then exposed to UV light through a photomask, which contains the desired PCB pattern. The UV light causes a chemical reaction in the photoresist, creating a patterned layer.
After the layer imaging process, the unwanted copper on the substrate is removed through etching. Etching is achieved by immersing the substrate in an etchant solution that selectively dissolves the exposed copper, leaving behind the desired circuit pattern. The etchant solution typically contains chemicals such as ferric chloride or ammonium persulfate.
To ensure precise and accurate etching, it's important to control the etching time, temperature, and agitation of the etchant solution. Over-etching can result in thin or weak traces, while under-etching can leave excess copper, causing short circuits or signal integrity issues.
Finishing: Protecting and Enhancing Your PCB
Finishing processes play a crucial role in protecting the PCB and facilitating efficient assembly. One of the essential finishing steps is the application of a solder mask. The solder mask is a protective layer that covers the copper traces, preventing oxidation, solder bridging, and environmental damage. It also provides insulation between adjacent traces and pads.
Surface finish technologies are used to enhance the solderability of the PCB and facilitate the soldering process during assembly. JLCPCB offers HASL (leaded/lead-free), ENIG, and OSP (with OSP mainly for copper-core boards; FR-4 boards support all three, while 6+ layers and RF boards typically use ENIG). HASL involves immersing the PCB in a bath of molten solder, followed by hot air leveling to remove excess solder, leaving a uniform coating on the copper surfaces. This method is cost-effective and widely used in the industry. ENIG is a popular surface finish for its excellent solderability and corrosion resistance. It involves depositing a thin layer of nickel followed by a layer of gold on the copper surfaces. The gold layer provides a reliable surface for soldering and ensures good electrical contacts. OSP is a surface finish that involves applying an organic compound to protect the copper surfaces during storage and assembly. It is cost-effective and environmentally friendly, but it may require additional steps to ensure good solderability.
HASL involves immersing the PCB in a bath of molten solder, followed by hot air leveling to remove excess solder, leaving a uniform coating on the copper surfaces. This method is cost-effective and widely used in the industry.
ENIG is a popular surface finish for its excellent solderability and corrosion resistance. It involves depositing a thin layer of nickel followed by a layer of gold on the copper surfaces. The gold layer provides a reliable surface for soldering and ensures good electrical contacts.
OSP is a surface finish that involves applying an organic compound to protect the copper surfaces during storage and assembly. It is cost-effective and environmentally friendly, but it may require additional steps to ensure good solderability.
Legend printing is another finishing step that involves adding identification markings and component references on the PCB. These markings facilitate assembly and troubleshooting processes. Legend printing can be achieved using methods such as screen printing or inkjet printing.
By selecting the appropriate finishing techniques, you can protect your PCB from environmental and mechanical stresses while enhancing its functionality and reliability during assembly and operation.
Advanced Manufacturing Techniques: Pushing the Boundaries
In addition to the fundamental steps of PCB manufacturing, there are advanced techniques that have revolutionized the industry and enabled the production of more complex and high-performance PCBs.
Multilayer PCB fabrication is a technique used when the circuit design requires more than two layers of copper traces. JLCPCB supports multilayer PCBs from 1 to 32 layers with controlled impedance available for 4+ layers (tolerance ±10%). Multilayer PCBs are created by laminating multiple layers of substrate material with copper foils in between. Each layer is patterned with the desired circuitry, and vias are drilled to establish electrical connections between the layers. The stack-up and arrangement of layers are carefully designed to ensure signal integrity, power distribution, and thermal management. Multilayer PCBs allow for increased circuit density, reduced size, and improved electrical performance, making them suitable for advanced applications such as high-speed communication systems, computer motherboards, and complex electronic devices.
Surface Mount Technology (SMT) is another significant advancement in PCB manufacturing. SMT involves mounting electronic components directly onto the surface of the PCB, as opposed to through-hole components that require leads passing through drilled holes. SMT components are typically smaller, lighter, and more efficient, allowing for higher circuit densities and improved signal integrity. SMT components are placed on the PCB using automated assembly machines, which increase the speed and accuracy of the assembly process. SMT has become the standard in most electronic devices due to its cost-effectiveness, reliability, and compatibility with modern manufacturing techniques.
These advanced manufacturing techniques require specialized equipment, skilled operators, and careful design considerations. By leveraging multilayer PCB fabrication and SMT, you can achieve compact, high-performance PCB designs that meet the demanding requirements of modern electronics.
Quality Control Measures and Inspection Methods
Quality control is a critical aspect of PCB manufacturing to ensure that the final product meets the highest standards of performance and reliability. Several quality control measures and inspection methods are employed throughout the manufacturing process to detect and prevent defects.
Visual inspection is the initial step in quality control, where trained personnel visually inspect the PCBs for any visible defects. This includes checking for proper alignment of components, solder joints, solder mask coverage, and any physical damage or anomalies.
Automated Optical Inspection (AOI) is a more advanced inspection method that utilizes high-resolution cameras and sophisticated software algorithms to inspect PCBs for defects. AOI systems capture images of the PCB and compare them with the expected design parameters. It can detect issues such as missing components, misaligned components, solder joint defects, and incorrect polarity. AOI provides faster and more accurate inspection results compared to manual visual inspection.
X-ray inspection is employed to examine hidden internal features of the PCB, such as vias, BGA (Ball Grid Array) solder joints, and inner layers. X-ray inspection allows for non-destructive testing and provides valuable information about the quality and integrity of the solder joints, especially in complex or high-density designs.
In-circuit testing (ICT) is performed on assembled PCBs to verify the electrical functionality of individual components and connections. ICT involves the use of specialized test probes that make contact with specific test points on the PCB. By applying controlled voltages and currents, the ICT system can identify faulty components, open or short circuits, and other electrical issues.
Functional testing is the final step in quality control, where the assembled PCB is tested under real-world operating conditions to ensure its functionality and performance. Functional testing may involve simulating different inputs and measuring the corresponding outputs to verify the proper operation of the PCB.
By implementing robust quality control measures and inspection methods, PCB manufacturers like JLCPCB can ensure the delivery of high-quality and reliable PCBs that meet customer expectations and industry standards.
Conclusion:
The process of PCB manufacturing involves several intricate steps, from substrate selection to layer imaging, etching, finishing, and quality control. Each stage plays a crucial role in creating high-quality PCBs that meet the requirements of modern electronics.
JLCPCB, with its advanced manufacturing capabilities and commitment to quality assurance, is a trusted partner in bringing your PCB designs to life.
Unlock the full potential of your electronic designs by partnering with us. With JLCPCB as your trusted manufacturing partner, you can confidently bring your innovative ideas to fruition and make a lasting impact in the world of electronics!
Q: What substrate materials does JLCPCB offer?
JLCPCB provides standard FR-4 (Tg 130°C/155°C), polyimide (PI) for flexible PCBs, and Rogers/PTFE materials for high-frequency applications.
Q: What is the maximum number of layers JLCPCB can manufacture?
JLCPCB supports up to 32-layer multilayer PCBs, with controlled impedance (±10%) available for 4+ layers.
Q: Which surface finishes are available?
JLCPCB offers HASL (leaded/lead-free), ENIG, and OSP. ENIG is recommended for 6+ layers and RF boards.
Q: How does JLCPCB ensure PCB quality?
Through visual inspection, AOI, X-ray, in-circuit testing (ICT), and functional testing at every stage.
Keep Learning
An Inside Look at the Modern PCB Manufacturing Steps
key takeaways Early Defect Trapping: CAM DFM and AOI catch inner-layer opens and shorts before lamination seals the board. DFM Prevention: Automated checks catch acid traps, copper slivers, and clearance shortfalls early. Reliable Interconnects: Chemical desmear clears resin smear from hole walls to prevent thermal failure. 100% Net Testing: Flying probe or bed-of-nails systems test every net for opens and shorts before packing. IPC Compliance: Final QA verifies annular rings and plating thickness aga......
Inside the Factory: A Breakdown of the PCB Manufacturing Process
Key Takeaways CAM Prep Prevents Errors: CAM verifies designs against real factory tolerances to catch bad drill files and board outline shorts before production. Material Selection Controls Heat: Standard FR4 softens near 130C, while high Tg options stay rigid at 170C for demanding thermal environments. Inner Layers Etch First: Cores must be etched and inspected before lamination, as internal traces cannot be reached after pressing. Plating Thickness Ensures Reliability: Holes need resin cleaning and ......
Advanced PCB Via Filling Options for Superior Signal Integrity and BGA Layouts
Key Takeaways Prevents BGA solder wicking by sealing holes to stop solder from draining during reflow. Frees up routing space by using Type VII via-in-pad to eliminate dog-bone traces. Selects non-conductive resin for flat pads and copper-epoxy for heat transfer. Requires surface grinding to keep dimples under 25 microns for good paste printing. Uses cross-section coupons and flying probe tests to verify hidden fill quality. A PCB via is normally a hollow plated hole, but that open structure creates a......
The Smart Advantages of Rounded Corners in Modern PCB Design
Key Takeaways Rounded corners reduce stress concentration and prevent chipping, cracking, and delamination. They improve safety, handling, and perfect fit in enclosures with matching radii. Use R0.5–R1.0 mm for small boards, R1.0–R2.0 mm for standard designs. Internal corners must respect router bit limits (min. R0.5 mm); external corners are more flexible. Maintain 0.3–0.5 mm edge clearance and use CNC routing with mouse bites for panelization. No extra cost — highly recommended for reliability and p......
Why Accurate NPTH Design Matters for Reliable PCB Manufacturing
Key Takeaways NPTH are mechanical holes (no copper plating) used for mounting, alignment, and tooling. Poor NPTH design often causes PCB cracks during assembly or screw tightening. Follow key rules: ±0.08 mm tolerance, ≥0.5 mm diameter, 0.2–0.3 mm copper clearance. Keep adequate material around edge holes and clearly mark NPTH in fabrication files. Proper NPTH design + DFM checks ensure reliability from prototype to mass production. Ever get a slight crack in a finished PCB when putting it into an enc......
How to Design and Manufacture Reliable Slot Holes in PCBs
Key Takeaways Slot holes are elongated openings ideal for flat pins, connectors, shields, and board alignment. Minimum sizes: 0.5 mm (plated) and 1.0 mm (non-plated); prefer rounded ends with length ≥ 2.5× width. Maintain proper annular ring, edge clearance, and DFM rules to prevent breakout and plating issues. Use overlapping drills for short plated slots and routing for longer ones. Good slot design greatly improves mechanical strength, thermal performance, and assembly reliability. JLCPCB’s precisi......