How to Avoid Copper Peel Off
3 min
- Improvement and Optimization Strategies
- Conclusion
Hot Air Solder Leveling (HASL) involves coating the surface of the exposed copper with a layer of tin alloy to prevent oxidation and provide a good soldering surface for subsequent assembly. The basic process of HASL is to briefly immerse the PCB board into a high-temperature liquid tin bath. Through the action of flux and high-temperature tin, a copper-tin alloy (IMG) is formed. Then, on guide rails, the board is lifted out while high-pressure gas blows away excess tin from non-copper areas and levels out any uneven solder on the pads.
The HASL process provides good solderability. However, during the actual HASL operation, there is a tendency for copper peel-off: in single-sided PCBs this most commonly occurs to plated holes, and in double-sided PCBs to through-hole pads with narrow annular rings, especially for long slotted holes. This copper peel-off has its main causes:
1. The HASL tin bath temperature of 275-300°C greatly exceeds the board's glass transition temperature (TG point). When subjected to the high temperature of the tin bath and the high-pressure gas jet, the board experiences strong stress. Without the mechanical support from wide surface solder pads, the copper in PTH holes can easily separate from the hole walls.
2. During HASL, copper and tin combine to form a copper-tin alloy, which can corrode away some of the copper, thereby reducing adhesion to the board substrate.
Improvement and Optimization Strategies
To illustrate, let's use the analogy of climbing a cliff. If both hands can hold onto the protruding face of the cliff, and the gripping area is larger, climbing becomes easier.
Similarly, the copper surface within the hole walls behaves similarly. When both top and bottom layers have solder pads (typically recommended to have 0.3 mm or larger annular ring), the adhesion is stronger, and the occurrence of copper peel-off is significantly reduced.
Conclusion
For single-sided or double-sided PCBs with small solder pads, consider switching to double-sided PCBs (with solder pads larger than 0.3mm) or adopting ENIG surface treatment. Gold-plated solder pads have a smoother surface and are suitable for BGA boards.
If conversion to double-sided PCBs isn't feasible due to insufficient clearance or other reasons, consider using ENIG.
For cases where copper in hole walls is unwanted, opt for non-copper-plated holes. If connectivity between both sides is needed, use vias at the edges of the solder pads (for high-current applications, ensure an adequate number of vias are added).
Keep Learning
How to Master PCB Impedance Testing for High-Speed Designs
Key Takeaways Verification via TDR: Impedance testing uses Time-Domain Reflectometry (TDR) on test coupons to verify high-speed traces. Real-World Factors: Actual impedance is shifted by manufacturing variables, including trace undercut, solder mask, and pressed dielectric thickness. Design-to-Fab Loop: Use the manufacturer's exact stackup Dk values for layout and TDR reports to refine revisions within $\pm 10\%$ tolerance. An impedance test can be the difference between a USB 3.0 link that works reli......
Guardians of Quality: A Complete Walkthrough of PCB Inspection Standards
Key Takeaways Layered Defense: Combining AOI, AXI, ICT, and FCT covers all inspection blind spots. Paste Printing: Solder paste causes up to 60% of defects, making early checks vital. IPC Standards: IPC Class 3 tightens BGA void limits from 25% to 10%, raising costs. Thermal Balance: Equal layout heating balances reflow pull to prevent tombstoning. Design Control: Clear test pads and visible polarity marks ensure reliable automated checks. PCB inspection is not one check performed at the end of produc......
Ensuring Superior Solderability: The Critical Role of Testing in Reliable PCB Production
Key Takeaways Core Purpose: Verifies solder wetting before assembly to prevent yield drops and joint failures. Destructive Test: Per J-STD-002, tested components and coupons cannot be reused in production. Pass Standards: Requires 95 percent solder coverage on leads and 80 percent on exposed thermal pads. Key Defects: Catches non-wetting (exposed metal), dewetting (solder pulling back), and black pad on ENIG. DFM Prevention: Use thermal relief, keep silkscreen off pads, and select the right surface fi......
Solder Joint Inspection in PCB Manufacturing : A Complete Guide to Catching Defects Early
Key Takeaways Solder Joint Inspection is critical in modern PCB manufacturing to catch defects early and ensure product reliability. By combining Solder Paste Inspection (SPI), 3D AOI for visible joints, and X-ray for hidden BGA/QFN issues, manufacturers can effectively detect common defects such as bridging, cold joints, tombstoning, and head-in-pillow. Following IPC-A-610 standards with a layered inspection strategy significantly reduces field failures while improving first-pass yield. JLCPCB’s prof......
3D AOI Inspection Explained : How It Catches Defects That 2D Systems Miss
Key Takeaways 3D AOI Inspection has become essential in modern PCB assembly by using advanced height and volume measurement to detect critical solder defects that traditional 2D AOI systems routinely miss, such as lifted leads, insufficient solder, head-in-pillow, and component coplanarity issues. By delivering precise 3D data through structured light or Moire technology, it significantly reduces false calls, improves first-pass yield, and ensures long-term reliability according to IPC-A-610 standards......
How Sustainable Materials and Expert Manufacturing Ensure RoHS Compliant PCBs
Have you ever experienced that a finished shipment of products was detained at the EU customs due to a single component on the board not passing the RoHS screening? It is higher than most engineers think, and the financial blow is far bigger than the impounded goods. Wasted time, remodeling expenses, and a compliance audit that is capable of halting your whole product introduction, that is the actual cost of doing RoHS wrong. The point is as follows: RoHS-compliant PCBs cease to be a checkbox exercise......