Border Layer Thickness: Impact on PCB Dimensions and V-Grooves
7 min
- Example Scenario
- Handling Shapes and Grooves
- Why Centerline Referencing Ensures Manufacturing Consistency
- FAQ about Border Layer Thickness
- Conclusion
Key Takeaways
The line width of the Border Layer has no impact on final PCB dimensions or V-groove (V-cut) characteristics. At JLCPCB, all routing and scoring operations reference the centerline of the Mechanical Layer outline, ensuring consistent board size with ±0.1mm precision and uniform 25° V-cuts regardless of whether you use 0.1mm or 1.0mm lines. Understanding this centerline principle allows designers to focus on visibility and clarity in EDA tools while achieving reliable, high-precision manufacturing results every time.
When it comes to designing a PCB, understanding the implications of border layer (board outline) thickness is essential for accurate fabrication and panelization. In this blog post, we will examine a practical example with different line widths on the Border Layer (0.1mm vs 1.0mm) to clarify their effects on final board dimensions and V-cut (V-groove) processing during panelization. We will also cover key JLCPCB manufacturing considerations to help you avoid common DFM issues.
Example Scenario
Imagine we have a PCB design with two different line widths on the border layer: 0.1mm and 1.0mm, respectively. Now let's address the following questions:
Will the dimensions of the final board be different?
No. The thickness (line width) of the border lines does not directly impact the overall dimensions of the board. At JLCPCB, all routing and cutting operations reference the centerline of the border lines defined on the Mechanical Layer (typically Mechanical 1/GM1). Whether your border line is 0.1mm or 1.0mm wide, the final board outline remains consistent.
Typical Dimension Tolerances at JLCPCB:
· CNC Routing: ±0.1mm (Precision) / ±0.2mm (Regular)
· V-scoring: ±0.4mm (slightly larger due to material expansion during separation)
This centerline-based approach ensures high precision and repeatability across different design tools.
During panelization, will the V-grooves be cut according to the thickness of the border layer?
No. V-grooves (V-cuts) are processed according to JLCPCB’s predefined specifications and are completely independent of the border line width. The V-cut is performed along the centerline with a standard 25° angle, typically leaving about 1/3 of the board thickness as connecting material for easy manual or roller separation.
Key JLCPCB V-Cut Specifications:
| Parameter | Specification | Notes |
|---|---|---|
| V-Cut Angle | 25 degrees | Double-sided V-cut |
| Min Panel Size | 70mm x 70mm | Both length and width |
| Min Connecting Edge | 3mm (≥5mm for ≤0.8mm thick) | Rectangular boards |
| Copper Clearance to Centerline | ≥0.4mm | To prevent copper exposure |
| Not Supported | 0.4mm board thickness | - |
| Dimension Tolerance | ±0.4mm | Due to separation |
V-cuts must be straight horizontal or vertical lines that span the entire panel. This standardization guarantees uniform groove depth and strength regardless of your design’s border line width.
Handling Shapes and Grooves
To gain a comprehensive understanding, let's also discuss how shapes and grooves are handled in such a scenario.
Shapes drawn inside the board:
When designing shapes within the board, such as cutouts or internal features, they are typically routed based on the centerline of the line. The actual width of the shape will be determined by the routing tool, irrespective of the border line's width.
Why Centerline Referencing Ensures Manufacturing Consistency
Beyond the direct impact on dimensions and V-grooves, understanding the centerline referencing principle is crucial for achieving consistent results across different PCB designs and panelization methods. At JLCPCB, the fabrication system interprets all Mechanical Layer border lines by their geometric center. This means that even if you intentionally draw a very thick 1.0mm border line for better visibility in your EDA software, the actual CNC routing tool or V-scoring blade will always follow the exact center path.

approach offers several key advantages
- Dimensional Stability: Final board size remains identical regardless of line width, with standard CNC routing tolerance controlled within ±0.1mm (precision) to ±0.2mm (regular).
- V-Cut Reliability: The 25° V-scoring process maintains uniform remaining thickness (approximately 1/3 of total board thickness), ensuring boards separate cleanly without cracking or leaving excessive material.
- Error Reduction: It eliminates ambiguity caused by varying design habits across KiCad, Altium, or Eagle, preventing common panelization issues such as misaligned grooves or oversized boards.
Practical Design Recommendations
When working with border layers, we recommend:
1. Set line width between 0.1mm and 0.5mm for optimal visibility without cluttering the view.
2. Always place the primary board outline on Mechanical Layer 1 (GM1), as it receives processing priority.
3. Maintain at least 0.4mm copper clearance from the centerline of any V-cut to avoid burrs or short circuits after separation.
4. For high-precision applications (e.g., RF or tight-tolerance mechanical assemblies), consider adding alignment marks near the border to further verify post-fabrication dimensions.
By following these centerline-based practices, engineers can confidently use different line widths during the design phase without worrying about downstream manufacturing variations. This standardized method is one of the reasons JLCPCB can deliver consistent quality even for complex multi-board panels.
Solid lines used to depict grooves:
For solid shapes, including filled polygons or copper pours, they are manufactured based on the actual width of the drawn shape. The thickness of the border layer does not influence the dimensions of internal solid shapes on the PCB.
FAQ about Border Layer Thickness
Q: Does changing the border layer line width affect the final PCB dimensions?
No. At JLCPCB, all cutting operations (CNC routing and V-scoring) are based on the centerline of the border lines on the Mechanical Layer. Whether your line width is 0.1mm or 1.0mm, the final board size remains exactly the same.
Q: Will different border line widths result in different V-groove (V-cut) depths or thicknesses?
No. V-cuts are processed according to JLCPCB’s standardized specifications (25° angle, ~1/3 board thickness remaining) and are completely independent of your border line width.
Q: Which Mechanical Layer should I use for the board outline?
We strongly recommend using Mechanical Layer 1 (GM1) for the primary board outline. This layer has processing priority and helps avoid manufacturing confusion.
Q: What is the recommended border line width for best results?
A line width between 0.1mm and 0.5mm is ideal. It provides good visibility in your design software without cluttering the layout. Thicker lines (e.g. 1.0mm) are fine for visibility but offer no manufacturing advantage.
Q: What is the copper clearance requirement near V-cuts?
Please keep copper at least 0.4mm away from the centerline of any V-cut. This prevents burrs, short circuits, or exposed copper after board separation.
Q: Can I mix different border line widths in the same design or panel?
Yes, you can. As long as the centerlines are consistent, JLCPCB’s manufacturing system will produce accurate and uniform results. Different widths are only for your design visibility and will not affect the final product.
Conclusion
In this example, we have explored the impact of different line widths on the border layer of a PCB design. We have learned that the thickness of the border line does not affect the board dimensions, as all cuts are referenced to the centerline of the border lines. Additionally, V-grooves are cut according to predefined specifications, independent of the border layer thickness.
Understanding these concepts is crucial for designing PCBs accurately. By considering the relationship between border layer thickness, board dimensions, and V-grooves, you can ensure the desired outcomes in your PCB fabrication process. JLCPCB hope this example has shed light on the topic. If you have any further questions or need assistance with your PCB design, feel free to reach out to us.
Keep Learning
Flex PCB Fabrication: Process, Materials, Design Rules & Cost
Many of the basic steps in rigid PCB fabrication also apply to flexible PCB fabrication. However, it is made with thin polyimide or PET films that can swell or shrink during processing due to moisture and temperature changes. These material attributes bring further complexities to considerations of layer alignment, coverlay openings, and bend-zone design. For instance, if there's not enough room for adhesive flow in a coverlay opening, or if a via falls in a bend zone, manufacturing defects or assembl......
Smart PCB Array Design for Higher Yield and Lower Production Costs
Key Takeaways Smart PCB array design is a critical strategy for achieving higher manufacturing yield and significantly lower production costs. By optimizing panelization with proper board spacing, V-scoring, tab routing, and mouse bites, designers can dramatically improve material utilization by 20-30%, enhance production throughput, and simplify handling and depaneling while minimizing mechanical stress and defects. Effective use of fiducials and careful component clearance further ensures high-quali......
Why Accurate NPTH Design Matters for Reliable PCB Manufacturing
Key Takeaways NPTH are mechanical holes (no copper plating) used for mounting, alignment, and tooling. Poor NPTH design often causes PCB cracks during assembly or screw tightening. Follow key rules: ±0.08 mm tolerance, ≥0.5 mm diameter, 0.2–0.3 mm copper clearance. Keep adequate material around edge holes and clearly mark NPTH in fabrication files. Proper NPTH design + DFM checks ensure reliability from prototype to mass production. Ever get a slight crack in a finished PCB when putting it into an enc......
Gerber of PCB: A Comprehensive Guide
Introduction: Printed Circuit Boards (PCBs) are the backbone of modern electronics, serving as the platform on which components are mounted and interconnected. One of the most critical elements in PCB design and manufacturing is the Gerber file. Gerber files are the standard format used to communicate the design of a PCB to the manufacturer. These files provide precise information about the PCB layers, component placement, copper traces, and more. Understanding Gerber files is essential for anyone inv......
Electronic Board Manufacturing: Efficient Strategy and Quality Control Processes
Electronic board manufacturing is a critical process in the electronics industry, and the quality of the boards produced can significantly impact the performance and reliability of the final product. Therefore, it is essential to follow efficient strategies and quality control processes throughout the manufacturing process to ensure the highest quality of the boards. In this article, we will explore the various steps involved in electronic board manufacturing, including materials selection, design and......
Best Practices for Successful Electronic Manufacturing
Key Takeaways Mastering best practices in electronic manufacturing — from optimized PCB design and DFM to rigorous testing, verification, and high-quality production — is essential for achieving reliable, cost-effective, and timely electronic products. By following proven methodologies, leveraging advanced tools like EasyEDA, and partnering with a trusted manufacturer such as JLCPCB, designers and engineers can significantly reduce errors, accelerate time-to-market, and ensure superior performance acr......