How to Choose the Thickness of PCB
7 min
- Characteristics and Application of different PCB thicknesses
- Key factors affecting PCB thickness:
- How to Choose the Appropriate PCB Thickness
- PCB Thickness Selection FAQ
- Conclusion
First,
In the world of electronic products, the PCB is often referred to as the "heart" of the device. It interconnects all components, making board thickness one of the most important parameters. Choosing the right PCB thickness directly affects the electrical performance, mechanical stability, thermal management, and long-term reliability of the final electronic product.
The process of selecting PCB thickness is influenced by various factors, such as product application scenarios, board material, and number of copper layers. Therefore, these factors must be comprehensively considered when selecting the PCB thickness.
Characteristics and Application of different PCB thicknesses
JLCPCB offers standard FR-4 thicknesses including 0.4 mm, 0.6 mm, 0.8 mm, 1.0 mm, 1.2 mm, 1.6 mm, and 2.0 mm (thicknesses above 2.5 mm are available for high-layer boards up to 4.5 mm overall). Each thickness range has distinct advantages and limitations.
| Thickness | Typical Applications | Key Characteristics | JLCPCB Notes |
|---|---|---|---|
| 0.4 mm | Smartphones, wearables, drones | Ultra-light, highly flexible | ENIG only, no panelization |
| 0.6 mm | Compact consumer devices | Good flexibility | Max 100×100mm (2L), no HASL |
| 0.8–1.2 mm | IoT, consumer electronics | Balanced cost & performance | Max 300×300mm |
| 1.6 mm | General electronics, motherboards | Industry standard, excellent balance | Most popular FR-4 thickness |
| 2.0 mm+ | Automotive, industrial, high-power | High rigidity, better heat dissipation | Higher cost, ideal for heavy components |
Ultra-thin PCB (below 0.6 mm)
Ultra-thin PCBs (≤ 0.6 mm) are lightweight, flexible, and ideal for space-constrained products such as smartphones, tablets, wearables, robotics, laptops, and drones. However, they have limited mechanical strength and are prone to warping. At JLCPCB, 0.4 mm boards only support ENIG finish and cannot be panelized; 0.6 mm boards have maximum size restrictions.
Mid-Range Thin PCBs (0.6-1.6 mm)
Mid-range thin PCBs (0.8–1.6 mm) offer the best overall balance between mechanical strength, weight, cost, and manufacturability. This thickness range is suitable for the vast majority of electronic products, including computer motherboards, consumer electronics, IoT devices, home appliance control boards, and industrial controllers. The stiffness and stability are moderate, making them ideal for most standard applications. The 1.6 mm thickness is the most widely used industry standard for FR-4 substrates.
At JLCPCB, PCBs with thicknesses from 0.8 mm to 1.6 mm start at only $2, providing excellent cost performance. In addition, these thicknesses perform very well in multilayer boards (especially 4 to 8 layers) for controlled impedance routing, ensuring good signal integrity in high-speed designs.
Thicker PCBs (above 1.6 mm)
Thicker PCBs (above 1.6 mm, typically 2.0 mm and above) provide superior rigidity, load-bearing capacity, and thermal mass. They are particularly suitable for applications that require high-power components, heavy parts, or large board sizes. Common use cases include automotive electronics, industrial control systems, aerospace equipment, railway transportation, and high-current power boards. In harsh environments with high vibration, shock, or extreme temperatures, thicker boards offer significantly better mechanical stability and durability. They also help prevent warping and deformation in large-outline PCBs. Additionally, the greater thermal mass allows for better heat dissipation from high-current traces. However, thicker boards come with higher material costs and may require longer processing times.
Impact of Layer Stack-up on Thickness
The final board thickness is not only determined by the chosen thickness value but also by the layer stack-up. More layers require additional prepreg and core materials. For example, a 6-layer board at 1.6 mm needs a carefully designed stack-up (e.g., SIG/GND/PWR/SIG/GND/SIG) to maintain impedance and signal integrity. JLCPCB provides standard stack-up templates to help designers achieve target thickness while meeting electrical requirements.
Key factors affecting PCB thickness:
1. The number of PCB layers: The more copper layers a circuit board has, the greater its thickness will typically be.
2. Signal type: Circuit boards carrying high-power signals typically require thicker copper layers and wider traces, while circuit boards in low-power environments can be thinner.
3. Material selection: Different materials have varying thickness characteristics, and selecting different materials can impact the thickness of the circuit board.
4. Operating environment: In harsh environments (e.g., high vibration or mechanical stress), thin or flexible boards may not be the most suitable choice. Thicker copper traces, however, have greater thermal mass and better heat dissipation, making them more suitable for high currents and temperature variations.
5. Copper Thickness: The overall thickness of the PCB is influenced by the thickness of the copper layers it has. Thicker copper layers, such as 2 ounces or 3 ounces of copper, have a greater impact on the overall thickness compared to thinner copper layers. Contribute more than one ounce of copper.
6. Special requirements: Certain applications may necessitate customized circuit board thickness, such as high-density boards or circuit boards used in unique environments.
How to Choose the Appropriate PCB Thickness
When selecting a PCB type, you need to consider whether the thickness of the circuit board is suitable for the application requirements. Generally speaking, when choosing the thickness of a PCB, the following factors should be considered:
Clarify application needs and performance requirements: Before selecting the PCB thickness, it is important to have a clear understanding of the application performance requirements, various different scenarios, and component load-bearing requirements. This will ensure that the chosen thickness is able to meet the product's specific requirements.
Safety of the circuit board: If the circuit board must handle high voltage or high current, a thicker PCB is recommended to ensure safe operation and adequate clearance/creepage distances.
Mechanical properties of the circuit board: If the circuit board needs to withstand high mechanical influence, it is advisable to choose a thicker PCB to ensure its mechanical strength
Production cost: Thicker the PCB, the higher production cost. Therefore, when selecting a PCB, it is important to ensure product performance while also considering the maturity of production technology and the cost of the PCB thickness.
Generally speaking, the expected turnaround time for receiving custom PCB layer thicknesses is longer due to the unusual thickness specifications.
PCB Thickness Selection FAQ
Q: What is the standard PCB thickness?
The most common PCB thickness for FR-4 substrates in the electronics industry is 1.6 mm (approximately 62 mil), also known as the standard thickness. It is widely used for general consumer electronics, smart home devices, and industrial controls.
Q: When should I choose an ultra-thin PCB (below 0.6 mm)?
Ultra-thin PCBs are ideal for applications requiring minimal space and lightweight design, such as smartphones, tablets, wearable devices, laptops, drones, and robotics. However, they have lower load-bearing capacity and are not suitable for heavy components.
Q: What are the main factors affecting PCB thickness selection?
Key factors include: number of layers, signal type (high-power signals need thicker boards), material choice, operating environment (harsh conditions favor thicker boards), copper thickness (thicker copper increases overall thickness), and special requirements like high-density designs.
Q:Why choose a thicker PCB (above 1.6 mm)?
Thicker PCBs provide higher mechanical strength, better load-bearing capacity, and greater durability, making them suitable for high-power components, industrial control boards, automotive electronics, aerospace, and large-outline boards that resist deformation.
Q: How does the operating environment influence PCB thickness choice?
In harsh environments with high mechanical stress, vibration, or extreme temperatures, thicker PCBs are preferred for better stability and durability. Ultra-thin or flexible boards may not withstand such conditions, while thicker copper also improves heat dissipation under high currents.
Conclusion
Choosing the appropriate PCB thickness is a crucial factor in ensuring optimal board performance and reliability. Taking into account factors such as engineers' application needs, cost, and manufacturing capabilities, JLCPCB acts as a PCB manufacture and supports PCB production from 1 to 20 layers and offers a thickness range of 0.7mm to 2.5mm.Engineers can choose the appropriate thickness based on their specific requirements. Whether standard FR-4 or specialized materials are required, JLCPCB can provide customized solutions to meet specific thickness requirements.
Keep Learning
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......