Common problems and solutions in PCB design
4 min
- Unreasonable circuit layout
- Power supply noise interference
- Signal integrity issues
- Thermal management issues
- EMI/EMC Issues
- Component selection issues
- PCB size limitations
- Selecting a Package
- Manufacturing and assembly issues
- Conclusion :
PCB (Printed Circuit Board) design is a crucial aspect of electronic product development. During the design process, we often encounter challenging issues, which may include circuit design and wiring regulations. Understanding these common problems and their solutions can help engineers enhance the quality and efficiency of the design.
Unreasonable circuit layout
Circuit layout is crucial for maintaining signal integrity and electromagnetic compatibility. Unreasonable layout can lead to issues such as signal crosstalk and electromagnetic interference.
Solution:
1. Reasonably plan the hierarchy of the circuit board and separate high-speed signals from low-speed signals to minimize signal interference.
2. Divide the ground plane to prevent the formation of large-area ground plane loops and reduce electromagnetic interference.
3. Shorten the signal line as much as possible to minimize transmission delay and signal attenuation.
Power supply noise interference
Power supply noise may degrade circuit performance or even cause malfunction.
Solution:
1. Implement filter capacitors to eliminate power supply noise.
2. Add decoupling capacitors to the power supply to ensure stable power for each device.
3. Optimize the layout of the ground wire to ensure a solid ground wire reference plane and minimize noise resulting from the return flow of the ground wire.
Signal integrity issues
In high-speed signal transmission, maintaining signal integrity is a common challenge.
Solution:
1. Use the appropriate signal line width and spacing to ensure impedance matching and signal integrity.
2. Strengthen the ground reference plane of the signal layer to minimize the signal return path.
3. Implement terminal resistors and signal attenuators to minimize signal reflection and crosstalk.
Thermal management issues
High-power devices can lead to thermal issues, such as overheating and temperature unevenness.
Solution:
1. It is important to strategically design heat dissipation components, such as heat sinks and heat dissipation holes, to enhance heat dissipation efficiency.
2. Enhance heat dissipation by increasing the heat dissipation area to improve its ability.
3. Utilize a cooling pad to enhance the thermal contact between the device and the heat sink.
EMI/EMC Issues
Electromagnetic interference and electromagnetic compatibility issues can lead to degradation in system performance.
Solution:
1. Reasonably lay out the ground wire to minimize the return path and loop area.
2. Utilize a shielding cover to minimize electromagnetic radiation and electromagnetic interference from sensitive devices.
3. Apply a filter to eliminate high-frequency noise and interference.
Component selection issues
Using incorrect components may lead to unstable or unreliable circuit performance.
Solution:
1. Select the appropriate components and evaluate them based on design requirements and performance indicators.
2. Consider the temperature characteristics of the components to ensure that they operate normally within the specified temperature range.
3. Consider the reliability of components and select reliable brands and models.
PCB size limitations
Limitations on PCB size can result in layout challenges or signal integrity issues.
Solution:
1. Plan the layout reasonably, taking into account size restrictions when planning the device layout and signal line direction.
2. Use multi-layer boards to incorporate additional wiring layers and ground planes in order to enhance signal integrity and electromagnetic compatibility.
3. Optimize the signal line direction, minimize the length of the signal line, and reduce delay and interference as much as possible.
Selecting a Package
In PCB design, choosing the appropriate package is crucial as it directly impacts the layout, connection method, and reliability of components.
Solution:
1. Understand the functions and usage environment of the components, and choose the appropriate packaging type based on the design requirements, such as SMD, THT, BGA, etc.
2. Refer to the component data sheet or the supplier's recommended packaging to ensure that the selection meets the electrical and mechanical specifications.
3. Customized Packaging: If there is no standard package that meets the requirements, you can consider creating a custom package. This requires accurate dimensions and pin layout, as well as appropriate materials and processing techniques.
4. Utilize 3D modeling tools to validate the packaging, identify potential collisions between the package and other components, and guarantee the precision and assembly of the package.
Manufacturing and assembly issues
Issues that may arise during the manufacturing and assembly process include inadequate welding, component misalignment, and so on.
Solution:
1. Select the appropriate manufacturer to guarantee manufacturing quality and process reliability.
2. Conduct thorough prototype testing to verify the manufacturability and ease of assembly of the design.
3. Optimize the reflow process by using the appropriate reflow temperature and flux to enhance welding quality.
Conclusion :
During the PCB design process, it is inevitable to encounter various challenges. By employing hierarchical planning, rational layout, appropriate power and signal processing techniques, and effective thermal management, engineers can effectively address these issues and enhance the quality and performance of PCB designs.
Keep Learning
GPT-6 Astra PCB Design in KiCad: From Brief to Verified Native Project
Key Takeaways What OpenAI published: The launch page features a 15-second condensed clip of GPT-6 Astra performing PCB layout in KiCad. What the model did: It turned a four-line brief into a 44 × 34 mm, two-layer PCB, covering the circuit, footprints, component placement, routing, and a native two-sheet schematic. Where the work went: Placement and routing were only part of the work. Two linked schematic sheets, project-local libraries, and UUID-based links between 45 components and their footprints w......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
AI tools can now assist with PCB architecture, schematic generation, component selection, placement, routing, and design verification. However, different tools target different stages of the PCB workflow. This guide compares AI tools for PCB design based on what they actually do, what inputs they require, and where they fit within a real engineering workflow. In this guide, you will learn: The 6 types of AI PCB tools and the input each one needs What AI PCB design tools do, compared stage by stage How......
EasyEDA Pro vs KiCad: GPT-6 Astra PCB Design Compared
Key Takeaways What is being compared: Two versions of the same TPA3116D2 stereo amplifier project, each created by GPT-6 Astra in a different EDA tool. The comparison focuses on what you can actually do with the delivered project afterward. Ground copper: In the EasyEDA Pro project, the ground copper is stored as 28 fixed filled regions. In KiCad, it remains as two native copper zones that can automatically refill after layout changes. Verification: KiCad initially reported 46 schematic-parity issues.......
A Practical Guide to ODB Files for PCB Manufacturing
Key Takeaways All-in-One Data: ODB++ combines artwork, netlist, stackup, and drill spans in a single package. Fewer Errors: Embedded netlists allow CAM software to catch errors before production. Pre-Export Checks: Clear DRCs, close the board outline, and verify drill spans in a viewer. Best Practice: Use Gerber for quick quotes and keep ODB++ ready for engineering queries. A Gerber layer might simply say, “draw a 0.5 mm (20 mil) circle here.” ODB++ can describe that same feature as a pad on the VCC n......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......