PCB Art : Jaw-Dropping Designs & How to Make Your Own
6 min
- Some PCB Art Designs & Ideas
- Essential PCB Art Supplies & Aesthetic Hacks
- Create Custom PCB Art – Fast Workflow
- Ordering & Cost Optimisation for PCB Art
- From Design to Gerber – Final Polish
- Conclusion:
Usually, PCBs are designed to replicate complex circuits on a small board consisting of traces. All this is done to connect different components. However, when it comes to the aesthetics and functionality of a printed circuit board, various applications also exist, such as coloured PCBs and PCB cards. The rise of PCB art isn’t a fluke. And by the introduction of JLCPCB, this art became easier to fabricate. A community that loves to flex creativity and RGB. Engineers who want their work to be both functional and frame-worthy use PCB art designs. PCB art and coloured PCBs have transformed circuit boards from functional components to visual designs. Services like JLCPCB allow designers to create PCB art using copper layers, solder mask openings, and silkscreen.
Viral Hits and Community Obsession
One board with a coloured solder mask and different colours of silkscreen can go from prototype to viral in a single tweet. Here is the picture of an Arduino Mega, and see how pretty it looks. Community obsession with PCB art ideas happens for three reasons:
Shareability. Visual designs are perfect for social media and hardware show-and-tell.
Low friction. If you already know KiCad or Eagle, making art is primarily a design decision, not a skill.
Fab friendliness. Quick-turn fabs offer colour options.
If you want to get noticed, adding aesthetic choices to your next PCB design project is a shortcut to relevance.
Some PCB Art Designs & Ideas
You don’t need to be an illustrator to produce stunning PCB art. The best PCB art designs are combinations of clever compositions. See here the comparison of different colours by Ian Dunn here. It shows a comparison of soldermask, silkscreen and copper with different colour combinations:
Some tips are using copper pours for shading, and silkscreen for fine detail. Keep high-current traces away from delicate visual elements.
Geometric, Pop Culture & Interactive LED Pieces
Geometric patterns, such as Voronoi fills and concentric copper rings, are used to create elegant, artistic PCB pieces. These look amazing with their contrasting solder mask and exposed copper.
Pop culture references: Pixel-art sprites routed into copper and stylised logos are the ones liked by Gen-Z.
Interactive LED pieces: Using addressable LEDs or simple POV techniques to animate your art. This can turn static shapes into living displays. These are perfect PCB design projects for a portfolio.
Flexible, Rigid-Flex & Seasonal Art Boards
Flexible PCB art is utilised in wearable devices and bendable sculptures. Flex designs let you introduce movement as part of the artwork. On the other hand, Rigid-Flex boards combine rigid sections for logic and flex “wings”. They can be mixed together for unexpected shapes.
Holiday ornaments and limited-run seasonal designs are inexpensive ways to showcase custom PCB art. For example, a PCB batch can be dedicated towards any season or festival. Flex and rigid-flex options open new formal possibilities. However, increased DFM complexity and higher fabrication costs are also associated with these boards.
Essential PCB Art Supplies & Aesthetic Hacks
Soldermask Colours, Finishes & Fancy Cutouts
Soldermask choices like black are elegant but show dust. On the other hand, white makes silkscreen pop and looks great with LEDs. Purple and matte black are trendy. Use your soldermask like a background canvas. Surface finishes like ENIG (gold) and immersion silver add a touch of luxury. ENIG is expensive but looks fantastic on exposed copper art. HASL is cheap and retro, but not as refined. Exposed copper and cutouts create metallic highlights. Here are some tips:
- Use thin hatched copper pours for mid-tones.
- Combine silkscreen and cutouts to create a 3D illusion.
- Stagger silkscreen layers if your fab supports two-tone silkscreen for depth.
Create Custom PCB Art – Fast Workflow
You want to create custom PCB art quickly without violating DRC. Here’s a streamlined workflow:
Free Tools, Templates & Gerber Tricks
1) Tools: KiCad, Inkscape and EasyEDA are the tools to map a bitmap-to-polygon. These tools enable you to treat your board like vector art while preserving its electrical function.
2) Workflow steps:
- Design your circuitry and reserve a "canvas" region for art.
- Create artwork as SVG in Inkscape and simplify strokes to avoid hairline features.
- Import SVG into your EDA’s silkscreen or copper layer. Convert thin strokes to thick traces or polygons that meet your fabricator's minimum width.
- Run DRC to ensure no accidental copper overlap creates shorts.
- Use copper pours and tented vias for shading and texture.
3) Gerber tricks: Place artwork on the silkscreen for crisp lines and on copper for metallic accents. Use soldermask openings to create negative-space effects. Keep a template of standard element sizes, text height, and stroke width thickness that is thick enough so your designs are always manufacturable.
Panelizing for Cheap Orders
Panelizing is the secret to getting small art runs affordably. We can combine several small art boards into one larger panel by using mouse bites or V-cuts. Mix and match designs to amortise tooling and soldermask setup costs. Panelization reduces the per-board cost and provides spare boards for giveaways.
Ordering & Cost Optimisation for PCB Art
Panelizing, Layer Count & Quantity Strategies
2-layer boards are usually the most cost-effective for art. Reserve multilayer only for functional necessity. Standard thickness (1.6 mm) and 1 oz copper are the default fabrication settings. Only upgrade to 2 oz or thicker if the design requires it for mechanical reasons.
Ordering 10–50 boards often hits the sweet spot for hobbyist art runs. Each non-standard finish, silkscreen colour, or cutout incurs an additional cost. Combine similar orders and reuse panel layouts across different designs to reduce setup fees.
From Design to Gerber – Final Polish
Aesthetic vs DFM Balance Checklist
Before sending Gerbers, run through this checklist:
- Are silkscreen/line widths above your fab’s minimum printable width?
- Do exposed copper areas have a protective finish if needed?
- Are artistic copper pours electrically isolated from traces and pads where intended?
- Are cutouts manufacturable and within the fab’s tool size limits?
- Have you tented or covered vias that could impact the visual?
- Have you placed test points and assembly notes without clashing with your art?
Conclusion:
PCB art is where engineering meets aesthetics, and the results can be jaw-dropping. From geometric copper pours to interactive LED sculptures. PCB art designs let you show that technical work can be beautiful, shareable, and manufacturable. Use the right PCB art supplies and adopt a fast SVG-to-Gerber workflow.
Want to turn a favourite schematic into a signature art board? Start with a small 2-layer panel, pick a bold soldermask colour, and import a cleaned-up SVG for the silkscreen. Your next PCB design project might just be the one that gets pinned, shared, and remembered. Follow the JLCPCB guidelines to fabricate your own PCB art designs.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......