Thermal Management Strategies in PCB Layout Design
8 min
In the world of electronics, heat is the silent destroyer. It creeps into your circuits, degrading performance, shortening component lifespan, and, in extreme cases, turning your once-functioning PCB into a lifeless, overheated mess. The physical properties of your PCB substrates and copper conductors are the primary factors that determine how it will perform under pressure. Thermal properties, rigidity, dispersion, relative permittivity, and more will affect signal integrity, thermal management, and mechanical performance of your circuit board. When it comes to thermal conductivity, choosing the right substrate can help you combat temperature rise in your board with excessive use of active cooling measures. Thermal management in PCB layout design is not just an option it's a necessity.
With the right substrate material and components layout choices, you can implement a thermal management strategy that can help keep your circuit board temperature low without defaulting to the use of a substrate material with high thermal conductivity. Some simple PCB layout choices will have a big effect on temperature rise and overall thermal management throughout your circuit board. This article explores the challenges of managing heat in PCBs and offers proven strategies to keep your designs cool and reliable. To know more about PCBs see our detailed blog on PCB manufacturing process.
- PCB thermal management often involves a combination of design and helper components, such as heatsinks, to handle excess heat.
- Carefully selecting and distributing components and testing for thermal shock resilience are ways to improve PCB thermal management.
- High power density electronics are particularly difficult to manage thermally because they create a lot of heat very quickly.
Understanding the Heat Problem
Heat is generated in electronics primarily due to the resistance within components that converts electrical energy into thermal energy during operation. This occurs in semiconductors, resistors, and other elements as they process current. High frequencies, large currents, and inefficient circuit designs amplify heat generation. Effective heat dissipation is crucial to maintain performance and prevent damage. The heat dissipation equation is:
Q = I²R + V²/R + P
Where, Q is the heat generated, I is current, R is resistance, V is voltage, and P is additional power losses. In a PCB’s heat accumulation can come from several sources:
- Integrated circuits (ICs): The workhorses of a PCB are integrated circuits (ICs), which process data and carry out calculations. A result of their activities is heat.
- Components of power delivery: Power converters and voltage regulators control the flow of power within the PCB. When in use, these parts also release heat.
- Passive components: Resistors, capacitors, and inductors can produce heat, mainly when they are operating at high currents.
Effect of Excess Heat on a PCB:
High temperatures in PCBs lead to several issues, including reduced performance as components lose efficiency, resulting in throttling or failures. Prolonged exposure to heat accelerates the aging of electronic components, shortening their lifespan and increasing the likelihood of early failure. Additionally, overheating poses a significant risk of physical damage, such as cracked solder joints or delaminated PCB layers, which can cause irreversible board failures. Proper thermal management is essential to mitigate these risks and ensure reliable operation.
Importance of thermal management
Current silicon-based components have a junction temperature between about 125°C and 200°C. However, it is necessary to avoid reaching this value, otherwise the residual life of the component will deteriorate rapidly. In fact, it is estimated that an increase in operating temperature of 20°C, due to inefficient thermal management, can reduce component life by up to 50%. Heat in a PCB comes from various sources: power-hungry ICs, high-current traces, and even environmental factors. If this heat isn’t properly managed, it can cause:
- Component Failure: Overheating leads to premature failure of components like capacitors, ICs, and transistors.
- Performance Degradation: Excessive heat affects signal integrity and power efficiency.
- Safety Risks: High temperatures can result in melting or fire hazards in extreme scenarios.
High brightness LEDs, for instance, convert over 60% of the absorbed power into heat and therefore require special printed circuit boards capable of handling high temperatures without damaging the components.
Imagine designing a PCB for a high-power LED driver circuit. The MOSFET and driver IC generate significant heat. Which at higher voltages decrease the overall efficiency and convert a lot of energy as heat rather than radiative light.
Solution:
- Place thermal vias beneath the MOSFET and IC to transfer heat to a ground plane.
- Use 2 oz copper for better heat conduction.
- Add a heat sink on the MOSFET for direct heat dissipation.
- Perform a thermal simulation to validate the design.
Good thermal management ensures your PCB operates within safe temperature ranges, maximizing reliability and performance.
7 Universal Strategies for Thermal Management in a PCB:
1. Use Thermal Vias
Thermal vias transfer heat from hot components to internal or external layers for better dissipation. Use multiple small-diameter vias under high-power components like ICs or power transistors.
2. Optimize Copper Planes
Copper layers act as heat spreaders, distributing heat across the PCB. Increase copper thickness (e.g., 2 oz/ft² instead of 1 oz/ft²) to improve thermal conductivity.
3. Add Heat Sinks
Heat sinks dissipate heat by increasing the surface area exposed to air. Attach heat sinks to components with high thermal output and ensure good thermal contact using thermal paste or pads.
4. Use Thermal Pads and Conductive Adhesives
Thermal interface materials help transfer heat from components to PCBs or heat sinks. Choose materials with high thermal conductivity and low thermal resistance to improve efficiency.
5. Component Placement
Proper placement can significantly reduce thermal hotspots. Place high-power components near the edges of the PCB for better airflow. And keep heat-sensitive components away from high-power devices.
6. Airflow Management
Natural or forced airflow can carry heat away from the PCB. Align heat-generating components with airflow direction. Use fans or blowers for forced convection in high-power designs.
7. Thermal Simulations
Thermal analysis tools simulate heat distribution and help optimize PCB layouts before fabrication. Use software like ANSYS Icepak, SolidWorks Flow Simulation, or Altium Designer to identify and address thermal issues.
PCB Layout Guidelines for Better Thermals:
To reduce the thermal path length on a PCB, designers can use several techniques:
1) Track Design: Increase the spacing between tracks to distribute heat evenly and reduce hot spots, though this may be limited in compact PCBs. Use wide, short tracks with thicker copper for power components to handle high currents effectively, as recommended by IPC-2221 standards.
2) Thermal Vias: Add plated thermal vias to connect layers, allowing better heat transfer and airflow.
3) Copper Planes: Use large copper planes on outer or inner layers for efficient heat dissipation.
4) Heavy Copper Technology: For power applications, thick copper traces (up to 60 ounces) improve current handling and heat resistance.
Passive Techniques to Keep Electronics Cool:
Heat Sinks: Metallic vias conduct heat from heat-generating components, dissipating it across copper planes for effective thermal management. Usually, engineers attach heat sinks to heat-generating components like switching devices and power transistors.
Heat Pipes: Compact, fluid-filled pipes transfer heat via vaporization and condensation cycles, offering quiet, low-maintenance operation. These pipes contain small amounts of ammonia, nitrogen, acetone or water to absorb heat. Easily seen inside of a laptop with CPU.
Cooling Fans: By adding a cooling fan to a PCB, you can blow hot air out of an area, helping to prevent heat from building up.
Thermal Via Arrays: These arrays, especially filled and capped vias, efficiently dissipate heat, often placed near heat sources for optimal performance. You can generally find two main types of thermal via arrays used in PCBs, simple vias and filled and capped vias. Simple vias are often a popular choice, as they significantly reduce the PCB’s thermal resistance.
Thick Copper Traces: High-power applications use thick traces to distribute heat over larger areas as the addition of more copper allows the heat to dissipate over a larger surface area.
Conclusion:
Thermal management is a cornerstone of effective PCB design, ensuring reliability, performance, and safety. By integrating strategies like thermal vias, optimized copper planes, and heat sinks, you can combat heat buildup and keep your circuits cool under pressure. To explore more content related to design of high speed PCB see this blog, on EMI/EMC consideration.
Recall that a well-thought-out thermal management plan maximizes the usefulness and cost of your high-performance PCB, making it an investment that pays off over time. In PCB design, ignoring thermal management is like ignoring the weather while planning a picnic it's bound to ruin your day. So, plan ahead, simulate, and design for a cooler, more reliable product!
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Design Guidelines for PCB Using FR4 Substrates
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
Via Stitching Guide : Core Functions, Pitch Rules & Placement
key takeaway Core Purpose: Ties ground layers together to cut EMI, reduce impedance, and shorten return paths. Pitch Rules: Space vias at λ/10 for ground grids and λ/20 for edge rings and shielding fences. Layer Transitions: Place stitching vias adjacent to signal vias to minimize return current loop area. Avoid Over-Stitching: Overuse perforates power planes, alters trace impedance, and increases drilling costs. DFM Control: Follow hole spacing rules, tent non-test vias, and maintain proper edge copp......
Relay Pinout Explained: Diagrams, Pin Functions & Multimeter Testing
Key Takeaways Pin functions: A standard electromechanical relay has two coil pins, and each pole adds a common (COM), normally open (NO), and normally closed (NC) pin. Viewing side: Relay footprints are often drawn in bottom view, with the pins facing you. When a drawing does not state its view, confirm NC and NO with a continuity check. Relay Pin Count: A 5-pin relay is typically SPDT, a 4-pin relay is usually SPST, and an 8-pin relay is commonly DPDT. However, pin arrangements can vary between PCB, ......
How to Connect and Choose a Flyback Diode for a Relay
Key Takeaways Diode Placement: Connect the flyback diode across the relay coil, with its cathode connected to the positive side and its anode to the negative side. Why It Matters: When the relay switches off, the diode provides a safe path for the remaining coil current, preventing a high-voltage spike that could damage the transistor. Choosing the Right Diode: Select a diode with a reverse-voltage rating above the coil supply voltage and a forward-current rating suitable for the coil current. Common ......
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Reliable BMS Boards Start With Quality PCB Manufacturing
Key Takeaways Dual Duty: BMS PCBs handle heavy currents and millivolt sensing simultaneously, requiring strict layout isolation. Power & Heat: Currents over 10A need 2 oz+ copper pours with via stitching to drop resistance and heat. Clean Sensing: Kelvin differential routing and split grounds prevent load noise from corrupting cell voltage readings. Materials & Finish: High-Tg FR-4 and ENIG surface finishes ensure heat tolerance and flat mounting pads. DFM & Testing: Design for heavy-copper etch toler......
What is Solder Mask and How Does it Impact Your PCB Designs?
Solder mask may not be the most exciting topic in PCB manufacturing, but it's definitely one of the most crucial. Without proper solder mask, your Printed Circuit Boards (PCB's) could suffer from shorts, bridges, corrosion, and other costly and time-consuming issues. So, if you want to ensure the quality, reliability, and longevity of your electronic products, you need to know everything about solder mask - from it's purpose and types to it's application and design implementations. In this ultimate gu......