This website requires JavaScript.
Coupons
Ship to
Blog

Chip Scale Package (CSP) Explained: Types, Benefits & More

Published May 13, 2026, updated Nov 18, 2026

20 min

Table of Contents
  • What Is a Chip Scale Package (CSP)?
  • Why Chip Scale Packaging Matters in Modern Electronics
  • Types of Chip Scale Packages
  • Chip Scale Package vs Other IC Packages
  • How to Choose the Right IC Package
  • Advantages of Chip Scale Package
  • Disadvantages and Challenges of Chip Scale Package
  • Design Considerations for Chip Scale Package
  • CSP Assembly Process Explained
  • Applications of Chip Scale Package
  • From Design to Production: Reliable CSP Assembly with JLCPCB
  • Future Trends in Chip Scale Packaging
  • FAQs About Chip Scale Package
  • Conclusion
hdi pcb coupons

Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action.

By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds to automotive radar modules.

According to recent industry market research, the global WLCSP market was valued at USD 4.89 billion in 2024 and is projected to reach USD 37.49 billion by 2032 at a CAGR of 21.4%, a clear signal that chip scale packaging isn't a niche technology anymore.

This guide covers the types, process flows, design rules, and assembly considerations you actually need to work with CSPs.

What Is a Chip Scale Package (CSP)?

According to JEDEC standards, a chip-scale package is a chip-scale IC package where the body is ≤1.2× the die size. That definition is tight by design - it means most of the package footprint is active silicon, with almost nothing wasted on substrate overhang, molding margins, or unused leadframe area.

Key Characteristics of Chip Scale Package

  • Area-array I/O: Solder balls or bumps cover the bottom face - no perimeter leads.
  • Short interconnect: Die pad to PCB trace is under 300 µm, versus 3-8 mm in wire-bonded packages.
  • SMT-compatible: Despite fine pitch, CSPs go through standard surface-mount device processes: solder paste → pick-and-place → reflow.

CSP vs Traditional IC Packages

dip soic qfn and wlcsp package sizes for a 2x2mm die

Figure: Comparison of DIP, SOIC, QFN, and WLCSP package sizes for a 2x2mm die.

PackageSize vs DieTypical PitchI/O Style
DIP10-20×2.54 mmThrough-hole leads
SOIC3-8×1.27 mmSurface-mount leads
QFN1.5-3×0.5-0.8 mmPerimeter pads
BGA1.5-4×0.8-1.27 mmBall array
CSP≤1.2×0.3-0.5 mmBall/bump array

Why Chip Scale Packaging Matters in Modern Electronics

The Miniaturization Trend of Chip

PCB area per IC function has been shrinking for 20 years. A smartphone mainboard gives some ICs under 5 mm² to work with - space that a standard QFP couldn't fit into, even without any other components nearby. Chip scale packaging was the answer the industry developed: when the package is the size of the die, you stop losing board area to overhead.

While early devices used only a handful of WLPs, recent flagship smartphones such as the Apple iPhone 17 series and Samsung Galaxy S25 series integrate dozens of WLCSP and other chip-scale packages across sensors, PMICs, RF front-ends, audio codecs, wireless connectivity, and display control subsystems.

What Short Interconnect Actually Buys You

Every millimeter of conductor adds inductance. In a wire-bonded QFP, the signal path from die pad to PCB trace might span 5-8 mm. In a WLCSP, it's 150-300 µm. That difference translates directly to:

  • Lower parasitic inductance → less ringing on fast digital edges
  • Lower parasitic capacitance → better high-frequency signal integrity
  • Reduced ground bounce → cleaner power delivery on fast load transients
  • Lower switching losses → marginal but real power efficiency gains in battery-powered devices

This is why RF front-ends, PMICs, and high-speed memory controllers almost exclusively use CSP or wafer-level packaging in mobile applications.

Key Features of Chip Scale Package

FeatureDetail
Form factor≤1.2× die area - smallest standard SMT package category
Interconnect length150-300 µm (die to PCB)
I/O styleBottom-side solder ball or copper pillar array
Pitch range0.3 mm - 0.5 mm (most common: 0.4 mm)
Thermal pathThrough solder balls to PCB copper; no dedicated thermal pad
SMT compatibilityStandard reflow profile; requires fine-pitch paste printing equipment

Types of Chip Scale Packages

types of chip scale packages

Figure: The CSP family tree including WLCSP, FCCSP, and LFCSP types.

Wafer-Level Chip Scale Package (WLCSP)

The WLCSP package is the most compact CSP variant - and the most widely used in consumer electronics. This wafer-level chip-scale package is a true chip-scale packaging technology since the resulting package is the same size as the die. It differs from other BGA package types and laminate-based CSPs in that no bond wires or interposer connections are required.

What makes WLCSP different from other CSPs: All packaging steps - redistribution, bumping, passivation - happen at the wafer level, before dicing. You process thousands of dies simultaneously rather than one at a time.

WLCSP Structure

a wlcsp showing internal layers and solder bump

Figure: A WLCSP showing internal layers and solder bump.

The layer stack from silicon to solder ball:

  1. Passivation: Protects the active die surface; bond pad openings etched through
  2. Polymer stress buffer: Polyimide or PBO film; absorbs thermomechanical strain during thermal cycling
  3. Redistribution Layer (RDL): Copper traces routing from peripheral bond pads to the desired bump grid positions; single-layer RDL for simple designs, dual-layer for complex routing
  4. Under Bump Metallization (UBM): Ti/Cu/Ni or Ti/Cu stack; provides adhesion, diffusion barrier, and solder wettability
  5. Solder bumps: SAC305 alloy (96.5% Sn / 3% Ag / 0.5% Cu), 200-350 µm diameter

Quick note on cost

Because all steps happen at wafer level, cost scales with wafer area - not per-package assembly time. At high volumes with small die, WLCSP unit costs can undercut equivalent BGA or QFN options.

Flip-Chip Chip Scale Package (FCCSP)

A flip chip chip scale package (FCCSP) puts the die face-down on a thin organic substrate, with copper pillar bumps or solder bumps connecting die pads directly to the substrate routing layers below. Unlike WLCSP, there is a substrate between die and PCB solder balls.

flip chip chip scale package

Figure: Showing FCCSP structure with die, underfill, and substrate.

  • Why the substrate exists: Copper pillar pitch on modern SoC dies can be as fine as 40-100 µm. The organic substrate fans that out to 0.3-0.5 mm pitch compatible with PCB assembly. It also enables more routing layers than the thin RDL in a WLCSP.
  • Why underfill matters: Silicon CTE is ~3 ppm/°C. Organic substrate CTE is ~17 ppm/°C. Without underfill, thermal cycling cracks solder joints in hundreds of cycles. Underfill epoxy distributes that thermomechanical strain across the full interface instead of concentrating it at individual bumps.

FCCSP is the go-to format for high-pin-count application processors, networking ASICs, and high-bandwidth memory controllers - anywhere WLCSP's I/O density limits become a constraint.

Leadframe Chip Scale Package (LFCSP)

A leadframe chip scale package (LFCSP) uses the same stamped copper leadframe approach as a QFN, but trims the package body down to meet the ≤1.2× die size requirement. Wire bonds connect die to leadframe; mold compound encapsulates with minimal overhang.

leadframe chip scale package

Figure: Top-view and cross-section of an LFCSP structure with wire bonds.

LFCSP vs QFN - the key differences:

FeatureQFNLFCSP
Package-to-die ratio2-4×≤1.2×
Molding marginGenerousTrimmed to die edges
Lead countUp to 100+Typically ≤32
CostLowLow-Medium
Best forThermal-heavy, moderate I/OCompact, low-I/O designs

Note

LFCSP wins on cost for simple low-I/O parts - op-amps, LDOs, sensors - where the mature wire bonding supply chain keeps unit prices competitive with no wafer-level processing overhead.

Fan-In vs Fan-Out CSP

fan in wlcsp versus fan out csp

Figure: Comparison of fan-in WLCSP versus fan-out CSP.

Fan-In CSP (WLCSP is the canonical example):

  • All solder balls sit within the die footprint
  • I/O count limited by die area at the chosen pitch
  • A 2×2 mm die at 0.4 mm pitch supports roughly 12-16 usable balls
  • Lowest cost, smallest footprint

Fan-Out CSP:

  • Die is embedded in a reconstituted wafer or molded panel
  • RDL extends over surrounding mold compound beyond the original die edge
  • Balls placed outside the die area - breaks the I/O ceiling
  • Higher cost; package slightly larger than die but still very compact
  • Used for high-I/O SoCs and chiplet-based designs

Chip Scale Package vs Other IC Packages

PackageSize vs DiePitchPCB ComplexityReworkabilityBest Application
DIP10-20×2.54 mmMinimalEasyPrototyping, legacy
QFP4-8×0.4-0.8 mmLowModerateGeneral purpose
QFN1.5-3×0.5-0.8 mmLow-MediumModerateCompact thermal designs
CSP/WLCSP≤1.2×0.3-0.5 mmHigh (HDI)DifficultMobile, IoT, RF
BGA1.5-4×0.8-1.27 mmMediumDifficultHigh I/O SoCs
Bare Die (COB)1×-Very HighVery DifficultUltra-miniature

Chip Scale Package vs BGA

This is the comparison engineers most often need to make. While a typical BGA package would be 7.0 mm by 7.0 mm, an equivalent WLCSP would be 2.88 mm by 3.10 mm. That's roughly 6× less board area, which is significant.

chip scale package vs bga

Figure: Comparison between WLCSP and BGA packages for an identical die, demonstrating the significant reduction in physical footprint.

Size and Ball Pitch

  • WLCSP typically 0.3-0.5 mm pitch; package = die size
  • BGA typically 0.8-1.27 mm pitch; package 1.5-4× die size
  • CSP wins on board area; BGA wins on routability

Routing Complexity: At 0.8 mm BGA pitch, standard 4-layer PCBs with 100 µm trace/space can escape route most ball counts without via-in-pad. At 0.4 mm WLCSP pitch, you typically need:

  • ≤75 µm trace/space
  • Laser-drilled microvias
  • Via-in-pad (VIPPO) for any package with more than 2 rows

That moves the PCB into HDI territory - and adds cost. The package is cheaper; the board is more expensive. Evaluate system cost, not just package cost.

When to Choose CSP vs BGA

Choose CSP when...Choose BGA when...
Board area is the primary constraintI/O count exceeds ~100
I/O count is moderate (4-120)PCB routability must stay simple
Low parasitic inductance is criticalReworkability in production matters
Power dissipation is under ~500 mWDie is large and BGA overhead is acceptable

Chip Scale Package vs QFN

  • Thermal: QFN's exposed center thermal pad is a dedicated low-resistance heat path. For parts dissipating over 1 W, that matters - WLCSP distributes heat across all solder balls with no single thermal pad, which works for low-power ICs but becomes limiting above ~500 mW.
  • Assembly: QFN at 0.5-0.8 mm pitch is within reach of most standard SMT lines. WLCSP at 0.3-0.4 mm pitch requires finer stencils and tighter placement alignment.
  • Electrical: CSP wins - shorter interconnect, lower parasitics.
  • Rule of thumb: 200 mW Bluetooth SoC → CSP. 2 W motor driver → QFN.

CSP vs WLP - Clearing Up the Confusion

These terms overlap and cause real confusion. Here's the distinction:

  • WLP (Wafer-Level Package) = a manufacturing process - packaging steps happen at wafer level
  • CSP (Chip Scale Package) = a size specification - package is ≤1.2× die size
  • WLCSP = both: wafer-level processed AND chip-scale in size

All WLCSPs are CSPs. Not all CSPs are WLCSPs - FCCSP and LFCSP also meet the size spec but use substrate or leadframe processes.

How to Choose the Right IC Package

When to choose CSP:

  • Board area is your hardest constraint
  • I/O count is 4-120 (fan-in WLCSP); higher with fan-out
  • The design is RF, high-speed analog, or requires low parasitic inductance
  • Power dissipation is under ~500 mW (WLCSP) or ~2 W (FCCSP with thermal design)
  • Your PCB fabrication partner supports HDI

When NOT to use CSP:

  • Your PCB budget requires standard 2-layer or low-cost fab
  • I/O count is 200+
  • Power dissipation is high and a dedicated thermal pad is needed
  • Board-level rework is part of your production or field return process
  • The design must survive aggressive drop or vibration testing without underfill
FactorCSPBGAQFN
Board areaBestModerateModerate
Electrical performanceExcellentGoodGood
Thermal dissipationModerateModerateBest
PCB complexityHighMediumLow
ReworkabilityHardHardModerate
Package costMediumMedium-HighLow
High I/O countLimitedExcellentLimited

Note

Thermal dissipation depends heavily on PCB copper design and the specific CSP package technology used.

Advantages of Chip Scale Package

  • 20-80% smaller PCB footprint than traditional packages for the same die.
  • 10-20× lower parasitic inductance vs wire-bonded packages - critical for RF and fast digital designs.
  • Lower EMI and better RF behavior - A CSP IC package minimizes antenna effects and crosstalk due to ultra-short routing.
  • Reduced package inductance - The direct bump-to-pad connection ensures rapid switching without power integrity drops.
  • Better signal integrity - less ground bounce, lower SSN, reduced noise coupling in mixed-signal designs.
  • Scale economics - WLCSP cost scales with wafer area; at high volumes with small die, unit cost undercuts BGA equivalents.
  • Known Good Die - Wafer-level electrical test before dicing reduces PCB assembly yield losses from bad dies.

Disadvantages and Challenges of Chip Scale Package

  • Difficult Rework: Fine pitch and bottom-side I/O require specialized equipment for every rework attempt, including X-ray verification and precise thermal profiling. Plan for this cost explicitly if frequent repair is needed.
  • Sensitive Assembly: Eliminating the leadframe and mold compound makes WLCSP a fragile package. It requires careful handling and pick-and-place machines with compliant nozzle tips and precise Z-height control.
  • Requires HDI PCB: Fine pitch forces the use of sub-75 µm traces, laser-drilled microvias, and via-in-pad. This necessitates advanced HDI PCB design techniques, adding fabrication cost and lead time.
  • Thermal Cycling Reliability: CTE mismatch between silicon (~3 ppm/°C) and FR4 PCB (~17 ppm/°C) concentrates stress at the solder joints. For rigorous automotive or industrial applications, FCCSP with underfill is often required.
  • I/O Ceiling on Fan-In: A 2×2 mm WLCSP at 0.4 mm pitch holds roughly 12-16 usable balls. Increasing I/O requires a larger die area or fan-out processing, both of which add cost.

Design Considerations for Chip Scale Package

PCB Layout and Escape Routing

Getting signals out from under a WLCSP is the hardest routing task on most CSP boards. Three approaches:

wlcsp escape routing strategies

Figure: Comparing three WLCSP escape routing strategies: between-ball, via-in-pad, and dogbone.

StrategyWhen to UseLimitation
Between-ball trace routing≥0.5 mm pitch, outer rows onlyNot possible at 0.3-0.4 mm
Via-in-pad (VIPPO)Fine pitch, inner rowsAdds PCB cost; must be filled and capped
Dogbone routingModerate pitch with space availableNeeds clearance outside the pad

For packages with more than 2 ball rows, VIPPO is typically unavoidable for inner rows.

Pad and Solder Mask Rules

comparison of nsmd and smd pad designs for solder joints

Figure: Comparison of NSMD and SMD pad designs for solder joints

  • NSMD vs. SMD: Use NSMD pads for thermal fatigue reliability (the standard for consumer/IoT), as solder wets the pad sides for a stronger joint. Use SMD pads only if drop test performance is the primary concern.
  • Solder Mask Webbing: At 0.3-0.4 mm pitch, webbing is extremely thin (50-75 µm). Use Liquid Photoimageable (LPI) solder mask and confirm your PCB fab's registration tolerance to prevent mask shifting and solder bridging.

Via-in-Pad (VIPPO)

via in pad

Figure: Correct via-in-pad (VIPPO) structure compared to a defective unfilled via.

Unfilled vias trap flux and starve the solder joint above. If using via-in-pad, the VIPPO (Via-in-Pad, Plated Over) process is non-negotiable for reliability. This requires drilling, plating, epoxy-filling, and cap-plating the via perfectly flat before surface finish.

Thermal Management

WLCSPs lack dedicated thermal pads, making them entirely PCB-driven. Maximize copper pour under the component, stitch thermal vias to inner planes, and use 4-layer PCBs to effectively reduce θ_JA.

CSP Assembly Process Explained

Solder Paste Printing

Stencil design is critical and non-negotiable at fine pitch, and the standard SMT assembly process equipment requires specific tuning. Key parameters from manufacturer application notes:

  • Solder Paste Printing: Requires a 75-100 µm thick stencil (laser-cut stainless steel) with specific square apertures. Use Type 4 or finer solder paste.
  • Pick and Place: Demands automated fine-pitch machines with vision alignment (no mechanical centering). Use compliant nozzle tips and Z-height control to avoid bump damage.
  • Reflow: Follow a standard reflow soldering profile (SAC305 lead-free) keeping the ramp rate below 3°C/sec to prevent thermal shock to the silicon.
  • Inspection: Because joints are hidden beneath the die, 2D X-ray is mandatory to detect bridging and voids, while 3D CT X-ray is used for precise volumetric inspection.

Reliability Testing (JEDEC Standards)

TestStandardCondition
Temperature CyclingJESD22-A104-40°C to +125°C, 1000 cycles (consumer); 2000 cycles (automotive)
Drop TestJESD22-B111Critical for wearables and handheld devices
Moisture SensitivityJ-STD-020Typically MSL 1 or MSL 2
Bend TestIPC-9702Board-level mechanical stress

Applications of Chip Scale Package

1. Smartphones: Every flagship phone PCB is dense with CSP package technology. Power management ICs, RF transceivers, and audio codecs are all wafer-level packaged, as the size constraint is absolute for modern 6-8 mm thin devices.

2. Wearables: With usable board areas often under 20 cm², devices require the smallest available footprint, meaning a WLCSP package is used for virtually every IC in a competitive wearable design.

3. IoT Devices: Cost and size compete equally. WLCSP variants reduce module area while keeping component BOM costs highly competitive, and their lower parasitic losses extend battery life.

4. Medical Electronics: Implantable devices require sub-centimeter form factors with additional hermetic sealing for multi-year reliability.

5. Automotive Electronics: Used in ADAS and infotainment (AEC-Q006 qualified), though often less preferred in high-heat or high-stress industrial environments compared to space-constrained consumer applications.

6. CSP LED Packaging: The LED die is packaged with phosphor applied directly to die surfaces and solder bumps on the bottom (no leadframe), offering higher luminous efficacy and a superior thermal path directly to the PCB.

From Design to Production: Reliable CSP Assembly with JLCPCB

Getting a WLCSP design from schematic to assembled board involves more process discipline than standard SMT. Most early CSP failures in production come from insufficient PCB capability or lack of X-ray inspection - not the design itself.

Challenges Engineers Face with CSP Manufacturing

Two common failure modes catch engineers in their first build:

1. Fine-pitch paste printing failures - A paste printer running at ±50 µm registration accuracy struggles to hit ±25 µm demanded by 0.4 mm WLCSP pitch consistently across a full panel. The result: insufficient paste on edge balls, bridging on inner balls, or inconsistent deposit volumes that cause cold joints after reflow.

2. Hidden joint defects - Every solder joint under a WLCSP is invisible to AOI. Without X-ray inspection, voids, inner-row cold joints, and subtle bridging pass through functional test and fail in the field.

How JLCPCB Simplifies CSP-Based PCB Assembly

JLCPCB's PCB assembly service addresses both directly:

  • Fine-pitch SMT capability - Placement equipment handles 0.3 mm pitch components with vision-alignment feedback, not mechanical centering.
  • Stencil engineering - For WLCSP designs, aperture geometry is matched to the specific part pitch and pad type before paste printing begins.
  • X-ray inspection - Standard for fine-pitch ball grid components; not an optional add-on.
  • DFM review - Gerber files are checked against component specs before manufacturing starts - VIPPO requirements, solder mask web violations, and stencil aperture mismatches flagged on paper rather than in hardware.

via in pad with jlcpcb's fpov process

When to Use JLCPCB for CSP Projects

Whether you are validating a first-pass prototype featuring a WLCSP PMIC or scaling a dense wearable layout to full-volume production, flawless assembly is just as critical as the PCB design itself.

When high yield and precision matter most, JLCPCB provides the advanced manufacturing capabilities required to get your fine-pitch boards right on the first try. Get an instant quote for your CSP design at JLCPCB.

Get Quote Now

Future Trends in Chip Scale Packaging

Fan-Out Wafer-Level Packaging (FOWLP)

TSMC's InFO, ASE's FOCoS, and Samsung's FO-WLP are all production FOWLP platforms. The next evolution: multi-die FOWLP embedding heterogeneous dies in a single reconstituted wafer with inter-die RDL routing - the foundation of chiplet architectures for AI and 5G applications.

3D IC and TSV Stacking

Through-Silicon Vias enable vertical die stacking with electrical connections through the silicon. HBM (High Bandwidth Memory) is the most mature application - stacking 4-12 DRAM dies with 55 µm TSV pitch. Hybrid bonding (sub-10 µm pitch, copper-to-copper direct bond) is the next step for AI accelerator memory integration.

Heterogeneous Integration

The chiplet model - multiple specialized dies in one package - is moving down-market. Mixed-signal chiplets, integrated passive components, and RF front-end integration within CSP-format modules are in active development across TSMC, Intel, and the OSAT ecosystem.

AI and HPC Packaging

AI accelerators need enormous memory bandwidth at low latency. CoWoS (Chip-on-Wafer-on-Substrate), EMIB, and 3D-stacked die architectures are the current high-end solutions. Over the next decade, the interconnect density and thermal management techniques developed for AI packaging will propagate into mainstream CSP formats.

FAQs About Chip Scale Package

Q: Does a wafer-level chip scale package (WLCSP) require underfill?

Standard fan-in WLCSP packages used in consumer electronics usually do not require underfill, as the polymer stress buffer layer absorbs thermomechanical strain. However, for flip chip chip scale packages (FCCSP) or applications in extreme automotive environments, underfill epoxy is often necessary to prevent solder joint cracking from CTE mismatch.

Q: What type of solder paste is recommended for CSP package assembly?

Due to the fine pitch (0.3 mm-0.5 mm) of a CSP package, standard Type 3 solder paste is inadequate. Engineers should specify Type 4 (or even Type 5) no-clean solder paste, which features smaller solder spheres (25-36 µm) to ensure clean release from the fine stencil apertures and prevent bridging.

Q: Are chip-scale packages more expensive than traditional BGA or QFN?

At the component level, wafer-level packaging can actually be cheaper in high volumes because the packaging steps are applied to the entire wafer at once. However, the total system cost may increase because a chip-scale package often forces the use of more expensive HDI PCB fabrication and specialized fine-pitch assembly processes.

Q: How do I test or prototype with a chip-scale package?

Bare CSPs cannot be easily hand-soldered or probed with standard multimeter leads. For prototyping, engineers typically use breakout boards (adapters that convert the fine-pitch array to standard 2.54 mm headers) or rely on turnkey PCBA services like JLCPCB to machine-assemble the initial test boards.

Q: Where is the chip-scale package LED used?

SP LEDs are used in automotive headlamp modules, mini-LED backlights for display panels, high-power illumination fixtures, and any application requiring a small light-emitting point source with efficient heat dissipation and high luminous efficacy.

Conclusion

Chip scale packaging solves one problem - the package taking up space the silicon doesn't need - and delivers a cascade of benefits: smaller boards, shorter signal paths, lower parasitics, and, in high volumes, competitive unit costs. As electronics continue to shrink, mastering the chip-scale package (CSP) layout constraints will only become more critical for engineers. The shift toward advanced chip-scale packaging will continue to define the next generation of hardware.

For WLCSP and fine-pitch designs, JLCPCB offers full-stack fabrication and PCB assembly - including HDI with VIPPO, precision SMT, and standard X-ray inspection. Start with a free DFM review to catch errors early and avoid costly respins. Quote your design today.

Keep Learning