Border Layer Thickness: Impact on PCB Dimensions and V-Grooves
3 min
When it comes to designing a PCB, understanding the implications of border layer thickness is essential. In this blog post, we will take a closer look at an example to investigate whether different line widths on the border layer can affect the final board dimensions and the thickness of V-grooves during panelization.
Example Scenario
Imagine we have a PCB design with two different line widths on the border layer: 0.1mm and 1.0mm, respectively. Now let's address the following questions:
Will the dimensions of the final board be different?
The answer is no. The thickness of the border line does not directly impact the overall dimensions of the board. Regardless of the chosen line width for the border layer, all cuts are referenced to the centerline of the border lines. Consequently, the width and length of the board will remain consistent.
During panelization, will the V-grooves be cut according to the thickness of the border layer, creating V-grooves of different thicknesses?
No, the thickness of the border layer does not determine the thickness of the V-grooves. V-grooves are cut according to predefined specifications, independent of the border layer thickness. This ensures uniform V-groove thickness across the panel.
Handling Shapes and Grooves
To gain a comprehensive understanding, let's also discuss how shapes and grooves are handled in such a scenario.
Shapes drawn inside the board:
When designing shapes within the board, such as cutouts or internal features, they are typically routed based on the centerline of the line. The actual width of the shape will be determined by the routing tool, irrespective of the border line's width.
Solid lines used to depict grooves:
For solid shapes, including filled polygons or copper pours, they are manufactured based on the actual width of the drawn shape. The thickness of the border layer does not influence the dimensions of internal solid shapes on the PCB.
Conclusion
In this example, we have explored the impact of different line widths on the border layer of a PCB design. We have learned that the thickness of the border line does not affect the board dimensions, as all cuts are referenced to the centerline of the border lines. Additionally, V-grooves are cut according to predefined specifications, independent of the border layer thickness.
Understanding these concepts is crucial for designing PCBs accurately. By considering the relationship between border layer thickness, board dimensions, and V-grooves, you can ensure the desired outcomes in your PCB fabrication process. JLCPCB hope this example has shed light on the topic. If you have any further questions or need assistance with your PCB design, feel free to reach out to us.
Keep Learning
The Guide to Quick Turn PCBs : Fast Prototypes and Reliable Production
Have you ever calculated how much dead engineering time your team burns waiting for PCBs? If your standard fabrication turnaround is two to three weeks and your design needs three revision cycles, a modest number for anything beyond a breakout board. You are looking at wait time of 6 to 9 weeks alone. That is not a scheduling problem. That is a momentum killer, and it is exactly why quick-turn PCB fabrication has shifted from a nice-to-have to a strategic weapon in hardware development. The calculus i......
PCB Basic 3: Understanding PCB Manufacturing Processes
Welcome to the third installment of our PCB Basics series. In this article, we will unravel the step-by-step process of PCB manufacturing, guiding you through each stage with clarity and precision. Join us as we embark on this educational journey and discover how JLCPCB's advanced manufacturing capabilities and technology together with unparalleled commitment to quality assurance can elevate your PCB designs to next levels. Substrate Selection: Laying the Foundation One of the critical steps in PCB ma......
Electronic Board Manufacturing: Efficient Strategy and Quality Control Processes
Electronic board manufacturing is a critical process in the electronics industry, and the quality of the boards produced can significantly impact the performance and reliability of the final product. Therefore, it is essential to follow efficient strategies and quality control processes throughout the manufacturing process to ensure the highest quality of the boards. In this article, we will explore the various steps involved in electronic board manufacturing, including materials selection, design and......
Mastering Precision in PCB Drilling : Tools, Techniques, and Via Optimization for High-Quality Boards
In the modern multilayer boards, the accurate holes are used to connect internal copper layers and to assemble components. In our case, the drilling opens the vias and through-holes through which the signals are transferred among the layers, and it is the most important part of the PCB manufacturing, frankly speaking. The reason is that it provides the basis of vias and ensures that the various PCB layers are able to communicate with one another. All through-holes on the plated begin as a simple drill......
PCB Etching in Professional Fabrication : Modern Techniques and Industrial Strength
The etching of printed circuit boards is the selective removal of unwanted copper on a board to form the conductive traces and pads. It is effectively a subtractive process; after the photolithography or a printed resist mask has been applied, the remaining copper is removed with a chemical ether solution. It leaves the circuit pattern it was intended to create. Well, imagine that you are on the copper at the spa, you put it in the correct bath, and the undesired metal just dissolves. Etching is accur......
Laser Engraving vs. Professional PCB Fabrication : Understanding DIY Limitations and Industrial Advantages
In the conventional approach, we first apply a mask pattern and then remove metals using chemicals. In hobby electronics, using a laser engraver to make circuit boards is an exciting idea. The basic concept is to generate a laser to pattern a copper-clad board. Typically, a bare PCB is first coated with a dark resist layer that protects the copper. Then a laser cutter follows your circuit design to burn away the resist where copper traces should remain. After laser etching, the exposed copper is chemi......