Top 5 PCB Soldering Defects and How to Prevent Them
9 min
- What Are the Most Common PCB Soldering Defects And Why They Happen?
- Soldering Iron vs. Solder Paste Stencil: Choosing the Right Tool for the Job
- Pro Tips: How to Use a Stencil to Achieve Flawless Hand Soldering?
- How to Order Your High-Precision Stencil from JLCPCB in 5 Minutes?
- Fixing Mistakes: Essential Rework Tools for Every Maker
- Conclusion: Professional Quality Is Closer Than You Think
- Q: What is the finest pitch a laser-cut stencil handles reliably?
- Q: Does solder flux type matter for SMD work?
- Q: Why do solder balls appear even when I use a stencil?
- Q: Solder wick or solder sucker, which is better for SMD rework?
PCB design takes hours of careful work. You verify every trace and check every footprint. However, a single solder bridge or a brittle cold joint can ruin the entire project. Soldering defects like these can be an immense frustration for every engineer out there.
While a good soldering iron is essential, manual assembly has limits as components get smaller. That's where you have to approach the whole thing with strategy. Identifying the common defects isn't rocket science once you know what to look for.
In this guide, you get the 5 common PCB soldering defects and ways to prevent them. Let's get into it.
What Are the Most Common PCB Soldering Defects And Why They Happen?
Nearly every defect traces back to three variables: heat, volume, and alignment. Here is a diagnostic breakdown of what you will most likely encounter and what is actually driving each failure.
Solder Bridge:

A PCB solder bridge; This consists of two electrically isolated pads that are connected by excess solder. Mostly affected by them are fine-pitch packages such as QFN, TQFP, and 0201 passives, where pad gaps may be less than 0.2 mm. Slight paste excess or uneven reflow pulls molten metal sideways into that gap. These bridges are invisible to the naked eye but lethal to circuit function.
Cold Solder Joint:

The iron or the oven does not reach a high temperature of reflow, and the solder does not completely melt, thus adhering to the pad and the lead before wetting. It has a dull, grainy surface instead of a smooth and shiny one, is brittle to vibration, and unstable to thermal cycling. Poor solder flux coverage makes it worse: surface oxides block wetting even when the heat is technically adequate.
Tombstoning:

If one pad of a small passive reaches liquidus first, surface tension yanks the component upright. Tombstoning solder defects hit 0402 and 0201 components hardest. The cause is almost always asymmetric thermal loading from uneven paste deposits, mismatched pad sizes, or off-center placement.
Solder Balls:

Tiny beads scattered near a joint are not cosmetic. Anyone sitting between fine-pitch pins is a potential short. Solder balls form when moisture in the paste vaporizes during reflow preheat, spattering molten droplets outward. Paste that absorbed humidity, an aggressive ramp rate, or paste outside the pad boundary all produce them.
Insufficient or Excessive Solder:

Under-wetted pads pass initial testing, then fail after a few thermal cycles. Too many solder bridges adjacent to pads or bury the lead. On through-hole boards, excessive solder is the classic hand-soldering mistake. Feeding wire until the joint looks shiny instead of watching the fillet form correctly.
Soldering Iron vs. Solder Paste Stencil: Choosing the Right Tool for the Job

You need both. The question is knowing which one to reach for.
The Soldering Iron: The Versatile Classic
A temperature-controlled iron is irreplaceable for through-hole parts, wire connections, edge connectors, and spot rework. Nothing replaces the tactile feedback of drag-soldering 0.5 mm pitch leads.
Where it breaks down is scale and consistency. Applying identical paste volumes to 60 SMD pads by hand is genuinely difficult. Dwell time, tip angle, and wire feed rate drift subtly from pad to pad until rework starts eating more time than assembly.
The Solder Paste Stencil: The Precision Professional
A PCB stencil is a laser-cut stainless steel sheet with apertures that match exactly to every SMD pad. Place and trace solder paste using a squeegee over the board, then lift the pads in order to form a metered deposit on the pads. That gets rid of the two primary causes of SMT soldering defects, inconsiderate volume and misregistration.
Reflow and the paste collapses into clean, repeatable joints across the entire surface at once. First-pass yield climbs and rework time drops, whether you're building one unit or fifty. Take a look at our custom JLCPCB stencils to get a better idea.
Pro Tips: How to Use a Stencil to Achieve Flawless Hand Soldering?
Tip 1: Let the Aperture Control Volume
A well-designed SMT stencil sizes apertures using the area ratio formula. The aperture opening relative to the wall surface area governs how cleanly the paste transfers. Because every aperture is machined identically, every pad gets the same deposit. That uniformity makes solder bridging rare.
One catch: rough aperture walls cause smearing instead of clean release. This is addressed at the microscopic level using electropolished stencils, which visually enhances the quality of the deposit on small-pitch pads.
Tip 2: Hold the Squeegee at 45 Degrees
Angle matters more than pressure. At 45 degrees, the blade pushes paste into apertures while keeping the surface clean. Steeper and paste rolls ahead without filling; shallower and it smears. One smooth, continuous stroke outperforms short passes. Repeated strokes drag paste back out of apertures already filled.
Tip 3: Build a Quick Alignment Jig
Holding a stencil still while squeegeeing freehand is nearly impossible. Tape scrap PCB offcuts of matching thickness around three sides of your board to form a snug pocket. The board can't shift mid-stroke, and the stencil stays coplanar. Three minutes to set up, immediately visible improvement on 0402 and smaller.
Tip 4: Solder Flux Is Never Optional
Fresh paste contains solder flux, but for iron-based rework, adding flux before heat makes a real difference. It strips the oxide layer that blocks wetting. Afterwards, clean residue with flux remover. On high-frequency boards or anywhere leakage current matters, skipping that step is a slow route to reliability failures.
How to Order Your High-Precision Stencil from JLCPCB in 5 Minutes?
JLCPCB is producing stencils using 304 HTA stainless steel, of laser precision to +-0.003 mm. The cost starts at $3 USD, and it can take as fast as 12 hours to produce the parts, with no minimum order.
Now, let's get through the ordering process.
Three Ordering Methods:
There are three ways for you to order a stencil from JLCPCB.
Method A: Order with a PCB

You can simply order a stencil along with your base PCB order. It works like an add-on option with the base PCB order. After selecting the PCB parameters, simply scroll down, and you will see a button on the right side of “Stencil”. Toggle it, to get the options for inputting all the details.
Method B: Order the stencil individually

Another method is to order the stencil solely. Here, you simply go to the order now page and choose SMT-stencil from there. It will give you the option to upload gerber file, upload it, set the required parameters, and you are done.
Method C: Order from the PCB order history

If you already have a previous PCB order from JLCPCB, then you can use that to order a new stencil as well. To do that, just go to the order history and select the previous order. There, you will see a show all dropdown; click on that. Then, you will see a “Need stencil” option. Click on that to add your desired stencil.
Fixing Mistakes: Essential Rework Tools for Every Maker
Even a clean stencil-and-reflow workflow leaves finishing work. Connectors, through-hole parts, and the occasional shifted component all need manual attention.
Soldering Iron:
Still essential after reflow. Through-hole components, power terminals, and USB connectors do not go through the oven. A fine chisel tip handles drag-soldering fine-pitch leads and touching up bad solder joints that slipped through inspection.
Solder Wick:
Rosin-flux-impregnated braid pressed against a joint and heated draws molten solder out through capillary action. For clearing a solder bridge on fine-pitch pins, wick gives more control than a vacuum pump and won't lift a pad if used carefully.
Hot Air Rework Station:
Indispensable for removing SMD ICs, reflowing a cold joint cluster, or recovering tombstoned passives. Keep airflow low, apply flux first, and move heat slowly in circles around the component perimeter.
Flux Remover:
Rework leaves residue. On most boards, 99% isopropyl alcohol on a lint-free cloth handles it. On high-frequency paths or near fine-pitch ICs, purpose-formulated flux remover is more thorough. Some residues absorb moisture and create leakage paths exactly where you least want them.
Conclusion: Professional Quality Is Closer Than You Think
Soldering defects are no longer a matter of guesswork. A bridge means too much paste, while a tombstone indicates thermal issues. Using a precision stencil eliminates these variables and prevents most of these from even happening in the first place.
And when we speak of precision stencil, we have to mention JLCPCB. They offer high-quality, laser-cut stencils starting at just $1. With 304 HTA stainless steel and ultra-fast 12-hour production, you get industrial-grade results at an unbeatable price. Get a $11 stencil coupon and try it JLCPCB yourself.
Frequently Asked Questions:
Q: What is the finest pitch a laser-cut stencil handles reliably?
Electropolished stainless handles down to 0.3 mm pitch reliably. Below that, nano-coated or step stencils are the right tool. JLCPCB’s ±0.003 mm precision covers essentially every fine-pitch SMD package in current production.
Q: Does solder flux type matter for SMD work?
Significantly. No-clean flux leaves a non-corrosive residue convenient for production. Water-soluble requires extensive rinsing. Rosin is also beneficial in hand-soldering; it is always good to wash with the flux remover afterwards. Acid-core flux should not be used on electronics, as it causes copper corrosion.
Q: Why do solder balls appear even when I use a stencil?
Three causes: paste that absorbed humidity, a preheat ramp that climbs too fast, or paste deposited outside the pad boundary. Store paste at 0–10°C in a sealed container, use a proper reflow soak zone, and verify stencil alignment. Solve all three, and solder balls essentially stop.
Q: Solder wick or solder sucker, which is better for SMD rework?
Wick wins for fine-pitch SMD. It gives precise control and applies no mechanical force that could lift a pad. A solder sucker is faster for clearing through-hole barrels. On SMD pads, one careless pump stroke can peel the pad off the substrate
Keep Learning
DC Jack Soldering: How to Solder a DC Barrel Jack / Power Connector
Key Takeaways Confirm polarity before the iron touches the board: Check the adapter label, device marking, and jack pinout for center-positive versus center-negative wiring, because reversed polarity can destroy a regulator or microcontroller instantly. Deliver enough heat for the big joints: DC jack terminals are high-mass, so use a larger chisel or bevel tip, more heat or dwell, and flux until solder fills the plated hole and leaves a shiny fillet instead of a dull, grainy surface. Build in mechanic......
How to Solder a JST Connector: Through-Hole, SMT, and Board-to-Board Guide
Key Takeaways Soldering a connector is electrical and mechanical at once: Seat the header flush and square, tack one corner pin, verify alignment, then solder the remaining pins and every mechanical anchor tab, because plugging and cable forces travel through the housing and hold-downs rather than the signal pins. Match the method to the mount type: Through-hole headers need full barrel fill with a larger tip and flux for heat-sinking power pins, SMT headers need tack-and-align with hold-down tabs ful......
How to Tin a Soldering Iron: First Use & Re-Tinning
Key Takeaways Tin from the first heat-up: Bring the iron to roughly 315–370 °C (600–700 °F), wipe the tip on brass wool, and melt fresh flux-cored solder onto every working face until a thin mirror-bright film covers it, then wipe away the excess and lay down one more light coat. Re-tin by condition, not the clock: Keep a film of solder on the tip at all times, re-tin the moment wetting turns patchy, and lay down a generous coat before shutdown so oxidation cannot start while the iron sits idle. Never......
How to Solder an Audio Jack to a PCB
Key Takeaways Confirm the exact pinout first: TS, TRS, and TRRS jacks differ in conductor count and PCB terminal numbering, and TRRS wiring follows CTIA or OMTP standards, so always map every pin from the manufacturer datasheet and PCB footprint before soldering. Control heat and solder: Use a fine-tip iron, flux, and a minimal amount of solder, tack one pin to keep the jack flush and square, then solder each contact pin by pin to prevent bridges between closely spaced terminals. Finish and verify: So......
How to Solder SMD LEDs: A Step-by-Step Guide for Iron, Hot Air, and Reflow
Key Takeaways Confirm polarity and orientation first: Identify the anode and cathode before applying any heat, because a reversed SMD LED will not light and correcting it costs another thermal cycle. Match the method to the job: A fine-tip iron suits one or a few LEDs, hot air is best for rework and single-part replacement, and solder paste with reflow is fastest for complete boards. Keep solder and heat minimal: A small, fully wetted fillet and short dwell times protect the LED die, phosphor, and enc......
How to Solder a Potentiometer (PCB, Panel & Guitar Pots)
Key Takeaways Identify the wiper terminal: In most potentiometers, the middle pin is the wiper. Always verify with a multimeter before soldering. Pre-tin surfaces: Tin both the terminals and wires before joining to ensure strong, clean solder joints. Control heat carefully: Use a temperature-controlled iron and keep contact time short (below 260°C for a few seconds) to avoid damaging the internal resistive track. Test after soldering: Always check continuity and sweep the shaft while measuring output ......