Selecting the Right Solder Paste for Your PCB Assembly
5 min
- What is Solder Paste?
- Types of Solder Paste by Alloy Composition
- Flux Types in Solder Paste:
- Alloy Defects in Soldering:
- Other Parameters for a Right Solder Paste:
- Conclusion
Choosing the soldering paste is essential and we may follow some guidelines when going for it. Variations in flux residue, alloy strength, alloy flexibility, void control, wetting properties, and other performance metrics can all have a big impact. In PCB assembly, solder paste is a sticky conductive medium which makes the joint between two metals, in case of electronics we may say two wires or the lead of two components. A seamless, error-free production run or expensive rework or product problems might be caused by the choice of solder paste. Simple solder paste needs to cover:
- Quality: Pick a solder paste that complements your design, materials, and heating method the best.
- Throughput: Make use of solder that facilitates quicker, more effective heating and printing.
- Cost: To lower total manufacturing costs, strike a balance between material.
Everything you need to know about selecting the best solder paste for your PCB assembly will be covered in this extensive guide. It includes types of paste, compositions of flux types, particle sizes and important industry standards.
What is Solder Paste?
A combination of flux and powdered solder alloy, solder paste is a viscous substance that can be used for PCB screen or stencil printing. The solder particles melt when heated (reflowed), creating robust, conductive connections between PCB pads and component leads.
Basic Composition of Solder Paste:
Metal powder alloy (92–96% by weight) and flux (6–10% by weight).
A detailed list of alloy and flux medium types is provided below. We have written a comprehensive article on the benefits and drawbacks of lead-free and leaded solders because some alloys contain lead.
Types of Solder Paste by Alloy Composition
Your first step is to select the appropriate alloy type. Which is based on performance requirements and regulatory compliance. Lead content, melting temperature and alloy powder particle size are the three main factors, when selecting a solder alloy. The compositions in different types of alloys are as follows:
Flux Types in Solder Paste:
The flux component has a major impact on the quality of the solder junction and the need for cleaning after assembly. Here is a proper guide to flux selection that we have created.
1. No-Clean: Used in consumer goods where cleaning is unfeasible, this type of product does not require post-soldering cleaning.
2. RMA (Rosin Mildly Activated): It is utilized in general PCB assembly and is good for moderate activities with less residue
3. Water-Soluble: Applied to high-activity applications where soldering is more necessary. It is dependable and easily cleaned with a water dip.
Alloy Defects in Soldering:
Since lead-free solder is still a relatively new technology, various issues are still being resolved. Typical soldering flaws include:
Composition Issues: Composition problems include tin whiskers (in tin-rich alloys), changes in alloy composition due to prolonged heating, and problems with melting temperature or particle size.
Usage Errors: It includes poor wetting on pads at high temperatures, solder beading from inadequate paste deposition, tombstoning from uneven paste, and cracks from thermal or mechanical stress.
Other Causes: They include surface tension issues in lead-free soldering, cracks from elevated soldering temperatures, voids from mismatched flux or materials, and PCB warping.
Other Parameters for a Right Solder Paste:
1. Mesh Size (Particle Size):
Particle size is a determining factor in solder paste's appropriateness for various PCB designs. Type 5 solder paste is advised for ultra-fine pitch applications of 0.3 mm or smaller. Fine-pitch components of about 0.4 mm are best suited for Type 4 paste. Which has particles that range in size from 20 to 40 μm. Type 3 solder paste is frequently used for conventional SMT applications with a pitch of 0.5 mm. Here is the basic guide:
- Type 3: Suitable for standard SMT (≥0.5 mm pitch)
- Type 4: Ideal for fine-pitch (0.4 mm pitch)
- Type 5: Best for ultra-fine pitch (0.3 mm or smaller)
Finer powder is indicated by a higher mesh number, whereas larger particles are indicated by a lower mesh number. For best results, the particle size should be 1/4th of the stencil aperture.
2. Viscosity:
This factor influences the paste's behavior while handling and printing. Lower viscosity ones can print more quickly, also they need lower cleaning and are easy to dispense. For fine-pitch printing, higher viscosity is preferable.
- 200–600 Pa·S: Best for automated dispensing.
- 600–1200 Pa·S: Best for stencil printing.
Viscosity rises when at rest and falls when disturbed. Additionally, it is sensitive to temperature; greater temperatures cause viscosity to decrease.
Conclusion
A PCB assembly requires careful consideration of alloy composition, flux type and particle. Lead-free, no-clean solder paste with Type 3/4 particle sizes will satisfy performance for electronics. And it also comes under regulatory requirements for the majority of contemporary devices. Choose a solder paste that comes with fewer faults. The solder paste must also be compatible with the assembly process and industry standards processes. The information compiled for the best-case scenario is as follows:
- Flux Type: Choose No-clean for standard electronics and WS for aerospace.
- Particle Size: Choose Type 4/5 for fine-pitch and Type 3 for general use ones.
- Melting Point: Lead-free (215–220°C) and Leaded has (185°C).
Popular Articles
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Wire Bonding vs Flip Chip: Key Differences in Semiconductor Packaging
In the rapidly evolving world of semiconductor packaging, the choice between Wire Bonding and Flip Chip technology is more than just a mechanical decision—it is a strategic pivot that dictates your product’s performance, thermal limits, and bottom line. Are you looking for the cost-effective reliability of traditional interconnects, or does your application demand the high I/O density and superior signal integrity of modern flip-chip architectures? In this comprehensive guide, we draw on years of high......
Chip Scale Package (CSP) Explained: Types, Benefits & More
Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action. By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds t......
How to Solder Wires to a Circuit Board Properly: Step-by-Step Guide
Learning how to solder wires to a circuit board is a fundamental skill for electronics repair, prototyping, and PCB assembly. Whether you are attaching power leads, signal wires, or test connections, a weak solder joint can cause intermittent failures, lifted pads, or long-term reliability issues. In this step-by-step guide, you'll learn the correct tools, preparation methods, and soldering techniques needed to create strong, clean, and reliable wire-to-PCB connections. From preparing the wire and PCB......
BGA Reballing Explained: Complete Process, Tools, Risks, and Best Practices
In modern electronics design, the Ball Grid Array (BGA) is the standard for high-performance silicon, enabling thousands of I/O connections in a tiny footprint. However, this density creates a "black box" scenario: connections are hidden, and defects like cold joints or thermal fatigue cracks are invisible to the naked eye. Unlike a QFP that can be fixed with a soldering iron, a failed BGA threatens the viability of the entire board. BGA reballing is the critical solution to this problem. It is the pr......
SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
Surface Mount Devices (SMDs) are essential components in modern electronic devices, including smartphones, tablets, and IoT systems. Unlike older through-hole methods, where components were inserted through drilled PCB holes, soldering SMD components manually can be challenging, especially for beginners. The extremely small sizes and tight spacing on modern PCBs require high precision, and achieving reliable solder joints often depends on using the best SMD soldering tools. Common issues arising from ......
IC Package Types Explained: A Practical Guide for PCB Designers
Walk into any electronics lab, and you'll hear the same debate: "Which IC package should I use here?" It sounds like a simple question until you realise the answer determines your PCB footprint, thermal headroom, assembly process, rework feasibility, and field reliability - all at once. This guide breaks down every major IC package type used in modern PCB design, helping you understand the differences between common IC package types in plain engineering language so you can make the right call from the......