This website requires JavaScript.
Coupons APP Download
Ship to
Blog

Top 10 PCB Design Tips for High-Quality SMT Soldering

Published Nov 25, 2025, updated Feb 05, 2026

15 min

Table of Contents
  • PCB Design and Successful SMT Soldering: An Essential Connection
  • #1 Perfect Your Land Patterns (Pads) for Reliable SMT Soldering
  • #2 Optimize Copper Pours and Thermal Reliefs for Stable Soldering Performance
  • #3 Control Component Placement and Spacing in PCB Design for SMT Assembly
  • #4 Optimize Solder Mask Definitions (SMD vs. NSMD) for Clean Solder Joints
  • #5 Use Vias Strategically to Improve Thermal Management and Solderability
  • #6 Design for the Solder Paste Stencil to Ensure Consistent Reflow Results
  • #7 Include Clear and Accurate Fiducial Marks for SMT Alignment Precision
  • #8 Keep Silkscreen Off Pads to Prevent SMT Soldering Defects
  • #9 Orient Components for Efficient SMT Placement and Reflow
  • #10 Plan for Panelization to Reduce Depaneling Stress and Solder Joint Damage
  • Ensuring High-Quality SMT Soldering from PCB Design to PCB Assembly
  • Conclusion
  • FAQs about SMT Soldering

Surface Mount Technology (SMT) soldering defects, including bridging, tombstoning, and open joints, are not random production errors; they are part of the printed circuit board design.

These fundamental PCB design flaws lead to expensive issues, including extensive rework, unsuccessful validation tests, severe field failures, and postponed project schedules.

This article presents 10 technical PCB design tips that improve soldering outcomes, grounded in Design for Manufacturability (DFM) principles. These achievable changes can be made in your ECAD software before production for high-quality, high-yield SMT assembly. Whether you're an experienced engineer working with complex, high-density boards or a hobbyist on your first SMT assembly project, mastering these DFM principles is crucial for reliable and robust SMT assembly.

PCB Design and Successful SMT Soldering: An Essential Connection

To understand why PCB design is so critical, let's briefly visualize the SMT soldering process:

1. A stencil is used to print precise dots of solder paste onto the PCB's pads.

2. A pick-and-place machine populates the board with components.

3. The entire SMT assembly passes through a reflow oven for soldering, where a carefully controlled thermal profile melts the paste, allowing it to wick onto the pads and component leads, forming a solid electro-mechanical joint upon cooling.

Every design choice you make directly dictates the physics of this SMT soldering process. The geometry of your pads, the proximity of components, and the management of thermal mass all control how that solder paste melts, flows, and solidifies. An unbalanced PCB design creates an unbalanced physical process, which leads to soldering defects.

SMT soldering defects

Four SMT soldering defects: tombstoning, bridging, an open joint, and solder balling.

Your PCB design expertise is the first half of the equation; the second is a manufacturing partner who can execute your vision with precision and catch potential issues before they become costly.

JLCPCB's automated PCB assembly service isn't just about SMT assembly; it includes free, advanced DFM checks to identify potential SMT defects, from silkscreen on pads to insufficient clearances. This ensures your PCB design intent is perfectly realized on the first run.

Learn more about JLCPCB's advanced PCB Manufacturing & Assembly Capabilities

Here are the 10 most impactful tips to ensure your PCB design is optimized for high-quality SMT soldering.

#1 Perfect Your Land Patterns (Pads) for Reliable SMT Soldering

The land pattern, or pad, is the literal foundation of the solder joint. The most common PCB design mistake is using incorrect pad sizes - either too large, too small, or, most critically, unbalanced for a single component.

For two-terminal passive SMD components (like 0402 resistors or 0603 capacitors), the thermal mass of both pads must be identical. If one pad is significantly larger than the other, it will heat up more slowly in the reflow oven. This uneven heating causes the solder on the smaller, hotter pad to reflow first. The resulting surface tension pulls that end of the component, causing the other end to lift vertically. This is the classic "tombstoning" or "Manhattan" effect.

Solution: Prevention is the solution. Always adhere to the component manufacturer's recommended footprint dimensions, which are available in the datasheet. If you must create a custom footprint, follow industry standards. For passive components, this means ensuring perfect symmetry in pad dimensions and thermal connections.

Also Read: How to Prevent Solder Defects During Reflow Soldering

#2 Optimize Copper Pours and Thermal Reliefs for Stable Soldering Performance

This is a direct extension of Tip #1. A pad connected directly to a large copper plane (a ground or power pour) creates a massive, unbalanced heat sink. The plane will draw heat away from the pad, preventing it from reaching reflow temperature at the same rate as an isolated pad.

Even if the land patterns are identical, this thermal imbalance will cause tombstoning or, in less extreme cases, a cold, unreliable joint on the plane-connected side. The component will be pulled toward the pad that reflows first.

Solution: Use thermal reliefs (also called thermal "spokes" or "ties") to connect pads to large copper areas. A thermal relief is a small trace of copper between the pad and the plane, often in a 2- or 4-spoke pattern. This design drastically reduces the thermal connection, allowing the pad to heat up quickly and uniformly with its counterpart.

As a design rule, use four 10 mils (0.254mm) spokes for most connections. Modifying their width, as needed, can optimize thermal isolation while meeting high-current electrical solutions.

Also Read: Tips regarding improving the thermal management of PCBs

PCB Thermal Relief Pad Design

PCB design comparison showing a pad without and with a 4-spoke thermal relief connection to a copper pour.

#3 Control Component Placement and Spacing in PCB Design for SMT Assembly

While a densely populated board can be a design goal, packing the plan too tightly may result in manufacturing defects. These defects may arise in several forms:

Bridging: Fine-pitch components placed too close together can cause solder bridge issues.

Rework/Inspection: When components do not have sufficient clearance (generally <0.5mm - 1mm), they almost certainly won't get inspected by Automated Optical Inspection (AOI) or reworked.

Heat Shadowing: During reflow, migration occurs when a large component "shadows" a small component nearby. The large component absorbs the IR radiation from the reflow process and prevents it from reflowing properly.

Solution: Have a clear rule in your ECAD software for component clearance. A good start is around 0.5mm from smaller passives and 1-2mm from larger ICs. This is a critical DFM check that you can perform using JLCPCB’s free online DFM tool, which automatically detects costly placement errors before production begins.

#4 Optimize Solder Mask Definitions (SMD vs. NSMD) for Clean Solder Joints

The solder mask (the protective green/black/etc layer) is crucial for the soldering process, not merely for aesthetics. A frequent mistake is failing to deliberately design the interaction between the mask opening and the copper pad. There are two main types:

1. Solder Mask Defined (SMD): In this method, the solder mask opening is intentionally made smaller than the copper pad. Consequently, the solderable area is precisely determined by the solder mask itself.

2. NSMD (Non-Solder Mask Defined): In this configuration, the solder mask opening is larger than the copper pad. The copper pad itself determines the solderable area, as there is a visible gap between the mask and the pad.

A Solder Mask Defined VS Non-Solder Mask Defined PCB pad

The difference between a Solder Mask Defined (SMD) and Non-Solder Mask Defined (NSMD) PCB pad.

Solution: For most SMT components, NSMD is strongly preferred. Why? It allows the molten solder to bond not only to the top of the copper pad but also to its sides, creating a stronger, more reliable fillet.

SMD pads, while useful for components like BGAs to prevent bridging, create a weaker joint that is more prone to cracking under mechanical stress. JLCPCB's advanced PCB fabrication process can reliably produce both, but designing SMD pads requires special attention.

If your PCB design requires SMD pads, you must ensure the solder mask clearance is smaller than the copper pad. Crucially, the mask must overlap the copper by at least 3 mil (0.076mm) on all sides to account for manufacturing registration tolerances.

Learn How to Order Boards with Solder Mask Defined Pads from JLCPCB.

#5 Use Vias Strategically to Improve Thermal Management and Solderability

Vias are critical for routing, but placing an open via on or too close to a surface-mount technology (SMT) pad can lead to significant problems. During the reflow process, the molten solder can be drawn away from the pad and down into the via barrel due to capillary action. This phenomenon, known as "solder wicking," depletes the solder from the joint, resulting in a weak connection or a completely open circuit.

Solution: The best practice is to place vias away from the pad and connect them with a short trace. If high-density routing (like for a BGA) forces you to use via-in-pad, it must be specified as an advanced manufacturing process. This means the via must be filled (typically with non-conductive epoxy) and then plated over (capped) with copper to create a flat, solderable surface.

JLCPCB's via-in-pad process uses resin-filled and plated-over vias. It allows vias to be placed on any BGA pad without affecting subsequent SMT assembly.

via-in-pad

Comparison of JLCPCB’s plated via-in-pad vs standard

#6 Design for the Solder Paste Stencil to Ensure Consistent Reflow Results

Designers often mistakenly assume solder paste stencils are direct replicas of copper pads. This is a key area for optimization that has been overlooked. Stencil apertures, which dictate the volume and shape of deposited solder paste, should be intentionally designed. For fine-pitch components (e.g., those with a pitch less than 0.5mm), a 1:1 aperture can result in excessive paste, causing bridging.

Solution: Specify stencil modifications in your fabrication data.

● For fine-pitch integrated circuits (ICs), a reduction in aperture area of 5-10% is suggested.

● To prevent tombstoning in 0402/0201 passive components, modify the rectangular aperture to a "U-shape" or "home-plate" shape, pointing inwards. This adjustment alters the surface tension forces.

JLCPCB offers three advanced stencil technologies: Nano-coating, electropolishing, and Ultrasonic-resistant adhesive. By uploading your custom stencil layer (paste layer), JLCPCB ensures that these advanced aperture designs are fabricated exactly as you intended, giving you direct control over solder paste volume.

Component TypePad PitchRecommended Aperture StylePurpose
0402/0201 PassiveN/AU-Shape or Home-Plate (Inward)Prevents tombstoning
Fine-Pitch QFP/QFN< 0.5mm5-10% Area ReductionPrevents bridging
BGA0.8mm90% Area Circle (1:0.9)Controls solder volume

Table of stencil aperture recommendations for SMT components like 0402 passives and fine-pitch QFPs.

#7 Include Clear and Accurate Fiducial Marks for SMT Alignment Precision

Fiducials are small, circular copper patterns that act as optical alignment targets for automated assembly equipment. The pick-and-place machine's vision system uses these fiducial marks to determine the exact location and orientation of the PCB. Without them, the machine is "flying blind" and may misplace components, especially fine-pitch parts.

Solution: Include at least two (preferably three) "global fiducials" on the corners of your board and "local fiducials" for fine-pitch components. A standard design is a 1mm diameter copper pad with a 2mm diameter solder mask opening.

Following this standard ensures your board is compatible with JLCPCB's high-speed automated SMT lines, reducing setup time and guaranteeing placement accuracy.

Standard practice of the placement of fiducial marks

Standard practice of the placement of fiducial marks, including three global fiducials, two local fiducials per board, and four panel fiducials.

#8 Keep Silkscreen Off Pads to Prevent SMT Soldering Defects

This is a basic DFM check that is surprisingly easy to miss: allowing silkscreen (the white/black text) to overlap a solderable pad. Silkscreen is non-conductive ink. If it's on a pad, it creates a physical barrier that blocks the soldering process, resulting in an open circuit or a weak joint.

Solution: During your final PCB design review, run your DRC (Design Rule Check) and also do a visual check. Ensure all silkscreen elements are clipped to have a clear, safe distance (e.g., 0.1-0.2mm) from all exposed copper pads.

PCB solder mask

A 'Do and Don't' comparison for PCB solder mask.

The 'Do' side shows pads correctly exposed from the mask. The 'Don't' side shows pads incorrectly covered by the slikscrenn text.

This is one of the most common errors caught by JLCPCB's free, automated DFM check tool JLCDFM when you upload your Gerber files, saving you from a simple but costly mistake.

#9 Orient Components for Efficient SMT Placement and Reflow

Random component orientation directly hinders the speed and quality of SMT assembly. It complicates both automated (AOI) and manual inspection, leading to more errors. Particularly for polarized components such as diodes, inconsistent "north" and "south" facing orientations are a significant source of errors.

Solution: Inspection-oriented design. Standardize your orientations. For example, have all polarized capacitors face "north" or "west." Have all ICs use pin 1 in the same location (e.g., top-left). This simple housekeeping simplifies the programming of AOI systems, making inspection faster, more accurate, and more reliable.

#10 Plan for Panelization to Reduce Depaneling Stress and Solder Joint Damage

Your board isn't manufactured in isolation; it's part of a larger panel, typically separated by V-grooves (score lines) or "mouse bites" (breakaway tabs). After assembly, the boards are "depaneled" or broken apart. This action imparts significant mechanical stress and flexion to the board, which can fracture brittle components like MLCCs.

Solution: Keep sensitive components (MLCCs, BGAs, crystals) away from board edges, especially V-groove lines (a 3mm-5mm keep-out is safe). If you're designing your own panel, be sure to follow your manufacturer's guidelines.

JLCPCB provides clear documentation on panelization requirements for PCB assembly orders, ensuring your boards can be safely assembled and depanelled without damaging components.

Ensuring High-Quality SMT Soldering from PCB Design to PCB Assembly

As these 10 PCB design tips demonstrate, robust SMT soldering quality is a matter of correct planning. It's a direct result of proactive design choices that shift quality control from "post-production inspection" to "pre-production design." You are effectively engineering away the most common failures before they ever have a chance to occur.

Of course, a great PCB design is just the start. That design is handed off to a manufacturing partner who must verify it. This is where processes like SPI (Solder Paste Inspection) to check paste volume, multi-zone reflow profiling to ensure thermal uniformity, and post-reflow AOI (Automated Optical Inspection) and X-ray (for BGAs/QFNs) become critical for validating the results of your careful design.

A great design deserves a high-quality, transparent manufacturing process. JLCPCB’s SMT assembly service utilizes high-speed pick-and-place machines, reflow ovens for precise thermal control, and mandatory 3D SPI/AOI to ensure your design rules translate into perfect soldering joints. This combination of your DFM-optimized design and our advanced assembly process is the key to first-pass success.

Conclusion

Achieving high-quality SMT soldering is not a mysterious process; it's a predictable physical process largely within the designer's control. By incorporating these 10 Design for Manufacturing (DFM) principles - ranging from precise land patterns and thermal reliefs to strategic planning for stencils and depaneling - you are doing more than just designing a circuit; you are designing for assembly.

This proactive approach is crucial for minimizing manufacturing risks, cutting rework costs, and delivering a more reliable, professional, and successful final product.

Partnering with an advanced assembly service like JLCPCB, which automatically detects all DFM issues, amplifies these advantages and ensures your carefully designed board is manufactured to the highest quality.

FAQs about SMT Soldering

Q1: What is the most common SMT soldering defect, and how do I prevent it?

Solder bridging is one of the most common. This is where solder connects two or more pads that should not be connected. It's best prevented during PCB design by ensuring correct pad-to-pad spacing, defining a proper solder mask "dam" between pads, and (as discussed in Tip #6) specifying reduced apertures in the solder paste stencil.

JLCPCB's free DFM check can help flag potential bridging risks, and our precision stencil service ensures your custom apertures are fabricated accurately.

Q2: What is the influence of PCB surface finish (e.g., ENIG vs HASL) on SMT soldering?

The surface finish has a direct influence on solderability and pad flatness. ENIG (Electroless Nickel Immersion Gold) provides a very flat, reliable, and oxide-resistant surface that is perfect for fine-pitch SMT and BGA components. Lead-free HASL (Hot Air Solder Leveling) is more economical, but leaves a slightly uneven surface.

Both options are available at JLCPCB, allowing you to choose the surface finish that best meets your design specifications.

Q3: What is a "solder mask dam" and why is it important for SMT assembly?

A solder mask dam (or "web") is the thin strip of solder mask material that is designed to exist between two adjacent pads, such as the pins on a fine-pitch IC.

Its sole purpose is to act as a physical barrier to prevent molten solder from flowing ("bridging") from one pad to the next. If your solder mask expansion rules are too large, this dam can become too thin or disappear entirely, dramatically increasing the risk of solder bridges during SMT assembly.

solder mask dam

The solder mask dam is visible as the gap between two pads.

Q4: What is "solder balling," and is it a design or manufacturing issue?

Solder balling, where tiny spheres of solder are left scattered on the board after reflow, can be caused by both. From a PCB design perspective, it can occur if solder mask apertures are significantly larger than the pads, allowing solder paste to squeeze out and form balls. However, it is more frequently a manufacturing process issue.

JLCPCB minimizes these risks through tightly controlled processes, including using fresh, high-quality solder paste, managing board moisture, and employing optimized reflow profiles in our 10-zone ovens to ensure complete and clean solder activation.

Solder Balling in SMT Assembly

Solder Balling in SMT Assembly

Keep Learning