Basic Design of Solder Mask
10 min
- Purpose of Solder Mask
- Solder Mask Design
- Solder Mask Manufacturing
- Solder Mask Openings & Their Impact on Pad Geometries
- Difference Between Solder Paste and Solder Mask Layers
- Emphasis:
- FAQ about Design of Solder Mask
- Conclusion
Key Takeaways
- Negative Mask: Openings on the solder mask layer remove ink to expose copper pads.
- Standard Expansion: Standard 1/2-layer designs require a 0.05 mm (2 mil) expansion per side.
- LDI 1:1 Precision: Multilayer LDI tech enables 1:1 pad matching with ±0.02 mm accuracy.
- Solder Mask Dams: Dams require ≥ 0.10 mm pad spacing for green ink (1oz); narrower gaps are removed.
A standard double-sided PCB consists of multiple functional layers built upon a central dielectric substrate (Core Board). From the center outwards, these include the Top/Bottom Copper Layers, Top/Bottom Solder Mask Layers, and Top/Bottom Silkscreen Layers. Electrical connectivity between the top and bottom copper layers is achieved through Plated Through Holes (PTH). Note that standard double-sided boards only use through-hole PTHs; blind or buried vias are exclusively reserved for multilayer PCBs.
Purpose of Solder Mask
1. Prevents moisture and the intrusion of various chemicals and electrolytes, which can cause oxidation and corrosion of the copper traces, compromising electrical performance.
2. Guards against external mechanical scratches, thus maintaining insulation between copper traces and preventing short circuits.
3. Prevents unintended solder connections during component soldering, avoiding short circuits.
4. Reduces the consumption of pad surface finish (e.g., ENIG, HASL) in non-solderable areas.
5. Enhances the aesthetics of the board by giving it various colors.
Solder Mask Design
Solder Mask, as the name implies, is not about preventing all soldering. Some novice engineers may mistakenly believe that patterns drawn on the solder mask layer cause areas to be not solderable. This understanding is incorrect. Solder Mask refers to the areas on the board where solder resist ink is applied. As it is a negative pattern, the areas with patterns on the solder mask layer are not coated with ink. To facilitate understanding, let's use a snowy landscape analogy:
Imagine a pavilion (A) as the solder mask layer. After a heavy snowfall, the ground below the pavilion (B) will not have snow (solder resist ink), while the area not covered by the pavilion (C) will be entirely covered in snow (solder resist ink). Using this analogy, we return to PCB design for solder mask:
1. Patterns on the copper layer represent the copper traces.
2. Patterns on the solder mask layer remove ink coverage.
3. Areas where the copper layer and solder mask layer overlap on the same side create exposed copper (solder-coated or gold-plated) regions.
Solder Mask Manufacturing
In the actual production process, after drilling and copper plating the board, unwanted copper areas are removed, leaving behind the required copper areas (the traces). The process of soldermask production then begins:
1. The etched copper traces undergo processes such as board scrubbing and acid washing to remove oxide and impurities, roughen the copper surface for better adhesion with solder resist ink.
2. The entire board is coated with solder resist ink, dried, and a solder mask film is placed over the board. Ultraviolet (UV) light exposure causes the solder resist ink to solidify where soldermask patterns are present, protecting the designated areas.
3. Subsequent development and cleaning remove any uncured ink, revealing the original copper surface. Tin or gold plating can then be applied in later steps.
Solder Mask Openings & Their Impact on Pad Geometries
Solder mask openings (windows) are traditionally designed slightly larger than their corresponding copper pads (typically 0.05 mm / 2 mil expansion per side, or 0.1 mm overall). This design margin prevents solder mask ink from encroaching onto the solderable copper pad surface due to optical registration tolerances during standard UV exposure. However, this expansion alters the physical geometry of pads in three key design scenarios:
1. Isolated Pads (No connected traces): The exposed copper pad size remains as designed. However, because the solder mask opening expands outward, a narrow ring of bare dielectric substrate (FR-4) is exposed surrounding the copper pad perimeter.
2. Pads Connected to Traces:A short segment of the copper trace adjacent to the pad becomes exposed alongside the pad. During reflow soldering, molten solder may wick along this exposed trace section, potentially reducing the solder volume on the pad and causing uneven solder fillet formation or tombstoning.
3. Solder Mask Defined (SMD) Pads on Large Copper Planes: For pads created inside a large copper pour (e.g., ground planes or heat sinks), the functional pad geometry is defined strictly by the edge of the solder mask opening. Solder mask expansion directly enlarges the exposed copper region, making the pad larger than specified in the EDA footprint.
Advanced Multilayer Manufacturing: LDI 1:1 Precision Matching
Traditional PCB fabrication uses film-based photolithography, requiring expansion margins to compensate for film stretch and registration offsets. To overcome these limits on fine-pitch designs, JLCPCB has deployed High-Precision Laser Direct Imaging (LDI) technology across multilayer PCB production lines:
·Zero Expansion (1:1 Ratio): LDI directly writes the solder mask pattern onto the board using computer-controlled laser beams, achieving alignment tolerances within $\pm 0.02\text{ mm}$. This enables a 1:1 match between solder mask openings and copper pads on multilayer PCBs without risking solder mask encroachment.
·Preventing Trace Exposure: A 1:1 opening completely avoids unwanted trace exposure near fine-pitch ICs, preserving impedance boundaries and preventing solder bridges during assembly.
·Custom Expansion Options: For 1-layer and 2-layer boards utilizing standard process routes, or for specialized DFM requirements, designers can specify "Do not modify original solder mask size" during ordering. Ensure that your Gerber production files are carefully reviewed before final approval.
Solder Mask Bridge (Dam) Specifications for Fine-Pitch ICs
On dense IC designs (such as QFP, QFN, and BGA components), maintaining a narrow strip of solder mask ink—known as a Solder Mask Bridge or Dam—between adjacent pin pads is crucial. The dam acts as a physical barrier against liquid solder bridging and pin shorts during SMT reflow.
The manufacturability of a solder mask dam depends heavily on the pad-to-pad spacing, finished copper thickness, and ink color flow dynamics. Below are JLCPCB's standard manufacturing specifications:
JLCPCB Solder Mask Dam Design Guidelines:
| Process & Material Configuration | Finished Copper 1 oz (35 μm) | Finished Copper 2 oz (70 μm) |
|---|---|---|
| Standard Inks (Green, Red, Yellow, Blue, Purple) | Minimum Pad Spacing ≥ 0.10 mm (4 mil) | Minimum Pad Spacing ≥ 0.20 mm (8 mil) |
| Pigmented Inks (Matte/Glossy Black, White) | Minimum Pad Spacing ≥ 0.13 mm (5.1 mil) | Minimum Pad Spacing ≥ 0.20 mm (8 mil) |
| Solder Mask Expansion (1/2 Layer Standard) | 0.05 mm (2 mil) per side | 0.05 mm (2 mil) per side |
| Multilayer Opening Ratio (LDI Process) | 1:1 with Pad Size | 1:1 with Pad Size |
Difference Between Solder Paste and Solder Mask Layers
Solder Paste Layer: Used by stencil manufacturers to create stencils, ensuring precise application of solder paste onto component pads for subsequent SMT processing.
Solder Mask Layer: Used in PCB manufacturing, areas with patterns on the solder mask layer remain uncoated by solder resist, while areas without patterns are covered in solder resist ink.
Emphasis:
To have specific traces, copper areas, or pads remain uncoated by solder resist ink and coated with solder (or gold), you must add a soldermask layer pattern. Only the areas of the copper geometry overlapping with this soldermask pattern will have exposed copper and be treated with the selected surface finish (e.g., HASL, ENIG).
In contrast, paste layers are exclusively for stencil creation and have no relevance to PCB production. PCB review engineers do not handle or provide paste layer files.
Soldermask Bridge Fabrication
For densely packed IC pads, in order to reduce the risk of solder flowing to adjacent IC pins and causing shorts during soldering, soldermask bridges can be designed (i.e. applying a layer of soldermask ink between the two IC pads). According to JLCPCB’s manufacturing process, soldermask bridges may be applied when the following conditions are met:
FAQ about Design of Solder Mask
Q: What is the main difference between Solder Mask and Solder Paste layers in PCB design?
The Solder Mask Layer is used during PCB fabrication to define areas where green/color solder resist ink should be removed to expose copper pads for soldering. It operates on a negative pattern logic. The Solder Paste Layer (Paste Mask) is used exclusively by stencil manufacturers to cut laser openings in metal stencils for applying solder paste during SMT assembly. Paste mask files are not processed by PCB review engineers.
Q: Why are solder mask openings traditionally larger than copper pads?
Traditional PCB fabrication utilizes film-based UV photolithography, which requires an expansion margin (typically 0.05 mm / 2 mil per side) to compensate for optical registration tolerances and mechanical alignment offsets. This ensures that solder mask ink does not accidentally cover any portion of the solderable copper pad surface.
Q: How does JLCPCB's LDI technology achieve a 1:1 solder mask opening on multilayer PCBs?
JLCPCB utilizes high-precision Laser Direct Imaging (LDI) technology for multilayer boards, which directly writes the solder mask patterns onto the PCB using computer-controlled laser beams. LDI improves alignment accuracy to within ±0.02 mm, eliminating the need for solder mask expansion and allowing a 1:1 match between openings and copper pads without risking ink encroachment or trace exposure.
Q: What is a Solder Mask Bridge (Dam), and why is it important for fine-pitch ICs?
A Solder Mask Bridge (Dam) is a narrow strip of solder mask ink retained between two adjacent copper pads. It serves as a physical barrier during SMT reflow soldering to prevent liquid solder from flowing between pins and causing bridge short circuits, which is critical for fine-pitch packages like QFP, QFN, and BGA.
Q: What happens if the pad spacing on my design is too tight to form a solder mask bridge?
According to JLCPCB manufacturing guidelines, if pad spacing is less than the required minimum limit (e.g., <0.10 mm for 1oz green ink, or <0.13 mm for black/white ink), JLCPCB engineers will automatically remove the solder mask dams to form a single gang opening. This prevents thin, unadhered ink dams from peeling off during development and contaminating pads.
Conclusion
The solder mask is applied as a negative pattern, meaning that areas with patterns on the solder mask layer are not coated with the protective ink. This allows for the desired copper traces and pads to be exposed for soldering.
During PCB manufacturing, the solder mask is applied to the board and solidified using UV light. It helps prevent moisture and chemicals from damaging the copper traces and provides insulation between them to avoid short circuits.
It's important to design the solder mask with consideration for the size of solder mask windows, which should be slightly larger than the associated pads to account for any alignment errors. This may slightly change the shape of some pads.
To summarize, the solder mask is a protective layer that prevents solder from adhering to unwanted areas on the PCB. It helps maintain the integrity and reliability of the circuit by protecting the copper traces and preventing short circuits.
Popular Articles
• AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
• GPT-6 Astra PCB Design in KiCad: From Brief to Verified Native Project
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• How to Design Your Own Keyboard PCB: From Layout to Firmware
Keep Learning
AI Tools for PCB Design: Which Tool Fits Your Workflow Stage?
Note This article is intended to provide an independent technical overview of AI-powered PCB design tools based on publicly available product information. Product features and capabilities may change over time. AI tools can now assist with PCB architecture, schematic generation, component selection, placement, routing, and design verification. However, different tools target different stages of the PCB workflow. This guide compares AI tools for PCB design based on what they actually do, what inputs th......
KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
Key Takeaways Claude can design PCBs in KiCad: By connecting Claude to KiCad through an MCP server, you can use AI to create and modify PCB designs. In this project, Claude helped turn a 5 A XL4015 buck converter netlist into a two-layer, 63 × 33 mm PCB layout with zero ERC violations and zero DRC errors after minor initial fixes. Set up Claude securely: Use a KiCad MCP server that starts in read-only mode. Review the server code before installing it, connect through stdio, and allow editing only in a......
From Concept to Production: PCB DFM Guidelines and Analysis
Key Takeaways PCB DFM (Design for Manufacturing) is the bridge between design intent and manufacturing reality, ensuring a board can actually be fabricated and assembled with high yield. Essential DFM guidelines cover trace width and spacing, annular rings, via placement and drill sizes, soldermask and silkscreen, surface finish, and panelization. Modern DFM analysis is data-driven and automated, and many manufacturers now offer free DFM tools that check Gerber and drill files against fabrication and ......
Understanding PCB Resistance: Key Factors, Testing Methods, and Design Best Practices
How easily current flows through a circuit board is determined by its resistance. Although some resistance is provided by each trace and component on the board, the objective is to reduce it. When the material that electrons pass through blocks or slows down their flow, resistance results. Energy is lost as a result of this obstruction, frequently as heat. Trace resistance is a crucial factor in determining the circuit's operational current in power-related circuits, such as amplifier units. To guaran......
PCB Routers: Essential Tools for Modern Circuit Design
Introduction In modern PCB production, routing machines (commonly called PCB routers or CNC routers) play a critical role. They are used to cut the board outline, create V-grooves for depanelization, mill slots, and finish edges with high precision. As electronic devices become smaller and more complex, PCB routers ensure clean, accurate, and repeatable results. This article explains what PCB routers are, their types, key applications, best practices, and how JLCPCB integrates advanced routing in its ......
Creating Clear and Professional Reference Designators for Better PCB Assembly
Key Takeaways Reference designators are essential for accurate PCB assembly, debugging, and maintenance. Use minimum 0.8 mm text height and 0.15 mm line width for clear silkscreen printing. Keep designators on solder mask with proper clearance from pads and vias. Maintain consistent font, size, and orientation across the board. For high-density designs, use an assembly drawing instead of crowded silkscreen. Always run DFM checks to avoid overlapping or missing labels. Ever wonder about the little labe......