Microprocessor vs. Integrated Circuit: Key Differences, Types, and Applications
7 min
- 1. What is an Integrated Circuit?
- 2. What is a Microprocessor?
- 3. Different Types of Integrated Circuits:
- 4. Types of Microprocessors:
- Conclusion:
In electronics things origin from silicon and today we will discuss two different silicon pieces. It is not a type of battle, but a race of price to performance ratio. An integrated circuit is a piece of a semiconductor chip that houses thousands to billions of transistors in it. Integrated circuits house the basic structure of MOS transistors on a small piece of a silicon wafer. The MOS transistors are connected in a way that achieves the same functionality of a larger setup. And these MOS transistors are used to implement only a specific kind of function. These are not made programmable, just do an operation if connected in the circuit. Yet, by using a single IC more than one function can be implemented by changing the external circuit.
On the other hand a microprocessor is a full system containing a CPU and several daughter ICs. It can be programmed as per the instructions, In the following section we will discuss more about it. You can trace back the origin of the integrated circuit to the 1960s. The idea of shrinking circuits to thumb-size was a popular one. This is because it saves cost, space, and changes how electronics are designed over the years. In this blog we will:
Learn what an integrated circuit is.
Learn what a microprocessor is.
Explore challenges in designing with both microprocessors and integrated circuits.
1. What is an Integrated Circuit?
The integrated circuit, sometimes called a chip or microchip, is a semiconductor wafer, often made of silicon, that integrates a collection of electronic circuits, including resistors, transistors, capacitors, and diodes, that are connected together to perform a specific function. Before the use of ICs, components such as transistors and resistors were wired together on a circuit board. But with the introduction of the IC, these components are now formed on a smaller, single chip.
In the early days, computers were made with vacuum tubes that formed the logic circuits. Because of its large size and expensive construction, the first computer was not ideal for mainstream use. The invention of the transistor, which regulates the flow of current or voltage and acts as a switch for electronic signals. The invention of the integrated circuit (IC) helped revolutionize the use of electronic signals such as transistors in a much smaller and more lucrative design. A single integrated circuit can contain thousands to millions of such electronic circuits, depending on the computing power.While integrated circuits (ICs) are designed and fabricated directly on silicon wafers, printed circuit boards (PCBs) serve as the platform where these ICs are mounted and interconnected with other components. Companies like JLCPCB specialize in producing high-quality PCBs that enable engineers to assemble and test their circuit designs efficiently.
2. What is a Microprocessor?
So is a microprocessor an integrated circuit? The answer is yes, and it is considered one of the most complex of its kind. Does it contain the same MOS transistors inside it? The answer is yes. Then what is the difference between the two: ICs contain a certain set of transistor (fixed) connections. But in microprocessors we can program each set of transistors according to our application. After a perfect programming a microprocessor action is converted into IC and made fixed to cut down the cost.
A microprocessor is a computer processor that combines the functions of a central processing unit (CPU) on a single integrated circuit or chip. It is used in a computer system to perform logical and computational tasks so that other external circuitry, including memory or peripheral ICs, can perform their intended functions.
In general, microprocessors are used in applications where the task is not predefined, such as computers or video games, where the task is dependent on the user. In these cases, microprocessors are suitable because they support a wide range of computing applications.
3. Different Types of Integrated Circuits:
Integrated Circuits (ICs for short) can be divided into three major categories according to their functions. Because in electronics either there is switching or amplification: Analog integrated circuits, digital integrated circuits and hybrid integrated circuits.
Analog Integrated Circuits:
Analog integrated circuits, also known as linear circuits, focus on generating, amplifying, and processing various analog signals. These signals are continuous and their amplitude changes over time. Typical analog signals include audio signals, video signals, temperature sensor outputs, etc. The main characteristic of analog integrated circuits is the proportional relationship between input and output signals, so they are widely used in signal processing, filtering, amplification, modulation and demodulation.
Digital Integrated Circuits:
Digital integrated circuits are used to generate, amplify and process various digital signals. A digital signal is a signal with discrete values in time and amplitude, usually represented by a binary system. These circuits perform logical and arithmetic operations and are commonly found in computers, communications equipment, digital entertainment equipment, and more.
The main characteristic of digital integrated circuits is that they perform discrete operations, allowing the storage, processing and transmission of digital data.
Mixed-Signal Integrated Circuits:
Digital/analog hybrid integrated circuits combine elements of analog and digital circuits and are used to process analog and digital signals simultaneously. Such circuits are important in many applications, especially in communications, embedded systems, and sensors. Hybrid digital/analog integrated circuits allow digital systems to interact with the analog environment, such as converting analog sensor data to digital signals, digitally controlling the operation of analog circuits, or transmitting digital data to analog outputs.
4. Types of Microprocessors:
Microprocessors can be broadly divided into three main categories: general-purpose high-performance microprocessors, embedded microprocessors and digital signal processors, and microcontrollers.
General-Purpose High-Performance Microprocessor:
First of all, general-purpose high-performance microprocessors are designed to pursue excellent computing performance and are usually used to run general-purpose software. Such processors are usually equipped with complex and powerful operating systems. These processors are at the heart of modern computers and are used to perform a variety of tasks, from mathematical calculations to graphics processing, and from multimedia applications to complex data analysis. Representatives of general-purpose processors include the central processing units (CPUs) of desktop computers and notebook computers.
Embedded Microprocessors and Digital Signal Processors:
Secondly, embedded microprocessors and digital processors focus on providing high performance to solve application problems in specific fields. This type of processor plays a key role in consumer electronics such as cellular phones, CD players, and more. Some famous high-performance embedded processors include ARM, Am386EM, Power PC, MIPS, X86, i960, SH RISC, etc. DSP is a separate field of electronics that play a very wide role.
Microcontroller:
Finally, microcontrollers are usually cheaper and have the greatest market demand. They are mainly used in automatic control equipment, such as automobiles, air conditioners, automatic machinery and other fields. The representative of microcontrollers is a single chip microcomputer. Its main feature is high integration, which makes the device small in size, low in power consumption and high in reliability. Compared with embedded microprocessors, microcontrollers pay more attention to the needs of self-control equipment, so they are widely used in the field of automation. Typical microcontrollers include 8051, PIC32, MCS-96/196/296, MCS-251, C166/167, P51XA, 68K series, C540, MCU 8XC930/931, C541, ARM7/9/10, STM32, AVR32, etc.
Conclusion:
Finally, the relationship between microprocessors and integrated circuits is akin to the intricate interplay of specificity and generality. Both integrated circuits and microprocessors are an essential part of understanding and creating embedded systems. Integrated circuits have allowed us to scale how we utilize and incorporate transistors and other electronic circuits into electronic designs. And without integrated circuits, we wouldn’t have microprocessors. Microprocessors allow us to place CPU functionality into devices, which has made our everyday devices capable of performing advanced computations and tasks.
Popular Articles
• SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
• How to Solder SMD Components Like a Pro [2026 Updated]
• SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
• SMD Capacitor Codes: Identification, Markings, and Polarity
• SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and Assembly
Keep Learning
Ceramic Capacitor Code Guide: Values, Tolerance, and Voltage
Key Takeaways Three-Digit Rule: The first two digits represent the significant figures, while the third indicates the power-of-ten multiplier. The resulting capacitance is expressed in picofarads (pF). Common Values: Code 104 represents 100,000 pF (100 nF or 0.1 µF), while 103 represents 10,000 pF (10 nF or 0.01 µF). Tolerance Letters: Letters indicate capacitance tolerance. Common examples include J (±5%), K (±10%), and M (±20%). For small capacitance values, B, C, and D specify tolerances in pF. Vol......
What is a HDMI RF Modulator? A Complete Guide
What is an HDMI RF Modulator? An HDMI RF modulator is a device that converts high-definition multimedia interface (HDMI) signals into Radio frequency (RF) signals. This allows HDMI-compatible devices, such as Blu-ray players, gaming consoles, and streaming devices, to transmit audio and video content over coaxial cables, making them compatible with older television sets or distribution systems that use RF signals. These modulators are particularly useful in settings where legacy TV systems are still i......
SMD Inductor Code: How to Read Inductor Markings and Values
Key Takeaways Three digits are read in µH: 100 is 10 µH and 101 is 100 µH. The third digit is the number of zeros, not part of the value. R and N are decimal points: R in microhenries (4R7 = 4.7 µH), N in nanohenries (2N2 = 2.2 nH). A trailing letter is a tolerance: K is ±10% and M is ±20%. On RF inductors below about 10 nH, C and D mean ±0.2 nH and ±0.5 nH. Most small chip inductors are unmarked: identify them from the BOM or reel label first, then with an LCR meter at the right test frequency. The m......
A Complete Guide to Surface Mount Device (SMD)
Imagine holding a smartphone in your hand. Inside that sleek device lies a complex network of thousands of miniature components — resistors smaller than a grain of rice, capacitors thinner than a fingernail, and integrated circuits containing millions of transistors. Without Surface Mount Technology (SMT) and its compact Surface Mount Devices (SMDs), none of this would exist. Just a few decades ago, electronics were bulky. Radios filled desks, computers filled rooms, and assembling a circuit meant dri......
TSSOP Package Guide: Dimensions, Pitch, Footprint & SMT Soldering
Key Takeaways Lead span, not body width: Build the footprint from the lead span (6.4 mm or 8.1 mm tip to tip), not the 4.4 mm or 6.1 mm body width. MSOP vs TSSOP: Check the width in the drawing before reusing a footprint: MSOP-8 and TSSOP-8 share pitch and body length, and some vendors label a 3.0 mm-wide package TSSOP8. Mask dams: A standard TSSOP footprint leaves a 0.20 mm pad gap: enough for solder mask dams on 1 oz copper, no margin on 2 oz, and no dams on JLCPCB flex boards. Thermal pad: On HTSSO......
Understanding the Role of PCB Controllers in Electronic Design
A PCB Controller is an important part of designing and building electrical systems. It controls the functions of different mechanical parts on a printed circuit board (PCB) and makes sure they can talk to each other easily. People use PCB controllers in a lot of different situations, from home technology to factory automation. The purpose of this article is to discuss the importance of PCB controllers, including the different kinds, their uses, and the best ways to choose and use them. 1. What is a PC......