How to Prevent Solder Balls in PCB Assembly: A Complete Guide
9 min
- What Are Solder Balls in PCB Assembly?
- Causes of Solder Ball Formation
- How SMT Stencil Design Directly Influences Solder Balling?
- Professional Strategies to Eliminate Solder Balls During Assembly
- Why JLCPCB Stencils Are the Standard for Reliable PCB Assembly?
- Final Thoughts:
- Q: What is the difference between a solder ball and a solder bead?
- Q: How many solder balls are allowed per IPC-A-610?
- Q: Can I reuse solder paste left on the stencil?
- Q: Does nitrogen (N₂) reflow reduce solder balling?
- Q: What do tombstoning and solder balls both appearing indicate?

Take one of the boards off the line, and put it under the microscope, and there they are, little metallic balls here and there on the solder mask. This is one of the reasons why solder balls are dangerous, because they do not lead to immediate failure.
A ball sitting clear of any conductor looks harmless until the product vibrates, thermally cycles, and the ball migrates into a gap between two traces. Six months later: an intermittent fault with no obvious cause. They're also a process signal where consistent balling means something has drifted.
This guide covers what IPC-A-610 defines, what physically causes them, how stencil design drives or prevents them, and the practical steps to keep them off boards.
What Are Solder Balls in PCB Assembly?

IPC-A-610 defines solder balls as small spheres of solder separated from the main pool during reflow, ejected or stranded particles that ended up somewhere unintended.
Usually, the non-conformance begins at diameters over 0.13 mm, or more than five per 600 mm². Even in-spec balls are a latent short circuit on high-density boards. It's when mechanical stress moves them.
The typical location of these defects is variable. Sometimes there are balls under chip components, indicating paste slump. Or sometimes there are balls near via barrels that indicate outgassing. And fine balls scattered broadly suggest moisture.
Causes of Solder Ball Formation

Five root causes cover most solder ball defects, and on real lines, they stack. Slightly oxidised paste combined with an aggressive ramp rate produces far more balling than either problem alone.
Solder Paste Slump:
Paste is thixotropic, that is, it flows under squeegee pressure and hardens when at rest. Cold slump happens at room temperature due to low viscosity or humidity uptake.
Hot slump is worse in the pre-heat zone, the paste softens before flux activates, and spreads onto the solder mask. And when wetting, it pulls the main mass back onto the pad. Stranded particles on the mask have nowhere to bond and solidify as solder balls.
Oxidation:
Flux must reduce metal oxides on solder powder and PCB pads before reaching the liquidus, which is approximately 217°C for SAC305.
When the oxide burden is too high, aged paste, degraded OSP, boards stored past shelf life, flux exhausts itself before coalescence completes, leaving unfused particles as independent balls. ENIG handles this far better than OSP, as the table below shows:
PCB Pad Finish: Oxidation and Solder Ball Risk Comparison
| Finish | Solderability | Oxidation Risk | Solder Ball Risk |
| HASL (Sn/Pb) | Excellent | Low | Low |
| Lead-Free HASL | Good | Low–Medium | Low–Medium |
| ENIG | Excellent | Very Low | Very Low |
| OSP | Good (short shelf) | Medium–High | Medium–High |
| Immersion Ag | Very Good | Low (tarnish risk) | Low |
| Immersion Sn | Good | Medium | Medium |
Moisture:
Moisture that is present is suddenly vaporised in the oven, and the solder particles are ejected, thus physically, before they are attached to the joint using flux. The pattern is distinctive: fine balls scattered broadly across the board rather than clustered near specific pads.
Reflow Profile Errors:
Ramp rates above 2°C/s through pre-heat cause solvent evaporation violent enough to carry solder particles with it. An insufficient soak phase at 150–200°C, where the flux removes oxides, means the solder reaches the liquidus before coalescence conditions are met.
Both problems are confirmed only with a thermal profiler on the actual board, not the oven controller.
Poor Paste Printing:
Excessive squeegee pressure smears paste across the solder mask between pads, isolated deposits with no metallic surface to wet. They ball up in the oven right where they sit. A worn stencil compounds it: ragged aperture walls create torn deposits that transfer smears to subsequent boards.
How SMT Stencil Design Directly Influences Solder Balling?
The stencil defines every paste deposit on the board. Get the aperture geometry wrong, and downstream fixes become compensations rather than solutions.
Area Ratio:
Area Ratio = aperture opening area ÷ aperture wall area, and it must exceed 0.66 for reliable paste release. Below that threshold, adhesion to the walls wins the deposit tears on stencil separation, leaving fragments that become solder balls.
Mixed-technology boards often need step stencils precisely because no single foil thickness satisfies the area ratio for every pad simultaneously.
Aperture Reduction and Shape:
Sizing apertures 10–20% smaller than the pad buffers against placement-induced paste displacement. For passives, shape matters: home-plate apertures taper toward the component body, concentrating paste at pad extremities and away from the centre where squeeze-out occurs.
Bow-tie and U-shapes serve the same purpose on progressively smaller components.
Wall Smoothness:
Rough walls cause dog-earing deposit corners tear on stencil lift, stick to the underside, and transfer back to boards as isolated solder mask smears.
Electropolished stencils remove microscopic wall irregularities; nano-coated stencils add a hydrophobic layer that actively repels paste. Both reduce deposit variation and underside cleaning frequency.
Precision stencil services make sure they are using the right aperture design. Because that's where it all starts.
Professional Strategies to Eliminate Solder Balls During Assembly

Prevention is cheaper than rework. Most solder ball problems are fixed before the board enters the oven. Here are the golden rules to eliminate solder balls.
● Store paste at 3–10°C. Warm sealed cartridges to room temperature for 4 hours before opening. Opening cold causes condensation directly on the paste surface.
● Hold SMT room humidity at 40–60% RH. Above 60%, printed boards absorb moisture within hours.
● Wipe the stencil underside every 3–5 prints with IPA solvent. Fine-pitch work warrants every print.
● Reflow within 1 hour of printing. Beyond 2 hours, clean and reprint.
● Profile the board with a thermal probe, not the oven controller. Confirm ramp rate stays under 2°C/s and soak duration matches the board's thermal mass.
● Audit pick-and-place nozzle force on small passives. Bottoming into the paste deposit squeezes material outward on every cycle.
Why JLCPCB Stencils Are the Standard for Reliable PCB Assembly?
Stencil quality determines paste deposit quality. There's no downstream compensation for dimensional variability introduced at the print stage. And that's where JLCPCB comes in with their top-tier stencil production.
High-precision technology
For starters, they ensure exceptional accuracy of up to ±0.003 mm using 30 high-precision LPKF laser cutting machines. It guarantees compliance with area ratios even on 0.4 mm pitch pads.
Premium Materials and Durability
Almost every stencil from JLCPCB comes with a durable 304 HTA stainless steel build. With this material, you can easily expect impeccable hardness and thermal stability. No worries of facing deformities even after multiple printing cycles.
Advanced Finishing Options
JLCPCB offers advanced post-processing options like -
● Electropolishing: This finishing process ensures smoother aperture walls. It also removes any kind of micro burrs of slag left from laser cutting.
● Nano-Coating: A Nano-coating finish makes the stencil ideal for PCBs that have BGA, QFN, or different fine-pitch components. It’s great for higher SMT first pass yield.
Versatile Customization
JLCPCB supports a wide range of custom requirements. You can choose between framed stencils for automated machines or frameless versions for manual assembly.
● Step Stencils: These involve localized "step-up" or "step-down" thickness on one sheet. This guarantees fine-pitch and large-scale components of the correct volume of paste needed to have high-quality joints on mixed-technology boards.
● Fiducials: JLCPCB offers three different fiducial options. For a perfect alignment, you can define etched through or half-etched fiducials.
Other than these, you get plenty of customization options.
Fast Turnaround and Affordability
Reliability is not at a high cost. Tailor-made stencils begin at $3. The automated production line has a build time of up to 12 hours. The majority of the orders are shipped within 24 hours, that keep your project on schedule. Stop solder balling with high-precision SMT stencils from JLCPCB. Claim your $11 coupon now and upgrade your assembly quality today!
Final Thoughts:
Solder balls are preventable. The physics of each failure mode is well understood, and every root cause responds to process discipline, paste storage, room environment, stencil condition, and profile verification.
None of it requires capital investment. When balls do appear, their location on the board is diagnostic information: use it before reaching for the rework iron.
Ensuring a clean assembly starts with high-fidelity tooling. In case you are scaling production, you can learn more about our JLCPCB stencils that can work as a solution to counter these frequent reflow defects.
Frequently Asked Questions:
Q: What is the difference between a solder ball and a solder bead?
A solder ball is a free-standing sphere ejected away from the joint with no metallic bond to anything. A solder bead is larger and elongated, physically attached to a chip component termination caused by paste squeezed out during placement and reflowed against the end-cap. Both fail IPC-A-610 when they are in violation of electrical clearance; however, the corrective actions are different, addressing stencil and profile issues, beading points, placement force, and aperture shape.
Q: How many solder balls are allowed per IPC-A-610?
To a maximum of five per 600 mm 2, with a diameter of 0.13 mm or less, so long as they are encapsulated or free of the smallest electrical clearance. Exceed any one condition, and it's a non-conformance. Most mature lines treat two or three per 600 mm² as a process flag rather than waiting for the IPC limit.
Q: Can I reuse solder paste left on the stencil?
Within limits. Most manufacturers specify 4–8 hours maximum on-stencil life. Paste recovered within that window, tested for viscosity, and refrigerated, sealed can be reused. Paste left overnight, visibly dried at the edges, or exposed to humidity above 60% RH should be discarded.
Q: Does nitrogen (N₂) reflow reduce solder balling?
Yes. Nitrogen holds oven oxygen below 100 ppm, so solder powder isn't re-oxidising during ramp and soak while the flux is trying to clean it. Flux completes oxide reduction with capacity to spare, coalescence is more complete, and fewer satellite particles remain. The most pronounced benefit is with SAC305 and other lead-free alloys. The trade-off is the nitrogen operating cost.
Q: What do tombstoning and solder balls both appearing indicate?
Tombstoning needs unequal wetting forces, usually unequal paste volumes on the two pads. When solder balls also appear, those deposits are poorly contained, spreading onto the solder mask. Together, they point strongly at a stencil problem or excessive squeegee pressure rather than a profile issue. Check print quality with a 3D SPI system before touching the oven.
Keep Learning
How to Master PCB Reflow Soldering at Home Using a Hot Plate and Stencil
Soldering small SMD components like 0402s, QFNs, or BGAs with a standard iron produces inconsistent joints and defects. Reflow soldering at home using a hot plate offers a controlled, repeatable method for melting solder paste across multiple pads simultaneously. Engineers and hobbyists achieve uniform joints and reduced bridging with proper temperature control. High-precision PCB stencils guide solder paste placement, ensuring each pad receives the exact volume for fine-pitch and high-density layouts......
DC Jack Soldering: How to Solder a DC Barrel Jack / Power Connector
Key Takeaways Confirm polarity before the iron touches the board: Check the adapter label, device marking, and jack pinout for center-positive versus center-negative wiring, because reversed polarity can destroy a regulator or microcontroller instantly. Deliver enough heat for the big joints: DC jack terminals are high-mass, so use a larger chisel or bevel tip, more heat or dwell, and flux until solder fills the plated hole and leaves a shiny fillet instead of a dull, grainy surface. Build in mechanic......
How to Solder a JST Connector: Through-Hole, SMT, and Board-to-Board Guide
Key Takeaways Soldering a connector is electrical and mechanical at once: Seat the header flush and square, tack one corner pin, verify alignment, then solder the remaining pins and every mechanical anchor tab, because plugging and cable forces travel through the housing and hold-downs rather than the signal pins. Match the method to the mount type: Through-hole headers need full barrel fill with a larger tip and flux for heat-sinking power pins, SMT headers need tack-and-align with hold-down tabs ful......
How to Tin a Soldering Iron: First Use & Re-Tinning
Key Takeaways Tin from the first heat-up: Bring the iron to roughly 315–370 °C (600–700 °F), wipe the tip on brass wool, and melt fresh flux-cored solder onto every working face until a thin mirror-bright film covers it, then wipe away the excess and lay down one more light coat. Re-tin by condition, not the clock: Keep a film of solder on the tip at all times, re-tin the moment wetting turns patchy, and lay down a generous coat before shutdown so oxidation cannot start while the iron sits idle. Never......
How to Solder an Audio Jack to a PCB
Key Takeaways Confirm the exact pinout first: TS, TRS, and TRRS jacks differ in conductor count and PCB terminal numbering, and TRRS wiring follows CTIA or OMTP standards, so always map every pin from the manufacturer datasheet and PCB footprint before soldering. Control heat and solder: Use a fine-tip iron, flux, and a minimal amount of solder, tack one pin to keep the jack flush and square, then solder each contact pin by pin to prevent bridges between closely spaced terminals. Finish and verify: So......
How to Solder SMD LEDs: A Step-by-Step Guide for Iron, Hot Air, and Reflow
Key Takeaways Confirm polarity and orientation first: Identify the anode and cathode before applying any heat, because a reversed SMD LED will not light and correcting it costs another thermal cycle. Match the method to the job: A fine-tip iron suits one or a few LEDs, hot air is best for rework and single-part replacement, and solder paste with reflow is fastest for complete boards. Keep solder and heat minimal: A small, fully wetted fillet and short dwell times protect the LED die, phosphor, and enc......