How JLCPCB’s Flex PCB Enable Smarter GPS Tracking Devices
3 min
- Product introduction
- How JLCPCB Supported the Project
- Conclusion
Smart tracking technologies require reliable, high-performance hardware to function effectively. QIYUE TECH, an IoT company, uses JLCPCB’s Flex PCBs to improve the performance and compact design of its smart tracking devices, such as the TR-DOG® series and anti-tamper GPS smartwatches. These flexible PCBs provide the durability and adaptability needed for consistent performance in dynamic real-world environments.
Product introduction
Meet the TR‑DOG Series
The TR‑DOG® system combines a handheld display, smart collar, and mobile app to provide a comprehensive dog tracking solution.
● It can track up to 20 dogs simultaneously.
● It uses dual-mode communication (RF and 4G) for a tracking range of up to 15 kilometers and unlimited reach with 4G.
● It provides precise real-time positioning with fast updates every 2.5s.
● Features: collar sharing, anti-loss alerts, and training stimuli like vibration and mild electrical pulses
● Designed for outdoor reliability: IPX7 waterproofing makes it suitable for harsh environments such as outdoor training and wilderness search and rescue.
TR‑DOG ® Series
Two Flex PCBs manufactured by JLCPCB are used in the internal construction.
Discover the Anti-Tamper Positioning Smartwatch
This GPS smartwatch is a rugged, all-day wearable that offers secure tracking, health monitoring, and instant alerts.
● It uses multi-system positioning with GPS, BDS (BeiDou Navigation Satellite System), WIFI, and LBS for accurate real-time location.
● It has IPX8 waterproof certification, making it suitable for continuous 24/7 wear.
● Real-time health monitoring: heart rate, blood pressure, oxygen levels, and temperature
● Intelligent safety features: disassembly alerts, offline alarms, and companion separation warnings, and tamper protection
The Anti-Tamper Positioning Smartwatch
Six Flex PCBs manufactured by JLCPCB are used in the internal construction.
How JLCPCB Supported the Project
Both the TR-DOG trackers and anti-tamper smartwatches require internal designs that are compact, rugged, and highly adaptable, which flexible PCBs perfectly meet. Flex PCBs enable compact and robust circuit designs, making them indispensable to wearables and smart devices. In these projects, JLCPCB’s Flex PCB solutions were critical in bringing high-performance and space-saving designs to reality.
1. High-Precision Flexible Design & Compactness: TR-DOG series products use JLCPCB’s ultra-thin, lightweight, and bend-resistant Flex PCBs. It allows for a compact internal layout, saving space for batteries, sensors, and other essential components.
2. Extreme-Condition Reliability: JLCPCB’s Flex PCBs are built to handle fast movement, vibrations, and harsh conditions, which is ideal for high-speed hound tracking and forest terrain. Their excellent bend and vibration resistance ensures stable device performance during fast tracking and rough terrain traversal under rain, dust, or sudden hits. These flexible PCBs also work reliably in a wide temperatures range, from -40°C up to 150°C.
3. Guaranteed Dynamic Flex Life: JLCPCB’s Flex PCBs can bend more than 100,000 times, ensuring long-term reliability under constant mechanical stress.
Conclusion
The TR‑DOG collaboration and Anti-Tamper Positioning Smartwatch showcase the versatility of JLCPCB’s Flex PCB in wearable tech and IoT devices, proving that rugged, intelligent, and high-performance wearable electronics are within easy reach. We welcome more new partnerships to further unlock the potential of flexible PCBs in future-ready smart devices.
Popular Articles
• ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
• From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
• Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
• PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
• Premium Portable Speaker Built with 8-Layer PCBs, DSP & Smart Amps
Keep Learning
From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
Note Motivation: Replaced a dust-prone membrane keyboard with a durable, custom DIY alternative. Specs: 87-key TKL layout powered by Raspberry Pi Pico (RP2040), featuring hot-swap support, QMK, OLED, and an encoder. Design: A unique 3-layer PCB stack featuring symmetrical routing, an exposed controller, and visible "diode art". Support: Designed using EasyEDA and fabricated by JLCPcB, the project was submitted to the EasyEDA Spark program successfully securing parts and materials sponsorship for its d......
Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
In the world of FPGA development, having a reliable, low-cost JTAG programmer used to mean either buying expensive vendor cables or adding high-cost FTDI chips to every board. Maker Khaled Magdy changed that by turning a $4 Raspberry Pi Pico into a fully functional JTAG adapter using DirtyJTAG firmware and OpenFPGALoader — then had his custom FPGA boards professionally assembled by JLCPCB. The entire solution is 100% open-source. You can download the firmware, follow the Windows installation steps, an......
ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
Key Takeaways Accessible Design: ANGELO is an open-source €10 listening aid created to assist everyday voice amplification. Analog Audio Architecture: Uses a TL072 op-amp to boost speech frequencies (1–4 kHz) with low latency and low power. EasyEDA & JLCPCB Workflow: Designed in EasyEDA and produced via JLCPCB SMT assembly for fast, reliable hardware execution. The ANGELO Project Overview ANGELO is an open-source audio hardware project designed to amplify voices and improve everyday communication expe......
Athena: Building a High-Performance 6-Layer PCB for Rocket Avionics
Key Takeaways Athena is an open-source flight computer with a triple-MCU architecture, redundant sensors, and multiple communication interfaces on a compact 6-layer PCB. The 80 × 140 mm board integrates three STM32 MCUs, three IMUs, barometers, GNSS, LoRa, Bluetooth, CAN, USB, flash storage, SD card, and power management. The 6-layer PCB provides routing capacity, organized power distribution, signal organization, and compact functional integration for this complex design. The project demonstrates how......
PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
Key Takeaways The piBrick Pocket-CM5 is a fully functional, smartphone-sized Raspberry Pi CM5 handheld PC with a physical QWERTY keyboard, AMOLED display, and M.2 NVMe SSD The project utilizes JLCPCB's 4-layer PCB fabrication with controlled impedance (90-ohm for USB, 100-ohm for PCIe/MIPI DSI) to maintain signal integrity Designed using EasyEDA and fabricated by JLCPCB, the project was submitted to the EasyEDA Spark program, successfully securing parts and materials sponsorship for its development. J......
Designing a Precision 72-LED Wearable Watch: Building a 40mm Round PCB with JLCPCB SMT Assembly
Key Takeaways This case study explores the design and fabrication of a 72-LED wearable watch built on a precision 40mm round PCB. Learn how JLCPCB SMT assembly eliminated hand-soldering 70+ 0603 LEDs, how ENIG surface finish ensures reliability in wearable applications, and how a clever panelization strategy with mouse-bite breakaway tabs enabled automated assembly of a circular board. The project demonstrates a complete workflow from EasyEDA schematic capture to firmware optimization and commercial-g......