Building a Custom Laptop with JLCPCB's Full Services
2 min
- How JLCPCB Enabled This Custom Laptop Project
- Conclusion
Imagine designing a laptop from the ground up—not just assembling parts, but crafting its circuits, chassis, and cooling systems by hand.
"This is a fully custom-built laptop project where I designed and manufactured many of the key components, with the help of JLCPCB's outstanding services. While I didn't design the main motherboard itself, I developed and integrated many of the surrounding subsystems and mechanical elements myself."
This project shows how a maker leveraged JLCPCB's full-service manufacturing, including PCB, FPC, CNC, and 3D printing, to bring a highly integrated custom laptop to life. While the motherboard was sourced, every other subsystem and mechanical component was built from scratch. Curious how it all came together? Let's explore the details of this impressive build, and how JLCPCB helped make it possible.
How JLCPCB Enabled This Custom Laptop Project
JLCPCB played a central role in this ambitious DIY laptop by providing multiple manufacturing services under one roof:
- High-quality 6-layer PCB production ensured reliability for power delivery, USB4, audio, and battery management.
- Custom FPCs (flexible printed circuits) enabled high-speed USB4 transmission in a compact form factor.
- CNC machining of the chassis, the laptop’s main body, ensured tight tolerances and a professional internal fit.
- 3D printing services brought precision speaker enclosures for an original multi-driver audio system.
- A custom CPU cooler heat spreader for optimal thermal performance.
- Affordable pricing and fast turnaround made rapid prototyping and iteration possible.
Conclusion
"This project highlights how JLCPCB's PCB, FPC, CNC, and 3D printing capabilities can come together to support the development of complex, highly integrated hardware — even a custom laptop!"
According to the creator, achieving this level of precision and integration would have been nearly impossible without JLCPCB's reliability and range of services. It's a powerful example of how even individual makers can deliver professional-grade results with the right partner.
From signal integrity to thermal performance, this build proves what's possible when creativity meets capability. JLCPCB didn't just supply parts—we helped bring a complete product vision to life.
Popular Articles
• ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
• From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
• Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
• PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
• Premium Portable Speaker Built with 8-Layer PCBs, DSP & Smart Amps
Keep Learning
From Membrane Frustration to Custom Mechanical Mastery: Taifur's V3 Full Keyboard Project
Note Motivation: Replaced a dust-prone membrane keyboard with a durable, custom DIY alternative. Specs: 87-key TKL layout powered by Raspberry Pi Pico (RP2040), featuring hot-swap support, QMK, OLED, and an encoder. Design: A unique 3-layer PCB stack featuring symmetrical routing, an exposed controller, and visible "diode art". Support: Designed using EasyEDA and fabricated by JLCPcB, the project was submitted to the EasyEDA Spark program successfully securing parts and materials sponsorship for its d......
Turn Your Raspberry Pi Pico into a Professional JTAG Programmer with DirtyJTAG & OpenFPGALoader
In the world of FPGA development, having a reliable, low-cost JTAG programmer used to mean either buying expensive vendor cables or adding high-cost FTDI chips to every board. Maker Khaled Magdy changed that by turning a $4 Raspberry Pi Pico into a fully functional JTAG adapter using DirtyJTAG firmware and OpenFPGALoader — then had his custom FPGA boards professionally assembled by JLCPCB. The entire solution is 100% open-source. You can download the firmware, follow the Windows installation steps, an......
ANGELO Project with JLCPCB: Building an Open-Source Audio PCB for a Listening Aid
Key Takeaways Accessible Design: ANGELO is an open-source €10 listening aid created to assist everyday voice amplification. Analog Audio Architecture: Uses a TL072 op-amp to boost speech frequencies (1–4 kHz) with low latency and low power. EasyEDA & JLCPCB Workflow: Designed in EasyEDA and produced via JLCPCB SMT assembly for fast, reliable hardware execution. The ANGELO Project Overview ANGELO is an open-source audio hardware project designed to amplify voices and improve everyday communication expe......
Athena: Building a High-Performance 6-Layer PCB for Rocket Avionics
Key Takeaways Athena is an open-source flight computer with a triple-MCU architecture, redundant sensors, and multiple communication interfaces on a compact 6-layer PCB. The 80 × 140 mm board integrates three STM32 MCUs, three IMUs, barometers, GNSS, LoRa, Bluetooth, CAN, USB, flash storage, SD card, and power management. The 6-layer PCB provides routing capacity, organized power distribution, signal organization, and compact functional integration for this complex design. The project demonstrates how......
PiBrick Pocket-CM5: A Compact Raspberry Pi CM5 Handheld PC Built with JLCPCB
Key Takeaways The piBrick Pocket-CM5 is a fully functional, smartphone-sized Raspberry Pi CM5 handheld PC with a physical QWERTY keyboard, AMOLED display, and M.2 NVMe SSD The project utilizes JLCPCB's 4-layer PCB fabrication with controlled impedance (90-ohm for USB, 100-ohm for PCIe/MIPI DSI) to maintain signal integrity Designed using EasyEDA and fabricated by JLCPCB, the project was submitted to the EasyEDA Spark program, successfully securing parts and materials sponsorship for its development. J......
Designing a Precision 72-LED Wearable Watch: Building a 40mm Round PCB with JLCPCB SMT Assembly
Key Takeaways This case study explores the design and fabrication of a 72-LED wearable watch built on a precision 40mm round PCB. Learn how JLCPCB SMT assembly eliminated hand-soldering 70+ 0603 LEDs, how ENIG surface finish ensures reliability in wearable applications, and how a clever panelization strategy with mouse-bite breakaway tabs enabled automated assembly of a circular board. The project demonstrates a complete workflow from EasyEDA schematic capture to firmware optimization and commercial-g......