The Ultimate Guide to PCB Layout Design
11 min
- Introduction
- Steps Involved in PCB Layout Design
- Best Practices for PCB Layout Design
- Power, Ground and Signal Trace Considerations
- The Importance of Testing in PCB Design
- FAQs:PCB Layout Design
- Conclusion:PCB Layout Design
Key Takeaways
PCB Layout Fundamentals: Component placement and routing are essential to achieving optimal PCB performance, reliability, and manufacturability.
Follow a Structured Design Process: Start with schematic transfer and board dimension definition, followed by stackup planning, component placement, routing, and design file generation.
Optimize Placement and Signal Integrity: Proper component placement, signal integrity, and thermal management are key to creating a reliable PCB layout.
Consider DFM Requirements: Follow PCB design rules and manufacturer-specific DFM requirements to prevent potential manufacturing issues.
Perform Regular ERC and DRC Checks: Identify design problems early through electrical and design rule checks to ensure the PCB is ready for manufacturing.
Introduction
Printed Circuit Board (PCB) layout design is the foundation of any electronic device, from simple gadgets to highly complex systems. PCB layout design is the process of arranging electronic components and routing connections on a board to create a functional and efficient circuit. The goal is to achieve the smallest possible footprint while maintaining signal integrity and ensuring thermal and electrical performance.
There is a lot that goes into any engineered circuit board design, from a basic printed circuit to a complex non rigid PCB. Any new electronic device will start as a block diagram and/or a set of electronics schematics. Once you have your schematics finished and validated, you can follow the steps below to create modern PCB designs and layouts. A well-designed PCB ensures optimal performance, reliability, and manufacturability. In this guide, we’ll explore the key aspects of PCB layout design, including best practices, important considerations, and steps to create an efficient PCB layout.
Steps Involved in PCB Layout Design
Step 1: Schematic Design Entry
Step 2: Define PCB Dimensions
Step 3: Synchronize Schematics to Your PCB Board Design
Step 4: Designing Your PCB Stackup
Step 5: Defining PCB Board Design Rules and DFM Requirements
Step 6: Component Placement
Step 7: Routing
Step 8: Add Labels and Identifiers
Step 9: Generate Design Output Files
Step 1: Schematic Design Entry
The first step is creating a schematic, a blueprint that defines how components are interconnected. Each component symbol is placed, and connections are drawn between them. The schematic serves as a reference for component placement and routing in the layout phase.
Step 2: Define PCB Dimensions
Before placing components, determine the size and shape of the PCB based on the device's physical constraints. Consider mechanical requirements such as mounting holes and connectors.
Step 3: Synchronize Schematics to Your PCB Board Design
All the tools in a CAD software work in a united design environment, where the schematic, printed circuit board layout, and BOM are interlinked and can be accessed simultaneously. To transfer schematics document information to PCB, Click on Design » Convert schematics to PCB.
Step 4: Designing Your PCB Stack-up
Stack-up is important to consider early on in the PCB design stage due to impedance, which refers to how much and how quickly electricity can travel down a trace. The stackup plays a role in how the mechanical engineer can design and fit the PCB into the device. Prior to placing components you should define the PCB layout (i.e. shape, layer stackup) using the Layer Stackup Manager, shown below.If you’re new to the printed circuit design world, most modern PCB board design concepts will start with a 4-layer board on FR4. If you’re working on a high speed/high frequency circuit board design, you can use the JLCPCB online impedance calculator tool.
Step 5: Defining PCB Board Design Rules and DFM Requirements
The number of PCB board design rule categories is extensive and you may not need to use all of these available rules for every design. DRC contains the information of:
1. Clearances between objects in the PCB layout, such as between traces and pads.
2. Copper or solder mask feature size limits
3. Routing rules, including trace width and length limitations that can be enforced on certain nets.
This is just a sample of the rules that can govern any PCB layout, but these rules are designed to help ensure a board is manufacturable at the required scale with your fabricator's standard capabilities.
Step 6: Component Placement
Component placement is a critical step that influences the overall performance of the PCB. Follow these guidelines:
- Group related components: Place components that work together, such as resistors and capacitors, close to each other.
- Prioritize critical components: Position components like microcontrollers, power regulators, and signal processors first.
- Consider heat dissipation: Ensure that heat-generating components have adequate space and access to heat sinks or ventilation.
Step 7: Routing
Routing involves creating the actual paths (traces) that electrically connect the components. Some key factors to keep in mind are trace width, minimize trace length and signal integrity. Routing is done on the basis of type of PCB, RF PCB has different requirements than a Power PCB. Sometimes we require impedance matching, no reflections and sometimes maximum current flow on the basis of which different routing schemes can be utilized.
Step 8: Add Labels and Identifiers
With the circuit board layout verified you are ready to add labels, identifiers, markings, logos, or any other imagery to your board. It is a good idea to include reference designators for components as this will assist in PCB board assembly. You can also add a company logo and part numbers using the image tools and text tools in the PCB Editor. These elements need to be placed in the Top Overlay or Bottom Overlay layers in the PCB layout.
Step 9: Generate Design Output Files
Before you create your manufacturer deliverables, it’s always a good idea to verify your circuit board layout by running a design rule check (DRC). If your board checks out, then you’re ready to release your manufacturer deliverables.
Once your board has passed the final DRC, you need to generate the design files for your manufacturer. The design files should include all the information and data necessary to build your board. For most manufacturers, you will be able to use a set of Gerber files as shown below; however, some manufacturers prefer other manufacturing file formats (IPC-2581 or ODB++). To know more details about these other PCB file formats visit this article.
Best Practices for PCB Layout Design
1. Optimize Component Placement:
Proper component placement can reduce routing complexity and improve signal performance. Position critical components like microcontrollers and power supplies first, followed by passive components such as resistors and capacitors.
2. Minimize Crosstalk and EMI:
High-speed signals are prone to crosstalk and EMI. To mitigate this Use ground planes to shield signals, Maintain distance between high-speed and low-speed signals. Avoid sharp angles and long parallel traces.
3. Keep Thermal Management in Mind:
Power-intensive components generate heat, which can affect performance and lifespan. To address this Position heat-generating components near heat sinks or allow airflow around them. Use thermal vias to distribute heat across multiple layers.
4. Verify Design Rules:
Each PCB manufacturer has specific design rules regarding trace width, spacing, and layer count. Ensure your layout complies with these rules to avoid manufacturing issues.
Power, Ground and Signal Trace Considerations
The above tips focused on best PCB practices that can be implemented in a design. You also need to route the power, ground and signal traces as per the design specification. Completing this step efficiently will help ensure your signals have a reliable path to travel to keep your board functioning properly. Here are three main factors to keep in mind:
1. Power and Ground Planes
One fundamental PCB layout design rule is to keep your power and ground planes internally within your board. Dedicated power and ground planes improve signal integrity and reduce noise. These layers distribute power evenly across the board and provide a return path for signals, minimizing ground loops and voltage drops. You should also keep your digital and analog grounds separate in a similar fashion. Try only to have analog lines cross your analog ground to reduce capacitive coupling.
2. Track Design
This step also involves connecting signal traces according to your schematic. You always want your traces to be as short and direct as possible. If you have horizontal trace routing on one side of the PCB, place vertical traces on the other side. Keep the impedance matching and reflection rules in mind while routing high speed lines.
For power design your board may require multiple nets with different currents, which will determine the net width you need. Using a trace width calculator can help with this step. Tracks that are around 10 mils thick can only take a current of around one Ampere, while a track that is 250 mils thick can carry as much 15 Amps with a 30 degree Celsius temperature rise.
3. Pad and Hole Dimension
You'll also need to determine pad and hole dimensions early in the PCB design process. As the size of the pads and holes decreases, getting the right pad-to-hole size ratio becomes more crucial. It’s especially critical when working with via holes. Shape of the PCB pads is also a crucial parameter. PCB footprints can vary according to the manufacturing process.
The Importance of Testing in PCB Design
Throughout the PCB design process, as well as the rest of the PCB manufacturing process, you should continuously check your work. Catching problems early on will help minimize their impact and reduce the costs of fixing them. Two common tests electrical rules check and the design rules check can be performed at early stages. These tests will help you solve many of the more significant problems you may encounter. Once you can pass your ERC and DRC tests without any problems, you should check the routing of every signal and compare your board to your schematic in detail.
FAQs:PCB Layout Design
1. What is the difference between PCB design and PCB layout?
PCB design is the whole process — system architecture, schematic capture, component selection and ERC — and defines how the circuit works. PCB layout is the physical stage that follows: stackup, component placement, routing and DRC, defining how the board is built. Design produces the schematic, netlist and BOM; layout produces Gerber, drill and assembly files. One cannot fix the other.
2. What software is used for PCB layout?
EasyEDA is the most accessible choice, and the tool JLCPCB's layout team primarily uses. It is free, runs in the browser or as a desktop client, and covers schematics up to 500 sheets / 100,000 pins and designs of 30,000 devices or 100,000 pads in the Pro edition. Its LCSC-linked library, 3D preview, Gerber viewer and one-click JLCPCB ordering keep design and production in one place.
Other tools: Altium Designer for complex commercial boards, KiCad as open-source, Eagle for subscription-based hobby work, Allegro/OrCAD for enterprise high-speed design.
JLCPCB's PCB Layout Service accepts schematics from EasyEDA, KiCad 8/9/10, Altium, Allegro, OrCAD and PADS. You get a free review and quote in about 3 hours; engineers handle placement, routing and DRC/DFM, delivering source files, Gerber, BOM and CPL in as fast as 3 working days. Schematic design itself is not included.
3. What are Gerber files and why do I need them?
Gerber (RS-274X) is the universal manufacturing format, with one file per layer — copper, solder mask, silkscreen, board outline — plus a separate Excellon drill file. Fabricators cannot open native CAD files, so Gerber data is what actually drives production. It is tool-independent and freezes the design exactly as approved, removing ambiguity over layers and silkscreen. Export Gerber and drill together, zip them for JLCPCB, and check them in a Gerber viewer first — a missing drill file is a common cause of delays.
Conclusion:PCB Layout Design
PCB layout design is a critical skill that directly affects the performance, reliability, and cost of an electronic device. By following best practices such as optimizing component placement, maintaining signal integrity, and ensuring proper thermal management you can create a PCB layout that meets both technical and manufacturing requirements. Investing time in the design phase will pay off with better-performing, more reliable devices in the long run.
Whether you’re a novice or an experienced designer, understanding the nuances of PCB layout design is essential for creating high-quality electronics. With the right tools and techniques, JLCPCB PCB Layout Service can help you overcome design challenges and produce efficient, cost-effective circuit boards.
Also read: https://jlcpcb.com/blog/pcb-design-rules-and-guidelines-a-complete-best-practices-guide
Keep Learning
Multilayer PCB Design Guidelines: Stack-up and Layout Best Practices
Key Takeaways Stack-up is the foundation: The layer arrangement defines signal integrity, impedance control, and EMI performance — plan it before routing a single trace. Symmetric, reference-heavy designs prevent failures: A balanced stack-up with ground planes adjacent to every signal layer avoids warpage, ensures return path continuity, and minimizes crosstalk. DFM rules ensure manufacturability: Aspect ratio, annular rings, material selection, and symmetric copper distribution are critical to produ......
How to Reduce Noise and EMI in PCB Layout: A Comprehensive Design Guide
Key Takeaways EMI origins: EMI stems from structural layout deficiencies — poor return paths, interrupted reference planes, and large loop areas create antenna structures that radiate unwanted energy. Loop area is critical: Minimizing current loop areas through solid ground planes adjacent to signal layers is the single most effective EMI reduction technique. Placement defines noise: Component placement establishes current loops before routing. Group by function (power, analog, digital, RF), isolate a......
What is the Difference Between PCB Design and Layout?
The difference between PCB design and PCB layout trips up more engineers than you’d expect. While often used interchangeably, these are distinct disciplines. The gap between them is where many projects quietly go sideways. Simply put, PCB design is the logical foundation, while PCB layout is the physical implementation. A flawless schematic can fail in production due to poor layout, and even the best layout engineer can’t rescue it. Below, we provide a detailed breakdown of the differences between the......
How PCB Layout Design Services Improve Circuit Board Performance?
Here is a myth that costs hardware teams money: if the schematic is correct, the board will work correctly. In truth, the schematic will take you halfway. The physical layout is what makes a product really work. PCB layouts transform a circuit diagram into something that you can build and ship. It controls signal integrity, thermal behavior, EMI, and assembly yield simultaneously. With the increased speed and density of designs, it has become a discipline by itself. But not every engineering team can ......
Mastering PCB Design: A Step-by-Step PCB Layout Process Guide
Key Takeaways Process over improvisation: A repeatable, standardized PCB layout process—not luck—is what turns a working schematic into a board that succeeds on the first spin. Placement drives everything: Component layout and functional block partitioning are the most impactful steps; good placement makes routing easy, poor placement makes it impossible. Route critical signals manually first: Clocks, differential pairs, sensitive analog nets, and power switching loops must be hand-routed before auto-......
BGA PCB Design Complete Guide: Layout and Routing Guidelines
Key Takeaways Define pad type first: Always confirm SMD or NSMD pad strategy before routing BGA fanout. NSMD is generally preferred for better solder joint formation, while SMD suits very small pads or tight mask registration. Match the process to the pitch: 0.8 mm BGAs work with dog-bone fanout and standard vias; 0.5 mm BGAs typically need via-in-pad or HDI routing. Picking the right via strategy early saves layers and cost. Place decoupling capacitors on the bottom side: Mount MLCCs directly under t......