Introduction to FPGA Architecture: How FPGAs Work and Why They Matter
6 min
- 1. Configurable Logic Blocks (CLBs):
- 2. Interconnect / Routing Fabric
- 3. I/O Blocks (IOBs)
- 4. DSP Slices (Digital Signal Processing Units)
- 5. Block RAM (BRAM)
- 6. Clock Management Blocks
- 7. Hard IP Cores
- 8. Configuration Memory
- Putting It All Together:
Digital circuits implementation is done using ASIC or gate array-based ICs. But there is one more programmable logic functional IC which can implement any logic just by programming; these are known as PLDs (programmable logic devices). There are a lot of them available, but our main focus today is on Field-Programmable Gate Arrays (FPGAs). Unlike fixed-function integrated circuits (ICs), FPGAs allow engineers to reconfigure the hardware itself after manufacturing. Now using one FPGA, I can realize many different circuits from signal processing to machine learning and embedded. But what exactly is inside an FPGA, and how is it different from other ICs on the globe? To answer this, we have to look at the internal architecture of FPGAs. This guide is all about key components of FPGA architecture, the building blocks that make it possible to implement custom digital systems.
1. Configurable Logic Blocks (CLBs):
At the heart of every FPGA are Configurable Logic Blocks (CLBs). These are the fundamental units where digital logic is implemented. Inside a CLB, there is:
- Lookup Tables (LUTs): These are the small memory structures that are used to implement logic functions. A 4-input LUT can represent any truth table with 4 inputs.
- Flip-Flops/Registers: Flops are used for storing single-bit data and creating sequential circuits.
- Multiplexers: Route signals within the CLB; they are used to select one from the different LUT inputs.
Each CLB can be configured to perform basic logic operations (AND, OR, and XOR). Almost all complex combinational and sequential functions can be implemented here. By combining thousands of CLBs, designers can build custom digital circuits like adders, multiplexers, and counters.
2. Interconnect / Routing Fabric
An FPGA would be useless if CLBs were isolated. The interconnect fabric connects CLBs, I/O blocks, memory, and other components. There are programmable switches and wiring channels also along with programmable logic (CLB). These interconnects are also programmed in the code, which connects the different blocks inside, and all this is controlled with the help of a bit stream file. The flexibility of the interconnect is what makes FPGAs so powerful. It’s like the highway system inside the chip, dynamically re-routed depending on the design.
3. I/O Blocks (IOBs)
Since FPGAs sit on a PCB and must communicate with the outside world, I/O Blocks (IOBs) handle this task. These are the cells that are used to send the computed data to external devices and also take the data from sensors. Each I/O block is programmable and supports multiple voltage standards (e.g., LVCMOS, LVTTL, LVDS). These input output blocks are differentiated on the basis of drive strength, slew rate, and pull-up/pull-down resistors. Some modern FPGAs also have the function of high-speed transceivers for PCIe or Ethernet. IOBs make FPGAs highly flexible in mixed environments, allowing them to interface with legacy systems.
4. DSP Slices (Digital Signal Processing Units)
Modern FPGAs include dedicated DSP slices to accelerate arithmetic-intensive operations. It includes multiply-accumulate (MAC) units for fast arithmetic. An FPGA with DSP capabilities has fixed-point and floating-point operations.
Instead of using LUTs (which are slower and less efficient), DSP blocks are hardwired silicon designed for speed. For example, in audio or video processing pipelines, DSP blocks handle filtering and transformation at high speed.
5. Block RAM (BRAM)
Another essential feature is on-chip memory, commonly known as Block RAM (BRAM). It is distributed across the FPGA fabric. And can be configured as a single-port or dual-port memory. It sizes from a few kilobytes to several megabytes, depending on the FPGA family. And very useful for buffering data, storing lookup tables, or implementing FIFOs. For applications such as image buffering, protocol handling, or digital filters, BRAM provides low-latency memory much closer to the logic compared to external DRAM.
6. Clock Management Blocks
To ensure everything inside the FPGA operates synchronously, clock management is critical. That's why the FPGA has an onboard clock management circuit consisting of phase lock loops(PLLs) for frequency stability. Mixed-Mode Clock Managers (MMCMs) for frequency division and multiplication. And a proper clock distribution network for minimal skew. FPGAs often require multiple clocks for different subsystems (one clock for the CPU core, another for high-speed I/O). Clock management blocks made all this possible.
7. Hard IP Cores
While most FPGA resources are reconfigurable, modern FPGAs also integrate Hard Intellectual Property (Hard IP) cores. These are fixed-function blocks optimized for common tasks.
Examples of Hard IP:
- High-speed transceivers (SerDes).
- DDR memory controllers.
- PCI Express interfaces.
- Ethernet MACs.
- Cryptographic engines.
Instead of implementing these functions in LUTs (which would consume too many resources), hard IP cores deliver better performance and lower power because they are fully optimized. These are widely implemented in digital design, for example, to take the data out of a sensor digitally, we need I2C, UART, or SPI, and in the FPGA these are available as IPs.
8. Configuration Memory
Finally, what makes an FPGA field-programmable is its configuration memory. Most FPGAs use SRAM-based configuration. At power-up, the FPGA is blank and must load a bitstream from external flash or a host processor. The bitstream defines:
- CLB functionality.
- Routing paths.
- I/O configurations.
- DSP/BRAM usage.
Putting It All Together:
Let’s summarize the FPGA architecture components:
- CLBs → Programmable logic functions.
- Interconnect Fabric → Wiring highways.
- IOBs → External communication.
- DSP Blocks → High-speed math units.
- BRAM → Local memory.
- Clock Managers → Stable, synchronized timing.
- Hard IP Cores → Fixed-function accelerators.
- Configuration Memory → Defines everything.
With these building blocks, engineers can implement anything from simple counters to entire CPUs and AI accelerators, all on the same FPGA chip.
Conclusion:
FPGAs are not only used in VLSI, but they also play a very important role in DSP and power IC design. You can make any type of controller inside an FPGA due to the fact that they stand out because of their reconfigurability and parallelism. FPGAs allow designers to build custom hardware architectures; on the other hand, microcontrollers are limited to sequential instruction processing. For beginners, understanding FPGA architecture starts with the eight above-listed components. Each plays a unique role, and together, they form a flexible digital playground for engineers. FPGAs are used to bridge the gap between prototyping flexibility and ASIC-level performance.
Keep Learning
6-Layer PCB Stackup and Buildup Guidelines
Printed Circuit Boards (PCBs) are the backbone of modern electronics, providing the necessary infrastructure for connecting and supporting various electronic components. As electronic devices become more complex and compact, the demand for multi-layer PCBs has increased. Among these, the 6-layer PCB is a popular choice for many applications. This article will delve into the specifics of 6-layer PCB stackup, its applications, optimal configurations, and guidelines for selecting the best manufacturer. W......
Designing Antennas on PCB: A Beginner to Advance Guide
In today’s world of widespread wireless connectivity, the demand for small, affordable, and reliable antennas is higher than ever. Antennas act as real-world implementations of electromagnetic wave principles. They enable the sending and receiving of signals for a variety of wireless uses. While there is a lot of theoretical and experimental research in this area, only a few designs become widely used in actual products. Among the different options, Printed Circuit Board (PCB) antennas have become a p......
Understanding Multilayer PCB Stackup
Key Takeaways Layer Arrangement: Optimize signal, ground, and power layer placement for better performance. Material Selection: Choose suitable core, prepreg, and copper materials. Signal Integrity: Control impedance and minimize crosstalk and EMI. Stackup Design: Use symmetrical structures to reduce warpage risks. Manufacturability: Consider layer count, via structures, and manufacturing limits early in design. Performance & Cost: Balance electrical requirements, reliability, and production costs. In......
PCB Antenna Design: Types, Principles, and Best Practices
In the world surrounded with wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. Antennas are the application of electromagnetic waves. There are many theories and practicals available on antennas, but only few of them get recognised. For wireless data transfer the one solution can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating t......
Effective Escape Routing Strategies for High-Density BGA Success
Key Takeaways Escape routing is essential for successfully fanning out high-density BGAs, especially at 0.5 mm pitch and below. Use dogbone fanout for ≥0.5 mm; switch to via-in-pad (filled & capped) for finer pitches. HDI microvias and stacked vias significantly improve routing density and reduce layer count. Maintain symmetry and short stubs for differential pairs to preserve signal integrity. Combine smart stackup, DFM checks, and capable fabrication for reliable, high-yield results. Ever put a 484-......
ESP32 BLE Guide: Choosing the Right Chip and Designing Your PCB
Key Takeaways ESP32 BLE support: Most ESP32 chips support Bluetooth Low Energy (BLE), except the ESP32-S2, which supports only Wi-Fi, and the ESP32-P4, which has no built-in wireless radio. The original ESP32 also supports Bluetooth Classic, while newer models offer Bluetooth 5 features. Wi-Fi and BLE coexistence: Wi-Fi and BLE share the same 2.4 GHz radio and take turns using it. Heavy Wi-Fi activity can reduce BLE throughput or interrupt scanning, so both functions need to be tested together. Power ......