Understanding FPGA: An In-Depth Guide
4 min
- What is an FPGA?
- Why Do We Need an FPGA?
- Inner Structure of an FPGA:
- How Logic is Made Inside an FPGA:
- Working and Programming Basics of FPGA:
- What Type of Circuits Can Be Programmed in an FPGA?
- Is Arduino an FPGA?
- Conclusion:
When I was a young electronics engineer I was very curious to know about FPGAs, Field-Programmable Gate Arrays (FPGAs) are a class of semiconductor devices designed to be configured by a user after manufacturing. They contain a sea of gates inside, which can be programmed by the user to depict a chip behavior without fabricating an actual one. Unlike traditional microcontrollers or processors, FPGAs offer unparalleled flexibility in implementing custom hardware logic. This article explores FPGA fundamentals, applications, advantages, structure, working principles, and programming basics.
What is an FPGA?
An FPGA (Field-Programmable Gate Array) is an integrated circuit (IC) that can be programmed and reprogrammed to execute specific hardware-level tasks. Unlike ASICs (Application-Specific Integrated Circuits), which are custom-built for a single application, FPGAs provide versatility by allowing users to define and modify the logic configuration. The main advantage of an FPGA is that we can change the programming logic and check the functionality of different chips, which gives a lot of flexibility. If we can test the logic in hand without fabricating an actual chip, any logical error can be removed on the hardware ground which can save a lot of time, effort and money.
Why Do We Need an FPGA?
- Hardware Flexibility: Custom digital circuits are required for specialized tasks.
- Parallel Processing: High-speed operations need simultaneous computations.
- Rapid Prototyping: Hardware designers need a platform to test and validate before committing to an ASIC.
- Low-Latency Processing: Tasks demand real-time performance without software overhead.
- Reconfigurability: Systems require updates or modifications without redesigning hardware.
Inner Structure of an FPGA:
An FPGA consists of the following key components:
- Configurable Logic Blocks (CLBs): These contain logic elements like Look-Up Tables (LUTs), flip-flops, and multiplexers that execute digital logic.
- Interconnects: Programmable routing paths that link different logic blocks.
- Input/Output Blocks (IOBs): Provide interfaces to external devices.
- Clocking Resources: Dedicated circuits for clock signal distribution.
- Memory Blocks: RAM and register arrays for temporary data storage.
- Digital Signal Processing (DSP) Blocks: Specialized units for mathematical operations.
How Logic is Made Inside an FPGA:
The logic inside an FPGA is implemented using Look-Up Tables (LUTs), which store predefined truth tables for combinational logic. For example simple logic gates, adders, subtractors and multipliers. Flip-flops and multiplexers help in sequential logic implementation. The entire circuit is configured using a Hardware Description Language (HDL) such as VHDL or Verilog. Usually these hardware descriptive languages use a newer version of C programming with some additional logic and syntax. Overall now a hardware circuit can be made using a Verilog code through a software like Vivado.
Working and Programming Basics of FPGA:
1. Design Entry:
The design may contain a few hundreds to thousands of active logic gates and a multiplexer circuit inside a FPGA. Users can define logic using HDL (Verilog/VHDL) or schematic-based design is an alternative method.
2. Synthesis & Implementation
In this step a physical gate level circuit is made inside the software through the written program. And verification is done with respect to all input/outputs.
- Converts the HDL code into a netlist (logic gates & connections).
- The netlist is mapped to FPGA resources.
3. Bitstream Generation
The compiled design is converted into a bitstream file that configures the FPGA. It is the same as the hex file, used to program microcontrollers but this time with FPGA logical code language.
4. Programming the FPGA
- The bitstream is loaded onto the FPGA using a JTAG programmer.
What Type of Circuits Can Be Programmed in an FPGA?
FPGAs are used in a wide range of applications, including:
- Digital Signal Processing (DSP): Image processing, audio filtering.
- Embedded Systems: Custom processors, real-time control.
- Cryptography: High-speed encryption algorithms.
- Networking: Packet processing, network switching.
- AI & Machine Learning: Accelerators for neural networks.
- Industrial Automation: PLCs and real-time monitoring systems.
Is Arduino an FPGA?
No, Arduino is not an FPGA. The differences are outlined below:
While both can be used for embedded systems, FPGAs allow hardware-level customizations, whereas Arduino runs software on a fixed microcontroller. To power these things, we need a smps power supply. In usual we use switched mode type supplies if not designed keeping layout consideration in mind it will add noise to the system, see our detailed layout design guide on switch mode power supplies.
Conclusion:
FPGAs are powerful, flexible hardware platforms used in applications requiring high performance, real-time processing, and reconfigurability. Unlike ASICs, they allow design modifications post-manufacturing, making them ideal for prototyping and specialized tasks. Although more complex than microcontrollers like Arduino, FPGAs offer unmatched control over hardware design, making them a crucial tool in modern electronics.
Keep Learning
Signal Integrity and Jitter Analysis Using Eye Diagrams
The way a signal travels across a wire varies depending on the transmitter and receiver. This is where methods for error identification and correction are useful. However, how can we tell if a signal is different? It goes without saying that we need to use a device to track at both TX-RX ends and view the data bit by bit. And why is the signal shifting, and is it possible to stop the cause? Yes, it is somewhat feasible, but there is little we can do to protect a wireless channel from noise. Due to EMI......
The Benefits of Coplanar Waveguide in High-Frequency PCB Design
Key Takeaways Coplanar waveguide (especially GCPW) improves high-frequency PCB performance by keeping the return path close and confining fields, which boosts signal integrity and reduces EMI/radiation. It also gives more impedance/layout flexibility (tuning both trace width and gap), but demands tighter manufacturing control of gap tolerances, copper roughness, and material Dk/Df—so field-solver impedance design and DFM checks are essential, with low-loss laminates preferred at higher GHz. Have you e......
6-Layer PCB Stackup and Buildup Guidelines
Printed Circuit Boards (PCBs) are the backbone of modern electronics, providing the necessary infrastructure for connecting and supporting various electronic components. As electronic devices become more complex and compact, the demand for multi-layer PCBs has increased. Among these, the 6-layer PCB is a popular choice for many applications. This article will delve into the specifics of 6-layer PCB stackup, its applications, optimal configurations, and guidelines for selecting the best manufacturer. W......
Designing Antennas on PCB: A Beginner to Advance Guide
In today’s world of widespread wireless connectivity, the demand for small, affordable, and reliable antennas is higher than ever. Antennas act as real-world implementations of electromagnetic wave principles. They enable the sending and receiving of signals for a variety of wireless uses. While there is a lot of theoretical and experimental research in this area, only a few designs become widely used in actual products. Among the different options, Printed Circuit Board (PCB) antennas have become a p......
Understanding Multilayer PCB Stackup
Key Takeaways Layer Arrangement: Optimize signal, ground, and power layer placement for better performance. Material Selection: Choose suitable core, prepreg, and copper materials. Signal Integrity: Control impedance and minimize crosstalk and EMI. Stackup Design: Use symmetrical structures to reduce warpage risks. Manufacturability: Consider layer count, via structures, and manufacturing limits early in design. Performance & Cost: Balance electrical requirements, reliability, and production costs. In......
PCB Antenna Design: Types, Principles, and Best Practices
In the world surrounded with wireless communication, the demand for compact, inexpensive and reliable antennas has never been higher. Antennas are the application of electromagnetic waves. There are many theories and practicals available on antennas, but only few of them get recognised. For wireless data transfer the one solution can be usage of Printed Circuit Board (PCB) antennas. Using PCB antennas represents a convenient solution for integrating them directly into electronic devices, eliminating t......